powered by CADENAS

Social Share

Window cleaner (3637 views - Tooling)

Window cleaning, or window washing, is the cleaning of architectural glass used for structural, lighting, or decorative purposes. It can be done manually, using a variety of tools for cleaning and access. Technology is also employed and increasingly, automation. Commercial work is contracted variously from in-person transactions for cash or barter, to formal tender processes. Regulations, licensing, technique, equipment and compensation vary nationally and regionally.
Go to Article

Explanation by Hotspot Model

Window cleaner

Window cleaner

Window cleaning, or window washing, is the cleaning of architectural glass used for structural, lighting, or decorative purposes. It can be done manually, using a variety of tools for cleaning and access. Technology is also employed and increasingly, automation.

Commercial work is contracted variously from in-person transactions for cash or barter, to formal tender processes. Regulations, licensing, technique, equipment and compensation vary nationally and regionally.

Tools

Chamois & scrim

Chamois is a basic method used to loosen and remove dirt, followed by a buffing with cheesecloth, or scrim.

Water & squeegee

Generally, chemicals are added to water, and a device such as a brush or cloth-covered handle is dipped into the resulting solution and used to scrub glass. A squeegee is then used to sluice the dirt and water mixture from the glass.

Chemicals added to the solution range from dish soap and glass cleaner to Trisodium Phosphate and etching salt. In sub-freezing temperatures, anti-freezing chemicals are added to the solution to prevent it from crystallizing on the pane before it is sluiced off.

Water-fed poles

Any of a variety of types of telescopic poles, fitted at the upper end with a brush and water jets, fed either from vehicle-borne tanks of deionised water or by on-site production of deionised water using a domestic or commercial water outlet. The water is filtered by either a two-stage or three-stage filtration process, involving a carbon filter, and two de-ionization filters, or a carbon filter, a reverse osmosis membrane filter, and a de-ionization resin filter. The filtered water contains a TDS (total dissolved solids) of less than 5 ppm. (parts per million.) The brush is used to agitate the debris off the window, while spraying water, and then the brush is lifted a few inches from the glass to rinse the glass with the pure water jets. Fan jets are used for hydrophobic glass, and "pencil" jets are used for hydrophilic glass. The de-ionized water is lacking in ions, so it will pull solids off the glass and dissolve the solids into the water, aiding in the cleaning process. Because there are no solids dissolved in the water, the windows dry clear without water spots. Water-fed poles vary in length. The longest poles are about 70 feet, and can reach up to six storeys. Water-fed cleaning is also referred to as pure water cleaning. It is common in the UK and becoming common in the US.

Access

A scissor lift aerial work platform is being used to access high windows.

Where glass is found are window cleaners, and methods of access and equipment related to both access and cleaning vary nationally and regionally. If a window is not easily accessible using one type of equipment then it is advisable to combine different tools to be able to clean it properly.

Ladders

Ladders ranging in size from a single step to the extent (and beyond) of local regulations are used to access windows for cleaning purposes.

Supported scaffolding

Not to be confused with suspended scaffolding, these are temporary work platforms typically erected from a lower level to gain access at height.

Aerial work platforms

Aerial work platforms are variously configured and powered machines, designed to deliver workers to otherwise inaccessible areas. An example of one of these machines is the scissor lift, as it is known in Australia, along with cherry pickers and spiders.

Suspended platform or cradle

An extreme window cleaning scenario with intense height and a very deep sloping overhang.

Not to be confused with supported scaffolding. Devices designed for ascent and/or descent via wire rope by mechanical or manual means.

  • Boatswain's chair (bosun's chair): A boatswain's chair is a single-person seat designed for controlled descent of rope. Often referred to as "rope descent systems" (RDS), these are typically anchored to a roof structure, counterweight configuration, or connecting points designed for the purpose. Note: These are always temporarily installed for the purpose of access. However, their anchor points can be either temporary or permanent.
  • Suspended platform: An access platform for one or more workers with manual or motor driven devices for raising and lowering via rope. Platforms may be fitted to high rise buildings or skyscrapers, or assembled from components to suit architecture and nature of work being performed. Note: These can be either temporary or permanent. Both having their own unique governing codes and regulations. Permanent suspended platforms are often known as building maintenance units (BMU) and their platforms are also known as gondolas in Europe.

Windowsill access

Direct access to a window obtained by egress from that window. This method is still used at the Empire State Building in New York City.[1][not in citation given]

High rise window cleaning

Windows that needed cleaning became higher as buildings became higher. A trade in window cleaning developed, for instance, in New York City in the late 19th century when early skyscrapers were being built. The height increased the risk to the washers. At first, washers cleaned skyscraper windows by standing on the window ledge and holding onto the frame. Later, leather safety belts attached to anchor bolts were introduced and then scaffolds. For example, the Otis Elevator Company built an electrically operated scaffold for use at Lever House.[2]

Three window cleaners were working at the World Trade Center at the time of the September 11 attacks. Jan Demczur, working in the North Tower, survived and helped save five other people who had been trapped in an elevator with him. Roko Camaj and Fabian Soto, working in the South Tower, were killed.[2]

Hazards of the trade

Risks include slipping on water or soap, and falling from heights. In 1932 in New York, an average of one out of every two hundred window cleaners was killed per year.[2] On May 29, 1962, four window cleaners were killed when a scaffold fell at the Equitable Life Building.[2][3][4] In 1993 Local 32BJ, the New York window cleaners' union, launched an apprentice training program, increasing job safety among its members, although increasing numbers of New York window cleaners are non-unionized.[2]

Unlike in Scotland, there is no government licensing in the United States, England or Wales - this means anyone can claim to be a window cleaner. Window cleaning is considered the most dangerous job in the UK.[5] Several window cleaners die each year, and many are injured.[6]

Many window cleaning businesses are claiming that laws are about to come into force due to European Directive 2001/45/EC that will make ladders illegal for window cleaners. However, the government denies this stipulation, as ladder use for window cleaning is "low risk and short duration":[7]

To clarify the situation HSE is not attempting to ban ladders or stepladders, but ladders should not be the automatic first choice of access. They should only be used after a suitable assessment of the alternatives and the prevailing site conditions. The selection process for access equipment is coming under increasing scrutiny at HSE inspections. This guidance clarifies that for short duration work like window cleaning, provided a number of well-recognised precautions are taken, ladders will remain a common tool for many jobs.[6]

The Working at Height Regulations came into force in 2005 and does not ban ladders[7] but merely restricts their use to safe methods, i.e. foot it by person or with a ladderstopper:

4.2.2. The feet of portable ladders must be prevented from slipping during use by securing the stiles at or near their upper or lower ends, by any anti-slip device or by any other arrangement of equivalent effectiveness. Ladders used for access must be long enough to protrude sufficiently beyond the access platform, unless other measures have been taken to ensure a firm handhold. Interlocking ladders and extension ladders must be used so that the different sections are prevented from moving relative to one another. Mobile ladders must be prevented from moving before they are stepped on.[8][9]

The HSE favours the use of scaffold towers, i.e. temporary workstations, for window cleaning but acknowledges this is rather awkward:

"For some jobs, a mobile elevating work platform will be the best option. However, for many jobs, especially on domestic and small commercial buildings, risk assessment will demonstrate that because of the short duration of the work and features on the building that cannot be altered, ladders are the only realistic option."[10]

Although WFP systems are hailed as safer than ladders, the Health and Safety Executive acknowledges[10] that such systems spill large amounts of water which either the window cleaner or their client could slip on.

Ecology and water shortages

Another issue is how "green" window cleaning companies are seen to be. During the spring of 2006 Defra considered banning the non-essential use of water and extending their already tight restrictions to prevent the use of water-fed safer which reach up to 60 ft. Window cleaners could return to the bucket-and-mop method, because Health and Safety Working at Heights allows such for temporary access.[7] Many window cleaners and window cleaning companies argue that their usage of water is minimal in comparison with water usages of large industry and energy companies, and that their water usage accounts for a small percentage of overall water consumption in developed countries.[11] [12]

Technological progress and decline in labor requirements

Much progress has been made in the area of minimizing the need for labor in this industry by use of technology. The availability of technology such as the pressure washer has made it more efficient. More recently, in high tech societies the use of fully automated robotic window cleaners is starting to become common.[13]

Cultural references

Windows cleaning and window cleaners are the subject of songs, films and comment, often with comic intent. Examples include George Formby's comic song "The Window Cleaner", also known as "When I'm Cleaning Windows" is one of the best known. Films about window cleaners include The Window Cleaner (1968)[14] and Confessions of a Window Cleaner (1978).[15] Journalists sometimes comment on the peculiarities of the trade.[16]

Images

See also



This article uses material from the Wikipedia article "Window cleaner", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing