Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Torso | |
---|---|
Human male torso | |
Details | |
Identifiers | |
Latin | truncus |
TA | A01.1.00.013 |
FMA | 7181 |
Anatomical terminology |
The torso or trunk is an anatomical term for the central part of the many animal bodies (including that of the human) from which extend the neck and limbs.[1] The torso includes the thorax and the abdomen.
Most critical organs are housed within the torso. In the upper chest, the heart and lungs are protected by the rib cage, and the abdomen contains most of the organs responsible for digestion: the stomach, which breaks down partially digested food via gastric acid; the liver, which respectively produces bile necessary for digestion; the large and small intestines, which extract nutrients from food; the anus, from which fecal wastes are egested; the rectum, which stores feces; the gallbladder, which stores and concentrates bile; the kidneys, which produce urine, the ureters, which pass it to the bladder for storage; and the urethra, which excretes urine and in a male passes sperm through the seminal vesicles. Finally, the pelvic region houses both the male and female reproductive organs.
The torso also harbours many of the main groups of muscles in the body, including the:
The organs, muscles, and other contents of the torso are supplied by nerves, which mainly originate as nerve roots from the thoracic and lumbar parts of the spinal cord. Some organs also receive a nerve supply from the vagus nerve. The sensation to the skin is provided by:
Wikimedia Commons has media related to Torsos. |
This article uses material from the Wikipedia article "Torso", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D