powered by CADENAS

Social Share

Bar stool (7517 views - Interior Design)

Bar stools are a type of tall chair, often with a foot rest to support the feet. The height and narrowness of bar stools makes them suitable for use at bars and high tables in pubs or bars. In the 2010s, bar stools are becoming more popular in homes, usually placed at the kitchen counter, kitchen island, or a home bar. Bar stools are becoming more popular in homes because they are available in varied styles. Bar stools also allow for a higher view when eating, drinking, or socializing.
Go to Article

Explanation by Hotspot Model

Bar stool

Bar stool

Bar stool

Licensed under Creative Commons Attribution-Share Alike 4.0 (Frank C. Müller).

Bar stools are a type of tall chair, often with a foot rest to support the feet. The height and narrowness of bar stools makes them suitable for use at bars and high tables in pubs or bars. In the 2010s, bar stools are becoming more popular in homes, usually placed at the kitchen counter, kitchen island, or a home bar.[citation needed] Bar stools are becoming more popular in homes because they are available in varied styles. Bar stools also allow for a higher view when eating, drinking, or socializing.

Types

There are many different types of construction materials and models. Bar stools are often made of wood or metal. Bar stools are made with and without armrests, backs, and padding or upholstery on the seat surface. Bar stools can range from basic wooden designs to more complex ones with adjustable height. Extra tall and extra short are common features, as well as indoor bar stools and outdoor bar stools. In commercial settings, swivel and floor mounted bar stools are common. Floor mounting renders the stool immovable, so it cannot be stolen or used as a weapon in a bar fight. Floor-mounted stools are generally mounted on a column, but stools with legs can also be secured to the floor using metal brackets.

The normal seat height for a bar stool is 30 in (76 cm) with a 26 in (66 cm) stool being used against kitchen counters. Extra tall 36 in (91 cm) stools are increasingly used in contemporary styles with high pub tables to create a visual effect in modern interiors. Counter height bar stools have a seat height of 24" (61cm). By comparison a conventional dining chair seat height is 18 in (46 cm). Some bar stools use polyurethane foam as comfortable padding.[citation needed]. Bar stools can be made from rattan or bamboo; these stools can be used to create a tiki bar effect. A popular style in bars and restaurants is a retro 1950 and 1960s look[citation needed] which use chrome and vinyl stools combined with matching benches or diner chairs. Stacking stools are often favored for their space-saving qualities. Some establishments use matching bar stools and chairs.

Aluminum is often used outdoors. Stacking aluminum stools and patio chairs are used by commercial premises. Indoors, wood and upholstery are popular in traditional settings. Bar stools are used in pool or billiard halls and the style of chair customized for such use is often called a "spectator chair". Bar stools are used in Ireland during weekends by followers of the English Premier League, a practice which led to the creation of the pejorative term "barstoolers" by supporters of the League of Ireland. Bar stools are a growth area in the consumer market and online purchasing is on the increase[citation needed]. Bar stools can be made to order and customers can specify a wide range of fabrics and finishes as well as specifying other options such as height and custom foot rests. Both wooden and metal bar stools, including stainless and chrome styles and adjustable height features are popular.[citation needed]



This article uses material from the Wikipedia article "Bar stool", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art