Licensed under Creative Commons Attribution-Share Alike 3.0 (No machine-readable author provided. David.Monniaux assumed (based on copyright claims).).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (April 2013) (Learn how and when to remove this template message) |
A billiard table, billiards table, or pool table is a bounded table on which billiards-type games (cue sports) are played. In the modern era, all billiards tables (whether for carom billiards, pool or snooker) provide a flat surface usually made of quarried slate, that is covered with cloth (usually of a tightly-woven worsted wool called baize), and surrounded by vulcanized rubber cushions, with the whole elevated above the floor.[1]:115, 238 More specific terms are used for specific sports, such as snooker table and pool table, and different-sized billiard balls are used on these table types. An obsolete term is billiard board, used in the 16th and 17th centuries.[1]:27[2]
This section needs expansion with: subsections on rails, frame, etc.. You can help by adding to it. (August 2007) |
Cushions (also sometimes called "rail cushions", "cushion rubber", or rarely "bumpers") are located on the inner sides of a table's wooden rails. There are several different materials and design philosophies associated with cushion rubber. The cushions are made from an elastic material such as vulcanized (gum or synthetic) rubber. The chiefly American jargon "rails" more properly applies to the wooded outer segments of the table to which the cushions are affixed.
The purpose of the cushion rubber is to cause the billiard balls to rebound off the rubber while minimizing the loss of kinetic energy.
When installed properly the distance from the nose of the cushion to the covered slate surface is 1 7⁄16"[3] while using a regulation 2 1⁄4" ball set.
The profile of the rail cushion, which is the cushion's angle in relation to the bed of the table, varies between table types. The standard on American pool tables is the K-66 profile, which as defined by the BCA has a base of 1 3⁄16 inches and a nose height of 1 inch.[4] This[clarification needed] causes the balls' rebound to be somewhat predictable during game play.
On a carom table, the K-55 profile is used (with a somewhat sharper angle than pool cushions). K-55 cushions have cloth, usually canvas, vulcanized into the top of the rubber to adjust rebound accuracy and speed.[4]
Finally, snooker tables may use an L-shaped profile, such as the L77 profile. This is mostly[clarification needed] because snooker uses balls of a smaller diameter and smaller pocket entrances than pool does.
The bed – the cloth-covered horizontal playing surface – is, on good-quality equipment, made of solid, finely ground slabs of slate, most often from Italy, Brazil or China. Small pool tables may use only one or two pieces of slate, while carom, English billiards and tournament-size pool tables use three. Full-size snooker tables require five. The gap between slates is filled with a hard-drying putty, epoxy or resin, then sanded to produce a seamless surface, before being covered with the cloth. When several pieces of slate are joined poorly it is possible for the resin to deform and cause an uneven playing surface; it can also be difficult to move once joined.
Tables for the home market usually use slate beds as well, but the slate is often thinner, down to about 1⁄2 inch (13 mm). The early table beds were made of cloth-covered wooden boards. Today, inexpensive but not very rigid or durable materials used for the beds of low-end tables (e.g. for children's recreation rooms) still include wood, especially medium-density fibreboard and plywood, as well as plastics and other synthetic materials under various trade names.
Billiard cloth (sometimes erroneously called felt) is a specific type of cloth that covers the top of the table's "playing area". Both the rails and slate beds are covered with 21–24 ounce billiard cloth (although some less expensive 19oz cloths are available) which is most often green in color (representing the grass of the original lawn games that billiards evolved from), and consists of either a woven wool or wool/nylon blend called baize.
Most bar tables, which get lots of play, use the slower, thicker blended felt because it is cheaper. Worsted cloth is more expensive but lasts longer. This type of cloth is called a woolen cloth. By contrast, high quality pool cloth is usually made of a napless weave such as worsted wool, which gives a much faster roll to the balls. This "speed" of the cloth affects the amounts of swerve and deflection[citation needed] of the balls, among other aspects of game finesse. Snooker cloth traditionally has a directional nap, upon which the balls behave differently when rolling against vs. running with the direction of the nap.
Sights, also known as diamonds (for their traditional shape), are inlaid at precise, evenly spaced positions along the rails of some tables (not usually on snooker tables) to aid in the aiming of bank or kick shots. There are seven along each long rail (with the side pocket interfering with where the seventh one would go, on pocket billiard tables) and three along each short rail, with each of the four corners counting as another in the mathematical systems that the diamonds are used to calculate. These sights divide the playing surface into equal squares. Books, even entire series of books, have been written on geometric and algebraic systems of aiming using the diamonds.
Spots are often used to mark the head and foot spots on the cloth. Other markings may be a line drawn across the head string (or across the balk line with the "D", in British-style pool). Another case is the outline of the triangle rack behind the foot spot where the balls are racked in straight pool, since the outline of this area is strategically important throughout the game. In artistic pool, lines may be drawn between opposite sights putting a grid on the playing surface. Other grid patterns are used in various forms of balkline billiards. A recent table marking convention, in European nine-ball, is the break box.
Pocketless carom billiards tables are used for such games as three-cushion billiards, straight rail, balkline, artistic billiards and cushion caroms.
Regulation 10 × 5 foot carom billiards tables have a playing surface (measured between the noses of the cushions) is 2.84 meters by 1.42 meters (9.32 × 4.65 feet) with a 5 millimeter allowance.[5] The standard height range of the table, measured from the playing surface to the ground is between 75 and 80 centimeters.
The slate bed of a carom billiard table must have a minimum thickness of 45 millimeters and is often heated to about 5 degrees C (9 deg F) above room temperature, which helps to keep moisture out of the cloth to aid the balls rolling and rebounding in a consistent manner, and generally makes a table play faster. A heated table is required under international carom rules and is an especially important requirement for the games of three-cushion billiards and artistic billiards.[1]:115, 238
Heating table beds is an old practice. Queen Victoria had a billiard table that was heated using zinc tubes, although the aim at that time was chiefly to keep the then-used ivory balls from warping. The first use of electric heating was for an 18.2 balkline tournament held in December 1927 between Welker Cochran and Jacob Schaefer, Jr. The New York Times announced it with fanfare: "For the first time in the history of world's championship balkline billiards a heated table will be used..."[1]:115, 238[6]
A pool table, or pocket billiards table (as the sport's governing body prefers to call it), has six pockets – one at each corner of the table (corner pockets) and one at the midpoint of each of the longer sides (side pockets or middle pockets). Historically, as old engravings show, tables sometimes used to be made with only four pockets, but the rest of this section addresses six-pocket pool tables.
Pocket billiard tables come in different sizes, typically referred to as 9-foot (2.7 m), 8.5 ft (2.6 m), 8 ft (2.4 m), or 7 ft (2.1 m) tables. In all cases, the table is rectangular with a 2:1 ratio (e.g. 9 × 4.5 ft).
There are only two sizes approved for tournament play by the International Olympic Committee-recognized sport governing body of pool, the World Pool-Billiard Association (WPA), and its various regional and national affiliates; under the World Standardised Rules of pool, these are the 9 × 4.5 ft and 8 × 4 ft models.[7][8] For a 9-ft table, the playing surface (the dimensions between the noses of the cushions) measures 100 inches (254 cm) by 50 inches (127 cm) with a 1⁄8-inch (3.2 mm) margin of error for either dimension. For an 8-ft table, the playing surface measures 92 inches (234 cm) by 46 inches (117 cm), with the same 1⁄8 inch variance allowed.
In the UK as well as a number of other British Commonwealth and European countries, the typical pool table is a 7-foot model – or even 6 × 3.5 ft (1.83 × 0.91 m) for the pub and home market. These are the sizes used by internationally standardised blackball and the amateur World Eightball Pool Federation, as well as informal pub pool.[9] The 7-foot size is also frequently used in North American amateur leagues, and are common coin-operated fixtures in bars and other venues. The playing surface for a 7-foot table is 76 inches (193 cm) by 38 inches (96.5 cm).
Pockets, usually rimmed at the back with leather or plastic, may have leather mesh or cloth bags or plastic cups, or elongated wire racks, to catch the balls, common in home billiard rooms and pool halls, or in the coin-operated tables found in bars/pubs may instead lead to ball-return troughs inside the table, which channel the balls into a collection chamber on one side of the table (or, in non-coin-op models, on the racking end of the table). A disadvantage to pockets with bags or cups is that if too many balls go into the same pocket, it will fill up the receptacle and prevent any more balls from going in that pocket, requiring that some be moved out of the pocket manually before shooting again.
Regardless of table size, the WPA standard (sometimes informally called "American-style") table has wide, angular pockets that funnel notably inward, generally 1.75 to 2.25 times as wide at the opening as the diameter of the 2 1⁄4-inch (57 mm) balls, wider at the side (middle) pockets than the corners. WEPF pool (sometimes informally called "British-style" or "Commonwealth-style") is played with 2 to 2 1⁄8-in (51–54 mm) balls, and this type of table has smaller, narrow pockets (the width is calculated as the ball diameter multiplied by 1.6, and is consistent at all six pockets), with rounded entrances and nearly parallel sides, like those on a snooker table. One tactical consequence of this design difference is that the jaws of the WPA-type pocket are often used exactly like a horizontal version of the backboard of a basketball goal, to rebound the ball into the pocket; this technique does not work on blackball tables, and even shots down the cushion into a corner pocket are more difficult. The same also holds true of snooker and Russian pyramid tables, with similar "tight" pockets with rounded openings; all require more precise shots than WPA-style pool.
For tournament competition under WPA world-standardized rules (and league play under derived rulesets), the bed of the pocket billiard table must be made of slate no less than 1 inch (2.54 cm) thick. The flatness of the table must be divergent by no greater than 0.02 inches (0.51 mm) lengthwise and 0.01 inches (0.25 mm) across the width.[7]
A table designed for the games snooker and English billiards is usually called a snooker table, although more accurately it is in fact a Billiards table (the baulkline is not used in snooker).
The playing area of a tournament English billiards/snooker table, as standardized by the World Professional Billiards and Snooker Association (WPBSA) and the amateur International Billiards and Snooker Federation (IBSF) which uses WPBSA rules,[10] measures 11 feet 8.5 inches by 5 ft 10 in (356.9 cm by 177.8 cm) with a tolerance of ± 0.5 in (13 mm),[11] though commonly referred to as 12 ft by 6 ft. Smaller tables, approximately 10 ft by 5 ft down to half size, are also sometimes used in pubs, homes and smaller snooker halls. The height from the floor to the top of the cushion is between 2 ft 9.5 in and 2 ft 10.5 in (85.1 cm and 87.6 cm).[11]
A snooker table has six pockets, one at each corner and one at the center of each of the longest side cushions. The pockets are around 86 mm (3.5 in),[clarification needed] though high-class tournaments may use slightly smaller pockets to increase difficulty. The amount of undercut (trimmed underside of the rubber cushion's protruding nose at the pocket opening),[12]:8 if any, has a strong effect on how easily a ball is accepted by the pocket (the "pocket speed"). On snooker and English billiards tables, the pocket entries are rounded, while pool tables have sharp "knuckles". This affects how accurate shots need to be to get into a pocket, and how fast they can be when not dead-on, including shots that run along and against a cushion, making snooker more difficult to play than pool. According to the WPBSA official rule book, "the pocket openings shall conform to the templates owned and authorised by The World Professional Billiards and Snooker Association (WPBSA)".[11] The WPBSA and IBSF rule books' equipment sections do not actually specify the measurements and shapes of these proprietary templates[10][11] which change from time to time, requiring that the templates be dated.[13] The organisations do not recognise tournament play or records (maximum breaks, etc.) if not performed on tables that conform to then-current templates.[13][14]
The cushions (sometimes known as rails, though that term properly applies to the wood sections to which the cushions are attached) are usually made of vulcanized rubber.
The baulk area is marked by a baulk line drawn on the cloth across the width of the table at 29 inches (737 mm) from and parallel to the face of the bottom cushion.[11] A semicircle with a radius of 11.5 inches (292 mm) centered on this line within baulk forms the "D"[11] in which the cue ball must be placed when breaking or after the cue ball has been potted or shot off the table. The position of four of the colours are marked along the long string (lengthwise centre) of the table, perpendicular to the baulk line: the black spot, 12.75 inches (324 mm) from the top cushion; the centre spot or blue spot, located at the midpoint between the bottom and top cushions; the pyramid spot or pink spot, located midway between the centre spot and the top cushion; and the baulk spot or brown spot, located at the midpoint of the baulk line[11] (and, thus of the "D"). Due to its obviousness, the brown spot is not always marked (neither are the unmistakable green and yellow spots,[11] at the left and right intersections, respectively, of the baulk line and the "D"'s curve.[1]:116, 278[11] The exact placing of these markings are different on smaller tables, but proportional to the full-size model.
The playing surface of a good quality snooker table has a bed of slate and is covered with baize cloth, traditionally green, though many other colours are now available. The thickness of this cloth determines the table's speed (lack of friction) and responsiveness to spin, thicker cloths being longer lasting but slower and less responsive. The nap of the cloth can affect the run of the balls, especially on slower shots and shots played with sidespin applied to the cue ball. A snooker table traditionally has the nap running from the baulk to the top end and is brushed and ironed in this direction.
Other types of billiard tables are used for specific games, such as Russian pyramid, Asian four ball. Games such as bagatelle often had more than six holes, including straight through the bed in the middle of the table, a feature still found in bar billiards and bumper pool.
There are novelty billiard tables, often for pool, that come in various shapes including zig-zag, circular, and hexagonal. For the home market, many manufacturers have produced billiard tables (in the broad sense) that double as dining tables or as table tennis or other gaming tables, with removable hard tops.
Russian pyramid ball at a corner pocket. The relative size of the ball and the pocket makes the game very challenging.
An original Ford Mustang converted into a novelty pool table, exhibited at the 2011 Montreal International Auto Show.
Toy billiard tables are also sold in children's toy shops.
Snooker Table Full Specification with standard Size
Pool games | ||
---|---|---|
Carom billiards | ||
Other games | ||
Resources | ||
Major tournaments | ||
Categories | ||
|
This article uses material from the Wikipedia article "Billiard table", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Air sports
• Aerobatics
• Air racing
• Cluster ballooning
• Hopper ballooning
Wingsuit flying
• Gliding
• Hang gliding
• Powered hang glider
• Human powered aircraft
• Model aircraft
• Parachuting
• Banzai skydiving
• BASE jumping
• Skydiving
• Skysurfing
• Wingsuit flying
• Paragliding
• Powered paragliding
• Paramotoring
• Ultralight aviation
Archery
• Field archery
• Flight archery
• Gungdo
• Indoor archery
• Kyūdō
• Popinjay
• Target archery
Ball-over-net games
• Badminton
• Ball badminton
• Biribol
• Bossaball
• Fistball
• Footbag net
• Football tennis
• Footvolley
• Hooverball
• Jianzi
• Padel
• Peteca
• Pickleball
• Platform tennis
• Sepak takraw
• Sipa
• Throwball
• Volleyball
• Beach volleyball
• Water volleyball
• Paralympic volleyball
• Wallyball
• Ringo
Basketball family
• Basketball
• Beach basketball
• Deaf basketball
• Streetball
• Water basketball
• Wheelchair basketball
• Cestoball
• Korfball
• Netball
• Fastnet
• Indoor netball
• Ringball
• Slamball
Bat-and-ball (safe haven)
• Baseball
• Softball
• Slow pitch
• Fast-pitch softball
• 16-inch softball
• Bat and trap
• British baseball – four posts
• Brännboll – four bases
• Corkball – four bases (no base-running)
• Cricket – two creases
• Indoor cricket
• Limited overs cricket
• One Day International
• Test cricket
• Twenty20
• Danish longball
• Kickball
• Kilikiti
• Lapta – two salos (bases)
• The Massachusetts Game – four bases
• Matball
• Oina
• Old cat – variable
• Over-the-line – qv
• Palant
• Pesäpallo – four bases
• Punchball
• Rounders – four bases or posts
• Scrub baseball – four bases (not a team game per se)
• Stickball – variable
• Stool ball – two stools
• Tee-ball
• Town ball – variable
• Vigoro – two wickets
• Wireball
• Wiffleball
Baton twirling
• Baton twirling
Acro sports
• Ballet
• Dancing
• Cheerleading
• Gymnastics
Performance sports
• Drum corps
• Marching band
Board sports
• Skateboarding
• Scootering
• Casterboarding
• Freeboard (skateboard)
• Longboarding
• Streetboarding
• Skysurfing
• Streetluge
• Snowboarding
• Mountainboarding
• Sandboarding
• Snowkiting
• Surfing
• Wakesurfing
• Bodyboarding
• Riverboarding
• Skimboarding
• Windsurfing
• Wakeboarding
• Kneeboarding
• Paddleboarding
Catch games
• Dodgeball
• Ga-ga
• Keep away
• Kin-Ball
• Newcomb ball
• Quidditch
• Rundown (a.k.a. Pickle)
• Yukigassen
Climbing
• Abseiling
• Aid climbing
• Ice climbing
• Mixed climbing
• Mountaineering
• Rock climbing
• Bouldering
• Deep-water soloing
• Sport climbing
• Traditional climbing
• Other
• Canyoning (Canyoneering)
• Coasteering
• Hiking
• Rope climbing
• Pole climbing
Cycling
• Artistic cycling
• BMX
• Cyclo-cross
• Cross-country mountain biking
• Cycle polo
• Cycle speedway
• Downhill mountain biking
• Dirt jumping
• Enduro mountain biking
• Freestyle BMX
• Hardcourt Bike Polo
• Road bicycle racing
• Track cycling
• Underwater cycling
Skibob
• Skibobbing
Unicycle
• Mountain unicycling
• Unicycling
• Unicycle basketball
• Unicycle hockey
• Unicycle trials
Combat sports: wrestling and martial arts
• Aiki-jūjutsu
• Aikido
• Jujutsu
• Judo
• Brazilian jiu-jitsu
• Sambo (martial art)
• Sumo
• Wrestling
• Amateur wrestling
• Greco-Roman wrestling
• Freestyle wrestling
• Folk wrestling
• Boli Khela
• Collar-and-elbow
• Cornish wrestling
• Dumog
• Glima
• Gouren
• Kurash
• Lancashire wrestling
• Catch wrestling
• Malla-yuddha
• Mongolian wrestling
• Pehlwani
• Professional wrestling
• Schwingen
• Shuai jiao
• Ssireum
• Varzesh-e Pahlavani
• Yağlı Güreş
• Greek wrestling
Striking
• Choi Kwang-Do
• Cockfighting
• Boxing
• Bokator
• Capoeira
• Fujian White Crane
• Karate
• Kenpō
• Kickboxing
• Lethwei
• Muay Thai
• Pradal serey
• Sanshou
• Savate
• Shaolin Kung Fu
• Sikaran
• Silat
• Subak
• Taekkyeon
• Taekwondo
• Taidō
• Tang Soo Do
• Wing Chun
• Zui quan
Mixed or hybrid
• Baguazhang
• Bando
• Bartitsu
• Bujinkan
• Hapkido
• Hwa Rang Do
• Jeet Kune Do
• Kajukenbo
• Kalaripayattu
• Krav Maga
• Kuk Sool Won
• Marine Corps Martial Arts Program
• Mixed martial arts
• Northern Praying Mantis
• Ninjutsu
• Pankration
• Pencak Silat
• Sanshou
• Shidōkan Karate
• Shōrin-ryū Shidōkan
• Shoot boxing
• Shootfighting
• Shorinji Kempo
• Systema
• T'ai chi ch'uan
• Vajra-mushti
• Vale tudo
• Vovinam
• Xing Yi Quan
• Zen Bu Kan Kempo
Weapons
• Axe throwing
• Battōjutsu
• Boffer fighting
• Eskrima
• Egyptian stick fencing
• Fencing
• Gatka
• Hojōjutsu
• Iaidō
• Iaijutsu
• Jōdō
• Jogo do pau
• Jūkendō
• Jittejutsu
• Kendo
• Kenjutsu
• Krabi–krabong
• Kung fu
• Kyūdō
• Kyūjutsu
• Modern Arnis
• Naginatajutsu
• Nguni stick-fighting
• Okinawan kobudō
• Shurikenjutsu
• Silambam
• Sōjutsu
• Sword fighting
• Wushu
• Kumdo
• Wing Chun
Skirmish
• Airsoft
• Laser tag
• Paintball
Cue sports
• Carom billiards
• Three-cushion
• Five-pins
• Balkline and straight rail
• Cushion caroms
• Four-ball (yotsudama)
• Artistic billiards
• Novuss (and cued forms of carrom)
• Pocket billiards (pool)
• Eight-ball
• Blackball (a.k.a. British eight-ball pool)
• Nine-ball
• Straight pool (14.1 continuous)
• One-pocket
• Three-ball
• Seven-ball
• Ten-ball
• Rotation
• Baseball pocket billiards
• Cribbage (pool)
• Bank pool
• Artistic pool
• Trick shot competition
• Speed pool
• Bowlliards
• Chicago
• Kelly pool
• Cutthroat
• Killer
• Russian pyramid
• Snooker
• Sinuca brasileira
• Six-red snooker
• Snooker plus
• Hybrid carom–pocket games
• English billiards
• Bottle pool
• Cowboy
• Obstacle variations
• Bagatelle
• Bar billiards
• Bumper pool
• Table Sports
• Foosball
Equine sports
• Buzkashi
• Barrel racing
• Campdrafting
• Cirit
• Charreada
• Chilean rodeo
• Cross country
• Cutting
• Dressage
• Endurance riding
• English pleasure
• Equitation
• Eventing
• Equestrian vaulting
• Gymkhana
• Harness racing
• Horse racing
• Horseball
• Hunter
• Hunter-jumpers
• Jousting
• Pato
• Reining
• Rodeo
• Show jumping
• Steeplechase
• Team penning
• Tent pegging
• Western pleasure
Fishing
• Angling
• Big-game fishing
• Casting
• Noodling
• Spearfishing
• Sport fishing
• Surf fishing
• Rock fishing
• Fly fishing
• Ice fishing
Flying disc sports
• Beach ultimate
• Disc dog
• Disc golf
• Disc golf (urban)
• Dodge disc
• Double disc court
• Flutterguts
• Freestyle
• Freestyle competition
• Goaltimate
• Guts
• Hot box
• Ultimate
Football
• Ancient games
• Chinlone
• Cuju
• Episkyros
• Harpastum
• Kemari
• Ki-o-rahi
• Marn Grook
• Woggabaliri
• Yubi lakpi
• Medieval football
• Ba game
• Caid
• Calcio Fiorentino
• Camping (game)
• Chester-le-Street
• Cnapan
• Cornish hurling
• Haxey Hood
• Knattleikr
• La soule
• Lelo burti
• Mob football
• Royal Shrovetide Football
• Uppies and Downies
• Association football
• Jorkyball
• Paralympic football
• Powerchair Football
• Reduced variants
• Five-a-side football
• Beach soccer
• Futebol de Salão
• Futsal
• Papi fut
• Indoor soccer
• Masters Football
• Street football
• Freestyle football
• Keepie uppie
• Swamp football
• Three sided football
• Australian football
• Nine-a-side footy
• Rec footy
• Metro footy
• English school games
• Eton College
• Field game
• Wall game
• Harrow football
• Gaelic football
• Ladies' Gaelic football
• Gridiron football
• American football
• Eight-man football
• Flag football
• Indoor football
• Arena football
• Nine-man football
• Six-man football
• Sprint football
• Touch football
• Canadian football
• Street football (American)
• Rugby football
• Beach rugby
• Rugby league
• Masters Rugby League
• Mod league
• Rugby league nines
• Rugby league sevens
• Tag rugby
• Touch football
• Wheelchair rugby league
• Rugby union
• American flag rugby
• Mini rugby
• Rugby sevens
• Tag rugby
• Touch rugby
• Rugby tens
• Snow rugby
• Hybrid codes
• Austus
• Eton wall game
• International rules football
• Samoa rules
• Speedball
• Universal football
• Volata
Golf
• Miniature golf
• Match play
• Skins game
• Speed golf
• Stroke play
• Team play
• Shotgun start
Gymnastics
• Acrobatic gymnastics
• Aerobic gymnastics
• Artistic gymnastics
• Balance beam
• Floor
• High bar
• Parallel bars
• Pommel horse
• Still rings
• Uneven bars
• Vault
• Juggling
• Rhythmic gymnastics
• Ball
• Club
• Hoop
• Ribbon
• Rope
• Rope jumping
• Slacklining
• Trampolining
• Trapeze
• Flying trapeze
• Static trapeze
• Tumbling
Handball family
• Goalball
• Hitbal
• Tchoukball
• Team handball
• Beach handball
• Czech handball
• Field handball
• Torball
• Water polo
Hunting
• Beagling
• Big game hunting
• Deer hunting
• Fox hunting
• Hare coursing
• Wolf hunting
Ice sports
• Bandy
• Rink bandy
• Broomball
• Curling
• Ice hockey
• Ringette
• Ice yachting
• Figure skating
Kite sports
• Kite buggy
• Kite fighting
• Kite landboarding
• Kitesurfing
• Parasailing
• Snow kiting
• Sport kite (Stunt kite)
Mixed discipline
• Adventure racing
• Biathlon
• Duathlon
• Decathlon
• Heptathlon
• Icosathlon
• Modern pentathlon
• Pentathlon
• Tetrathlon
• Triathlon
Orienteering family
• Geocaching
• Orienteering
• Rogaining
• Letterboxing
• Waymarking
Pilota family
• American handball
• Australian handball
• Basque pelota
• Jai alai
• Fives
• Eton Fives
• Rugby Fives
• Frisian handball
• Four square
• Gaelic handball
• Jeu de paume
• Palla
• Patball
• Valencian pilota
Racquet (or racket) sports
• Badminton
• Ball badminton
• Basque pelota
• Frontenis
• Xare
• Beach tennis
• Fives
• Matkot
• Padel
• Paleta Frontón
• Pelota mixteca
• Pickleball
• Platform tennis
• Qianball
• Racketlon
• Racquetball
• Racquets
• Real tennis
• Soft tennis
• Speed-ball
• Speedminton
• Squash
• Hardball squash
• Squash tennis
• Stické
• Table tennis
• Tennis
Remote control
• Model aerobatics
• RC racing
• Robot combat
• Slot car racing
Rodeo-originated
• Bullriding
• Barrel Racing
• Bronc Riding
• Saddle Bronc Riding
• Roping
• Calf Roping
• Team Roping
• Steer Wrestling
• Goat Tying
Running
• Endurance
• 5K run
• 10K run
• Cross-country running
• Half marathon
• Marathon
• Road running
• Tower running
• Ultramarathon
• Sprint
• Hurdles
Sailing / Windsurfing
• Ice yachting
• Land sailing
• Land windsurfing
• Sailing
• Windsurfing
• Kiteboarding
• Dinghy sailing
Snow sports
• Alpine skiing
• Freestyle skiing
• Nordic combined
• Nordic skiing
• Cross-country skiing
• Telemark skiing
• Ski jumping
• Ski touring
• Skijoring
• Speed skiing
Sled sports
• Bobsleigh
• Luge
• Skibobbing
• Skeleton
• Toboggan
Shooting sports
• Clay pigeon shooting
• Skeet shooting
• Trap shooting
• Sporting clays
• Target shooting
• Field target
• Fullbore target rifle
• High power rifle
• Benchrest shooting
• Metallic silhouette
• Practical shooting
• Cowboy action shooting
• Metallic silhouette shooting
Stacking
• Card stacking
• Dice stacking
• Sport stacking
Stick and ball games
• Hornussen
Hockey
• Hockey
• Ball hockey
• Bando
• Bandy
• Rink bandy
• Broomball
• Moscow broomball
• Field hockey
• Indoor field hockey
• Floorball
• Ice hockey
Ice hockey
• Pond hockey
• Power hockey
• Ringette
• Sledge hockey
• Underwater ice hockey
• Roller hockey
• Inline hockey
• Roller hockey (Quad)
• Skater hockey
• Rossall Hockey
• Spongee
• Street hockey
• Underwater hockey
• Unicycle hockey
Hurling and shinty
• Cammag
• Hurling
• Camogie
• Shinty
• Composite rules shinty-hurling
Lacrosse
• Lacrosse
• Box lacrosse
• Field lacrosse
• Women's lacrosse
• Intercrosse
Polo
• Polo
• Bicycle polo
• Canoe polo
• Cowboy polo
• Elephant polo
• Horse polo
• Segway polo
• Yak polo
Street sports
• Free running
• Freestyle footbag
• Freestyle football
• Powerbocking
• Parkour
• Scootering
• Street workout
Tag games
• British bulldogs (American Eagle)
• Capture the flag
• Hana Ichi Monme
• Hide and seek
• Jugger
• Kabaddi
• Kho kho
• Kick the can
• Oztag
• Red rover
• Tag
Walking
• Hiking
• Backpacking (wilderness)
• Racewalking
• Bushwhacking
• Walking
Wall-and-ball
• American handball
• Australian handball
• Basque pelota
• Butts Up
• Chinese handball
• Fives
• Gaelic handball
• International fronton
• Jorkyball
• Racquetball
• Squash
• Squash tennis
• Suicide (game)
• Valencian frontó
• Wallball
• Wallyball
Aquatic & paddle sports
• Creeking
• Flyak
• Freeboating
• Sea kayaking
• Squirt boating
• Surf kayaking
• Whitewater kayaking
Rafting
• Rafting
• White water rafting
Rowing
• Rowing (sport)
• Gig racing
• Coastal and ocean rowing
• Surfboat
• Single scull
Other paddling sports
• Dragon boat racing
• Stand up paddle boarding
• Water polo
• Canoe polo
• Waboba
Underwater
• Underwater football
• Underwater rugby
• Underwater hockey
Competitive swimming
• Backstroke
• Breaststroke
• Butterfly stroke
• Freestyle swimming
• Individual medley
• Synchronized swimming
• Medley relay
Kindred activities
• Bifins (finswimming)
• Surface finswimming
Subsurface and recreational
• Apnoea finswimming
• Aquathlon (underwater wrestling)
• Freediving
• Immersion finswimming
• Scuba diving
• Spearfishing
• Snorkelling
• Sport diving (sport)
• Underwater hockey
• Underwater orienteering
• Underwater photography (sport)
• Underwater target shooting
Diving
• Cliff diving
• Diving
Weightlifting
• Basque traditional weightlifting
• Bodybuilding
• Highland games
• Olympic weightlifting
• Powerlifting
• Strength athletics (strongman)
• Steinstossen
Motorized sports
• Autocross (a.k.a. Slalom)
• Autograss
• Banger racing
• Board track racing
• Demolition derby
• Desert racing
• Dirt track racing
• Drag racing
• Drifting
• Folkrace
• Formula racing
• Formula Libre
• Formula Student
• Hillclimbing
• Ice racing
• Kart racing
• Land speed records
• Legends car racing
• Midget car racing
• Monster truck
• Mud bogging
• Off-road racing
• Pickup truck racing
• Production car racing
• Race of Champions
• Rally raid
• Rallycross
• Rallying
• Regularity rally
• Road racing
• Short track motor racing
• Snowmobile racing
• Sports car racing
• Sprint car racing
• Street racing
• Stock car racing
• Time attack
• Tractor pulling
• Touring car racing
• Truck racing
• Vintage racing
• Wheelstand competition
Motorboat racing
• Drag boat racing
• F1 powerboat racing
• Hydroplane racing
• Jet sprint boat racing
• Offshore powerboat racing
• Personal water craft
Motorcycle racing
• Auto Race
• Board track racing
• Cross-country rally
• Endurance racing
• Enduro
• Freestyle motocross
• Grand Prix motorcycle racing
• Grasstrack
• Hillclimbing
• Ice racing
• Ice speedway
• Indoor enduro
• Motocross
• Motorcycle drag racing
• Motorcycle speedway
• Off-roading
• Rally raid
• Road racing
• Superbike racing
• Supercross
• Supermoto
• Supersport racing
• Superside
• Track racing
• Trial
• TT racing
• Free-style moto
Marker sports
• Airsoft
• Archery
• Paintball
• Darts
Musical sports
• Color guard
• Drum corps
• Indoor percussion
• Marching band
Fantasy sports
• Quidditch
• Hunger Games(Gladiating)
• Pod Racing
• Mortal Kombat(MMA)
Other
• Stihl Timbersports Series
• Woodsman
Overlapping sports
• Tennis
• Polocrosse
• Badminton
• Polo
Skating sports
• Aggressive inline skating
• Artistic roller skating
• Figure skating
• Freestyle slalom skating
• Ice dancing
• Ice skating
• Inline speed skating
• Rinkball
• Rink hockey
• Roller derby
• Roller skating
• Short track speed skating
• Skater hockey
• Speed skating
• Synchronized skating
Freestyle skiing
• Snowboarding
• Ski flying
• Skibob
• Snowshoeing
• Skiboarding