Licensed under Creative Commons Attribution 2.5 (Silberwolf).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (August 2010) (Learn how and when to remove this template message) |
Tapered roller bearings are rolling element bearings that can support axial forces (i.e., they are good thrust bearings) as well as radial forces.
The inner and outer ring raceways are segments of cones and the rollers are tapered so that the conical surfaces of the raceways, and the roller axes, if projected, would all meet at a common point on the main axis of the bearing. This geometry makes the motion of the cones remain coaxial, with no sliding motion between the raceways and the OD of the rollers.
This conical geometry creates a linear contact patch which permits greater loads to be carried than with spherical (ball) bearings, which have point contact. The geometry means that the tangential speeds of the surfaces of each of the rollers are the same as their raceways along the whole length of the contact patch and no differential scrubbing occurs.
The rollers are stabilized and restrained by a flange on the inner ring, against which their large end slides, which stops the rollers from popping out due to the "pumpkin seed effect" of their conical shape.
The larger the half angles of these cones the larger the axial force that the bearing can sustain.
Tapered roller bearings are separable into a cone assembly and a cup. The non-separable cone assembly consists of the inner ring, the rollers, and a cage that retains & evenly spaces the rollers. The cup is simply the outer ring. Internal clearance is established during mounting by the axial position of the cone relative to the cup, although preloaded installations without clearance are common.
Metric tapered roller bearings follow the designation system defined by ISO 355.
On March 23, 1895, John Lincoln Scott, a farmer and carpenter from Wilmot, Indiana was awarded a patent from the United States Patent Office for his invention of the tapered roller bearing. The purpose of his invention was to improve the performance of wagon wheels used in farming. In 1898, Henry Timken was awarded a patent[1] for the tapered roller bearing. At the time, Timken was a carriage-maker in St. Louis and held three patents for carriage springs. However, it was his patent for tapered roller bearings that allowed his company to become successful.
Tapered roller bearings were a breakthrough at the end of the 19th century because bearings used in wheel axles had not changed much since ancient times. They consisted of a cylindrical seat on the frame and part of the axle enclosed in a case or box that held a lubricant. These were called journal bearings and relied on the lubricant to form a fluid bearing. Without adequate lubrication,[2] journal bearings would fail due to the excessive heat caused by friction. Timken was able to significantly reduce the friction on his axle bearings by adding tapered elements which actually rolled while transferring the load evenly from axle to frame through the hardened steel inner and outer rings and the rollers - his tapered roller bearing.
The tapered roller bearing in combination with modern lubricants is extremely durable and is used almost universally in applications involving rotating axle and transmission shafts. Bearing durability is such that these shafts often require no maintenance for hundreds of thousands of kilometers of operation.
In many applications tapered roller bearings are used in back-to-back pairs so that axial forces can be supported equally in either direction.
Pairs of tapered roller bearings are used in car and vehicle wheel bearings where they must cope simultaneously with large vertical (radial) and horizontal (axial) forces. Tapered roller bearings are commonly used for moderate speed, heavy duty applications where durability is required. Common real world applications are in agriculture, construction and mining equipment, axle systems, gear box, engine motors and reducers, propeller shaft, railroad axle-box, differential, wind turbines, etc.
This article uses material from the Wikipedia article "Tapered roller bearing", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD