powered by CADENAS

Social Share

Praseodymium (10444 views - Periodic Table Of Elements)

Praseodymium is a chemical element with symbol Pr and atomic number 59. It is the third member of the lanthanide series and is traditionally considered to be one of the rare-earth metals. Praseodymium is a soft, silvery, malleable and ductile metal, valued for its magnetic, electrical, chemical, and optical properties. It is too reactive to be found in native form, and pure praseodymium metal slowly develops a green oxide coating. Praseodymium always occurs naturally together with the other rare-earth metals. It is the fourth most common rare-earth element, making up 9.1 parts per million of the Earth's crust, an abundance similar to that of boron. In 1841, Swedish chemist Carl Gustav Mosander extracted a rare-earth oxide residue he called didymium from a residue he called "lanthana", in turn separated from cerium salts. In 1885, the Austrian chemist Baron Carl Auer von Welsbach separated didymium into two elements that gave salts of different colours, which he named praseodymium and neodymium. The name praseodymium comes from the Greek prasinos (πράσινος), meaning "green", and didymos (δίδυμος), "twin". Like most rare-earth elements, praseodymium most readily forms the +3 oxidation state, which is the only stable state in aqueous solution, although the +4 oxidation state is known in some solid compounds and, uniquely among the lanthanides, the +5 oxidation state is attainable in matrix-isolation conditions. Aqueous praseodymium ions are yellowish-green, and similarly praseodymium results in various shades of yellow-green when incorporated into glasses. Many of praseodymium's industrial uses involve its ability to filter yellow light from light sources.
Go to Article

Praseodymium

Praseodymium

Praseodymium,  59Pr
General properties
Pronunciation /przəˈdɪmiəm/[1]
pray-zee-ə-DIM-ee-əm
Appearance grayish white
Standard atomic weight (Ar) 140.90766(2)[2]
Praseodymium in the periodic table


Pr

Pa
ceriumpraseodymiumneodymium
Atomic number (Z) 59
Group, period group n/a, period 6
Block f-block
Element category   lanthanide
Electron configuration [Xe] 4f3 6s2
Electrons per shell
2, 8, 18, 21, 8, 2
Physical properties
Spectral lines
Phase (at STP) solid
Melting point 1208 K ​(935 °C, ​1715 °F)
Boiling point 3403 K ​(3130 °C, ​5666 °F)
Density (near r.t.) 6.77 g/cm3
when liquid (at m.p.) 6.50 g/cm3
Heat of fusion 6.89 kJ/mol
Heat of vaporization 331 kJ/mol
Molar heat capacity 27.20 J/(mol·K)
Vapor pressure
P (Pa) 1 10 100 1 k 10 k 100 k
at T (K) 1771 1973 (2227) (2571) (3054) (3779)
Atomic properties
Oxidation states 5, 4, 3, 2 ​(a mildly basic oxide)
Electronegativity Pauling scale: 1.13
Ionization energies
  • 1st: 527 kJ/mol
  • 2nd: 1020 kJ/mol
  • 3rd: 2086 kJ/mol
Atomic radius empirical: 182 pm
Covalent radius 203±7 pm
Miscellanea
Crystal structuredouble hexagonal close-packed (dhcp)
Speed of sound thin rod 2280 m/s (at 20 °C)
Thermal expansion α, poly: 6.7 µm/(m·K) (at r.t.)
Thermal conductivity 12.5 W/(m·K)
Electrical resistivity α, poly: 0.700 µΩ·m (at r.t.)
Magnetic ordering paramagnetic[3]
Magnetic susceptibility +5010.0·10−6 cm3/mol (293 K)[4]
Young's modulus α form: 37.3 GPa
Shear modulus α form: 14.8 GPa
Bulk modulus α form: 28.8 GPa
Poisson ratio α form: 0.281
Vickers hardness 250–745 MPa
Brinell hardness 250–640 MPa
CAS Number 7440-10-0
History
Discovery Carl Auer von Welsbach (1885)
Main isotopes of praseodymium
Iso­tope Abun­dance Half-life (t1/2) Decay mode Pro­duct
141Pr 100% stable
142Pr syn 19.12 h β 142Nd
ε 142Ce
143Pr syn 13.57 d β 143Nd
| references | in Wikidata

Praseodymium is a chemical element with symbol Pr and atomic number 59. It is the third member of the lanthanide series and is traditionally considered to be one of the rare-earth metals. Praseodymium is a soft, silvery, malleable and ductile metal, valued for its magnetic, electrical, chemical, and optical properties. It is too reactive to be found in native form, and pure praseodymium metal slowly develops a green oxide coating.

Praseodymium always occurs naturally together with the other rare-earth metals. It is the fourth most common rare-earth element, making up 9.1 parts per million of the Earth's crust, an abundance similar to that of boron. In 1841, Swedish chemist Carl Gustav Mosander extracted a rare-earth oxide residue he called didymium from a residue he called "lanthana", in turn separated from cerium salts. In 1885, the Austrian chemist Baron Carl Auer von Welsbach separated didymium into two elements that gave salts of different colours, which he named praseodymium and neodymium. The name praseodymium comes from the Greek prasinos (πράσινος), meaning "green", and didymos (δίδυμος), "twin".

Like most rare-earth elements, praseodymium most readily forms the +3 oxidation state, which is the only stable state in aqueous solution, although the +4 oxidation state is known in some solid compounds and, uniquely among the lanthanides, the +5 oxidation state is attainable in matrix-isolation conditions. Aqueous praseodymium ions are yellowish-green, and similarly praseodymium results in various shades of yellow-green when incorporated into glasses. Many of praseodymium's industrial uses involve its ability to filter yellow light from light sources.

Characteristics

Physical

Praseodymium is the third member of the lanthanide series. In the periodic table, it appears between the lanthanides cerium to its left and neodymium to its right, and above the actinide protactinium. It is a ductile metal with a hardness comparable to that of silver.[5] Its 59 electrons are arranged in the configuration [Xe]4f36s2; theoretically, all five outer electrons can act as valence electrons, but the use of all five requires extreme conditions and normally, praseodymium only gives up three or sometimes four electrons in its compounds. Praseodymium is the first of the lanthanides to have an electron configuration conforming to the Aufbau principle, which predicts the 4f orbitals to have a lower energy level than the 5d orbitals; this does not hold for lanthanum and cerium, because the sudden contraction of the 4f orbitals does not happen until after lanthanum, and is not strong enough at cerium to avoid occupying the 5d subshell. Nevertheless, solid praseodymium takes on the [Xe]4f25d16s2 configuration, with one electron in the 5d subshell like all the other trivalent lanthanides (all but europium and ytterbium, which are divalent in the metallic state).[6]

Like most lanthanides, praseodymium usually only uses three electrons as valence electrons, as afterwards the remaining 4f electrons are too strongly bound: this is because the 4f orbitals penetrate the most through the inert xenon core of electrons to the nucleus, followed by 5d and 6s, and this increases with higher ionic charge. Praseodymium nevertheless can continue losing a fourth and even occasionally a fifth valence electron because it comes very early in the lanthanide series, where the nuclear charge is still low enough and the 4f subshell energy high enough to allow the removal of further valence electrons.[7] Thus, similarly to the other early trivalent lanthanides, praseodymium has a double hexagonal close-packed crystal structure at room temperature. At about 560 °C, it transitions to a face-centered cubic structure, and a body-centered cubic structure appears shortly before the melting point of 935 °C.[8]

Praseodymium, like all of the lanthanides (except lanthanum, ytterbium, and lutetium, which have no unpaired 4f electrons), is paramagnetic at room temperature.[9] Unlike some other rare-earth metals, which show antiferromagnetic or ferromagnetic ordering at low temperatures, praseodymium is paramagnetic at all temperatures above 1 K.[3]

Isotopes

Praseodymium has only one stable and naturally occurring isotope, 141Pr. It is thus a mononuclidic element, and its standard atomic weight can be determined with high precision. This isotope has 82 neutrons, a magic number that confers additional stability.[10] This isotope is produced in stars through the s- and r-processes (slow and rapid neutron capture, respectively).[11]

All other praseodymium isotopes have half-lives under a day (and most under a minute), with the single exception of 143Pr with a half-life of 13.6 days. Both 143Pr and 141Pr occur as fission products of uranium. The primary decay mode of isotopes lighter than 141Pr is inverse beta decay or electron capture to isotopes of cerium, while that of heavier isotopes is beta decay to isotopes of neodymium.[10]

Chemistry

Praseodymium metal tarnishes slowly in air, forming a spalling oxide layer like iron rust; a centimetre-sized sample of praseodymium metal corrodes completely in about a year.[12] It burns readily at 150 °C to form praseodymium(III,IV) oxide, a nonstoichiometric compound approximating to Pr6O11:[13]

12 Pr + 11 O2 → 2 Pr6O11

This may be reduced to praseodymium(III) oxide (Pr2O3) with hydrogen gas.[14] The dark-coloured praseodymium(IV) oxide, PrO2, is the most oxidised product of the combustion of praseodymium and is only obtained by reaction of praseodymium metal with pure oxygen at 400 °C and 282 bar.[14] The reactivity of praseodymium conforms to periodic trends, as it is one of the first and thus one of the largest lanthanides.[7] At 1000 °C, many praseodymium oxides with composition PrO2−x exist as disordered, nonstoichiometric phases with 0 < x < 0.25, but at 400–700 °C the oxide defects are instead ordered, creating phases of the general formula PrnO2n−2 with n = 4, 7, 9, 10, 11, 12, and ∞. These phases PrOy are sometimes labelled α and β′ (nonstoichiometric), β (y = 1.833), δ (1.818), ε (1.8), ζ (1.778), ι (1.714), θ, and σ.[15]

Praseodymium is quite electropositive and reacts slowly with cold water and quite quickly with hot water to form praseodymium(III) hydroxide:[13]

2 Pr (s) + 6 H2O (l) → 2 Pr(OH)3 (aq) + 3 H2 (g)

Praseodymium metal reacts with all the halogens to form trihalides:[13]

2 Pr (s) + 3 F2 (g) → 2 PrF3 (s) [green]
2 Pr (s) + 3 Cl2 (g) → 2 PrCl3 (s) [green]
2 Pr (s) + 3 Br2 (g) → 2 PrBr3 (s) [green]
2 Pr (s) + 3 I2 (g) → 2 PrI3 (s)

The tetrafluoride, PrF4, is also known, and is produced by reacting a mixture of sodium fluoride and praseodymium(III) fluoride with fluorine gas, producing Na2PrF6, following which sodium fluoride is removed from the reaction mixture with liquid hydrogen fluoride.[16] Additionally, praseodymium forms a bronze diiodide; like the diiodides of lanthanum, cerium, and gadolinium, it is a praseodymium(III) electride compound.[16]

Praseodymium dissolves readily in dilute sulfuric acid to form solutions containing the chartreuse Pr3+ ions, which exist as [Pr(H2O)9]3+ complexes:[13][17]

2 Pr (s) + 3 H2SO4 (aq) → 2 Pr3+ (aq) + 3 SO2−
4
(aq) + 3 H2 (g)

Dissolving praseodymium(IV) compounds in water results in solutions containing the yellow Pr4+ ions;[18] because of the high positive standard reduction potential of the Pr4+/Pr3+ couple at +3.2 V, these ions are unstable in aqueous solution, oxidising water and being reduced to Pr3+. The value for the Pr3+/Pr couple is −2.35 V.[6]

Although praseodymium(V) in the bulk state is unknown, the existence of praseodymium in its +5 oxidation state (with the stable electron configuration of the preceding noble gas xenon) under noble-gas matrix isolation conditions was reported in 2016. The species assigned to the +5 state were identified as [PrO2]+, its O2 and Ar adducts, and PrO22-O2).[19]

Organopraseodymium compounds are very similar to those of the other lanthanides, as they all share an inability to undergo π backbonding. They are thus mostly restricted to the mostly ionic cyclopentadienides (isostructural with those of lanthanum) and the σ-bonded simple alkyls and aryls, some of which may be polymeric.[20] The coordination chemistry of praseodymium is largely that of the large, electropositive Pr3+ ion, and is thus largely similar to those of the other early lanthanides La3+, Ce3+, and Nd3+. For instance, like lanthanum, cerium, and neodymium, praseodymium nitrates form both 4:3 and 1:1 complexes with 18-crown-6, whereas the middle lanthanides from promethium to gadolinium can only form the 4:3 complex and the later lanthanides from terbium to lutetium cannot successfully coordinate to all the ligands. Such praseodymium complexes have high but uncertain coordination numbers and poorly defined stereochemistry, with exceptions resulting from exceptionally bulky ligands such as the tricoordinate [Pr{N(SiMe3)2}3]. There are also a few mixed oxides and fluorides involving praseodymium(IV), but it does not have an appreciable coordination chemistry in this oxidation state like its neighbour cerium.[21]

History

In 1751, the Swedish mineralogist Axel Fredrik Cronstedt discovered a heavy mineral from the mine at Bastnäs, later named cerite. Thirty years later, the fifteen-year-old Vilhelm Hisinger, from the family owning the mine, sent a sample of it to Carl Scheele, who did not find any new elements within. In 1803, after Hisinger had become an ironmaster, he returned to the mineral with Jöns Jacob Berzelius and isolated a new oxide, which they named ceria after the dwarf planet Ceres, which had been discovered two years earlier.[22] Ceria was simultaneously and independently isolated in Germany by Martin Heinrich Klaproth.[23] Between 1839 and 1843, ceria was shown to be a mixture of oxides by the Swedish surgeon and chemist Carl Gustaf Mosander, who lived in the same house as Berzelius; he separated out two other oxides, which he named lanthana and didymia.[24] He partially decomposed a sample of cerium nitrate by roasting it in air and then treating the resulting oxide with dilute nitric acid. The metals that formed these oxides were thus named lanthanum and didymium.[25] While lanthanum turned out to be a pure element, didymium was not and turned out to be only a mixture of all the stable early lanthanides from praseodymium to europium, as had been suspected by Marc Delafontaine after spectroscopic analysis, though he lacked the time to pursue its separation into its constituents. The heavy pair of samarium and europium were only removed in 1879 by Paul-Émile Lecoq de Boisbaudran and it was not until 1885 that Carl Auer von Welsbach separated didymium into praseodymium and neodymium.[26] Since neodymium was a larger constituent of didymium than praseodymium, it kept the old name with disambiguation, while praseodymium was distinguished by the leek-green colour of its salts (Greek πρασιος, "leek green").[27]

Occurrence and production

Praseodymium is not particularly rare, making up 9.1 mg/kg of the Earth's crust. This value is between those of lead (13 mg/kg) and boron (9 mg/kg), and makes praseodymium the fourth-most abundant of the lanthanides, behind cerium (66 mg/kg), neodymium (40 mg/kg), and lanthanum (35 mg/kg); it is less abundant than the rare-earth elements yttrium (31 mg/kg) and scandium (25 mg/kg).[27] Instead, praseodymium's classification as a rare-earth metal comes from its rarity relative to "common earths" such as lime and magnesia, the few known minerals containing it for which extraction is commercially viable, as well as the length and complexity of extraction.[28]

The Pr3+ ion is similar in size to the early lanthanides of the cerium group (those from lanthanum up to samarium and europium) that immediately follow in the periodic table, and hence it tends to occur along with them in phosphate, silicate and carbonate minerals, such as monazite (MIIIPO4) and bastnäsite (MIIICO3F), where M refers to all the rare-earth metals except scandium and the radioactive promethium (mostly Ce, La, and Y, with somewhat less Nd and Pr).[27] Bastnäsite is usually lacking in thorium and the heavy lanthanides, and the purification of the light lanthanides from it is less involved. The ore, after being crushed and ground, is first treated with hot concentrated sulfuric acid, evolving carbon dioxide, hydrogen fluoride, and silicon tetrafluoride. The product is then dried and leached with water, leaving the early lanthanide ions, including lanthanum, in solution.[27]

The procedure for monazite, which usually contains all the rare earths, as well as thorium, is more involved. Monazite, because of its magnetic properties, can be separated by repeated electromagnetic separation. After separation, it is treated with hot concentrated sulfuric acid to produce water-soluble sulfates of rare earths. The acidic filtrates are partially neutralised with sodium hydroxide to pH 3–4, during which thorium precipitates as a hydroxide and is removed. The solution is treated with ammonium oxalate to convert rare earths to their insoluble oxalates, the oxalates are converted to oxides by annealing, and the oxides are dissolved in nitric acid. This last step excludes one of the main components, cerium, whose oxide is insoluble in HNO3.[28] Care must be taken when handling some of the residues as they contain 228Ra, the daughter of 232Th, which is a strong gamma emitter.[27]

Praseodymium may then be separated from the other lanthanides via ion-exchange chromatography, or by using a solvent such as tributyl phosphate where the solubility of Ln3+ increases as the atomic number increases. If ion-exchange chromatography is used, the mixture of lanthanides is loaded into one column of cation-exchange resin and Cu2+ or Zn2+ or Fe3+ is loaded into the other. An aqueous solution of a complexing agent, known as the eluant (usually triammonium edtate), is passed through the columns, and Ln3+ is displaced from the first column and redeposited in a compact band at the top of the column before being re-displaced by NH+
4
. The Gibbs free energy of formation for Ln(edta·H) complexes increases along the lanthanides by about one quarter from Ce3+ to Lu3+, so that the Ln3+ cations descend the development column in a band and are fractionated repeatedly, eluting from heaviest to lightest. They are then precipitated as their insoluble oxalates, burned to form the oxides, and then reduced to the metals.[27]

Applications

Leo Moser (son of Ludwig Moser, founder of the Moser Glassworks in what is now Karlovy Vary in the Czech Republic, not to be confused with the mathematician of the same name) investigated the use of praseodymium in glass colouration in the late 1920s, yielding a yellow-green glass given the name "Prasemit". However, at that time far cheaper colourants could give a similar colour, so Prasemit was not popular, few pieces were made, and examples are now extremely rare. Moser also blended praseodymium with neodymium to produce "Heliolite" glass ("Heliolit" in German), which was more widely accepted. The first enduring commercial use of purified praseodymium, which continues today, is in the form of a yellow-orange "Praseodymium Yellow" stain for ceramics, which is a solid solution in the zircon lattice. This stain has no hint of green in it; by contrast, at sufficiently high loadings, praseodymium glass is distinctly green rather than pure yellow.[29]

As the lanthanides are so similar, praseodymium can substitute for most other lanthanides without significant loss of function, and indeed many applications such as mischmetal and ferrocerium alloys involve variable mixes of several lanthanides, including small quantities of praseodymium. The following more modern applications involve praseodymium specifically, or at least praseodymium in a small subset of the lanthanides:[30]

Biological role and precautions

The early lanthanides act as essential cofactors for the methanol dehydrogenase of the methanotrophic bacterium Methylacidiphilum fumariolicum SolV, for which lanthanum, cerium, praseodymium, and neodymium alone are about equally effective.[38] Praseodymium is otherwise not known to have a biological role in any other organisms, but is not very toxic either. Intravenous injection of rare earths into animals has been known to impair liver function, but the main side effects from inhalation of rare-earth oxides in humans come from radioactive thorium and uranium impurities.[30]

  1. ^ "praseodymium". Oxford English Dictionary (3rd ed.). Oxford University Press. September 2005.  (Subscription or UK public library membership required.)
  2. ^ Meija, J.; et al. (2016). "Atomic weights of the elements 2013 (IUPAC Technical Report)". Pure Appl. Chem. 88 (3): 265–91. doi:10.1515/pac-2015-0305. 
  3. ^ a b Jackson, M. (2000). "Magnetism of Rare Earth" (PDF). The IRM quarterly. 10 (3): 1. 
  4. ^ Weast, Robert (1984). CRC, Handbook of Chemistry and Physics. Boca Raton, Florida: Chemical Rubber Company Publishing. pp. E110. ISBN 0-8493-0464-4. 
  5. ^ a b c Lide, D. R., ed. (2005). CRC Handbook of Chemistry and Physics (86th ed.). Boca Raton (FL): CRC Press. ISBN 0-8493-0486-5. 
  6. ^ a b Greenwood and Earnshaw, pp. 1232–5
  7. ^ a b Greenwood and Earnshaw, pp. 1235–8
  8. ^ "Phase Diagrams of the Elements", David A. Young, UCRL-51902 "Prepared for the U.S. Energy Research & Development Administration under contract No. W-7405-Eng-48".
  9. ^ Cullity, B. D.; Graham, C. D. (2011). Introduction to Magnetic Materials. John Wiley & Sons. ISBN 978-1-118-21149-6. 
  10. ^ a b Audi, Georges; Bersillon, O.; Blachot, J.; Wapstra, A.H. (2003). "The NUBASE Evaluation of Nuclear and Decay Properties". Nuclear Physics A. Atomic Mass Data Center. 729: 3–128. Bibcode:2003NuPhA.729....3A. doi:10.1016/j.nuclphysa.2003.11.001. 
  11. ^ Cameron, A. G. W. (1973). "Abundance of the Elements in the Solar System" (PDF). Space Science Reviews. 15: 121–146. Bibcode:1973SSRv...15..121C. doi:10.1007/BF00172440. Archived from the original (PDF) on 2011-10-21. 
  12. ^ "Rare-Earth Metal Long Term Air Exposure Test". Retrieved 2009-08-08. 
  13. ^ a b c d "Chemical reactions of Praseodymium". Webelements. Retrieved 9 July 2016. 
  14. ^ a b Greenwood and Earnshaw, pp. 1238–9
  15. ^ Greenwood and Earnshaw, pp. 643–4
  16. ^ a b Greenwood and Earnshaw, p. 1240–2
  17. ^ Greenwood and Earnshaw, pp. 1242–4
  18. ^ Sroor, Farid M.A.; Edelmann, Frank T. (2012). "Lanthanides: Tetravalent Inorganic". Encyclopedia of Inorganic and Bioinorganic Chemistry. ISBN 978-1-119-95143-8. doi:10.1002/9781119951438.eibc2033. 
  19. ^ Zhang, Qingnan; Hu, Shu-Xian; Qu, Hui; Su, Jing; Wang, Guanjun; Lu, Jun-Bo; Chen, Mohua; Zhou, Mingfei; Li, Jun (2016-06-06). "Pentavalent Lanthanide Compounds: Formation and Characterization of Praseodymium(V) Oxides". Angewandte Chemie International Edition. 55 (24): 6896–6900. ISSN 1521-3773. doi:10.1002/anie.201602196. 
  20. ^ Greenwood and Earnshaw, pp. 1248–9
  21. ^ Greenwood and Earnshaw, pp. 1244–8
  22. ^ Emsley, pp. 120–5
  23. ^ Greenwood and Earnshaw, p. 1424
  24. ^ Weeks, Mary Elvira (1932). "The Discovery of the Elements: XI. Some Elements Isolated with the Aid of Potassium and Sodium:Zirconium, Titanium, Cerium and Thorium". The Journal of Chemical Education. 9 (7): 1231–1243. Bibcode:1932JChEd...9.1231W. doi:10.1021/ed009p1231. 
  25. ^ See:
    • (Berzelius) (1839) "Nouveau métal" (New metal), Comptes rendus, 8 : 356–357. From p. 356: "L'oxide de cérium, extrait de la cérite par la procédé ordinaire, contient à peu près les deux cinquièmes de son poids de l'oxide du nouveau métal qui ne change que peu les propriétés du cérium, et qui s'y tient pour ainsi dire caché. Cette raison a engagé M. Mosander à donner au nouveau métal le nom de Lantane." (The oxide of cerium, extracted from cerite by the usual procedure, contains almost two fifths of its weight in the oxide of the new metal, which differs only slightly from the properties of cerium, and which is held in it so to speak "hidden". This reason motivated Mr. Mosander to give to the new metal the name Lantane.)
    • (Berzelius) (1839) "Latanium — a new metal," Philosophical Magazine, new series, 14 : 390–391.
  26. ^ Fontani, Marco; Costa, Mariagrazia; Orna, Virginia (2014). The Lost Elements: The Periodic Table's Shadow Side. Oxford University Press. 
  27. ^ a b c d e f Greenwood and Earnshaw, p. 1229–32
  28. ^ a b Patnaik, Pradyot (2003). Handbook of Inorganic Chemical Compounds. McGraw-Hill. pp. 444–446. ISBN 0-07-049439-8. Retrieved 2009-06-06. 
  29. ^ Kreidl, Norbert J. (1942). "RARE EARTHS*". Journal of the American Ceramic Society. 25 (5): 141. doi:10.1111/j.1151-2916.1942.tb14363.x. 
  30. ^ a b c d e McGill, Ian (2005), "Rare Earth Elements", Ullmann's Encyclopedia of Industrial Chemistry, 31, Weinheim: Wiley-VCH, p. 183–227, doi:10.1002/14356007.a22_607 
  31. ^ Rare Earth Elements 101 Archived 2013-11-22 at the Wayback Machine., IAMGOLD Corporation, April 2012, pp. 5, 7.
  32. ^ Rokhlin, L. L. (2003). Magnesium alloys containing rare earth metals: structure and properties. CRC Press. ISBN 0-415-28414-7. 
  33. ^ Suseelan Nair, K.; Mittal, M. C. (1988). "Rare Earths in Magnesium Alloys". Materials Science Forum. 30: 89. doi:10.4028/www.scientific.net/MSF.30.89. 
  34. ^ a b Emsley, pp. 423–5
  35. ^ "ANU team stops light in quantum leap". Retrieved 18 May 2009. 
  36. ^ Jha, A.; Naftaly, M.; Jordery, S.; Samson, B. N.; et al. (1995). "Design and fabrication of Pr3+-doped fluoride glass optical fibres for efficient 1.3 mu m amplifiers". Pure and Applied Optics: Journal of the European Optical Society Part A. 4 (4): 417. Bibcode:1995PApOp...4..417J. doi:10.1088/0963-9659/4/4/019. 
  37. ^ Borchert, Y.; Sonstrom, P.; Wilhelm, M.; Borchert, H.; et al. (2008). "Nanostructured Praseodymium Oxide: Preparation, Structure, and Catalytic Properties". Journal of Physical Chemistry C. 112 (8): 3054. doi:10.1021/jp0768524. 
  38. ^ Pol, Arjan; Barends, Thomas R. M.; Dietl, Andreas; Khadem, Ahmad F.; Eygensteyn, Jelle; Jetten, Mike S. M.; Op Den Camp, Huub J. M. (2013). "Rare earth metals are essential for methanotrophic life in volcanic mudpots". Environmental Microbiology. 16 (1): 255–64. PMID 24034209. doi:10.1111/1462-2920.12249. 

Bibliography

Further reading

  • R. J. Callow, The Industrial Chemistry of the Lanthanons, Yttrium, Thorium and Uranium, Pergamon Press, 1967.


This article uses material from the Wikipedia article "Praseodymium", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Periodic Table Of Elements

Element