Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
General properties | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Pronunciation |
/koʊpərˈnɪsiəm/ koe-pər-NIS-ee-əm | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Mass number | 285 (most stable isotope) | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Copernicium in the periodic table | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Atomic number (Z) | 112 | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Group, period | group 12, period 7 | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Block | d-block | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Element category | post-transition metal, alternatively considered a transition metal | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Electron configuration | [Rn] 5f14 6d10 7s2 (predicted)[1] | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Electrons per shell | 2, 8, 18, 32, 32, 18, 2 (predicted) | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Physical properties | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Phase (at STP) | gas[2] (predicted) | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Boiling point |
357+112 −108 K (84+112 −108 °C, 183+202 −194 °F)[3] | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Density when liquid (at m.p.) | 23.7 g/cm3 (predicted)[1] | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Atomic properties | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Oxidation states | 2, (1), 0 (parenthesized oxidation states are predictions)[1][4][5] | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Ionization energies | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Atomic radius | empirical: 147 pm (predicted)[1][5] | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Covalent radius | 122 pm (predicted)[6] | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Miscellanea | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Crystal structure |
hexagonal close-packed (hcp) (predicted)[7] | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
CAS Number | 54084-26-3 | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
History | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Naming | after Nicolaus Copernicus | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Discovery | Gesellschaft für Schwerionenforschung (1996) | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Main isotopes of copernicium | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| references | in Wikidata |
Copernicium is a chemical element with symbol Cn and atomic number 112. It is an extremely radioactive, synthetic element that can only be created in a laboratory. The most stable known isotope, copernicium-285, has a half-life of approximately 29 seconds. Copernicium was first created in 1996 by the GSI Helmholtz Centre for Heavy Ion Research near Darmstadt, Germany. It is named after the astronomer Nicolaus Copernicus.
In the periodic table of the elements, copernicium is a d-block transactinide element. During reactions with gold, it has been shown[9] to be an extremely volatile metal and a group 12 element, so much so that it is probably a gas at standard temperature and pressure.
Copernicium is calculated to have several properties that differ from its lighter homologues in group 12, zinc, cadmium and mercury; due to relativistic effects, it may even give up its 6d electrons instead of its 7s ones. Copernicium has also been calculated to possibly show the oxidation state +4, while mercury shows it in only one compound of disputed existence and zinc and cadmium do not show it at all, although more recent calculations cast doubt on this possibility. It has also been predicted to be more difficult to oxidize copernicium from its neutral state than the other group 12 elements.
Copernicium was first created on February 9, 1996, at the Gesellschaft für Schwerionenforschung (GSI) in Darmstadt, Germany, by Sigurd Hofmann, Victor Ninov et al.[10] This element was created by firing accelerated zinc-70 nuclei at a target made of lead-208 nuclei in a heavy ion accelerator. A single atom (a second was reported but was found to have been based on data fabricated by Ninov) of copernicium was produced with a mass number of 277.[10]
In May 2000, the GSI successfully repeated the experiment to synthesize a further atom of copernicium-277.[11][12] This reaction was repeated at RIKEN using the Search for a Super-Heavy Element Using a Gas-Filled Recoil Separator set-up in 2004 and 2013 to synthesize three further atoms and confirm the decay data reported by the GSI team.[13][14]
The IUPAC/IUPAP Joint Working Party (JWP) assessed the claim of copernicium's discovery by the GSI team in 2001[15] and 2003.[16] In both cases, they found that there was insufficient evidence to support their claim. This was primarily related to the contradicting decay data for the known nuclide rutherfordium-261. However, between 2001 and 2005, the GSI team studied the reaction 248Cm(26Mg,5n)269Hs, and were able to confirm the decay data for hassium-269 and rutherfordium-261. It was found that the existing data on rutherfordium-261 was for an isomer,[17] now designated rutherfordium-261m.
In May 2009, the JWP reported on the claims of discovery of element 112 again and officially recognized the GSI team as the discoverers of element 112.[18] This decision was based on the confirmation of the decay properties of daughter nuclei as well as the confirmatory experiments at RIKEN.[19]
Using Mendeleev's nomenclature for unnamed and undiscovered elements, copernicium should be known as eka-mercury. In 1979, IUPAC published recommendations according to which the element was to be called ununbium (with the corresponding symbol of Uub),[20] a systematic element name as a placeholder, until the element was discovered (and the discovery then confirmed) and a permanent name was decided on. Although widely used in the chemical community on all levels, from chemistry classrooms to advanced textbooks, the recommendations were mostly ignored among scientists in the field, who either called it "element 112", with the symbol of E112, (112), or even simply 112.[1]
After acknowledging the GSI team's discovery, the IUPAC asked them to suggest a permanent name for element 112.[19][21] On 14 July 2009, they proposed copernicium with the element symbol Cp, after Nicolaus Copernicus "to honor an outstanding scientist, who changed our view of the world".[22]
During the standard six-month discussion period among the scientific community about the naming,[23][24] it was pointed out that the symbol Cp was previously associated with the name cassiopeium (cassiopium), now known as lutetium (Lu).[25][26] For this reason, the IUPAC disallowed the use of Cp as a future symbol, prompting the GSI team to put forward the symbol Cn as an alternative. On 19 February 2010, the 537th anniversary of Copernicus' birth, IUPAC officially accepted the proposed name and symbol.[23][27]
Isotope |
Half-life [28] |
Decay mode[28] |
Discovery year |
Reaction |
---|---|---|---|---|
277Cn | 00000069 !0.69 ms | α | 1996 | 208Pb(70Zn,n) |
278Cn | 000010 !10? ms | α, SF ? | unknown | — |
279Cn | 0000002 !0.2? ms[29] | α, SF ? | unknown | — |
280Cn | 0000005 !0.5? ms[29] | α, SF ? | unknown | — |
281Cn | 000097 !97 ms | α | 2010 | 285Fl(—,α) |
282Cn | 0000008 !0.8 ms | SF | 2004 | 238U(48Ca,4n) |
283Cn | 004 !4 s | α, SF | 2002 | 238U(48Ca,3n) |
284Cn | 000097 !97 ms | α, SF | 2002 | 288Fl(—,α) |
285Cn | 029 !29 s | α | 1999 | 289Fl(—,α) |
286Cn | 008 !8.45 s ? | SF | 2016 | 294Lv(—,2α) |
Copernicium has no stable or naturally occurring isotopes. Several radioactive isotopes have been synthesized in the laboratory, either by fusing two atoms or by observing the decay of heavier elements. Seven different isotopes have been reported with atomic masses from 281 to 286, and 277. Most of these decay predominantly through alpha decay, but some undergo spontaneous fission.[28]
The isotope copernicium-283 was instrumental in the confirmation of the discoveries of the elements flerovium and livermorium.[30]
All copernicium isotopes are extremely unstable and radioactive; in general, heavier isotopes are more stable than the lighter. The most stable isotope, 285Cn, has a half-life of 29 seconds; 283Cn has a half-life of 4 seconds, and the unconfirmed 286Cn has a half-life of about 8.45 seconds. Other isotopes have half-lives shorter than 0.1 seconds. 281Cn and 284Cn both have half-lives of 97 ms, and the other two isotopes have half-lives slightly under one millisecond.[28] It is predicted that the heavy isotopes 291Cn and 293Cn may have half-lives longer than a few decades, and may have been produced in the r-process and be detectable in cosmic rays, though they would be about 10−12 times as abundant as lead.[31]
The lightest isotopes of copernicium have been synthesized by direct fusion between two lighter nuclei and as decay products (except for 277Cn, which is not known to be a decay product), while the heavier isotopes are only known to be produced by decay of heavier nuclei. The heaviest isotope produced by direct fusion is 283Cn; the three heavier isotopes, 284Cn, 285Cn, and 286Cn, have only been observed as decay products of elements with larger atomic numbers.[28] In 1999, American scientists at the University of California, Berkeley, announced that they had succeeded in synthesizing three atoms of 293Og.[32] These parent nuclei were reported to have successively emitted three alpha particles to form copernicium-281 nuclei, which were claimed to have undergone an alpha decay, emitting an alpha particle with decay energy of 10.68 MeV and half-life 0.90 ms, but their claim was retracted in 2001.[33] The isotope, however, was produced in 2010 by the same team. The new data contradicted the previous (fabricated)[34] data.[35]
Copernicium is the tenth and last member of the 6d series and is the heaviest group 12 element in the periodic table, below zinc, cadmium and mercury. It is predicted to differ significantly from the lighter group 12 elements. The valence s-subshells of the group 12 elements and period 7 elements are expected to be relativistically contracted most strongly at copernicium. This and the closed-shell configuration of copernicium result in it probably being a very noble metal. Its metallic bonds should also be very weak, possibly making it extremely volatile, like the noble gases, and potentially making it gaseous at room temperature.[1][36] However, it should be able to form metal–metal bonds with copper, palladium, platinum, silver, and gold; these bonds are predicted to be only about 15–20 kJ/mol weaker than the analogous bonds with mercury.[1]
Once copernicium is ionized, its chemistry may present several differences from those of zinc, cadmium, and mercury. Due to the stabilization of 7s electronic orbitals and destabilization of 6d ones caused by relativistic effects, Cn2+ is likely to have a [Rn]5f146d87s2 electronic configuration, using the 6d orbitals before the 7s one, unlike its homologues. The fact that the 6d electrons participate more readily in chemical bonding means that once copernicium is ionized, it may behave more like a transition metal than its lighter homologues, especially in the possible +4 oxidation state. In aqueous solutions, copernicium may form the +2 and perhaps +4 oxidation states.[1] The diatomic ion Hg2+
2, featuring mercury in the +1 oxidation state, is well-known, but the Cn2+
2 ion is predicted to be unstable or even non-existent.[1] Copernicium(II) fluoride, CnF2, should be more unstable than the analogous mercury compound, mercury(II) fluoride (HgF2), and may even decompose spontaneously into its constituent elements. In polar solvents, copernicium is predicted to preferentially form the CnF−
5 and CnF−
3 anions rather than the analogous neutral fluorides (CnF4 and CnF2, respectively), although the analogous bromide or iodide ions may be more stable towards hydrolysis in aqueous solution. The anions CnCl2−
4 and CnBr2−
4 should also be able to exist in aqueous solution.[1] Nevertheless, more recent experiments have casted doubt on the possible existence of HgF4, and indeed more recent calculations suggest that both HgF4 and CnF4 are actually unbound and of doubtful existence.[37] Analogous to mercury(II) cyanide (Hg(CN)2), copernicium is expected to form a stable cyanide, Cn(CN)2.[38]
Copernicium should be a very heavy metal with a density of around 23.7 g/cm3 in the solid state; in comparison, the most dense known element that has had its density measured, osmium, has a density of only 22.61 g/cm3. This results from copernicium's high atomic weight, the lanthanide and actinide contractions, and relativistic effects, although production of enough copernicium to measure this quantity would be impractical, and the sample would quickly decay.[1] However, some calculations predict copernicium to be a gas at room temperature, the first gaseous metal in the periodic table[1][36] (the second being flerovium), due to the closed-shell electron configurations of copernicium and flerovium.[39] The atomic radius of copernicium is expected to be around 147 pm. Due to the relativistic stabilization of the 7s orbital and destabilization of the 6d orbital, the Cn+ and Cn2+ ions are predicted to give up 6d electrons instead of 7s electrons, which is the opposite of the behavior of its lighter homologues.[1]
In addition to the relativistic contraction and binding of the 7s subshell, the 6d5/2 orbital is expected to be destabilized due to spin-orbit coupling, making it behave similarly to the 7s orbital in terms of size, shape, and energy. Hence copernicium may not be a noble metal, but rather a semiconductor[3] with a band gap of around 0.2 eV.[7] Copernicium is expected to crystallize in the hexagonal close-packed crystal structure, with lattice parameters a = 332 pm and c = 540 pm. The c/a ratio of 1.63 is the ideal value, establishing a kinship between solid copernicium and the solid noble gases, though its cohesive energy (enthalpy of crystallization) should be on the order of that of mercury rather than be near the lower value of the noble gases.[7]
Interest in copernicium's chemistry was sparked by predictions that it would have the largest relativistic effects in the whole of period 7 and group 12, and indeed among all 118 known elements.[1] Copernicium has the ground state electron configuration [Rn]5f146d107s2 and thus should belong to group 12 of the periodic table, according to the Aufbau principle. As such, it should behave as the heavier homologue of mercury and form strong binary compounds with noble metals like gold. Experiments probing the reactivity of copernicium have focused on the adsorption of atoms of element 112 onto a gold surface held at varying temperatures, in order to calculate an adsorption enthalpy. Owing to relativistic stabilization of the 7s electrons, copernicium shows radon-like properties. Experiments were performed with the simultaneous formation of mercury and radon radioisotopes, allowing a comparison of adsorption characteristics.[40]
The first chemical experiments on copernicium were conducted using the 238U(48Ca,3n)283Cn reaction. Detection was by spontaneous fission of the claimed parent isotope with half-life of 5 minutes. Analysis of the data indicated that copernicium was more volatile than mercury and had noble gas properties. However, the confusion regarding the synthesis of copernicium-283 has cast some doubt on these experimental results. Given this uncertainty, between April–May 2006 at the JINR, a FLNR–PSI team conducted experiments probing the synthesis of this isotope as a daughter in the nuclear reaction 242Pu(48Ca,3n)287Fl. In this experiment, two atoms of copernicium-283 were unambiguously identified and the adsorption properties indicated that copernicium is a more volatile homologue of mercury, due to formation of a weak metal-metal bond with gold, placing it firmly in group 12.[40]
In April 2007, this experiment was repeated and a further three atoms of copernicium-283 were positively identified. The adsorption property was confirmed and indicated that copernicium has adsorption properties completely in agreement with being the heaviest member of group 12.[40] These experiments also allowed the first experimental estimation of copernicium's boiling point: 84+112
−108 °C, so that it may be a gas at standard conditions.[3]
Because the lighter group 12 elements often occur as chalcogenide ores, experiments were conducted in 2015 to attempt to deposit copernicium atoms on a selenium surface to form copernicium selenide, CnSe. Reaction of copernicium atoms with trigonal selenium to form a selenide were observed, with ΔHadsCn(t-Se) > 48 kJ/mol, with the kinetic hindrance towards selenide formation being lower for copernicium than for mercury. This was unexpected as the stability of the group 12 selenides tends to decrease down the group from ZnSe to HgSe, while it increases down the group for the group 14 selenides from GeSe to PbSe.[41]
This article uses material from the Wikipedia article "Copernicium", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Element