powered by CADENAS

Social Share

Osmium (22487 views - Periodic Table Of Elements)

Osmium (from Greek ὀσμή osme, "smell") is a chemical element with symbol Os and atomic number 76. It is a hard, brittle, bluish-white transition metal in the platinum group that is found as a trace element in alloys, mostly in platinum ores. Osmium is the densest naturally occurring element, with a density of 22.59 g/cm3. Its alloys with platinum, iridium, and other platinum-group metals are employed in fountain pen nib tipping, electrical contacts, and other applications where extreme durability and hardness are needed.
Go to Article

Osmium

Osmium

Osmium,  76Os
General properties
Pronunciation /ˈɒzmiəm/
OZ-mee-əm
Appearance silvery, blue cast
Standard atomic weight (Ar) 190.23(3)[1]
Osmium in the periodic table
Ru

Os

Hs
rheniumosmiumiridium
Atomic number (Z) 76
Group, period group 8, period 6
Block d-block
Element category   transition metal
Electron configuration [Xe] 4f14 5d6 6s2
Electrons per shell
2, 8, 18, 32, 14, 2
Physical properties
Spectral lines
Phase (at STP) solid
Melting point 3306 K ​(3033 °C, ​5491 °F)
Boiling point 5285 K ​(5012 °C, ​9054 °F)
Density (near r.t.) 22.59 g/cm3
when liquid (at m.p.) 20 g/cm3
Heat of fusion 31 kJ/mol
Heat of vaporization 378 kJ/mol
Molar heat capacity 24.7 J/(mol·K)
Vapor pressure
P (Pa) 1 10 100 1 k 10 k 100 k
at T (K) 3160 3423 3751 4148 4638 5256
Atomic properties
Oxidation states 8, 7, 6, 5, 4, 3, 2, 1, 0, −1, −2, −4 ​(a mildly acidic oxide)
Electronegativity Pauling scale: 2.2
Ionization energies
  • 1st: 840 kJ/mol
  • 2nd: 1600 kJ/mol
Atomic radius empirical: 135 pm
Covalent radius 144±4 pm
Miscellanea
Crystal structurehexagonal close-packed (hcp)
Speed of sound thin rod 4940 m/s (at 20 °C)
Thermal expansion 5.1 µm/(m·K) (at 25 °C)
Thermal conductivity 87.6 W/(m·K)
Electrical resistivity 81.2 nΩ·m (at 0 °C)
Magnetic ordering paramagnetic[2]
Magnetic susceptibility +9.9·10−6 cm3/mol (298 K)[3]
Shear modulus 222 GPa
Bulk modulus 462 GPa
Poisson ratio 0.25
Mohs hardness 7.0
Brinell hardness 3490–4000 MPa
CAS Number 7440-04-2
History
Discovery and first isolation Smithson Tennant (1803)
Main isotopes of osmium
Iso­tope Abun­dance Half-life (t1/2) Decay mode Pro­duct
184Os 0.02% stable
185Os syn 93.6 d ε 185Re
186Os 1.59% 2.0×1015 y α 182W
187Os 1.96% stable
188Os 13.24% stable
189Os 16.15% stable
190Os 26.26% stable
191Os syn 15.4 d β 191Ir
192Os 40.78% stable
193Os syn 30.11 d β 193Ir
194Os syn 6 y β 194Ir
| references | in Wikidata

Osmium (from Greek ὀσμή osme, "smell") is a chemical element with symbol Os and atomic number 76. It is a hard, brittle, bluish-white transition metal in the platinum group that is found as a trace element in alloys, mostly in platinum ores. Osmium is the densest naturally occurring element, with a density of 22.59 g/cm3. Its alloys with platinum, iridium, and other platinum-group metals are employed in fountain pen nib tipping, electrical contacts, and other applications where extreme durability and hardness are needed.[4]

Characteristics

Physical properties

Osmium, remelted pellet

Osmium has a blue-gray tint and is the densest stable element, approximately twice the density of lead[5] and slightly denser than iridium.[6] Calculations of density from the X-ray diffraction data may produce the most reliable data for these elements, giving a value of 22.562±0.009 g/cm3 for iridium versus 22.587±0.009 g/cm3 for osmium.[7]

Osmium is a hard but brittle metal that remains lustrous even at high temperatures. It has a very low compressibility. Correspondingly, its bulk modulus is extremely high, reported between 395 and 462 GPa, which rivals that of diamond (443 GPa). The hardness of osmium is moderately high at 4 GPa.[8][9][10] Because of its hardness, brittleness, low vapor pressure (the lowest of the platinum-group metals), and very high melting point (the fourth highest of all elements, after only carbon, tungsten, and rhenium), solid osmium is difficult to machine, form, or work.

Chemical properties

Oxidation states of osmium
−2 Na
2
[Os(CO)
4
]
−1 Na
2
[Os
4
(CO)
13
]
0 Os
3
(CO)
12
+1 OsI
+2 OsI
2
+3 OsBr
3
+4 OsO
2
, OsCl
4
+5 OsF
5
+6 OsF
6
+7 OsOF
5
+8 OsO
4
, Os(NCH3)
4

Osmium forms compounds with oxidation states ranging from −2 to +8. The most common oxidation states are +2, +3, +4, and +8. The +8 oxidation state is notable for being the highest attained by any chemical element aside from iridium's +9[11] and is encountered only in xenon,[12][13] ruthenium,[14] hassium,[15] and iridium.[16] The oxidation states −1 and −2 represented by the two reactive compounds Na
2
[Os
4
(CO)
13
]
and Na
2
[Os(CO)
4
]
are used in the synthesis of osmium cluster compounds.[17][18]

The most common compound exhibiting the +8 oxidation state is osmium tetroxide. This toxic compound is formed when powdered osmium is exposed to air. It is a very volatile, water-soluble, pale yellow, crystalline solid with a strong smell. Osmium powder has the characteristic smell of osmium tetroxide.[19] Osmium tetroxide forms red osmates OsO
4
(OH)2−
2
upon reaction with a base. With ammonia, it forms the nitrido-osmates OsO
3
N
.[20][21][22] Osmium tetroxide boils at 130 °C and is a powerful oxidizing agent. By contrast, osmium dioxide (OsO2) is black, non-volatile, and much less reactive and toxic.

Only two osmium compounds have major applications: osmium tetroxide for staining tissue in electron microscopy and for the oxidation of alkenes in organic synthesis, and the non-volatile osmates for organic oxidation reactions.[23]

Osmium pentafluoride (OsF5) is known, but osmium trifluoride (OsF3) has not yet been synthesized. The lower oxidation states are stabilized by the larger halogens, so that the trichloride, tribromide, triiodide, and even diiodide are known. The oxidation state +1 is known only for osmium iodide (OsI), whereas several carbonyl complexes of osmium, such as triosmium dodecacarbonyl (Os
3
(CO)
12
), represent oxidation state 0.[20][21][24][25]

In general, the lower oxidation states of osmium are stabilized by ligands that are good σ-donors (such as amines) and π-acceptors (heterocycles containing nitrogen). The higher oxidation states are stabilized by strong σ- and π-donors, such as O2−
and N3−
.[26]

Despite its broad range of compounds in numerous oxidation states, osmium in bulk form at ordinary temperatures and pressures resists attack by all acids and alkalis, including aqua regia.[27]

Isotopes

Osmium has seven naturally occurring isotopes, six of which are stable: 184
Os
, 187
Os
, 188
Os
, 189
Os
, 190
Os
, and (most abundant) 192
Os
. 186
Os
undergoes alpha decay with such a long half-life (2.0±1.1)×1015 years, approximately 140 000 times the age of the universe, that for practical purposes it can be considered stable. Alpha decay is predicted for all seven naturally occurring isotopes, but it has been observed only for 186
Os
, presumably due to very long half-lives. It is predicted that 184
Os
and 192
Os
can undergo double beta decay but this radioactivity has not been observed yet.[28]

187
Os
is the daughter of 187
Re
(half-life 4.56×1010 years) and is used extensively in dating terrestrial as well as meteoric rocks (see rhenium-osmium dating). It has also been used to measure the intensity of continental weathering over geologic time and to fix minimum ages for stabilization of the mantle roots of continental cratons. This decay is a reason why rhenium-rich minerals are abnormally rich in 187
Os
.[29] However, the most notable application of Os isotopes in geology has been in conjunction with the abundance of iridium, to characterise the layer of shocked quartz along the Cretaceous–Paleogene boundary that marks the extinction of the dinosaurs 66 million years ago.[30]

History

Osmium was discovered in 1803 by Smithson Tennant and William Hyde Wollaston in London, England.[31] The discovery of osmium is intertwined with that of platinum and the other metals of the platinum group. Platinum reached Europe as platina ("small silver"), first encountered in the late 17th century in silver mines around the Chocó Department, in Colombia.[32] The discovery that this metal was not an alloy, but a distinct new element, was published in 1748.[33] Chemists who studied platinum dissolved it in aqua regia (a mixture of hydrochloric and nitric acids) to create soluble salts. They always observed a small amount of a dark, insoluble residue.[27] Joseph Louis Proust thought that the residue was graphite.[27] Victor Collet-Descotils, Antoine François, comte de Fourcroy, and Louis Nicolas Vauquelin also observed iridium the black platinum residue in 1803, but did not obtain enough material for further experiments.[27] Later the two French chemists Antoine-François Fourcroy and Nicolas-Louis Vauquelin identified a metal in a platinum residue they called ‘ptène’.[34]

In 1803, Smithson Tennant analyzed the insoluble residue and concluded that it must contain a new metal. Vauquelin treated the powder alternately with alkali and acids[35] and obtained a volatile new oxide, which he believed to be of this new metal—which he named ptene, from the Greek word πτηνος (ptènos) for winged.[36][37] However, Tennant, who had the advantage of a much larger amount of residue, continued his research and identified two previously undiscovered elements in the black residue, iridium and osmium.[27][35] He obtained a yellow solution (probably of cis–[Os(OH)2O4]2−) by reactions with sodium hydroxide at red heat. After acidification he was able to distill the formed OsO4.[36] He named it osmium after Greek osme meaning "a smell", because of the ashy and smoky smell of the volatile osmium tetroxide.[38] Discovery of the new elements was documented in a letter to the Royal Society on June 21, 1804.[27][39]

Uranium and osmium were early successful catalysts in the Haber process, the nitrogen fixation reaction of nitrogen and hydrogen to produce ammonia, giving enough yield to make the process economically successful. At the time, a group at BASF led by Carl Bosch bought most of the world's supply of osmium to use as a catalyst. Shortly thereafter, in 1908, cheaper catalysts based on iron and iron oxides were introduced by the same group for the first pilot plants, removing the need for the expensive and rare osmium.[40]

Nowadays osmium is obtained primarily from the processing of platinum and nickel ores.[41]

Occurrence

Although osmium is one of the even-numbered elements, which puts it in the upper half of elements commonly found in space, osmium is the least abundant stable element in Earth's crust with an average mass fraction of 50 parts per trillion in the continental crust.[42]

Osmium is found in nature as an uncombined element or in natural alloys; especially the iridium–osmium alloys, osmiridium (osmium rich), and iridosmium (iridium rich).[35] In nickel and copper deposits, the platinum group metals occur as sulfides (i.e., (Pt,Pd)S)), tellurides (e.g., PtBiTe), antimonides (e.g., PdSb), and arsenides (e.g., PtAs2); in all these compounds platinum is exchanged by a small amount of iridium and osmium. As with all of the platinum group metals, osmium can be found naturally in alloys with nickel or copper.[43]

Within Earth's crust, osmium, like iridium, is found at highest concentrations in three types of geologic structure: igneous deposits (crustal intrusions from below), impact craters, and deposits reworked from one of the former structures. The largest known primary reserves are in the Bushveld igneous complex in South Africa,[44] though the large copper–nickel deposits near Norilsk in Russia, and the Sudbury Basin in Canada are also significant sources of osmium. Smaller reserves can be found in the United States.[44] The alluvial deposits used by pre-Columbian people in the Chocó Department, Colombia are still a source for platinum group metals. The second large alluvial deposit was found in the Ural Mountains, Russia, which is still mined.[41][45]

Production

Osmium is obtained commercially as a by-product from nickel and copper mining and processing. During electrorefining of copper and nickel, noble metals such as silver, gold and the platinum group metals, together with non-metallic elements such as selenium and tellurium settle to the bottom of the cell as anode mud, which forms the starting material for their extraction.[46][47] In order to separate the metals, they must first be brought into solution. Several methods are available depending on the separation process and the composition of the mixture; two representative methods are fusion with sodium peroxide followed by dissolution in aqua regia, and dissolution in a mixture of chlorine with hydrochloric acid.[44][48] Osmium, ruthenium, rhodium and iridium can be separated from platinum, gold and base metals by their insolubility in aqua regia, leaving a solid residue. Rhodium can be separated from the residue by treatment with molten sodium bisulfate. The insoluble residue, containing Ru, Os and Ir, is treated with sodium oxide, in which Ir is insoluble, producing water-soluble Ru and Os salts. After oxidation to the volatile oxides, RuO
4
is separated from OsO
4
by precipitation of (NH4)3RuCl6 with ammonium chloride.

After it is dissolved, osmium is separated from the other platinum group metals by distillation or extraction with organic solvents of the volatile osmium tetroxide.[49] The first method is similar to the procedure used by Tennant and Wollaston. Both methods are suitable for industrial scale production. In either case, the product is reduced using hydrogen, yielding the metal as a powder or sponge that can be treated using powder metallurgy techniques.[50]

Neither the producers nor the United States Geological Survey published any production amounts for osmium. Estimations of the United States consumption date published from 1971,[51] which gives a consumption in the United States of 2000 troy ounces (62 kg), would suggest that the production is still less than 1 ton per year. In 2012, the estimated US production of osmium was 75 kg.[52]

Applications

Because of the volatility and extreme toxicity of its oxide, osmium is rarely used in its pure state, but is instead often alloyed with other metals. Those alloys are utilized in high-wear applications. Osmium alloys such as osmiridium are very hard and, along with other platinum-group metals, are used in the tips of fountain pens, instrument pivots, and electrical contacts, as they can resist wear from frequent operation. They were also used for the tips of phonograph styli during the late 78 rpm and early "LP" and "45" record era, circa 1945 to 1955. Although very durable compared to steel and chromium needle points, osmium-alloy tips wore out far more rapidly than competing, and costlier, sapphire and diamond tips and were discontinued.[53]

Osmium tetroxide has been used in fingerprint detection[54] and in staining fatty tissue for optical and electron microscopy. As a strong oxidant, it cross-links lipids mainly by reacting with unsaturated carbon–carbon bonds and thereby both fixes biological membranes in place in tissue samples and simultaneously stains them. Because osmium atoms are extremely electron-dense, osmium staining greatly enhances image contrast in transmission electron microscopy (TEM) studies of biological materials. Those carbon materials have otherwise very weak TEM contrast (see image).[23] Another osmium compound, osmium ferricyanide (OsFeCN), exhibits similar fixing and staining action.[55]

The tetroxide and a related compound potassium osmate are important oxidants for chemical synthesis, despite being very poisonous. For the Sharpless asymmetric dihydroxylation, which uses osmate for the conversion of a double bond into a vicinal diol, Karl Barry Sharpless won the Nobel Prize in Chemistry in 2001.[56][57] OsO4 is very expensive for this use, so KMnO4 is often used instead, even though the yields are less for this cheaper chemical reagent.[58]

In 1898 an Austrian chemist Auer von Welsbach developed the Oslamp with a filament made of osmium, which he introduced commercially in 1902. After only a few years, osmium was replaced by the more stable metal tungsten. Tungsten has the highest melting point among all metals, and its use in light bulbs increases the luminous efficacy and life of incandescent lamps.[36]

The light bulb manufacturer Osram (founded in 1906, when three German companies, Auer-Gesellschaft, AEG and Siemens & Halske, combined their lamp production facilities) derived its name from the elements of osmium and Wolfram (the latter is German for tungsten).[59]

Like palladium, powdered osmium effectively absorbs hydrogen atoms. This could make osmium a potential candidate for a metal-hydride battery electrode. However, osmium is expensive and would react with potassium hydroxide, the most common battery electrolyte.[60]

Osmium has high reflectivity in the ultraviolet range of the electromagnetic spectrum; for example, at 600 Å osmium has a reflectivity twice that of gold.[61] This high reflectivity is desirable in space-based UV spectrometers, which have reduced mirror sizes due to space limitations. Osmium-coated mirrors were flown in several space missions aboard the Space Shuttle, but it soon became clear that the oxygen radicals in the low Earth orbit are abundant enough to significantly deteriorate the osmium layer.[62]

The only known clinical use of osmium appears to be for synovectomy in arthritic patients in Scandinavia.[63] It involves the local administration of osmium tetroxide (OsO4), which is a highly toxic compound. The lack of reports of long-term side effects suggest that osmium itself can be biocompatible, although this depends on the osmium compound administered. In 2011, osmium(VI)[64] and osmium(II)[65] compounds were reported to show anticancer activity in vivo, it indicated a promising future for using osmium compounds as anticancer drugs.[66]

Precautions

Finely divided metallic osmium is pyrophoric[51] and reacts with oxygen at room temperature, forming volatile osmium tetroxide. Some osmium compounds are also converted to the tetroxide if oxygen is present.[51] This makes osmium tetroxide the main source of contact with the environment.

Osmium tetroxide is highly volatile and penetrates skin readily, and is very toxic by inhalation, ingestion, and skin contact.[69] Airborne low concentrations of osmium tetroxide vapor can cause lung congestion and skin or eye damage, and should therefore be used in a fume hood.[19] Osmium tetroxide is rapidly reduced to relatively inert compounds by polyunsaturated vegetable oils, such as corn oil.[70]

Price

Osmium is usually sold as a minimum 99.9% pure powder. Like other precious metals, it is measured by troy weight and by grams. Its price in 2012 was about $400 per troy ounce (or about $13,000 per kilogram), depending on the quantity and its supplier.[71][72]

  1. ^ Meija, J.; et al. (2016). "Atomic weights of the elements 2013 (IUPAC Technical Report)". Pure Appl. Chem. 88 (3): 265–91. doi:10.1515/pac-2015-0305. 
  2. ^ Lide, D. R., ed. (2005). "Magnetic susceptibility of the elements and inorganic compounds". CRC Handbook of Chemistry and Physics (PDF) (86th ed.). Boca Raton (FL): CRC Press. ISBN 0-8493-0486-5. 
  3. ^ Weast, Robert (1984). CRC, Handbook of Chemistry and Physics. Boca Raton, Florida: Chemical Rubber Company Publishing. pp. E110. ISBN 0-8493-0464-4. 
  4. ^ Hammond "Osmium", C. R., p. 4–25 in Lide, D. R., ed. (2005). CRC Handbook of Chemistry and Physics (86th ed.). Boca Raton (FL): CRC Press. ISBN 0-8493-0486-5. 
  5. ^ Lide 2004, pp. 4-39—4–96.
  6. ^ Arblaster, J. W. (1989). "Densities of osmium and iridium: recalculations based upon a review of the latest crystallographic data" (PDF). Platinum Metals Review. 33 (1): 14–16. 
  7. ^ Arblaster, J. W. (1995). "Osmium, the Densest Metal Known". Platinum Metals Review. 39 (4): 164. 
  8. ^ Weinberger, Michelle; Tolbert, Sarah; Kavner, Abby (2008). "Osmium Metal Studied under High Pressure and Nonhydrostatic Stress". Phys. Rev. Lett. 100 (4): 045506. Bibcode:2008PhRvL.100d5506W. PMID 18352299. doi:10.1103/PhysRevLett.100.045506. 
  9. ^ Cynn, Hyunchae; Klepeis, J. E.; Yeo, C. S.; Young, D. A. (2002). "Osmium has the Lowest Experimentally Determined Compressibility". Physical Review Letters. 88 (13): 135701. Bibcode:2002PhRvL..88m5701C. PMID 11955108. doi:10.1103/PhysRevLett.88.135701. 
  10. ^ Sahu, B. R.; Kleinman, L. (2005). "Osmium Is Not Harder Than Diamond". Physical Review B. 72 (11): 113106. Bibcode:2005PhRvB..72k3106S. doi:10.1103/PhysRevB.72.113106. 
  11. ^ "Iridium forms compound in +9 oxidation state". 
  12. ^ Selig, H.; Claassen, H. H.; Chernick, C. L.; Malm, J. G.; et al. (1964). "Xenon tetroxide – Preparation + Some Properties". Science. 143 (3612): 1322–3. Bibcode:1964Sci...143.1322S. JSTOR 1713238. PMID 17799234. doi:10.1126/science.143.3612.1322. 
  13. ^ Huston, J. L.; Studier, M. H.; Sloth, E. N. (1964). "Xenon tetroxide – Mass Spectrum". Science. 143 (3611): 1162–3. Bibcode:1964Sci...143.1161H. JSTOR 1712675. PMID 17833897. doi:10.1126/science.143.3611.1161-a. 
  14. ^ Barnard, C. F. J. (2004). "Oxidation States of Ruthenium and Osmium". Platinum Metals Review. 48 (4): 157. doi:10.1595/147106704X10801. 
  15. ^ "Chemistry of Hassium" (PDF). Gesellschaft für Schwerionenforschung mbH. 2002. Retrieved 2007-01-31. 
  16. ^ Gong, Yu; Zhou, Mingfei; Kaupp, Martin; Riedel, Sebastian (2009). "Formation and Characterization of the Iridium Tetroxide Molecule with Iridium in the Oxidation State +VIII". Angewandte Chemie International Edition. 48 (42): 7879. doi:10.1002/anie.200902733. 
  17. ^ Krause, J.; Siriwardane, Upali; Salupo, Terese A.; Wermer, Joseph R.; et al. (1993). "Preparation of [Os3(CO)11]2− and its reactions with Os3(CO)12; structures of [Et4N] [HOs3(CO)11] and H2OsS4(CO)". Journal of Organometallic Chemistry. 454: 263–271. doi:10.1016/0022-328X(93)83250-Y. 
  18. ^ Carter, Willie J.; Kelland, John W.; Okrasinski, Stanley J.; Warner, Keith E.; et al. (1982). "Mononuclear hydrido alkyl carbonyl complexes of osmium and their polynuclear derivatives". Inorganic Chemistry. 21 (11): 3955–3960. doi:10.1021/ic00141a019. 
  19. ^ a b Mager Stellman, J. (1998). "Osmium". Encyclopaedia of Occupational Health and Safety. International Labour Organization. p. 63.34. ISBN 978-92-2-109816-4. OCLC 35279504. 
  20. ^ a b Holleman, A. F.; Wiberg, E.; Wiberg, N. (2001). Inorganic Chemistry (1st ed.). Academic Press. ISBN 0-12-352651-5. OCLC 47901436. 
  21. ^ a b Griffith, W. P. (1965). "Osmium and its compounds". Quarterly Review of the Chemical Society. 19 (3): 254–273. doi:10.1039/QR9651900254. 
  22. ^ Subcommittee on Platinum-Group Metals, Committee on Medical and Biologic Effects of Environmental Pollutants, Division of Medical Sciences, Assembly of Life Sciences, National Research Council (1977). Platinum-group metals. National Academy of Sciences. p. 55. ISBN 0-309-02640-7. 
  23. ^ a b Bozzola, John J.; Russell, Lonnie D. (1999). "Specimen Preparation for Transmission Electron Microscopy". Electron microscopy : principles and techniques for biologists. Sudbury, Mass.: Jones and Bartlett. pp. 21–31. ISBN 978-0-7637-0192-5. 
  24. ^ Greenwood, N. N.; Earnshaw, A. (1997). Chemistry of the Elements (2nd ed.). Oxford:Butterworth-Heinemann. pp. 1113–1143, 1294. ISBN 0-7506-3365-4. OCLC 213025882. 
  25. ^ Gulliver, D. J; Levason, W. (1982). "The chemistry of ruthenium, osmium, rhodium, iridium, palladium and platinum in the higher oxidation states". Coordination Chemistry Reviews. 46: 1–127. doi:10.1016/0010-8545(82)85001-7. 
  26. ^ Peter A. Lay; W. Dean Harman (1992). Advances in Inorganic Chemistry. A. G. Sykes. Academic Press. p. 221. ISBN 0-12-023637-0. 
  27. ^ a b c d e f Hunt, L. B. (1987). "A History of Iridium" (PDF). Platinum Metals Review. 31 (1): 32–41. Retrieved 2012-03-15. 
  28. ^ Audi, G.; Bersillon, O.; Blachot, J.; Wapstra, A. H. (2003). "The NUBASE Evaluation of Nuclear and Decay Properties". Nuclear Physics A. Atomic Mass Data Center. 729: 3–128. Bibcode:2003NuPhA.729....3A. doi:10.1016/j.nuclphysa.2003.11.001. 
  29. ^ Dąbek, Józef; Halas, Stanislaw (2007). "Physical Foundations of Rhenium-Osmium Method – A Review". Geochronometria. 27: 23–26. doi:10.2478/v10003-007-0011-4. 
  30. ^ Alvarez, L. W.; Alvarez, W.; Asaro, F.; Michel, H. V. (1980). "Extraterrestrial cause for the Cretaceous–Tertiary extinction". Science. 208 (4448): 1095–1108. Bibcode:1980Sci...208.1095A. PMID 17783054. doi:10.1126/science.208.4448.1095. 
  31. ^ Venetskii, S. I. (1974). "Osmium". Metallurgist. 18 (2): 155–157. doi:10.1007/BF01132596. 
  32. ^ McDonald, M. (959). "The Platinum of New Granada: Mining and Metallurgy in the Spanish Colonial Empire". Platinum Metals Review. 3 (4): 140–145. 
  33. ^ Juan, J.; de Ulloa, A. (1748). Relación histórica del viage a la América Meridional (in Spanish). 1. p. 606. 
  34. ^ Haubrichs, Rolf; Zaffalon, Pierre-Leonard (2017). "Osmium vs. ‘Ptène’: The Naming of the Densest Metal". Johnson Matthey Technology Review. 61. doi:10.1595/205651317x695631. 
  35. ^ a b c Emsley, J. (2003). "Osmium". Nature's Building Blocks: An A-Z Guide to the Elements. Oxford, England, UK: Oxford University Press. pp. 199–201. ISBN 0-19-850340-7. 
  36. ^ a b c Griffith, W. P. (2004). "Bicentenary of Four Platinum Group Metals. Part II: Osmium and iridium – events surrounding their discoveries". Platinum Metals Review. 48 (4): 182–189. doi:10.1595/147106704X4844. 
  37. ^ Thomson, T. (1831). A System of Chemistry of Inorganic Bodies. Baldwin & Cradock, London; and William Blackwood, Edinburgh. p. 693. 
  38. ^ Weeks, M. E. (1968). Discovery of the Elements (7 ed.). Journal of Chemical Education. pp. 414–418. ISBN 0-8486-8579-2. OCLC 23991202. 
  39. ^ Tennant, S. (1804). "On Two Metals, Found in the Black Powder Remaining after the Solution of Platina". Philosophical Transactions of the Royal Society. 94: 411–418. JSTOR 107152. doi:10.1098/rstl.1804.0018. 
  40. ^ Smil, Vaclav (2004). Enriching the Earth: Fritz Haber, Carl Bosch, and the Transformation of World Food Production. MIT Press. pp. 80–86. ISBN 978-0-262-69313-4. 
  41. ^ a b George, Micheal W. "2006 Minerals Yearbook: Platinum-Group Metals" (PDF). United States Geological Survey USGS. Retrieved 2008-09-16. 
  42. ^ Wedepohl, Hans K (1995). "The composition of the continental crust". Geochimica et Cosmochimica Acta. 59 (7): 1217–1232. Bibcode:1995GeCoA..59.1217W. doi:10.1016/0016-7037(95)00038-2. 
  43. ^ Xiao, Z.; Laplante, A. R. (2004). "Characterizing and recovering the platinum group minerals—a review". Minerals Engineering. 17 (9–10): 961–979. doi:10.1016/j.mineng.2004.04.001. 
  44. ^ a b c Seymour, R. J.; O'Farrelly, J. I. (2001). "Platinum-group metals". Kirk Othmer Encyclopedia of Chemical Technology. Wiley. doi:10.1002/0471238961.1612012019052513.a01.pub2. 
  45. ^ "Commodity Report: Platinum-Group Metals" (PDF). United States Geological Survey USGS. Retrieved 2008-09-16. 
  46. ^ George, M. W. (2008). "Platinum-group metals" (PDF). U.S. Geological Survey Mineral Commodity Summaries. USGS Mineral Resources Program. 
  47. ^ George, M. W. 2006 Minerals Yearbook: Platinum-Group Metals (PDF). United States Geological Survey USGS. Retrieved 2008-09-16. 
  48. ^ Renner, H.; Schlamp, G.; Kleinwächter, I.; Drost, E.; et al. (2002). "Platinum group metals and compounds". Ullmann's Encyclopedia of Industrial Chemistry. Wiley. doi:10.1002/14356007.a21_075. 
  49. ^ Gilchrist, Raleigh (1943). "The Platinum Metals". Chemical Reviews. 32 (3): 277–372. doi:10.1021/cr60103a002. 
  50. ^ Hunt, L. B.; Lever, F. M. (1969). "Platinum Metals: A Survey of Productive Resources to industrial Uses" (PDF). Platinum Metals Review. 13 (4): 126–138. Retrieved 2008-10-02. 
  51. ^ a b c Smith, Ivan C.; Carson, Bonnie L.; Ferguson, Thomas L. (1974). "Osmium: An Appraisal of Environmental Exposure". Environmental Health Perspectives. 8: 201–213. JSTOR 3428200. PMC 1474945. PMID 4470919. doi:10.2307/3428200. 
  52. ^ "PLATINUM-GROUP METALS" (PDF). USGS. Retrieved 27 May 2013. 
  53. ^ Stephen D. Cramer & Bernard S. Covino, Jr. (2005). ASM Handbook Volume 13B. Corrosion: Materials. ASM International. ISBN 978-0-87170-707-9. 
  54. ^ MacDonell, Herbert L. (1960). "The Use of Hydrogen Fluoride in the Development of Latent Fingerprints Found on Glass Surfaces". The Journal of Criminal Law, Criminology, and Police Science. 51 (4): 465–470. JSTOR 1140672. doi:10.2307/1140672. 
  55. ^ Chadwick, D. (2002). Role of the sarcoplasmic reticulum in smooth muscle. John Wiley and Sons. pp. 259–264. ISBN 0-470-84479-5. 
  56. ^ Kolb, H. C.; Van Nieuwenhze, M. S.; Sharpless, K. B. (1994). "Catalytic Asymmetric Dihydroxylation". Chemical Reviews. 94 (8): 2483–2547. doi:10.1021/cr00032a009. 
  57. ^ Colacot, T. J. (2002). "2001 Nobel Prize in Chemistry" (PDF). Platinum Metals Review. 46 (2): 82–83. 
  58. ^ Osmium tetroxide as a reagent in organic chemistry — Master Organic Chemistry. Masterorganicchemistry.com. Retrieved on 2012-12-07.
  59. ^ Bowers, B., B. (2001). "Scanning our past from London: the filament lamp and new materials". Proceedings of the IEEE. 89 (3): 413–415. doi:10.1109/5.915382. 
  60. ^ Antonov, V. E.; Belash, I. T.; Malyshev, V. Yu.; Ponyatovsky, E. G. (1984). "The Solubility of Hydrogen in the Platinum Metals under High Pressure" (PDF). Platinum Metals Review. 28 (4): 158–163. 
  61. ^ Torr, Marsha R. (1985). "Osmium coated diffraction grating in the Space Shuttle environment: performance". Applied Optics. 24 (18): 2959. Bibcode:1985ApOpt..24.2959T. PMID 18223987. doi:10.1364/AO.24.002959. 
  62. ^ Gull, T. R.; Herzig, H.; Osantowski, J. F.; Toft, A. R. (1985). "Low earth orbit environmental effects on osmium and related optical thin-film coatings". Applied Optics. 24 (16): 2660. Bibcode:1985ApOpt..24.2660G. PMID 18223936. doi:10.1364/AO.24.002660. 
  63. ^ Sheppeard, H.; D. J. Ward (1980). "Intra-articular osmic acid in rheumatoid arthritis: five years' experience". Rheumatology. 19 (1): 25–29. PMID 7361025. doi:10.1093/rheumatology/19.1.25. 
  64. ^ Lau, T.-C; W.-X. Ni; W.-L. Man; M. T.-W. Cheung; et al. (2011). "Osmium(vi) complexes as a new class of potential anti-cancer agents". Chem. Commun. 47 (7): 2140–2142. doi:10.1039/C0CC04515B. 
  65. ^ Sadler, Peter; Steve D. Shnyder; Ying Fu; Abraha Habtemariam; et al. (2011). "Anti-colorectal cancer activity of an organometallic osmium arene azopyridine complex". Med. Chem. Commun. 2 (7): 666–668. doi:10.1039/C1MD00075F. 
  66. ^ Fu, Ying; Romero, María J.; Habtemariam, Abraha; et al. (2012). "The contrasting chemical reactivity of potent isoelectronic iminopyridine and azopyridine osmium(II) arene anticancer complexes". Chemical Science. 3 (8): 2485–2494. doi:10.1039/C2SC20220D. 
  67. ^ "Second LDEF post-retrieval symposium interim results of experiment A0034" (PDF). NASA. Retrieved 2009-06-06. 
  68. ^ Linton, Roger C.; Kamenetzky, Rachel R.; Reynolds, John M.; Burris, Charles L. (1992). "LDEF experiment A0034: Atomic oxygen stimulated outgassing". In NASA. Langley Research Center. NASA: 763. Bibcode:1992ldef.symp..763L. 
  69. ^ Luttrell, William E.; Giles, Cory B. (2007). "Toxic tips: Osmium tetroxide". Journal of Chemical Health and Safety. 14 (5): 40–41. doi:10.1016/j.jchas.2007.07.003. 
  70. ^ "How to Handle Osmium Tetroxide". University of California, San Diego. Archived from the original on February 21, 2006. Retrieved 2009-06-02. 
  71. ^ Osmium. Los Alamos National Laboratory's Chemistry Division
  72. ^ Live Osmium prices. TaxFreeGold.com. Accessed 6 April 2010



This article uses material from the Wikipedia article "Osmium", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Periodic Table Of Elements

Element