powered by CADENAS

Social Share

Dibutyl phthalate (16895 views - Material Database)

Dibutyl phthalate (DBP) is a commonly used plasticizer. It is also used as an additive to adhesives or printing inks. It is soluble in various organic solvents, e.g. in alcohol, ether and benzene. DBP is also used as an ectoparasiticide. DBP is also a putative endocrine disruptor
Go to Article

Dibutyl phthalate

Dibutyl phthalate

Dibutyl phthalate
Dibutyl phthalate
Names
Preferred IUPAC name
Dibutyl benzene-1,2-dicarboxylate
Other names
Dibutyl phthalate
Di-n-butyl phthalate
Butyl phthalate
n-Butyl phthalate
1,2-Benzenedicarboxylic acid dibutyl ester
o-Benzenedicarboxylic acid dibutyl ester
DBP
Palatinol C
Elaol
Dibutyl 1,2-benzene-dicarboxylate
Identifiers
3D model (JSmol)
ChEBI
ChemSpider
ECHA InfoCard 100.001.416
EC Number 201-557-4
KEGG
RTECS number TI0875000
UNII
Properties
C16H22O4
Molar mass 278.35 g·mol−1
Appearance Colorless to faint yellow oily liquid
Odor aromatic
Density 1.05 g/cm3 at 20 °C
Melting point −35 °C (−31 °F; 238 K)
Boiling point 340 °C (644 °F; 613 K)
13 mg/L (25 °C)
log P 4.72
Vapor pressure 0.00007 mmHg (20°C)[1]
-175.1·10−6 cm3/mol
Pharmacology
P03BX03 (WHO)
Hazards
Main hazards N), Harmful (Xi)
R-phrases (outdated) R50 R61 R62
S-phrases (outdated) S45 S53 S61
NFPA 704
Flammability code 1: Must be pre-heated before ignition can occur. Flash point over 93 °C (200 °F). E.g., canola oilHealth code 2: Intense or continued but not chronic exposure could cause temporary incapacitation or possible residual injury. E.g., chloroformReactivity code 0: Normally stable, even under fire exposure conditions, and is not reactive with water. E.g., liquid nitrogenSpecial hazards (white): no code
1
2
0
Flash point 157 °C (315 °F; 430 K) (closed cup)
402 °C (756 °F; 675 K)
Explosive limits 0.5 - 3.5%
Lethal dose or concentration (LD, LC):
5289 mg/kg (oral, mouse)
8000 mg/kg (oral, rat)
10,000 mg/kg (oral, guinea pig)[2]
4250 mg/m3 (rat)
25000 mg/m3 (mouse, 2 hr)[2]
US health exposure limits (NIOSH):
PEL (Permissible)
TWA 5 mg/m3[1]
REL (Recommended)
TWA 5 mg/m3[1]
IDLH (Immediate danger)
4000 mg/m3[1]
Except where otherwise noted, data are given for materials in their standard state (at 25 °C [77 °F], 100 kPa).
N verify (what is YN ?)
Infobox references

Dibutyl phthalate (DBP) is a commonly used plasticizer. It is also used as an additive to adhesives or printing inks. It is soluble in various organic solvents, e.g. in alcohol, ether and benzene. DBP is also used as an ectoparasiticide. DBP is also a putative endocrine disruptor[3]

Legislative control

European Union

The use of this substance in cosmetics, including nail polishes, is banned in the European Union under Directive 76/768/EEC 1976.[4]

The use of DBP has been restricted in the European Union for use in children's toys since 1999.[5]

An EU Risk Assessment has been conducted on DBP and the final outcome has now been published in the EU Official Journal. To eliminate a potential risk to plants in the vicinity of processing sites and workers through inhalation, measures are to be taken within the framework of the IPPC Directive (96/61/EC) and the Occupational Exposure Directive (98/24/EC)[6] Also includes the 2004 addendum.

United States

DBP was added to the California Proposition 65 (1986) list of suspected teratogens in November 2006. It is a suspected endocrine disruptor.[3] It was used in some nail polishes; all major producers began eliminating this chemical from nail polishes in the Fall of 2006.

DBP was permanently banned in children's toys, in concentrations of 1000 ppm or greater, under section 108 of the Consumer Product Safety Improvement Act of 2008 (CPSIA).

Production

DBP is produced by the reaction of n-butanol with phthalic anhydride. It is or was produced in the United States by Eastman Chemical Company, but the company announced in March 2011 that it would end production and exit the DBP and DEP (diethyl phthalate) market in December 2011.[7]

Exposure

Based on urine samples from people of different ages, the European Commission Scientific Committee on Health and Environmental Risks (SCHER) concluded that total exposures to individual phthalates in the general population are below tolerable daily intakes (TDI), except in the case of DBP for which efforts to further reduce exposures are needed.[8]

Biodegradation

The white rot fungus Polyporus brumalis degrades DBP.[9]

See also



This article uses material from the Wikipedia article "Dibutyl phthalate", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material