powered by CADENAS

Social Share

Zirconium dioxide (18778 views - Material Database)

Zirconium dioxide (ZrO 2), sometimes known as zirconia (not to be confused with zircon), is a white crystalline oxide of zirconium. Its most naturally occurring form, with a monoclinic crystalline structure, is the mineral baddeleyite. A dopant stabilized cubic structured zirconia, cubic zirconia, is synthesized in various colours for use as a gemstone and a diamond simulant.
Go to Article

Zirconium dioxide

Zirconium dioxide

Zirconium dioxide

Licensed under Creative Commons Attribution-Share Alike 3.0 (Materialscientist at the English language Wikipedia).

Zirconium dioxide
Names
IUPAC names
Zirconium dioxide
Zirconium(IV) oxide
Other names
Zirconia
Baddeleyite
Identifiers
ECHA InfoCard 100.013.844
Properties
ZrO
2
Molar mass 123.218 g/mol
Appearance white powder
Density 5.68 g/cm3
Melting point 2,715 °C (4,919 °F; 2,988 K)
Boiling point 4,300 °C (7,770 °F; 4,570 K)
negligible
Solubility soluble in HF, and hot H2SO4
2.13
Thermochemistry
50.3 J K−1 mol−1
–1080 kJ/mol
Hazards
Safety data sheet MSDS
Flash point Non-flammable
Lethal dose or concentration (LD, LC):
> 8.8 g/kg (oral, rat)
Related compounds
Other anions
Zirconium disulfide
Other cations
Titanium dioxide
Hafnium dioxide
Except where otherwise noted, data are given for materials in their standard state (at 25 °C [77 °F], 100 kPa).
Y verify (what is YN ?)
Infobox references

Zirconium dioxide (ZrO
2
), sometimes known as zirconia (not to be confused with zircon), is a white crystalline oxide of zirconium. Its most naturally occurring form, with a monoclinic crystalline structure, is the mineral baddeleyite. A dopant stabilized cubic structured zirconia, cubic zirconia, is synthesized in various colours for use as a gemstone and a diamond simulant.

Production, chemical properties, occurrence

Zirconia is produced by calcining zirconium compounds, exploiting its high thermal stability.[1]

Structure

Three phases are known: monoclinic <1,170 °C, tetragonal 1,170–2,370 °C, and cubic >2,370 °C.[2] The trend is for higher symmetry at higher temperatures, as is usually the case. A few percentage of the oxides of calcium or yttrium stabilize the cubic phase.[1] The very rare mineral tazheranite (Zr,Ti,Ca)O2 is cubic. Unlike TiO2, which features six-coordinate Ti in all phases, monoclinic zirconia consists of seven-coordinate zirconium centres. This difference is attributed to the larger size of Zr atom relative to the Ti atom.[3]

Chemical reactions

Zirconia is chemically unreactive. It is slowly attacked by concentrated hydrofluoric acid and sulfuric acid. When heated with carbon, it converts to zirconium carbide. When heated with carbon in the presence of chlorine, it converts to zirconium tetrachloride. This conversion is the basis for the purification of zirconium metal and is analogous to the Kroll process.

Engineering properties

Zirconium dioxide is one of the most studied ceramic materials. ZrO2 adopts a monoclinic crystal structure at room temperature and transitions to tetragonal and cubic at higher temperatures. The change of volume caused by the structure transitions from tetragonal to monoclinic to cubic induces large stresses, causing it to crack upon cooling from high temperatures.[4] When the zirconia is blended with some other oxides, the tetragonal and/or cubic phases are stabilized. Effective dopants include magnesium oxide (MgO), yttrium oxide (Y2O3, yttria), calcium oxide (CaO), and cerium(III) oxide (Ce2O3).[5]

Zirconia is often more useful in its phase 'stabilized' state. Upon heating, zirconia undergoes disruptive phase changes. By adding small percentages of yttria, these phase changes are eliminated, and the resulting material has superior thermal, mechanical, and electrical properties. In some cases, the tetragonal phase can be metastable. If sufficient quantities of the metastable tetragonal phase is present, then an applied stress, magnified by the stress concentration at a crack tip, can cause the tetragonal phase to convert to monoclinic, with the associated volume expansion. This phase transformation can then put the crack into compression, retarding its growth, and enhancing the fracture toughness. This mechanism is known as transformation toughening, and significantly extends the reliability and lifetime of products made with stabilized zirconia.[5][6]

The ZrO2 band gap is dependent on the phase (cubic, tetragonal, monoclinic, or amorphous) and preparation methods, with typical estimates from 5–7 eV (0.80–1.12 aJ).[7]

A special case of zirconia is that of tetragonal zirconia polycrystal, or TZP, which is indicative of polycrystalline zirconia composed of only the metastable tetragonal phase.

Uses

The main use of zirconia is in the production of ceramics,[8][9] with other uses including as a protective coating on particles of titanium dioxide pigments,[1] as a refractory material, in insulation, abrasives and enamels. Stabilized zirconia is used in oxygen sensors and fuel cell membranes because it has the ability to allow oxygen ions to move freely through the crystal structure at high temperatures. This high ionic conductivity (and a low electronic conductivity) makes it one of the most useful electroceramics.[1] Zirconium dioxide is also used as the solid electrolyte in electrochromic devices.

Zirconia is a precursor to the electroceramic lead zirconate titanate (PZT), which is a high-K dielectric, which is found in myriad components.

Niche uses

The very low thermal conductivity of cubic phase of zirconia also has led to its use as a thermal barrier coating, or TBC, in jet and diesel engines to allow operation at higher temperatures.[citation needed] Thermodynamically, the higher the operation temperature of an engine, the greater the possible efficiency. Another low thermal conductivity use is a ceramic fiber insulation for crystal growth furnaces, fuel cell stack insulation and infrared heating systems.

This material is also used in dentistry in the manufacture of 1) subframes for the construction of dental restorations such as crowns and bridges, which are then veneered with a conventional feldspathic porcelain for aesthetic reasons, or of 2) strong, extremely durable dental prostheses constructed entirely from monolithic zirconia, with limited but constantly improving aesthetics.[10]

Transformation toughened zirconia is used to make ceramic knives. Because of the hardness, ceramic-edged cutlery stays sharp longer than steel edged products.[11]

Due to its infusibility and brilliant luminosity when incandescent, it was used as an ingredient of sticks for limelight.[citation needed]

Zirconia has been proposed to electrolyze carbon monoxide and oxygen from the atmosphere of Mars to provide both fuel and oxidizer that could be used as a store of chemical energy for use with surface transportation on Mars. Carbon monoxide/oxygen engines have been suggested for early surface transportation use as both carbon monoxide and oxygen can be straightforwardly produced by zirconia electrolysis without requiring use of any of the Martian water resources to obtain hydrogen, which would be needed for the production of methane or any hydrogen-based fuels.[12]

Zirconia is also a potential high-k dielectric material with potential applications as an insulator in transistors.

Zirconia is also employed in the deposition of optical coatings; it is a high-index material usable from the near-UV to the mid-IR, due to its low absorption in this spectral region. In such applications, it is typically deposited by PVD.[13]

In jewelry making, some watch cases are advertised as being "black zirconium oxide".[14]

Diamond simulant

Single crystals of the cubic phase of zirconia are commonly used as diamond simulant in jewellery. Like diamond, cubic zirconia has a cubic crystal structure and a high index of refraction. Visually discerning a good quality cubic zirconia gem from a diamond is difficult, and most jewellers will have a thermal conductivity tester to identify cubic zirconia by its low thermal conductivity (diamond is a very good thermal conductor). This state of zirconia is commonly called cubic zirconia, CZ, or zircon by jewellers, but the last name is not chemically accurate. Zircon is actually the mineral name for naturally occurring zirconium silicate (ZrSiO4).

See also



This article uses material from the Wikipedia article "Zirconium dioxide", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material