powered by CADENAS

Social Share

Hydrate (11895 views - Material Database)

In chemistry, a hydrate is a substance that contains water or its constituent elements. The chemical state of the water varies widely between different classes of hydrates, some of which were so labeled before their chemical structure was understood.
Go to Article

Hydrate

Hydrate

In chemistry, a hydrate is a substance that contains water or its constituent elements. The chemical state of the water varies widely between different classes of hydrates, some of which were so labeled before their chemical structure was understood.

Chemical nature

Organic chemistry

In organic chemistry, a hydrate is a compound formed by the addition of water or its elements to another molecule. For example, ethanol, CH3–CH2–OH, is the product of the hydration reaction of ethene, CH2=CH2, formed by the addition of H to one C and OH to the other C, and so can be considered as the hydrate of ethene. A molecule of water may be eliminated, for example by the action of sulfuric acid. Another example is chloral hydrate, CCl3–CH(OH)2, which can be formed by reaction of water with chloral, CCl3–CH=O.

Many organic molecules, as well as inorganic molecules, form crystals that incorporate water into the crystalline structure without chemical alteration of the organic molecule (water of crystallization). The sugar trehalose, for example, exists in both an anhydrous form (melting point 203 °C) and as a dihydrate (melting point 97 °C). Protein crystals commonly have as much as 50% water content.

Molecules are also labeled as hydrates for historical reasons not covered above. Glucose, C6H12O6, was originally thought of as C6(H2O)6 and described as a carbohydrate. Methanol is often sold as "methyl hydrate", implying the incorrect formula CH3OH2, while the correct formula is CH3–OH.

Inorganic chemistry

Hydrates are inorganic salts "containing water molecules combined in a definite ratio as an integral part of the crystal"[1] that are either bound to a metal center or that have crystallized with the metal complex. Such hydrates are also said to contain water of crystallization or water of hydration. If the water is heavy water, where the hydrogen involved is the isotope deuterium, then the term deuterate may be used in place of hydrate.[citation needed]

 
Anhydrous
cobalt(II) chloride
CoCl2
Cobalt(II) chloride
hexahydrate
CoCl2•6H2O

A colorful example is cobalt(II) chloride, which turns from blue to red upon hydration, and can therefore be used as a water indicator.

The notation "hydrated compoundnH2O", where n is the number of water molecules per formula unit of the salt, is commonly used to show that a salt is hydrated. The n is usually a low integer, though it is possible for fractional values to occur. For example, in a monohydrate n is one, and in a hexahydrate n is 6. Numerical prefixes of Greek origin are:[2]

  • Hemi – 1/2
  • Mono – 1
  • Sesqui - 1½
  • Di – 2
  • Tri – 3
  • Tetra – 4
  • Penta – 5
  • Hexa – 6
  • Hepta – 7
  • Octa – 8
  • Nona – 9
  • Deca – 10
  • Undeca - 11
  • Dodeca - 12

A hydrate which has lost water is referred to as an anhydride; the remaining water, if any exists, can only be removed with very strong heating. A substance that does not contain any water is referred to as anhydrous. Some anhydrous compounds are hydrated so easily that they are said to be hygroscopic and are used as drying agents or desiccants.

Clathrate hydrates

Clathrate hydrates (also known as gas hydrates, gas clathrates, etc.) are water ice with gas molecules trapped within; they are a form of clathrate. An important example is methane hydrate (also known as gas hydrate, methane clathrate, etc.).

Nonpolar molecules such as methane can form clathrate hydrates with water, especially under high pressure. Although there is no hydrogen bonding of water molecules when methane is the guest molecule of the clathrate, guest-host hydrogen bonding often forms when the guest is a larger organic molecule such as tetrahydrofuran. In such cases the guest-host hydrogen bonds result in the formation of L-type Bjerrum defects in the clathrate lattice.[3]

Stability

The stability of hydrates is generally determined by the nature of the compounds, their temperature, and the relative humidity (if they are exposed to air).

See also



This article uses material from the Wikipedia article "Hydrate", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material