Names | |
---|---|
IUPAC name
Potassium chromate
| |
Other names
Chromic acid, (K2CrO4), dipotassium salt
| |
Identifiers | |
3D model (JSmol)
|
|
ChEBI | |
ChemSpider |
|
ECHA InfoCard | 100.029.218 |
EC Number | 232-140-5 |
PubChem CID
|
|
RTECS number | GB2940000 |
| |
| |
Properties | |
CrK2O4 | |
Molar mass | 194.19 g·mol−1 |
Appearance | Yellow powder |
Odor | odorless |
Density | 2.7320 g/cm3 |
Melting point | 968 °C (1,774 °F; 1,241 K) |
Boiling point | 1,000 °C (1,830 °F; 1,270 K) |
62.9 g/100 mL (20 °C) 75.1 g/100 mL (80 °C) 79.2 g/100 mL (100 °C) | |
Solubility | insoluble in alcohol |
−3.9·10−6 cm3/mol | |
Refractive index (nD)
|
1.74 |
Structure | |
rhombic | |
Hazards | |
Safety data sheet | Chemical Safety Data |
EU classification (DSD) (outdated)
|
Carc. Cat. 2 Muta. Cat. 2 Toxic (T) Irritant (Xi) Dangerous for the environment (N) |
R-phrases (outdated) | R49, R46, R36/37/38, R43, R50/53 |
S-phrases (outdated) | S53, S45, S60, S61 |
NFPA 704 | |
Related compounds | |
Other anions
|
Potassium dichromate Potassium molybdate Potassium tungstate |
Other cations
|
Sodium chromate Calcium chromate Barium chromate |
Except where otherwise noted, data are given for materials in their standard state (at 25 °C [77 °F], 100 kPa). | |
N verify (what is YN ?) | |
Infobox references | |
Potassium chromate is the inorganic compound with the formula (K2CrO4). This yellow solid is the potassium salt of the chromate anion. It is a common laboratory chemical, whereas sodium chromate is important industrially. It is a class two carcinogen as it contains hexavalent chromium.[1]
Two crystalline forms are known, both being very similar to the corresponding potassium sulfate. Orthorhombic β-K2CrO4 is the common form, but it converts to an α-form above 66 °C.[2] These structures are complex, although the sulfate adopts the typical tetrahedral geometry.[3]
It is prepared by treating potassium dichromate with potassium hydroxide.
In solution, the behavior of potassium and sodium dichromates are very similar. When treated with lead(II) nitrate, it gives an orange-yellow precipitate, lead(II) chromate.
Unlike the less expensive sodium salt, potassium salt is mainly used for laboratory work in situations where an anhydrous salt is required.[2] It is as an oxidizing agent in organic synthesis. It is used as in qualitative inorganic analysis, e.g. as a colorimetric test for silver ion. It is also used as an indicator in precipitation titrations with silver nitrate and sodium chloride (they can be used as standard as well as titrant for each other) as potassium chromate turns red in the presence of excess of silver ions.
Tarapacaite is the natural, mineral form of potassium chromate. It occurs very rarely and until now is known from only few localities on Atacama desert.[citation needed]
Potassium chromate is a carcinogen and strong oxidant.
This inorganic compound–related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Potassium chromate", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material