powered by CADENAS

Social Share

Cobalt(II) sulfate (22132 views - Material Database)

Cobalt(II) sulfate is any of the inorganic compounds with the formula CoSO4(H2O)x. Usually cobalt sulfate refers to the hydrate CoSO4.7H2O, which is one of the most commonly available salts of cobalt.
Go to Article

Cobalt(II) sulfate

Cobalt(II) sulfate

Cobalt(II) sulfate
Names
IUPAC name
Cobalt(II) sulfate
Identifiers
3D model (JSmol)
ChEBI
ChemSpider
ECHA InfoCard 100.030.291
EC Number 233-334-2
RTECS number GG3100000 (anhydrous)
GG3200000 (heptahydrate)
UNII
Properties
CoSO4∙(H2O)7
Molar mass 154.996 g/mol (anhydrous)
173.01 g/mol (monohydrate)
263.08 g/mol (hexahydrate)
281.103 g/mol (heptahydrate)
Appearance reddish crystalline (anhydrous, monohydrate)
pink salt (hexahydrate)
Odor odorless (heptahydrate)
Density 3.71 g/cm3 (anhydrous)
3.075 g/cm3 (monohydrate)
2.019 g/cm3 (hexahydrate)
1.948 g/cm3 (heptahydrate)
Melting point 735 °C (1,355 °F; 1,008 K)
anhydrous:
36.2 g/100 mL (20 °C)
38.3 g/100 mL (25 °C)
84 g/100 mL (100 °C)
heptahydrate:
60.4 g/100 mL (3 °C)
67 g/100 mL (70 °C)
Solubility anhydrous:
1.04 g/100 mL (methanol, 18 °C)
insoluble in ammonia
heptahydrate:
54.5 g/100 mL (methanol, 18 °C)
+10,000·10−6 cm3/mol
1.639 (monohydrate)
1.540 (hexahydrate)
1.483 (heptahydrate)
Structure
orthorhombic (anhydrous)
monoclinic (monohydrate, heptahydrate)
Hazards
Safety data sheet JT Baker MSDS
Carc. Cat. 2
Muta. Cat. 3
Repr. Cat. 2
Toxic (T)
Dangerous for the environment (N)
R-phrases (outdated) R49, R60, R22, R42/43, R68, R50/53
S-phrases (outdated) S53, S45, S60, S61
NFPA 704
Flammability code 0: Will not burn. E.g., waterHealth code 2: Intense or continued but not chronic exposure could cause temporary incapacitation or possible residual injury. E.g., chloroformReactivity code 0: Normally stable, even under fire exposure conditions, and is not reactive with water. E.g., liquid nitrogenSpecial hazards (white): no code
0
2
0
Flash point Non-flammable
Lethal dose or concentration (LD, LC):
424 mg/kg (oral, rat)
Except where otherwise noted, data are given for materials in their standard state (at 25 °C [77 °F], 100 kPa).
N verify (what is YN ?)
Infobox references

Cobalt(II) sulfate is any of the inorganic compounds with the formula CoSO4(H2O)x. Usually cobalt sulfate refers to the hydrate CoSO4.7H2O, which is one of the most commonly available salts of cobalt.

Properties, preparation, and structure

Cobalt(II) sulfate heptahydrate appears as red monoclinic crystals that liquify around 100 °C and become anhydrous at 250 °C. It is soluble in water, slightly soluble in ethanol, and especially soluble in methanol. The salts are paramagnetic.

It forms by the reaction of metallic cobalt, its oxide, hydroxide, or carbonate with aqueous sulfuric acid.[1]

The hexahydrate is a metal aquo complex consisting of octahedral [Co(H2O)6]2+ ions associated with sulfate anions.[2]

Uses

Cobalt is obtained from ores via the sulfate in many cases.[1][3]

Hydrated cobalt(II) sulfate is used in the preparation of pigments, as well as in the manufacture of other cobalt salts. Cobalt pigment is used in porcelains and glass. Cobalt(II) sulfate is used in storage batteries and electroplating baths, sympathetic inks, and as an additive to soils and animal feeds. For these purposes, the cobalt sulfate is produced by treating cobalt oxide with sulfuric acid.[1]

Health issues

Cobalt is essential for most higher forms of life, but more than a few milligrams each day is harmful. Rarely have poisonings resulted from cobalt compounds.[4] Upon inhalation of salts, there is some evidence for carcinogenicity.[1]

  1. ^ a b c d John D. Donaldson, Detmar Beyersmann "Cobalt and Cobalt Compounds" in Ullmann's Encyclopedia of Industrial Chemistry 2005, Wiley-VCH, Weinheim. doi:10.1002/14356007.a07_281.pub2
  2. ^ Elerman, Y. "Refinement of the crystal structure of CoSO4*6H2O" Acta Crystallographica, Section C: Crystal Structure Communications 1988, volume 44, p599-p601. doi:10.1107/S0108270187012447
  3. ^ Rarely, cobalt(II) sulfate is found in form of few crystallohydrate minerals, occurring among oxidation zones containing primary Co minerals (like skutterudite or cobaltite). These minerals are: biebierite (heptahydrate), moorhouseite (Co,Ni,Mn)SO4.6H2O, aplowite (Co,Mn,Ni)SO4.4H2O and cobaltkieserite (monohydrate).
  4. ^ 11.1.5 The unusual type of myocardiopathy recognized in 1965 and 1966 in Quebec (Canada), Minneapolis (Minnesota), Leuven (Belgium), and Omaha (Nebraska) was associated with episodes of acute heart failure (e/g/, 50 deaths among 112 beer drinkers).
Salts and esters of the sulfate ion
H2SO4 He
Li2SO4 BeSO4 B esters
ROSO3
(RO)2SO2
(NH4)2SO4
[N2H5]HSO4
(NH3OH)2SO4
NOHSO4
HOSO4 F Ne
Na2SO4
NaHSO4
MgSO4 Al2(SO4)3
Al2SO4(OAc)4
Si P SO42−
HSO3HSO4
(HSO4)2
Cl Ar
K2SO4
KHSO4
CaSO4 Sc2(SO4)3 Ti(SO4)2
TiOSO4
VSO4
V2(SO4)3
VOSO4
CrSO4
Cr2(SO4)3
MnSO4
Mn2(SO4)3
FeSO4
Fe2(SO4)3
CoSO4
Co2(SO4)3
NiSO4 CuSO4
Cu2SO4
[Cu(NH3)4(H2O)]SO4
ZnSO4 Ga2(SO4)3 Ge As Se Br Kr
RbHSO4
Rb2SO4
SrSO4 Y2(SO4)3 Zr(SO4)2 Nb Mo Tc Ru Rh PdSO4 Ag2SO4 CdSO4 In2(SO4)3 SnSO4 Sb2(SO4)3 Te I Xe
Cs2SO4 BaSO4   Hf Ta W Re Os Ir Pt Au Hg2SO4
HgSO4
Tl2SO4
Tl2(SO4)3
PbSO4 Bi2(SO4)3 Po At Rn
Fr Ra   Rf Db Sg Bh Hs Mt Ds Rg Cn Nh Fl Mc Lv Ts Og
La Ce2(SO4)3
Ce(SO4)2
Pr2(SO4)3 Nd Pm Sm Eu Gd Tb Dy Ho Er Tm Yb2(SO4)3 Lu
Ac Th Pa U(SO4)2
UO2SO4
Np Pu Am Cm Bk Cf Es Fm Md No Lr


This article uses material from the Wikipedia article "Cobalt(II) sulfate", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material