Licensed under Creative Commons Attribution-Share Alike 2.0 (Unkown).
This article does not cite any sources. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (April 2009) (Learn how and when to remove this template message) |
A magnetic base is a magnetic fixture based on a magnet that can effectively be turned "on" and "off" at will; they are often used in optics and metalworking, e.g., to hold a dial indicator.
The vertical post, side arm (as shown in the image at right) and the dial indicator (not shown) are connected by two swivelling connectors. These connectors allow free movement of the arms so that the indicator can be presented to the work in a suitable orientation. The magnetic base may have a "V" cut into the bottom of the base or the back. This "V" allows the base to be attached to a round bar such as the column of a drill press.
The base is made from two blocks of iron, with a round cavity bored through the centre. The halves are joined together with a non-ferrous material such as brass or aluminium. A round permanent magnet is inserted into the bored hole and a handle is attached to allow easy rotation of the magnet. This act of rotation changes the position of the magnetic field so that poles are in the two iron halves, where the iron blocks act as keepers (on position), or completely in the non-ferrous core (off position).
In this on position the field is effectively passing across an air gap (at the base and top). If this gap is bridged with another piece of iron (or steel in our case) it becomes part of the magnetic field's circuit and will be attracted with the full strength of the magnet.
A magnetic base can therefore be attached in a variety of positions to any attractive surface, allowing the base to be positioned in the best orientation for the part to be tested. Combine this with the flexibility of movement allowed by the arms gives the operator a large range of options in positioning the dial indicator.
An alternative to the post and swivelling connectors is an arrangement whereby a series of interconnecting swivels can be set in position by tightening or loosening a central member. This member may be made from wire rope as it has to be extremely flexible yet strong in tension, the possibilities for positioning this type is probably no more than the two post type but its advantage lies in the fact that there is only one mechanism (screw) to loosen or tighten the arrangement making it easier to use, unlike the other where a third hand is often wished for.
This article uses material from the Wikipedia article "Magnetic base", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD