Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Ferrouranium, also called ferro-uranium, is a ferroalloy, an alloy of iron and uranium, after World War II usually depleted uranium.
The alloy contains about 35–50% uranium and 1.5–4.0% carbon.[1] At least two intermetallic compounds of iron and uranium were identified: U6Fe and UFe2. Small amounts of uranium can drastically lower melting point of iron and vice versa. UFe
2 reportedly melts at 1230 °C, U
6Fe at 805 °C; a mixture of these two can have melting point as low as 725 °C, a mixture of iron and UFe
2 can have melting point of 1055 °C.[2] As ferrouranium readily dissolves in mineral acids, its chemical analysis is not problematic.[3]
Ferrouranium is used as a deoxidizer (more powerful than ferrovanadium), for denitrogenizing steel, for forming carbides, and as an alloying element. In ferrous alloys, uranium increases the elastic limit and the tensile strength. In high speed steels, it has been used to increase toughness and strength in amounts between 0.05–5%.[4] Uranium-alloyed steels can be used at very low temperatures; nickel-uranium alloys are resistant to even very aggressive chemicals, including aqua regia.[5]
The alloys did not prove to be commercially successful in long run.[6] However, during World War I and afterwards, uranium-doped steels were used for tools; large amounts of ferrouranium were produced between 1914–1916.[7]
This article uses material from the Wikipedia article "Ferrouranium", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material