Manganin is a trademarked name for an alloy of typically 84% copper, 12% manganese, and 4% nickel. It was first developed by Edward Weston in 1892, improving upon his Constantan (1887).
Manganin foil and wire is used in the manufacture of resistors, particularly ammeter shunts, because of its virtually zero temperature coefficient of resistance value[1] and long term stability. Several Manganin resistors served as the legal standard for the ohm in the United States from 1901 to 1990.[2] Manganin wire is also used as an electrical conductor in cryogenic systems, minimizing heat transfer between points which need electrical connections.
Manganin is also used in gauges for studies of high-pressure shock waves (such as those generated from the detonation of explosives) because it has low strain sensitivity but high hydrostatic pressure sensitivity.[3]
This section needs expansion. You can help by adding to it. (January 2011) |
In 1887 Edward Weston discovered that metals can have a negative temperature coefficient of resistance, inventing what he called his "Alloy No. 2." It was produced in Germany where it was renamed "Constantan".[4]
In 1892 Weston had finally completed his discovery of an alloy of copper, nickel, and manganese prepared by a complicated series of heat-treatments. In May, 1893, he received a basic patent on the composition, manufacture, and use of the material for electrical resistors. Production was carried out in Germany, and it became known as "Manganin". The availability of a practical conductive metal with an extremely constant resistance over the range of ordinary temperatures was a great advance in electrical technology and equipment design, but Weston did not receive general recognition for this.[5]
Electrical Properties
Mechanical Properties
Physical Properties
Thermal Properties
This article may be in need of reorganization to comply with Wikipedia's layout guidelines. Please help by editing the article to make improvements to the overall structure. (November 2012) (Learn how and when to remove this template message) |
Cu84/Mn12/Ni4 Temperature coefficient of resistivity TempDegC (Somerville 1910) 12 .000006 25 .000000 100 -.000042 250 -.000052 475 .000000 500 +.00011[6]
Resistance of Wires - 20 deg C Manganin Q = 44. x 10-6 ohm cm Gage B&S / ohms per cm / ohms per ft 10 .000836 .0255 12 .00133 .0405 14 .00211 .0644 16 .00336 .102 18 .00535 .163 20 .00850 .259 22 .0135 .412 24 .0215 .655 26 .0342 1.04 27 .0431 1.31 28 .0543 1.66 30 .0864 2.63 32 .137 4.19 34 .218 6.66 36 .347 10.6 40 .878 26.8[7]
This article uses material from the Wikipedia article "Manganin", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material
This website makes use of cookies to enhance browsing experience and provide additional functionality. By further using this site you agree that we are using the following cookies: