powered by CADENAS

Social Share

Rhodium (19646 views - Material Database)

Rhodium is a chemical element with symbol Rh and atomic number 45. It is a rare, silvery-white, hard, and chemically inert transition metal. It is a member of the platinum group. It has only one naturally occurring isotope, 103Rh. Naturally occurring rhodium is usually found as the free metal, alloyed with similar metals, and rarely as a chemical compound in minerals such as bowieite and rhodplumsite. It is one of the rarest and most valuable precious metals. Rhodium is a noble metal, resistant to corrosion, found in platinum or nickel ores together with the other members of the platinum group metals. It was discovered in 1803 by William Hyde Wollaston in one such ore, and named for the rose color of one of its chlorine compounds, produced after it reacted with the powerful acid mixture aqua regia. The element's major use (approximately 80% of world rhodium production) is as one of the catalysts in the three-way catalytic converters in automobiles. Because rhodium metal is inert against corrosion and most aggressive chemicals, and because of its rarity, rhodium is usually alloyed with platinum or palladium and applied in high-temperature and corrosion-resistive coatings. White gold is often plated with a thin rhodium layer to improve its appearance while sterling silver is often rhodium-plated for tarnish resistance. Rhodium detectors are used in nuclear reactors to measure the neutron flux level.
Go to Article

Rhodium

Rhodium

Rhodium,  45Rh
General properties
Pronunciation /ˈrdiəm/
ROH-dee-əm
Appearance silvery white metallic
Standard atomic weight (Ar) 102.90550(2)[1]
Rhodium in the periodic table
Co

Rh

Ir
rutheniumrhodiumpalladium
Atomic number (Z) 45
Group, period group 9, period 5
Block d-block
Element category   transition metal
Electron configuration [Kr] 4d8 5s1
Electrons per shell
2, 8, 18, 16, 1
Physical properties
Phase (at STP) solid
Melting point 2237 K ​(1964 °C, ​3567 °F)
Boiling point 3968 K ​(3695 °C, ​6683 °F)
Density (near r.t.) 12.41 g/cm3
when liquid (at m.p.) 10.7 g/cm3
Heat of fusion 26.59 kJ/mol
Heat of vaporization 493 kJ/mol
Molar heat capacity 24.98 J/(mol·K)
Vapor pressure
P (Pa) 1 10 100 1 k 10 k 100 k
at T (K) 2288 2496 2749 3063 3405 3997
Atomic properties
Oxidation states 6, 5, 4, 3, 2, 1,[2] −1, −3 ​(an amphoteric oxide)
Electronegativity Pauling scale: 2.28
Ionization energies
  • 1st: 719.7 kJ/mol
  • 2nd: 1740 kJ/mol
  • 3rd: 2997 kJ/mol
Atomic radius empirical: 134 pm
Covalent radius 142±7 pm
Miscellanea
Crystal structureface-centered cubic (fcc)
Speed of sound thin rod 4700 m/s (at 20 °C)
Thermal expansion 8.2 µm/(m·K) (at 25 °C)
Thermal conductivity 150 W/(m·K)
Electrical resistivity 43.3 nΩ·m (at 0 °C)
Magnetic ordering paramagnetic[3]
Magnetic susceptibility +111.0·10−6 cm3/mol (298 K)[4]
Young's modulus 380 GPa
Shear modulus 150 GPa
Bulk modulus 275 GPa
Poisson ratio 0.26
Mohs hardness 6.0
Vickers hardness 1100–8000 MPa
Brinell hardness 980–1350 MPa
CAS Number 7440-16-6
History
Discovery and first isolation William Hyde Wollaston (1804)
Main isotopes of rhodium
Iso­tope Abun­dance Half-life (t1/2) Decay mode Pro­duct
99Rh syn 16.1 d ε 99Ru
γ
101mRh syn 4.34 d ε 101Ru
IT 101Rh
γ
101Rh syn 3.3 y ε 101Ru
γ
102mRh syn 3.7 y ε 102Ru
γ
102Rh syn 207 d ε 102Ru
β+ 102Ru
β 102Pd
γ
103Rh 100% stable
105Rh syn 35.36 h β 105Pd
γ
| references | in Wikidata

Rhodium is a chemical element with symbol Rh and atomic number 45. It is a rare, silvery-white, hard, and chemically inert transition metal. It is a member of the platinum group. It has only one naturally occurring isotope, 103Rh. Naturally occurring rhodium is usually found as the free metal, alloyed with similar metals, and rarely as a chemical compound in minerals such as bowieite and rhodplumsite. It is one of the rarest and most valuable precious metals.

Rhodium is a noble metal, resistant to corrosion, found in platinum or nickel ores together with the other members of the platinum group metals. It was discovered in 1803 by William Hyde Wollaston in one such ore, and named for the rose color of one of its chlorine compounds, produced after it reacted with the powerful acid mixture aqua regia.

The element's major use (approximately 80% of world rhodium production) is as one of the catalysts in the three-way catalytic converters in automobiles. Because rhodium metal is inert against corrosion and most aggressive chemicals, and because of its rarity, rhodium is usually alloyed with platinum or palladium and applied in high-temperature and corrosion-resistive coatings. White gold is often plated with a thin rhodium layer to improve its appearance while sterling silver is often rhodium-plated for tarnish resistance.

Rhodium detectors are used in nuclear reactors to measure the neutron flux level.

History

Rhodium (Greek rhodon (ῥόδον) meaning "rose") was discovered in 1803 by William Hyde Wollaston,[5] soon after his discovery of palladium.[6][7][8] He used crude platinum ore presumably obtained from South America.[9] His procedure involved dissolving the ore in aqua regia and neutralizing the acid with sodium hydroxide (NaOH). He then precipitated the platinum as ammonium chloroplatinate by adding ammonium chloride (NH
4
Cl
). Most other metals like copper, lead, palladium and rhodium were precipitated with zinc. Diluted nitric acid dissolved all but palladium and rhodium. Of these, palladium dissolved in aqua regia but rhodium did not,[10] and the rhodium was precipitated by the addition of sodium chloride as Na
3
[RhCl
6
nH
2
O
. After being washed with ethanol, the rose-red precipitate was reacted with zinc, which displaced the rhodium in the ionic compound and thereby released the rhodium as free metal.[11]

After the discovery, the rare element had only minor applications; for example, by the turn of the century, rhodium-containing thermocouples were used to measure temperatures up to 1800 °C.[12][13] The first major application was electroplating for decorative uses and as corrosion-resistant coating.[14] The introduction of the three-way catalytic converter by Volvo in 1976 increased the demand for rhodium. The previous catalytic converters used platinum or palladium, while the three-way catalytic converter used rhodium to reduce the amount of NOx in the exhaust.[15][16][17]

Characteristics

Z Element No. of electrons/shell
27 cobalt 2, 8, 15, 2
45 rhodium 2, 8, 18, 16, 1
77 iridium 2, 8, 18, 32, 15, 2
109 meitnerium 2, 8, 18, 32, 32, 15, 2 (predicted)

Rhodium is a hard, silvery, durable metal that has a high reflectance. Rhodium metal does not normally form an oxide, even when heated.[18] Oxygen is absorbed from the atmosphere only at the melting point of rhodium, but is released on solidification.[19] Rhodium has both a higher melting point and lower density than platinum. It is not attacked by most acids: it is completely insoluble in nitric acid and dissolves slightly in aqua regia.

Chemical properties

Wilkinson's catalyst

Rhodium belongs to group 9 of the periodic table, but the configuration of electrons in the outermost shells is atypical for the group. This anomaly is also observed in the neighboring elements, niobium (41), ruthenium (44), and palladium (46).

Oxidation states
of rhodium
+0 Rh
4
(CO)
12
+1 RhCl(PH
3
)
2
+2 Rh
2
(O
2
CCH
3
)
4
+3 RhCl
3
, Rh
2
O
3
+4 RhF
4
, RhO
2
+5 RhF
5
, Sr
3
LiRhO
6
+6 RhF
6

The common oxidation state of rhodium is +3, but oxidation states from +0 to +6 are also observed.[20]

Unlike ruthenium and osmium, rhodium forms no volatile oxygen compounds. The known stable oxides include Rh
2
O
3
, RhO
2
, RhO
2
·xH
2
O
, Na
2
RhO
3
, Sr
3
LiRhO
6
and Sr
3
NaRhO
6
.[21] Halogen compounds are known in nearly the full range of possible oxidation states. Rhodium(III) chloride, rhodium(IV) fluoride, rhodium(V) fluoride and rhodium(VI) fluoride are examples. The lower oxidation states are stable only in the presence of ligands.[22]

The best-known rhodium-halogen compound is the Wilkinson's catalyst chlorotris(triphenylphosphine)rhodium(I). This catalyst is used in the hydroformylation or hydrogenation of alkenes.[23]

Isotopes

Naturally occurring rhodium is composed of only one isotope, 103Rh. The most stable radioisotopes are 101Rh with a half-life of 3.3 years, 102Rh with a half-life of 207 days, 102mRh with a half-life of 2.9 years, and 99Rh with a half-life of 16.1 days. Twenty other radioisotopes have been characterized with atomic weights ranging from 92.926 u (93Rh) to 116.925 u (117Rh). Most of these have half-lives shorter than an hour, except 100Rh (20.8 hours) and 105Rh (35.36 hours). It has numerous meta states, the most stable being 102mRh (0.141 MeV) with a half-life of about 2.9 years and 101mRh (0.157 MeV) with a half-life of 4.34 days (see isotopes of rhodium).[24]

In isotopes weighing less than 103 (the stable isotope), the primary decay mode is electron capture and the primary decay product is ruthenium In isotopes greater than 103, the primary decay mode is beta emission and the primary product is palladium.[25]

Occurrence

Rhodium is one of the rarest elements in the Earth's crust, comprising an estimated 0.0002 parts per million (2 × 10−10).[26] Its rarity affects its price and its use in commercial applications.

Mining and price

Rh price evolution.

The industrial extraction of rhodium is complex because the ores are mixed with other metals such as palladium, silver, platinum, and gold and there are very few rhodium-bearing minerals. It is found in platinum ores and extracted as a white inert metal that is difficult to fuse. Principal sources are located in South Africa; in river sands of the Ural Mountains; and in North America, including the copper-nickel sulfide mining area of the Sudbury, Ontario, region. Although the quantity at Sudbury is very small, the large amount of processed nickel ore makes rhodium recovery cost-effective.

The main exporter of rhodium is South Africa (approximately 80% in 2010) followed by Russia.[27] The annual world production is 30 tonnes. The price of rhodium is highly variable. In 2007, rhodium cost approximately eight times more than gold, 450 times more than silver, and 27,250 times more than copper by weight. In 2008, the price briefly rose above $10,000 per ounce ($350,000 per kilogram). The economic slowdown of the 3rd quarter of 2008 pushed rhodium prices sharply back below $1,000 per ounce ($35,000 per kilogram); the price rebounded to $2,750 by early 2010 ($97,000 per kilogram) (more than twice the gold price), but in late 2013, the prices were less than $1000.

Political and financial problems[clarification needed] led to very low oil prices and oversupply, causing most metals to drop in price. The economies of China, India and other emerging countries slowed in 2014 and 2015. In 2014 alone, 23,722,890 motor vehicles were produced in China, excluding motorbikes.[clarification needed] This resulted in a rhodium price of 740.00 US-$ per Troy ounce (31.1 grams) in late November 2015.[28]

Used nuclear fuels

Rhodium is a fission product of uranium-235; therefore, each kilogram of fission product contains a significant amount of the lighter platinum group metals including rhodium. Used nuclear fuel is a potential source of rhodium. However, the extraction is complex and expensive, and the presence of rhodium radioisotopes requires a period of cooling storage for multiple half-lives of the longest-lived isotope (about 10 years). These factors make the source unattractive and no large-scale extraction has been attempted.[29][30][31]

Applications

The primary use of this element is in automobiles as a catalytic converter, changing harmful unburned hydrocarbons, carbon monoxide, and nitrogen oxide exhaust emissions into less noxious gases. Of 30,000 kg of rhodium consumed worldwide in 2012, 81% (24,300 kg) went into and 8,060 kg was recovered from this application. About 964 kg of rhodium was used in the glass industry, mostly for production of fiberglass and flat-panel glass, and 2,520 kg was used in the chemical industry.[27]

Catalyst

In 2012, 81% of the world production of rhodium was consumed in automobile catalytic converters.[27] Rhodium is preferable to the other platinum metals in the reduction of nitrogen oxides to nitrogen and oxygen:[32]

2 NO
x
x O
2
+ N
2

Rhodium catalysts are used in a number of industrial processes, notably in catalytic carbonylation of methanol to produce acetic acid by the Monsanto process.[33] It is also used to catalyze addition of hydrosilanes to molecular double bonds, a process important in manufacture of certain silicone rubbers.[34] Rhodium catalysts are also used to reduce benzene to cyclohexane.[35]

The complex of a rhodium ion with BINAP is a widely used chiral catalyst for chiral synthesis, as in the synthesis of menthol.[36]

Ornamental uses

Rhodium finds use in jewelry and for decorations. It is electroplated on white gold and platinum to give it a reflective white surface at time of sale, after which the thin layer wears away with use. This is known as rhodium flashing in the jewelry business. It may also be used in coating sterling silver to protect against tarnish (silver sulfide, Ag2S, produced from atmospheric hydrogen sulfide, H2S). Solid (pure) rhodium jewelry is very rare, more because of the difficulty of fabrication (high melting point and poor malleability) than because of the high price.[37] The high cost ensures that rhodium is applied only as an electroplate.

Rhodium has also been used for honors or to signify elite status, when more commonly used metals such as silver, gold or platinum were deemed insufficient. In 1979 the Guinness Book of World Records gave Paul McCartney a rhodium-plated disc for being history's all-time best-selling songwriter and recording artist.[38]

Other uses

Rhodium is used as an alloying agent for hardening and improving the corrosion resistance[18] of platinum and palladium. These alloys are used in furnace windings, bushings for glass fiber production, thermocouple elements, electrodes for aircraft spark plugs, and laboratory crucibles.[39] Other uses include:

  • Electrical contacts, where it is valued for small electrical resistance, small and stable contact resistance, and great corrosion resistance.[40]
  • Rhodium plated by either electroplating or evaporation is extremely hard and useful for optical instruments.[41]
  • Filters in mammography systems for the characteristic X-rays it produces.[42]
  • Rhodium neutron detectors are used in combustion engineering nuclear reactors to measure neutron flux levels – this method requires a digital filter to determine the current neutron flux level, generating three separate signals: immediate, a few seconds delay, and a minute delay, each with its own signal level; all three are combined in the rhodium detector signal. The three Palo Verde nuclear reactors each have 305 rhodium neutron detectors, 61 detectors on each of five vertical levels, providing an accurate 3D "picture" of reactivity and allowing fine tuning to consume the nuclear fuel most economically.[43]

Precautions

Being a noble metal, pure rhodium is inert. However, chemical complexes of rhodium can be reactive. Median lethal dose (LD50) for rats is 198 mg of rhodium chloride (RhCl
3
) per kilogram of body weight.[44] Like the other noble metals, all of which are too inert to occur as chemical compounds in nature, rhodium has not been found to serve any biological function. In elemental form, the metal is harmless.[45]

People can be exposed to rhodium in the workplace by inhalation. The Occupational Safety and Health Administration (OSHA) has specified the legal limit (Permissible exposure limit) for rhodium exposure in the workplace at 0.1 mg/m3 over an 8-hour workday, and the National Institute for Occupational Safety and Health (NIOSH) has set the recommended exposure limit (REL), at the same level. At levels of 100 mg/m3, rhodium is immediately dangerous to life or health.[46] For soluble compounds, the PEL and REL are both 0.001 mg/m3.[47]

See also


AluminiumArsenical copperBerylliumBismuthChromiumCobaltCopperGalliumGlassGoldIndiumIronLeadMagnesiumMercuryNickelPlasticPlexiglasPlutoniumPotassiumStainless steelSteelStructural steelSilverSamariumTinUraniumZincZirconiumAluminium-lithium alloyAlnicoBirmabrightDuraluminHiduminiumHydronaliumItalmaMagnaliumAluminium alloyY alloyWood's metalRose's metalChromium hydrideNichromeMegalliumStelliteVitalliumBeryllium copperBillon (alloy)BrassCalamine brassChinese silverDutch metalGilding metalMuntz metalPinchbeck (alloy)TombacBronzeAluminium bronzeArsenical bronzeBell metalFlorentine bronzeGlucydurGuanín (bronze)GunmetalPhosphor bronzeOrmoluSpeculum metalConstantanCopper hydrideCopper–tungstenCorinthian bronzeCunifeCupronickelCymbal alloysDevarda's alloyElectrumHepatizonManganinMelchior (alloy)Nickel silverMolybdochalkosNordic GoldShakudōTumbagaAlGaGalfenolGalinstanColored goldRhoditeCrown goldElinvarField's metalFernicoFerroalloyFerroceriumFerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumInvarCast ironIron–hydrogen alloyPig ironKanthal (alloy)KovarStaballoyBulat steelCrucible steel41xx steelDamascus steelMangalloyHigh-speed steelMushet steelMaraging steelHigh-strength low-alloy steelReynolds 531Electrical steelSpring steelAL-6XNCelestriumAlloy 20Marine grade stainlessMartensitic stainless steelSanicro 28Surgical stainless steelZeron 100Silver steelTool steelWeathering steelWootz steelSolderTerneType metalElektron (alloy)Amalgam (chemistry)Magnox (alloy)AlumelBrightrayChromelHaynes InternationalInconelMonelNicrosilNisilNickel titaniumMu-metalPermalloySupermalloyNickel hydridePlutonium–gallium alloySodium-potassium alloyMischmetalLithiumTerfenol-DPseudo palladiumScandium hydrideSamarium–cobalt magnetArgentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiSterling silverTibetan silverTitanium Beta CTitanium alloyTitanium hydrideGum metalTitanium goldTitanium nitrideBabbitt (alloy)Britannia metalPewterQueen's metalWhite metalUranium hydrideZamakZirconium hydrideHydrogenHeliumBoronNitrogenOxygenFluorineMethaneMezzanineAtom

This article uses material from the Wikipedia article "Rhodium", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material