Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under GNU Free Documentation License 1.2 (Jonathunder).
It has been suggested that this article be merged with Qurabiya. (Discuss) Proposed since August 2017. |
Chocolate chip cookies | |
Alternative names | Biscuit |
---|---|
Course | Snack, dessert |
Place of origin | Persia, 7th century AD[1] |
Serving temperature | Often room temperature, although they may be served when still warm from the oven |
Cookbook: Cookie Media: Cookie |
A cookie is a baked or cooked good that is small, flat and sweet. It usually contains flour, sugar and some type of oil or fat. It may include other ingredients such as raisins, oats, chocolate chips, nuts, etc.
In most English-speaking countries except for the US and Canada, crisp cookies are called biscuits. Chewier biscuits are sometimes called cookies even in the UK.[2] Some cookies may also be named by their shape, such as date squares or bars.
Cookies or biscuits may be mass-produced in factories, made in small bakeries or home-made. Biscuit or cookie variants include sandwich biscuits, such as Custard creams, Jammie Dodgers, Bourbons and Oreos, with marshmallow or jam filling and sometimes dipped in chocolate or another sweet coating. Cookies are often served with beverages such as milk, coffee or tea. Factory-made cookies are sold in grocery stores, convenience stores and vending machines. Fresh-baked cookies are sold at bakeries and coffeehouses, with the latter ranging from small business-sized establishments to multinational corporations such as Starbucks.
In most English-speaking countries outside North America, including the United Kingdom, the most common word for a crisp cookie is biscuit.[2] The term cookie is normally used to describe chewier ones.[2] However, in many regions both terms are used.
In Scotland the term cookie is sometimes used to describe a plain bun.[3]
Cookies that are baked as a solid layer on a sheet pan and then cut, rather than being baked as individual pieces, are called bar cookies or traybakes.[2]
Its American name derives from the Dutch word koekje or more precisely its informal, dialect variant koekie[4] which means little cake, and arrived in American English with the Dutch settlement of New Netherland, in the early 1600s.
According to the Scottish National Dictionary, its Scottish name derives from the diminutive form (+ suffix -ie) of the word cook, giving the Middle Scots cookie, cooky or cu(c)kie. It also gives an alternative etymology, from the Dutch word koekje, the diminutive of koek, a cake. There was much trade and cultural contact across the North Sea between the Low Countries and Scotland during the Middle Ages, which can also be seen in the history of curling and, perhaps, golf.
Cookies are most commonly baked until crisp or just long enough that they remain soft, but some kinds of cookies are not baked at all. Cookies are made in a wide variety of styles, using an array of ingredients including sugars, spices, chocolate, butter, peanut butter, nuts, or dried fruits. The softness of the cookie may depend on how long it is baked.
A general theory of cookies may be formulated this way. Despite its descent from cakes and other sweetened breads, the cookie in almost all its forms has abandoned water as a medium for cohesion. Water in cakes serves to make the base (in the case of cakes called "batter"[5]) as thin as possible, which allows the bubbles – responsible for a cake's fluffiness – to better form. In the cookie, the agent of cohesion has become some form of oil. Oils, whether they be in the form of butter, vegetable oils, or lard, are much more viscous than water and evaporate freely at a much higher temperature than water. Thus a cake made with butter or eggs instead of water is far denser after removal from the oven.
Oils in baked cakes do not behave as soda tends to in the finished result. Rather than evaporating and thickening the mixture, they remain, saturating the bubbles of escaped gases from what little water there might have been in the eggs, if added, and the carbon dioxide released by heating the baking powder. This saturation produces the most texturally attractive feature of the cookie, and indeed all fried foods: crispness saturated with a moisture (namely oil) that does not sink into it.
Cookie-like hard wafers have existed for as long as baking is documented, in part because they deal with travel very well, but they were usually not sweet enough to be considered cookies by modern standards.[6]
Cookies appear to have their origins in 7th century AD Persia, shortly after the use of sugar became relatively common in the region.[1] They spread to Europe through the Muslim conquest of Spain. By the 14th century, they were common in all levels of society throughout Europe, from royal cuisine to street vendors.[citation needed]
With global travel becoming widespread at that time, cookies made a natural travel companion, a modernized equivalent of the travel cakes used throughout history. One of the most popular early cookies, which traveled especially well and became known on every continent by similar names, was the jumble, a relatively hard cookie made largely from nuts, sweetener, and water.
Cookies came to America through the Dutch in New Amsterdam in the late 1620s. The Dutch word "koekje" was Anglicized to "cookie" or cooky. The earliest reference to cookies in America is in 1703, when "The Dutch in New York provided...'in 1703...at a funeral 800 cookies...'"[7]
The most common modern cookie, given its style by the creaming of butter and sugar, was not common until the 18th century.[8]
Cookies are broadly classified according to how they are formed, including at least these categories:
Cookies also may be decorated with an icing, especially chocolate, and closely resemble a type of confectionery.
A variety of cookies, including gingerbread men and drop and molded cookies
A cookie cake is a large cookie that can be decorated with icing like a cake. This is made by Mrs. Fields
A Nice biscuit from Britain
This article uses material from the Wikipedia article "Cookie", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted