Licensed under Creative Commons Attribution-Share Alike 3.0 (
Owl Temporal range: Late Paleocene to recent | |
---|---|
Little owl (Athene noctua) | |
Otus jolandae call | |
Scientific classification | |
Kingdom: | Animalia |
Phylum: | Chordata |
Class: | Aves |
Clade: | Afroaves |
Order: | Strigiformes Wagler, 1830 |
Families | |
Strigidae | |
Range of the owl, all species. | |
Synonyms | |
Strigidae sensu Sibley & Ahlquist |
Owls are birds from the order Strigiformes, which includes about 200 species of mostly solitary and nocturnal birds of prey typified by an upright stance, a large, broad head, binocular vision, binaural hearing, sharp talons, and feathers adapted for silent flight. Exceptions include the diurnal northern hawk-owl and the gregarious burrowing owl.
Owls hunt mostly small mammals, insects, and other birds, although a few species specialize in hunting fish. They are found in all regions of the Earth except Antarctica and some remote islands.
Owls are divided into two families: the Strigidae family of true (or typical) owls; and the Tytonidae family of barn-owls.
Owls possess large, forward-facing eyes and ear-holes, a hawk-like beak, a flat face, and usually a conspicuous circle of feathers, a facial disc, around each eye. The feathers making up this disc can be adjusted to sharply focus sounds from varying distances onto the owls' asymmetrically placed ear cavities. Most birds of prey have eyes on the sides of their heads, but the stereoscopic nature of the owl's forward-facing eyes permits the greater sense of depth perception necessary for low-light hunting. Although owls have binocular vision, their large eyes are fixed in their sockets—as are those of most other birds—so they must turn their entire heads to change views. As owls are farsighted, they are unable to clearly see anything within a few centimeters of their eyes. Caught prey can be felt by owls with the use of filoplumes—hairlike feathers on the beak and feet that act as "feelers". Their far vision, particularly in low light, is exceptionally good.
Owls can rotate their heads and necks as much as 270°. Owls have 14 neck vertebrae compared to seven in humans, which makes their necks more flexible. They also have adaptations to their circulatory systems, permitting rotation without cutting off blood to the brain: the foramina in their vertebrae through which the vertebral arteries pass are about 10 times the diameter of the artery, instead of about the same size as the artery as in humans; the vertebral arteries enter the cervical vertebrae higher than in other birds, giving the vessels some slack, and the carotid arteries unite in a very large anastomosis or junction, the largest of any bird's, preventing blood supply from being cut off while they rotate their necks. Other anastomoses between the carotid and vertebral arteries support this effect.[1][2]
The smallest owl—weighing as little as 31 g (1 oz) and measuring some 13.5 cm (5 in)—is the elf owl (Micrathene whitneyi).[3] Around the same diminutive length, although slightly heavier, are the lesser known long-whiskered owlet (Xenoglaux loweryi) and Tamaulipas pygmy owl (Glaucidium sanchezi).[3] The largest owl by length is the great grey owl (Strix nebulosa), which measures about 70 cm (28 in) on average and can attain a length of 84 cm (33 in).[3] However, the heaviest (and largest winged) owls are two similarly sized eagle owls; the Eurasian eagle-owl (Bubo bubo) and Blakiston's fish owl (B. blakistoni). These two species, which are on average about 2.53 cm (1.00 in) shorter in length than the great grey, can both attain a wingspan of 2 m (6.6 ft) and a weight of 4.5 kg (10 lb) in the largest females.[3][4][5][6][7]
Different species of owls produce different sounds; this distribution of calls aids owls in finding mates or announcing their presence to potential competitors, and also aids ornithologists and birders in locating these birds and distinguishing species. As noted above, their facial discs help owls to funnel the sound of prey to their ears. In many species, these discs are placed asymmetrically, for better directional location.
Owl plumage is generally cryptic, although several species have facial and head markings, including face masks, ear tufts, and brightly coloured irises. These markings are generally more common in species inhabiting open habitats, and are thought to be used in signaling with other owls in low-light conditions.[8]
Sexual dimorphism is a physical difference between males and females of a species. Reverse sexual dimorphism, when females are larger than males, has been observed across multiple owl species.[9] The degree of size dimorphism varies across multiple populations and species, and is measured through various traits, such as wing span and body mass.[9] Overall, female owls tend to be slightly larger than males. The exact explanation for this development in owls is unknown. However, several theories explain the development of sexual dimorphism in owls.
One theory suggests that selection has led males to be smaller because it allows them to be efficient foragers. The ability to obtain more food is advantageous during breeding season. In some species, female owls stay at their nest with their eggs while it is the responsibility of the male to bring back food to the nest.[10] However, if food is scarce, the male first feeds himself before feeding the female.[11] Small birds, which are agile, are an important source of food for owls. Male burrowing owls have been observed to have longer wing chords than females, despite being smaller than females.[11] Furthermore, owls have been observed to be roughly the same size as their prey.[11] This has also been observed in other predatory birds,[10] which suggests that owls with smaller bodies and long wing chords have been selected for because of the increased agility and speed that allows them to catch their prey.
Another popular theory suggests that females have not been selected to be smaller like male owls because of their sexual roles. In many species, female owls may not leave the nest. Therefore, females may have a larger mass to allow them to go for a longer period of time without starving. For example, one hypothesized sexual role is that larger females are more capable of dismembering prey and feeding it to their young, hence female owls are larger than their male counterparts.[9]
A different theory suggests that the size difference between male and females is due to sexual selection: since large females can choose their mate and may violently reject a male's sexual advances, smaller male owls that have the ability to escape unreceptive females are more likely to have been selected.[11]
All owls are carnivorous birds of prey and live mainly on a diet of insects and small rodents such as mice, rats, and hares. Some owls are also specifically adapted to hunt fish. They are very adept in hunting in their respective environments. Since owls can be found in nearly all parts of the world and across a multitude of ecosystems, their hunting skills and characteristics vary slightly from species to species, though most characteristics are shared among all species.[citation needed]
Most owls share an innate ability to fly almost silently and also more slowly in comparison to other birds of prey. Most owls live a mainly nocturnal lifestyle and being able to fly without making any noise gives them a strong advantage over their prey that are listening for the slightest sound in the night. A silent, slow flight is not as necessary for diurnal and crepuscular owls given that prey can usually see an owl approaching. While the morphological and biological mechanisms of this silent flight are more or less unknown, the structure of the feather has been heavily studied and accredited to a large portion of why they have this ability. Owls’ feathers are generally larger than the average birds’ feathers, have fewer radiates, longer pennulum, and achieve smooth edges with different rachis structures.[12] Serrated edges along the owl’s remiges bring the flapping of the wing down to a nearly silent mechanism. The serrations are more likely reducing aerodynamic disturbances, rather than simply reducing noise.[12] The surface of the flight feathers is covered with a velvety structure that absorbs the sound of the wing moving. These unique structures reduce noise frequencies above 2 kHz,[13] making the sound level emitted drop below the typical hearing spectrum of the owl’s usual prey[13][14] and also within the owl’s own best hearing range.[citation needed] This optimizes the owl’s ability to silently fly to capture prey without the prey hearing the owl first as it flies in. It also allows the owl to monitor the sound output from its flight pattern.
The feather adaption that allows silent flight means that barn owl feathers are not waterproof. To retain the softness and silent flight, the barn owl cannot use the preen oil or powder dust that other species use for waterproofing. In wet weather, they cannot hunt and this may be disastrous during the breeding season. Barn owls are frequently found drowned in cattle drinking troughs, since they land to drink and bathe, but are unable to climb out. Owls can struggle to keep warm, because of their lack of waterproofing, so large numbers of downy feathers help them to retain body heat.[15]
Eyesight is a particular characteristic of the owl that aids in nocturnal prey capture. Owls are part of a small group of birds that live nocturnally, but do not use echolocation to guide them in flight in low-light situations. Owls are known for their disproportionally large eyes in comparison to their skulls. An apparent consequence of the evolution of an absolutely large eye in a relatively small skull is that the eye of the owl has become tubular in shape. This shape is found in other so-called nocturnal eyes, such as the eyes of strepsirrhine primates and bathypelagic fishes.[16] Since the eyes are fixed into these sclerotic tubes, they are unable to move the eyes in any direction.[17] Instead of moving their eyes, owls swivel their heads to view their surroundings. Owls' heads are capable of swiveling through an angle of roughly 270°, easily enabling them to see behind them without relocating the torso.[17] This ability keeps bodily movement at a minimum, thus reduces the amount of sound the owl makes as it waits for its prey. Owls are regarded as having the most frontally placed eyes among all avian groups, which gives them some of the largest binocular fields of vision. However, owls are farsighted and cannot focus on objects within a few centimeters of their eyes.[16][18] While owls are commonly believed to have great nocturnal vision due to their large (thus very light-gathering) eyes and pupils and/or extremely sensitive rod receptors, the true cause for their ability to see in the night is due to neural mechanisms which mediate the extraction of spatial information gathered from the retinal image throughout the nocturnal luminance range. These mechanisms are only able to function due to the large-sized retinal image.[19] Thus, the primary nocturnal function in the vision of the owl is due to its large posterior nodal distance; retinal image brightness is only maximized to the owl within secondary neural functions.[19] These attributes of the owl cause its nocturnal eyesight to be far superior to that of its average prey.[19]
Owls exhibit specialized hearing functions and ear shapes that also aid in hunting. They are noted for asymmetrical ear placements on the skull in some genera. Owls can have either internal or external ears, both of which are asymmetrical. Asymmetry has not been reported to extend to the middle or internal ear of the owl. Asymmetrical ear placement on the skull allows the owl to pinpoint the location of its prey. This is especially true for strictly nocturnal species such as the barn owls Tyto or Tengmalm's owl.[17] With ears set at different places on its skull, an owl is able to determine the direction from which the sound is coming by the minute difference in time that it takes for the sound waves to penetrate the left and right ears.[citation needed] The owl turns its head until the sound reaches both ears at the same time, at which point it is directly facing the source of the sound. This time difference between ears is a matter of about 0.00003 seconds, or 30 millionths of a second. Behind the ear openings are modified, dense feathers, densely packed to form a facial ruff, which creates an anterior-facing, concave wall that cups the sound into the ear structure.[20] This facial ruff is poorly defined in some species, and prominent, nearly encircling the face, in other species. The facial disk also acts to direct sound into the ears, and a downward-facing, sharply triangular beak minimizes sound reflection away from the face. The shape of the facial disk is adjustable at will to focus sounds more effectively.[17]
The prominences above a great horned owl's head are commonly mistaken as its ears. This is not the case; they are merely feather tufts. The ears are on the sides of the head in the usual location (in two different locations as described above).
While the auditory and visual capabilities of the owl allow it to locate and pursue its prey, the talons and beak of the owl do the final work. The owl kills its prey using these talons to crush the skull and knead the body.[17] The crushing power of an owl’s talons varies according to prey size and type, and by the size of the owl. The burrowing owl (Athene cunicularia), a small, partly insectivorous owl, has a release force of only 5 N. The larger barn owl (Tyto alba) needs a force of 30 N to release its prey, and one of the largest owls, the great horned owl (Bubo virginianus) needs a force over 130 N to release prey in its talons.[21] An owl’s talons, like those of most birds of prey, can seem massive in comparison to the body size outside of flight. The masked owl has some of the proportionally longest talons of any bird of prey; they appear enormous in comparison to the body when fully extended to grasp prey.[22] An owl’s claws are sharp and curved. The family Tytonidae has inner and central toes of about equal length, while the family Strigidae has an inner toe that is distinctly shorter than the central one.[21] These different morphologies allow efficiency in capturing prey specific to the different environments they inhabit.
The beak of the owl is short, curved, and downward-facing, and typically hooked at the tip for gripping and tearing its prey. Once prey is captured, the scissor motion of the top and lower bill is used to tear the tissue and kill. The sharp lower edge of the upper bill works in coordination with the sharp upper edge of the lower bill to deliver this motion. The downward-facing beak allows the owl’s field of vision to be clear, as well as directing sound into the ears without deflecting sound waves away from the face.[citation needed]
The coloration of the owl’s plumage plays a key role in its ability to sit still and blend into the environment, making it nearly invisible to prey. Owls tend to mimic the colorations and sometimes even the texture patterns of their surroundings, the common barn owl being an exception. Nyctea scandiaca, or the snowy owl, appears nearly bleach-white in color with a few flecks of black, mimicking their snowy surroundings perfectly. Likewise, the mottled wood-owl (Strix ocellata) displays shades of brown, tan, and black, making the owl nearly invisible in the surrounding trees, especially from behind. Usually, the only tell-tale sign of a perched owl is its vocalizations or its vividly colored eyes.
Most owls are nocturnal, actively hunting their prey in darkness. Several types of owls, however, are crepuscular—active during the twilight hours of dawn and dusk; one example is the pygmy owl (Glaucidium). A few owls are active during the day, also; examples are the burrowing owl (Speotyto cunicularia) and the short-eared owl (Asio flammeus).
Much of the owls' hunting strategy depends on stealth and surprise. Owls have at least two adaptations that aid them in achieving stealth. First, the dull coloration of their feathers can render them almost invisible under certain conditions. Secondly, serrated edges on the leading edge of owls' remiges muffle an owl's wing beats, allowing an owl's flight to be practically silent. Some fish-eating owls, for which silence has no evolutionary advantage, lack this adaptation.
An owl's sharp beak and powerful talons allow it to kill its prey before swallowing it whole (if it is not too big). Scientists studying the diets of owls are helped by their habit of regurgitating the indigestible parts of their prey (such as bones, scales, and fur) in the form of pellets. These "owl pellets" are plentiful and easy to interpret, and are often sold by companies to schools for dissection by students as a lesson in biology and ecology.[23]
Owl eggs typically have a white colour and an almost spherical shape, and range in number from a few to a dozen, depending on species and the particular season; for most, three or four is the more common number. In at least one species, female owls do not mate with the same male for a lifetime. Female burrowing owls commonly travel and find other mates, while the male stays in his territory and mates with other females.[24]
The systematic placement of owls is disputed. For example, the Sibley-Ahlquist taxonomy finds that, based on DNA-DNA hybridization, owls are more closely related to the nightjars and their allies (Caprimulgiformes) than to the diurnal predators in the order Falconiformes; consequently, the Caprimulgiformes are placed in the Strigiformes, and the owls in general become a family, the Strigidae. A recent study indicates that the drastic rearrangement of the genome of the accipitrids may have obscured any close relationship of theirs with groups such as the owls.[25] In any case, the relationships of the Caprimulgiformes, the owls, the falcons, and the accipitrid raptors are not resolved to satisfaction; currently, a trend to consider each group (with the possible exception of the accipitrids) as a distinct order is increasing.
Some 220 to 225 extant species of owls are known, subdivided into two families: typical owls (Strigidae) and barn-owls (Tytonidae). Some entirely extinct families have also been erected based on fossil remains; these differ much from modern owls in being less specialized or specialized in a very different way (such as the terrestrial Sophiornithidae). The Paleocene genera Berruornis and Ogygoptynx show that owls were already present as a distinct lineage some 60–57 million years ago (Mya), hence, possibly also some 5 million years earlier, at the extinction of the nonavian dinosaurs. This makes them one of the oldest known groups of non-Galloanserae landbirds. The supposed "Cretaceous owls" Bradycneme and Heptasteornis are apparently nonavialan maniraptors.[26]
During the Paleogene, the Strigiformes radiated into ecological niches now mostly filled by other groups of birds.[clarification needed] The owls as known today, though, evolved their characteristic morphology and adaptations during that time, too. By the early Neogene, the other lineages had been displaced by other bird orders, leaving only barn-owls and typical owls. The latter at that time were usually a fairly generic type of (probably earless) owls similar to today's North American spotted owl or the European tawny owl; the diversity in size and ecology found in typical owls today developed only subsequently.
Around the Paleogene-Neogene boundary (some 25 Mya), barn-owls were the dominant group of owls in southern Europe and adjacent Asia at least; the distribution of fossil and present-day owl lineages indicates that their decline is contemporary with the evolution of the different major lineages of typical owls, which for the most part seems to have taken place in Eurasia. In the Americas, rather an expansion of immigrant lineages of ancestral typical owls occurred.
The supposed fossil herons "Ardea" perplexa (Middle Miocene of Sansan, France) and "Ardea" lignitum (Late Pliocene of Germany) were more probably owls; the latter was apparently close to the modern genus Bubo. Judging from this, the Late Miocene remains from France described as "Ardea" aureliensis should also be restudied.[27] The Messelasturidae, some of which were initially believed to be basal Strigiformes, are now generally accepted to be diurnal birds of prey showing some convergent evolution towards owls. The taxa often united under Strigogyps[28] were formerly placed in part with the owls, specifically the Sophiornithidae; they appear to be Ameghinornithidae instead.[29][30][31]
:For fossil species and paleosubspecies of extant taxa, see the genus and species articles.
Unresolved and basal forms (all fossil)
Fossil genera
Placement unresolved
Fossil genera
Placement unresolved
Among the Kikuyu of Kenya, it was believed that owls were harbingers of death. If one saw an owl or heard its hoot, someone was going to die. In general, owls are viewed as harbingers of bad luck, ill health, or death. The belief is widespread even today.[33]
In Mongolia the owl is regarded as a benign omen. The great warlord Genghis Khan was hiding from enemies in a small coppice. An owl roosted in the tree above him, which caused his pursuers to think no man could be hidden there.[34]
In modern Japan, owls are regarded as lucky and are carried in the form of a talisman or charm.[35]
The modern West generally associates owls with wisdom. This link goes back at least as far as Ancient Greece, where Athens, noted for art and scholarship, and Athena, Athens' patron goddess and the goddess of wisdom, had the owl as a symbol.[36] Marija Gimbutas traces veneration of the owl as a goddess, among other birds, to the culture of Old Europe, long pre-dating Indo-European cultures.[37]
T. F. Thiselton-Dyer in his Folk-lore of Shakespeare says that "from the earliest period it has been considered a bird of ill-omen," and Pliny tells us how, on one occasion, even Rome itself underwent a lustration, because one of them strayed into the Capitol. He represents it also as a funereal bird, a monster of the night, the very abomination of human kind. Virgil describes its death-howl from the top of the temple by night, a circumstance introduced as a precursor of Dido's death. Ovid, too, constantly speaks of this bird's presence as an evil omen; and indeed the same notions respecting it may be found among the writings of most of the ancient poets."[38] A list of "omens drear" in John Keats' Hyperion includes the "gloom-bird's hated screech."[39] Pliny the Elder reports that owl's eggs were commonly used as a hangover cure.[40]
In Hinduism, an owl is the vahana, mount, of the Goddess Lakshmi.
People often allude to the reputation of owls as bearers of supernatural danger when they tell misbehaving children, "the owls will get you",[41] and in most Native American folklore, owls are a symbol of death. For example:
Encouraging natural predators to control rodent population is a natural form of pest control, along with excluding food sources for rodents. Placing a nest box for owls on a property can help control rodent populations (one family of hungry barn owls can consume more than 3,000 rodents in a nesting season) while maintaining the naturally balanced food chain.[53]
Although humans and owls frequently live together in harmony, there have been incidents when owls have attacked humans. In January 2013, a man from Inverness, Scotland suffered heavy bleeding and went into shock after being attacked by an owl, which was likely a 50-cm tall eagle owl.[54] The photographer Eric Hosking lost his left eye after attempting to photograph a tawny owl, which inspired the title of his 1970 autobiography, An Eye for a Bird.
All owls are listed in Appendix II of the international CITES treaty (the Convention on Illegal Trade in Endangered Species of Wild Fauna and Flora). Although owls have long been hunted, a 2008 news story from Malaysia indicates that the magnitude of owl poaching may be on the rise. In November 2008, TRAFFIC reported the seizure of 900 plucked and "oven-ready" owls in Peninsular Malaysia. Said Chris Shepherd, Senior Programme Officer for TRAFFIC's Southeast Asia office, "This is the first time we know of where 'ready-prepared' owls have been seized in Malaysia, and it may mark the start of a new trend in wild meat from the region. We will be monitoring developments closely." TRAFFIC commended the Department of Wildlife and National Parks in Malaysia for the raid that exposed the huge haul of owls. Included in the seizure were dead and plucked barn owls, spotted wood owls, crested serpent eagles, barred eagles, and brown wood owls, as well as 7,000 live lizards.[55]
Wikimedia Commons has media related to Strigiformes. |
Wikispecies has information related to: Strigiformes |
Look up owl in Wiktionary, the free dictionary. |
Eurasia:
North America:
Oceania:
Taxon identifiers |
|
---|
This article uses material from the Wikipedia article "Owl", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,data,libary,model,catalog,rendering,skull,bone,animal,reptile,bird,insect,mammal,class,classification,order,family,species,genus