Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (July 2015) (Learn how and when to remove this template message) |
Seahorses Temporal range: Lower Miocene to present – 23–0 Ma | |
---|---|
Hippocampus sp. | |
Scientific classification | |
Kingdom: | Animalia |
Phylum: | Chordata |
Class: | Actinopterygii |
Order: | Syngnathiformes |
Family: | Syngnathidae |
Subfamily: | Hippocampinae |
Genus: | Hippocampus Rafinesque, 1810[1][2] |
Species | |
see Species. |
Seahorse is the name given to 54 species of small marine fishes in the genus Hippocampus. "Hippocampus" comes from the Ancient Greek word hippos (ἵππος, híppos) meaning "horse" and kampos (κάμπος, kámpos) meaning "sea monster".[3] The word "seahorse" can also be written as two separate words (sea horse), or hyphenated (sea-horse).[4] Having a head and neck suggestive of a horse, seahorses also feature segmented bony armour, an upright posture and a curled prehensile tail.[5]
Seahorses are mainly found in shallow tropical and temperate waters throughout the world, from about 45°S to 45°N [6] and live in sheltered areas such as seagrass beds, estuaries, coral reefs, or mangroves. Four species are found in Pacific waters from North America to South America. In the Atlantic, H. erectus ranges from Nova Scotia to Uruguay. H. zosterae, known as the dwarf seahorse, is found in the Bahamas.
Colonies have been found in European waters such as the Thames Estuary.[7]
Three species live in the Mediterranean Sea: H. guttulatus (the long-snouted seahorse), H. hippocampus (the short-snouted seahorse), and H. fuscus (the sea pony). These species form territories; males stay within 1 m2 (11 sq ft) of habitat, while females range about one hundred times that.
Seahorses range in size from 1.5 to 35.5 cm (0.6 to 14.0 in).[8] They are named for their equine appearance with bent necks and long snouted heads followed by their distinctive trunk and tail. Although they are bony fish, they do not have scales, but rather thin skin stretched over a series of bony plates, which are arranged in rings throughout their bodies. Each species has a distinct number of rings.[9] Seahorses swim upright, another characteristic not shared by their close pipefish relatives, which swim horizontally. Razorfish are the only other fish that swim vertically. They swim upright propelling themselves by using the dorsal fin. The pectoral fins located on either side of the head are used for maneuvering. They lack the caudal fin typical of fishes. Their prehensile tail can only be unlocked in the most extreme conditions. They are adept at camouflage with the ability to grow and reabsorb spiny appendages depending on their habitat.[10]
Unusual among fish, a seahorse has a flexible, well-defined neck. It also sports a crown-like spine or horn on its head, termed a "coronet," which is distinct for each species.[citation needed]
Seahorses swim very poorly, rapidly fluttering a dorsal fin and using pectoral fins (located behind their eyes) to steer. The slowest-moving fish in the world is H. zosterae (the dwarf seahorse), with a top speed of about 5 ft (1.5 m) per hour.[11] Since they are poor swimmers, they are most likely to be found resting with their prehensile tails wound around a stationary object. They have long snouts, which they use to suck up food, and their eyes can move independently of each other like those of a chameleon.[12]
Anatomical evidence, supported by molecular, physical, and genetic evidence, demonstrates seahorses are highly modified pipefish. The fossil record of seahorses, however, is very sparse. The best known and best studied fossils are specimens of H. guttulatus (though literature more commonly refers to them under the synonym of H. ramulosus), from the Marecchia River Formation of Rimini Province, Italy, dating back to the Lower Pliocene, about 3 million years ago. The earliest known seahorse fossils are of two pipefish-like species, H. sarmaticus and H. slovenicus from the coprolitic horizon of Tunjice Hills, a middle Miocene lagerstätte in Slovenia dating back about 13 million years.[13] Molecular dating finds that pipefish and seahorses diverged during the Late Oligocene. This has led to speculation that seahorses evolved in response to large areas of shallow water, newly created as the result of tectonic events. The shallow water would have allowed the expansion of seagrass habitats that selected for the camouflage offered by the seahorses’ upright posture.[14] These tectonic changes occurred in the western Pacific Ocean, pointing to an origin there, with molecular data suggesting two later, separate invasions of the Atlantic Ocean.[15] In 2016, a study published in Nature found the seahorse genome to be the most rapidly evolving fish genome studied so far.[16]
The male seahorse is equipped with a pouch on the ventral, or front-facing, side of the tail. When mating, the female seahorse deposits up to 1,500 eggs in the male's pouch. The male carries the eggs for 9 to 45 days until the seahorses emerge fully developed, but very small. The young are then released into the water, and the male often mates again within hours or days during the breeding season.[17]
Before breeding, seahorses may court for several days. Scientists believe the courtship behavior synchronizes the animals' movements and reproductive states so the male can receive the eggs when the female is ready to deposit them. During this time, they may change color, swim side by side holding tails or grip the same strand of sea grass with their tails, and wheel around in unison in what is known as a "predawn dance". They eventually engage in a "true courtship dance" lasting about 8 hours, during which the male pumps water through the egg pouch on his trunk which expands and opens to display its emptiness. When the female’s eggs reach maturity, she and her mate let go of any anchors and drift upward snout-to-snout, out of the seagrass, often spiraling as they rise. They interact for about 6 minutes, reminiscent of courtship. The female then swims away until the next morning, and the male returns to sucking up food through his snout.[18] The female inserts her ovipositor into the male’s brood pouch and deposits dozens to thousands of eggs. As the female releases her eggs, her body slims while his swells. Both animals then sink back into the seagrass and she swims away.[citation needed]
During fertilization in Hippocampus kuda the brood pouch was found to be open only for six seconds while egg deposition occurred. During this time seawater entered the pouch where the spermatozoa and eggs meet in a seawater milieu. This hyperosmotic environment facilitates sperm activation and motility. The fertilization is therefore regarded as being physiologically ‘external’ within a physically ‘internal’ environment after the closure of the pouch.[19] It is believed that this protected form of fertilization reduces sperm competition among males. Within the Syngnathidae (pipefishes and seahorses) protected fertilization has not been documented in the pipefishes but the lack of any distinct differences in the relation of testes size to body size suggests that pipefishes may also have evolved mechanisms for more efficient fertilization with reduced sperm competition.[20]
The fertilized eggs are then embedded in the pouch wall and become surrounded by a spongy tissue.[21] The male supplies the eggs with prolactin, the same hormone responsible for milk production in pregnant mammals. The pouch provides oxygen, as well as a controlled environment incubator. Though the egg yolk contribute nourishment to the developing embryo, the male sea horses contribute additional nutrients such as energy- rich lipids and also calcium to allow them to build their skeletal system, by secreting them into the brood pouch that are absorbed by the embryos. Further they also offer immunological protection, osmoregulation, gas exchange and waste transport [22]
The eggs then hatch in the pouch, where the salinity of the water is regulated; this prepares the newborns for life in the sea.[18][23][24] Throughout gestation, which in most species requires two to four weeks, his mate visits him daily for “morning greetings”.
The number of young released by the male seahorse averages 100–1000 for most species, but may be as low as 5 for the smaller species, or as high as 2,500. When the fry are ready to be born, the male expels them with muscular contractions. He typically gives birth at night and is ready for the next batch of eggs by morning when his mate returns. Like almost all other fish species, seahorses do not nurture their young after birth. Infants are susceptible to predators or ocean currents which wash them away from feeding grounds or into temperatures too extreme for their delicate bodies. Less than 0.5% of infants survive to adulthood, explaining why litters are so large. These survival rates are actually fairly high compared to other fish, because of their protected gestation, making the process worth the great cost to the father. The eggs of most other fish are abandoned immediately after fertilization.[24]
Reproduction is energetically costly to the male. This brings into question why the sexual role reversal even takes place. In an environment where one partner incurs more energy costs than the other, Bateman's principle suggests that the lesser contributor takes the role of the aggressor. Male seahorses are more aggressive and sometimes “fight” for female attention. According to Amanda Vincent of Project Seahorse, only males tail-wrestle and snap their heads at each other. This discovery prompted further study of energy costs. To estimate the female’s direct contribution, researchers chemically analyzed the energy stored in each egg. To measure the burden on the males, oxygen consumption was used. By the end of incubation, the male consumed almost 33% more oxygen than before mating. The study concluded that the female's energy expenditure while generating eggs is twice that of males during incubation[18] confirming the standard hypothesis.[citation needed]
Why the male seahorse (and other members of the Syngnathidae) carries the offspring through gestation is unknown, though some researchers [25] believe it allows for shorter birthing intervals, in turn resulting in more offspring. Given an unlimited number of ready and willing partners, males have the potential to produce 17% more offspring than females in a breeding season. Also, females have “time-outs” from the reproductive cycle 1.2 times longer than those of males. This seems to be based on mate choice, rather than physiology. When the female’s eggs are ready, she must lay them in a few hours or eject them into the water column. Making eggs is a huge cost to her physically, since they amount to about a third of her body weight. To protect against losing a clutch, the female demands a long courtship. The daily greetings help to cement the bond between the pair.[26]
One common misconception about seahorses is that they mate for life. Many species of seahorses form pair bonds that last through at least the breeding season. Some species show a higher level of mate fidelity than others.[27][28] However, many species readily switch mates when the opportunity arises. H. abdominalis and H. breviceps have been shown to breed in groups, showing no continuous mate preference. Many more species' mating habits have not been studied, so it is unknown how many species are actually monogamous, or how long those bonds actually last.[29]
Although monogamy within fish is not common, it does appear to exist for some. In this case, the mate-guarding hypothesis may be an explanation. This hypothesis states, “males remain with a single female because of ecological factors that make male parental care and protection of offspring especially advantageous.”[30] Because the rates of survival for newborn seahorses are so low, incubation is essential. Though not proven, males could have taken on this role because of the lengthy period the females require to produce their eggs. If males incubate while females prepare the next clutch (amounting to a third of body weight), they can reduce the interval between clutches.[citation needed]
Seahorses feed on small crustaceans floating in the water or crawling on the bottom. With excellent camouflage and patience, seahorses ambush prey that floats within striking range. Mysid shrimp and other small crustaceans are favorites, but some seahorses have been observed eating other kinds of invertebrates and even larval fish. In a study of seahorses, the distinctive head morphology was found to give it a hydrodynamic advantage that creates minimal interference while approaching an evasive prey. Therefore, the seahorse has the ability to come within a very close range of copepods, on which they prey.[31][32] After successfully closing in on the prey without alerting it, the sea horse gives an upward thrust rapidly rotates the head aided by large tendons that store and release elastic energy, to bring its long snout close to the prey.This step is crucial for prey capture as suction only works with the mouth at a close range. This two phase prey capture mechanism is termed pivot-feeding.[32][33]
While feeding, they produce a distinctive click each time a food item is ingested. The same clicks are heard with social interactions.
Because data is lacking on the sizes of the various seahorse populations, as well as other issues including how many seahorses are dying each year, how many are being born, and the number used for souvenirs, there is insufficient information to assess their risk of extinction, and the risk of losing more seahorses remains a concern. Some species, such as the Paradoxical Seahorse, H. paradoxus,[34] may already be extinct. Coral reefs and seagrass beds are deteriorating, reducing viable habitats for seahorses.[35]
While many aquarium hobbyists keep them as pets, seahorses collected from the wild tend to fare poorly in home aquaria. Many eat only live foods such as brine shrimp and are prone to stress, which damages their immune systems and makes them susceptible to disease.[citation needed]
In recent years, however, captive breeding has become more popular. Such seahorses survive better in captivity, and are less likely to carry diseases. They eat frozen mysidacea (crustaceans) that are readily available from aquarium stores,[36] and do not experience the stress of moving out of the wild. Although captive-bred seahorses are more expensive, they take no toll on wild populations.[citation needed]
Seahorses should be kept in an aquarium with low flow and placid tank mates. They are slow feeders, so fast, aggressive feeders will leave them without food.[36] Seahorses can coexist with many species of shrimp and other bottom-feeding creatures. Gobies also make good tank-mates. Keepers are generally advised to avoid eels, tangs, triggerfish, squid, octopus, and sea anemones.[37]
Water quality is very important for the survival of seahorses in an aquarium. They are delicate species which should not be added to a new tank. The water parameters are recommended to be as follows although these fish may acclimatise to different water over time: Temperature: 23–28 °C (73–82 °F) pH: 8.1–8.4 Ammonia: 0 mg/l (0 ppm) (0.01 mg/l (0.01 ppm) may be tolerated for short periods) Nitrite: 0 mg/l (0 ppm) (0.125 mg/l (0.125 ppm) may be tolerated for short periods) S.G.: 1.021–1.024 at 23–24 °C (73–75 °F)[citation needed] A water-quality problem will affect fish behaviour and can be shown by clamped fins, reduced feeding, erratic swimming, and gasping at the surface.[38] Seahorses swim up and down, as well as using the length of the aquarium. Therefore, the tanks should ideally be twice as deep as the length of the adult seahorse.[citation needed]
Animals sold as "freshwater seahorses" are usually the closely related pipefish, of which a few species live in the lower reaches of rivers. The supposed true "freshwater seahorse" called H. aimei is not a valid species, but a synonym sometimes used for Barbour's and hedgehog seahorses. The latter, which is often confused with the former, can be found in estuarine environments, but is not actually a freshwater fish.[39]
Seahorse populations are thought to be endangered as a result of overfishing and habitat destruction. Despite a lack of scientific studies or clinical trials,[40][41] the consumption of seahorses is widespread in traditional Chinese medicine, primarily in connection with impotence, wheezing, nocturnal enuresis, and pain, as well as labor induction.[42] Up to 20 million seahorses may be caught each year to be sold for such uses.[43] Preferred species of seahorses include H. kellogii, H. histrix, H. kuda, H. trimaculatus, and H. mohnikei.[42] Seahorses are also consumed by the Indonesians, the central Filipinos, and many other ethnic groups.
Import and export of seahorses has been controlled under CITES since 15 May 2004. However, Indonesia, Japan, Norway, and South Korea have chosen to opt out of the trade rules set by CITES.
The problem may be exacerbated by the growth of pills and capsules as the preferred method of ingesting seahorses. Pills are cheaper and more available than traditional, individually tailored prescriptions of whole seahorses, but the contents are harder to track. Seahorses once had to be of a certain size and quality before they were accepted by TCM practitioners and consumers. Declining availability of the preferred large, pale, and smooth seahorses has been offset by the shift towards prepackaged preparations, which makes it possible for TCM merchants to sell previously unused, or otherwise undesirable juvenile, spiny, and dark-coloured animals. Today, almost a third of the seahorses sold in China are packaged, adding to the pressure on the species.[44]
Dried seahorse retails from US$600 to $3000 per kilogram, with larger, paler, and smoother animals commanding the highest prices. In terms of value based on weight, seahorses retail for more than the price of silver and almost that of gold in Asia.[45]
As of 2012[update] the 54 recognized species in this genus are:[46]
Pygmy seahorses are less than 15 millimeters (0.59 in) tall and 17 millimeters (0.67 in) wide members of the genus. Previously the term was applied exclusively to the species H. bargibanti but since 1997, discoveries have made this term obsolete. The species H. minotaur, H. denise, H. colemani, H. pontohi, H. severnsi, H. satomiae and H. waleananus have been described. Other species that are believed to be unclassified have also been reported in books, dive magazines and on the Internet. They can be distinguished from other species of seahorse by their 12 trunk rings, low number of tail rings (26–29), the location in which young are brooded in the trunk region of males and their extremely small size.[47] Molecular analysis (of ribosomal RNA) of 32 Hippocampus species found that H. bargibanti belongs in a separate clade from other members of the genus and therefore that the species diverged from the other species in the "ancient" past.[48]
Most pygmy seahorses are well camouflaged and live in close association with other organisms including colonial hydrozoans (Lytocarpus and Antennellopsis), coralline algae (Halimeda) sea fans (Muricella, Annella, Acanthogorgia). This combined with their small size accounts for why most species have only been noticed and classified since 2001.[47][49]
|date=
(help)
Wikimedia Commons has media related to Seahorse. |
Beasts | |
---|---|
Birds | |
Sea creatures | |
Legendary creatures | |
Others |
This article uses material from the Wikipedia article "Seahorse", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,data,libary,model,catalog,rendering,skull,bone,animal,reptile,bird,insect,mammal,class,classification,order,family,species,genus