This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (September 2014) (Learn how and when to remove this template message) |
In probability theory and statistics, a central moment is a moment of a probability distribution of a random variable about the random variable's mean; that is, it is the expected value of a specified integer power of the deviation of the random variable from the mean. The various moments form one set of values by which the properties of a probability distribution can be usefully characterised. Central moments are used in preference to ordinary moments, computed in terms of deviations from the mean instead of from zero, because the higher-order central moments relate only to the spread and shape of the distribution, rather than also to its location.
Sets of central moments can be defined for both univariate and multivariate distributions.
The nth moment about the mean (or nth central moment) of a real-valued random variable X is the quantity μn := E[(X − E[X])n], where E is the expectation operator. For a continuous univariate probability distribution with probability density function f(x), the nth moment about the mean μ is
For random variables that have no mean, such as the Cauchy distribution, central moments are not defined.
The first few central moments have intuitive interpretations:
The nth central moment is translation-invariant, i.e. for any random variable X and any constant c, we have
For all n, the nth central moment is homogeneous of degree n:
Only for n such that n equals 1, 2, or 3 do we have an additivity property for random variables X and Y that are independent:
A related functional that shares the translation-invariance and homogeneity properties with the nth central moment, but continues to have this additivity property even when n ≥ 4 is the nth cumulant κn(X). For n = 1, the nth cumulant is just the expected value; for n = either 2 or 3, the nth cumulant is just the nth central moment; for n ≥ 4, the nth cumulant is an nth-degree monic polynomial in the first n moments (about zero), and is also a (simpler) nth-degree polynomial in the first n central moments.
Sometimes it is convenient to convert moments about the origin to moments about the mean. The general equation for converting the nth-order moment about the origin to the moment about the mean is
where μ is the mean of the distribution, and the moment about the origin is given by
For the cases n = 2, 3, 4 — which are of most interest because of the relations to variance, skewness, and kurtosis, respectively — this formula becomes (noting that and
):,
... and so on,[2] following Pascal's triangle, i.e.
because
The following sum is a stochastic variable having a compound distribution
where the are mutually independent random variables sharing the same common distribution and
a random integer variable independent of the
with its own distribution. The moments of
are obtained as [3]
where is defined as zero for
.
In a symmetric distribution (one that is unaffected by being reflected about its mean), all odd central moments equal zero, because in the formula for the nth moment, each term involving a value of X less than the mean by a certain amount exactly cancels out the term involving a value of X greater than the mean by the same amount.
For a continuous bivariate probability distribution with probability density function f(x,y) the (j,k) moment about the mean μ = (μX, μY) is
This article uses material from the Wikipedia article "Central moment", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Flächenträgheitsmoment