powered by CADENAS

Social Share

Egg carton (6188 views - Basics)

An egg carton (also known as an egg box in British English) is a carton designed for carrying and transporting whole eggs.
Go to Article

Explanation by Hotspot Model

Egg carton

Egg carton

Egg carton

An egg carton (also known as an egg box in British English) is a carton designed for carrying and transporting whole eggs.

Description

These cartons have a dimpled form in which each dimple accommodates an individual egg and isolates that egg from eggs in adjacent dimples. This structure helps protect eggs against stresses exerted during transportation and storage by absorbing a lot of shock and limiting the incidents of fracture to the fragile egg shells. An egg carton can be made of various materials, including foamed plastics such as polystyrene foam, clear plastic or may be manufactured from recycled paper and molded pulp by means of a mechanized papier-mâché process.

Applications

An "egg crate mattress", while following a similar form, is not used for egg transport. It is a light weight camping mattress which makes use of the dimpled structure to distribute and cushion human weight. This foam structure is also occasionally used in packaging to dampen impact of sensitive material during travel.

Egg crate foam is used in shipping boxes and carrying cases to protect transported items.

Similarly, acoustic foam tiles which help in sound proofing and the limitation of acoustic resonance have a similar form to egg crates. Egg crate mattresses are occasionally used as an inexpensive but poor substitute to acoustic foam which must meet noise reduction and fire prevention standards.

Origins

Before its invention, eggs were carried in egg baskets. A predecessor to the modern egg box was invented by Thomas Peter Bethell of Liverpool in 1906 and marketed as the Raylite Egg Box. He created frames of interlocking strips of cardboard. These frames were themselves packed in cardboard or wooden boxes for transport by road or rail.[1]

The egg carton was invented in 1911 by newspaper editor Joseph Coyle of Smithers, British Columbia, to solve a dispute between a local farmer and hotel owner in Aldermere, near present day Telkwa, in British Columbia,[2] over the farmer's eggs often being delivered broken.

A version of the egg carton was patented in 1921 by Morris Koppelman. [3]

The egg carton was patented in 1969 by United Industrial Syndicate in Maine. UIS was a division of The Portland Company. The three inventors listed on the filing are Walter H. Howarth, Gerald A. Snow, and Harold A. Doughty.[4]

Unlike many products, trademarks and advertisements for egg brands are usually printed on the food container itself rather than on a separate container (as with breakfast cereals). This single-layer, distinctive packaging distinguishes egg cartons from different producers or quality on the retail shelf.

Sizes

Standard egg cartons have room for 12 eggs, but they can come in a variety of sizes:

Cartons

  • 3
  • 4
  • 6
  • 8
  • 10
  • 15
  • 18
  • 20

Trays

Trays are usually used to store fresh eggs from farms or at farmers markets. Plastic egg trays are also used by egg processors to wash and sanitize eggs. A cardboard sleeve or additional trays are used to protect eggs when using a tray format.

  • 20
  • 30
  1. ^ Patent GB190606248
  2. ^ B.C. inventor created better way to carry eggs
  3. ^ Koppelman, Morris (Jun 23, 1925), Container for eggs or the like 
  4. ^ A, Doughty Harold; H, Howarth Walter; A, Snow Gerald (Jul 29, 1969), Egg cartons 


This article uses material from the Wikipedia article "Egg carton", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted