powered by CADENAS

Social Share

Icebox (4361 views - Basics)

An icebox (also called a cold closet) is a compact non-mechanical refrigerator which was a common early-twentieth century kitchen appliance before the development of safe powered refrigeration devices.
Go to Article

Explanation by Hotspot Model

Icebox

Icebox

Icebox

Licensed under Public domain in the United States (Unkown).

An icebox (also called a cold closet) is a compact non-mechanical refrigerator which was a common[where?] early-twentieth century kitchen appliance before the development of safe powered refrigeration devices.

Design

Iceboxes had hollow walls that were lined with tin or zinc and packed with various insulating materials such as cork, sawdust, straw or seaweed. A large block of ice was held in a tray or compartment near the top of the box. Cold air circulated down and around storage compartments in the lower section. Some finer models had spigots for draining ice water from a catch pan or holding tank. In cheaper models a drip pan was placed under the box and had to be emptied at least daily. The user had to replenish the melted ice, normally by obtaining new ice from an iceman.

Iceboxes were commonly made of wood, most probably for ease of construction, insulation, and aesthetics; many were handsome pieces of furniture.

Use

Iceboxes date back to the days of ice harvesting, which had hit an industrial high that ran from the mid-19th century to the 1930s, when the refrigerator was introduced into the home. Most municipally consumed ice was harvested in winter from snow-packed areas or frozen lakes, stored in ice houses, and delivered domestically as iceboxes became more common. In 1907 survey of expenditures of New York City inhabitants, 81% of the families surveyed were found to possess "refrigerators" either in the form of ice stored in a tub or iceboxes.[1] The widespread use of iceboxes was partially credited with reduction of US infant mortality in summer months.[2]

With metropolitan growth, many sources of natural ice became contaminated from industrial pollution or sewer runoff. As early mechanical refrigerators became available, they were installed as large industrial plants producing ice for home delivery. Able to produce clean, sanitary ice year-round, their product gradually replaced ice harvested from ponds.

With widespread electrification and safer refrigerants, mechanical refrigeration in the home became possible. With the development of the chlorofluorocarbons (along with the succeeding hydrochlorofluorocarbons and hydrofluorocarbons), that came to replace the use of toxic ammonia gas, the refrigerator replaced the icebox. However, because of the prevalence of the icebox in recent human history, the name "icebox" is still used colloquially for the modern home refrigerator by older persons in some regions.

The horse-drawn ice wagon and the daily occupation of the iceman, who made regular door-to-door deliveries of block ice, was as much a social institution as the milkman.

Apartment buildings had small doors that opened to the ice box from the back porch. The ice man would bring the block of ice and insert it into the ice box through this door. Ice was delivered on a regular basis to these buildings and the people would pay for the ice. Children would go on the ice wagon and take chips of fallen ice as treats during the summer.

See also



This article uses material from the Wikipedia article "Icebox", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted