powered by CADENAS

Social Share

Wright Model B (7753 views - Transportation - Air Water Earth)

The Wright Model B was an early pusher biplane designed by the Wright brothers in the United States in 1910. It was the first of their designs to be built in quantity. Unlike the Model A, it featured a true elevator carried at the tail rather than at the front. It was the last Wright model to have an open-frame tail. The Model B was a dedicated two-seater with the pilot and a passenger sitting side-by-side on the leading edge of the lower wing. Besides their civil market, the Wrights were able to sell aircraft to the Aeronautical Division, U.S. Signal Corps (S.C. 3, 4, and 5) and to the United States Navy as hydroplanes (AH-4, -5-, and -6), in which services they were used as trainers. Furthermore, the Wrights were able to sell licenses to produce the aircraft domestically (to the Burgess Company and Curtis, which designated it Model F), as well as in Germany. The deal with Burgess was the first license-production of aircraft undertaken in the United States and most of the approximately one hundred Model Bs produced were actually built by Burgess. A modified Model B, redesignated Model EX (for Exhibition) achieved fame as the Vin Fiz Flyer, the first aircraft to cross the United States. Burgess also planned a refined version as the Model G, but this was never built.
Go to Article

Explanation by Hotspot Model

Wright Model B

Wright Model B

Model B
Burgess Model F replica preserved at Hill Aerospace Museum. The Burgess was a license-built variant of the Model B.
Role Sports plane
Manufacturer Wright Company
First flight 1910
Number built ca. 100
Unit cost
$5,000

The Wright Model B was an early pusher biplane designed by the Wright brothers in the United States in 1910. It was the first of their designs to be built in quantity. Unlike the Model A, it featured a true elevator carried at the tail rather than at the front. It was the last Wright model to have an open-frame tail. The Model B was a dedicated two-seater with the pilot and a passenger sitting side-by-side on the leading edge of the lower wing.

Besides their civil market, the Wrights were able to sell aircraft to the Aeronautical Division, U.S. Signal Corps (S.C. 3, 4, and 5[1]) and to the United States Navy as hydroplanes (AH-4, -5-, and -6), in which services they were used as trainers. Furthermore, the Wrights were able to sell licenses to produce the aircraft domestically (to the Burgess Company and Curtis, which designated it Model F), as well as in Germany. The deal with Burgess was the first license-production of aircraft undertaken in the United States and most of the approximately one hundred Model Bs produced were actually built by Burgess. A modified Model B, redesignated Model EX (for Exhibition) achieved fame as the Vin Fiz Flyer, the first aircraft to cross the United States. Burgess also planned a refined version as the Model G, but this was never built.

Survivors and replicas

At least three original Model Bs were extant in 2007.


Variants

Model B
Two-seat sports biplane, powered by a 35-hp (26-kW) Wright piston engine.
Model B-1
Civil seaplane variant with two steel and aluminum pontoons.
Model B-2
Civil seaplane variant with a single float.
Model EX
This modified Model B was the first aircraft to cross the United States.
Model F
This version was built under license by the Burgess Company.
Model G
Unbuilt version, it was intended to be built by Burgess Company.
Model G Aeroboat
Two aircraft, built for the US Navy in 1913 and 1914, similar to the Model F, and designated AH-19.

Operators

 United States

Specifications

General characteristics

  • Crew: One pilot
  • Capacity: one passenger
  • Length: 26 ft 0 in (7.93 m)
  • Wingspan: 39 ft 0 in (11.89 m)
  • Height: 8 ft 9 in ( m)
  • Wing area: 480 ft2 (44.6 m2)
  • Empty weight: 800 lb (363 kg)
  • Gross weight: 1,250 lb (567 kg)
  • Powerplant: 1 × Wright Vertical 4, 35 hp (26 kW)

Performance

  • Maximum speed: 45 mph (72 km/h)
  • Cruise speed: 40 mph (64 km/h)
  • Range: 110 miles (177 km)

See also



This article uses material from the Wikipedia article "Wright Model B", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht