powered by CADENAS

Social Share

Classification of Types of Construction (1310 views - Classification & Specification)

The Classification of types of construction (CC), is a nomenclature for the classification of constructions (i.e. buildings) according to their type. It is based on the CPC that was published by the United Nations in 1991. Its final version was approved in 1997. The decimal system classification - each type is qualified by a four-digit number - comprises: 2 Sections (1-digit) - Buildings, Civil engineering works 6 Divisions (2-digit) 20 Groups (3-digit) 46 Classes (4-digit) The CC is a "standard that must be taken into account in recording, collecting, processing, analysing, transmitting and disseminating data on construction works for statistical and record-keeping purposes" in various European countries and Eurostat.
Go to Article

Classification of Types of Construction

Classification of Types of Construction

The Classification of types of construction (CC), is a nomenclature for the classification of constructions (i.e. buildings) according to their type. It is based on the CPC that was published by the United Nations in 1991. Its final version was approved in 1997.[1][2]

The decimal system classification - each type is qualified by a four-digit number - comprises:[3]

  1. 2 Sections (1-digit) - Buildings, Civil engineering works
  2. 6 Divisions (2-digit)
  3. 20 Groups (3-digit)
  4. 46 Classes (4-digit)

The CC is a "standard that must be taken into account in recording, collecting, processing, analysing, transmitting and disseminating data on construction works for statistical and record-keeping purposes" in various European countries and Eurostat.[4][5][6] [7]

  1. ^ "METADATA / Classification of Types of Constructions (1998)". Retrieved 2017-06-20. 
  2. ^ "Glossary:Classification of types of construction (CC)". Retrieved 2017-06-20. 
  3. ^ http://ec.europa.eu/eurostat/ramon/documents/cc/publication/pdf/cc-en.zip
  4. ^ http://europa.eu/rapid/press-release_STAT-01-107_en.pdf
  5. ^ "CC–SI - Classification of Types of Constructions". Statistical Office of the Republic of Slovenia. 
  6. ^ "Polish Classification of Types of Constructions (PKOB)". The Polish Classification of Types of Constructions (PKOB) is a systematized list of construction objects which are the final products of construction activity. It was compiled based on the European Classification of Types of Construction (CC), which is in accordance with the UN recommendations. 
  7. ^ "Building permits issued for construction of new buildings". REPUBLIC OF BULGARIA National statistical institute. 


This article uses material from the Wikipedia article "Classification of Types of Construction", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Classification & Specification

eclass, ecl@ss, cobie,cibse, unspsc, ominclass, uniclass, taric number