powered by CADENAS

Social Share

End terminal (5004 views - Electrical Engineering)

End terminals (wire ferrules) are used to protect the stripped ends of stranded wires so that they can be connected to terminals without damage to individual wires. When using certain clamp types, such as the lift terminals, no wire end ferrules are required.
Go to Article

End terminal

End terminal


End terminals (wire ferrules) are used to protect the stripped ends of stranded wires so that they can be connected to terminals without damage to individual wires. When using certain clamp types, such as the lift terminals, no wire end ferrules are required.

See also



This article uses material from the Wikipedia article "End terminal", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced