Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Aamir515 at en.wikipedia).
A gazebo is a pavilion structure, sometimes octagonal or turret-shaped, often built in a park, garden or spacious public area.[1]
Gazebos are freestanding or attached to a garden wall, roofed, and open on all sides. They provide shade, shelter, ornamental features in a landscape, and a place to rest. Some gazebos in public parks are large enough to serve as bandstands or rain shelters.
Gazebos overlap with pavilions, kiosks,[2] alhambras, belvederes, follies, pergolas, and rotundas. Such structures are popular in warm and sunny climates. They feature in the literature of China, Persia, and many other classical civilizations. Examples of such structures are the garden houses at Montacute House in Somerset, England. The gazebo at Elton on the Hill in Nottinghamshire, thought to date from the late 18th or early 19th century, is a square crenelated, brick and stone tower with an arched opening. It is part of an extensive system of red-brick walled gardens.[3]
In contemporary England and North America, gazebos are typically built of wood and covered with standard roofing materials, such as shingles. Gazebos can be tent-style structures of poles covered by tensioned fabric. Gazebos may have screens to aid in the exclusion of flying insects.
Temporary gazebos are often set up in the campsites of music festivals in the United Kingdom and North America, usually accompanying tents around it.
A structure of a similar type found in villages in the Maldives is known as a holhuashi.[4]
The etymology given by Oxford Dictionaries is "Mid 18th century: perhaps humorously from gaze, in imitation of Latin future tenses ending in -ebo: compare with lavabo."[5] L. L. Bacon put forward a derivation from Casbah, a Muslim quarter around the citadel in Algiers.[6] W. Sayers proposed Hispano-Arabic qushaybah, in a poem by Cordoban poet Ibn Quzman (d. 1160).[7]
The word gazebo was used by British architects John and William Halfpenny in their book Rural Architecture in the Chinese Taste (1750). Plate 55 of the book, "Elevation of a Chinese Gazebo", shows "a Chinese Tower or Gazebo, situated on a Rock, and raised to a considerable Height, and a Gallery round it to render the Prospect more complete."
George Washington had a small eight-sided garden structure at Mount Vernon. Thomas Jefferson wrote about gazebos, then called summerhouses or pavilions.
A gazebo during winter, topped with a weather vane
Gazebo, United States, late 19th century
A gazebo positioned to shade fishing on Lake Mohonk in New York
Gazebo at Lake Junaluska, NC
A two story gazebo at Ammand Dam, Tabriz, Iran.
This article uses material from the Wikipedia article "Gazebo", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library