powered by CADENAS

Social Share

Darlington transistor (5723 views - Electronics & PCB)

In electronics, the Darlington transistor (commonly called a Darlington pair by those in the electronics industry) is a compound structure of a particular design made by two bipolar transistors connected in such a way that the current amplified by the first transistor is amplified further by the second one. This configuration gives a much higher current gain than each transistor taken separately.
Go to Article

Darlington transistor

Darlington transistor

In electronics, the Darlington transistor (commonly called a Darlington pair by those in the electronics industry) is a compound structure of a particular design made by two bipolar transistors connected in such a way that the current amplified by the first transistor is amplified further by the second one.[1] This configuration gives a much higher current gain than each transistor taken separately.

History

The Darlington configuration was invented by Bell Laboratories engineer Sidney Darlington in 1953. He patented the invention of having two or three transistors on a single chip sharing a collector.[2]

Behavior

A Darlington pair behaves like a single transistor[further explanation needed] with a high current gain (approximately the product of the gains of the two transistors[why?]). In fact, integrated devices[clarification needed] have three leads (B, C, and E), broadly analogous to those of a standard transistor.

A general relation between the compound current gain and the individual gains is given by:

If β1 and β2 are high enough (hundreds), this relation can be approximated with:

Advantages

A typical Darlington transistor has a current gain of 1000 or more, so that only a small base current is needed to make the pair switch on. Higher switching currents.

Disadvantages

One drawback is an approximate doubling of the base–emitter voltage. Since there are two junctions between the base and emitter of the Darlington transistor, the equivalent base–emitter voltage is the sum of both base–emitter voltages:

For silicon-based technology, where each VBEi is about 0.65 V when the device is operating in the active or saturated region, the necessary base–emitter voltage of the pair is 1.3 V.

Another drawback of the Darlington pair is its increased "saturation" voltage. The output transistor is not allowed to saturate (i.e. its base–collector junction must remain reverse-biased) because the first transistor, when saturated, establishes full (100%) parallel negative feedback between the collector and the base of the second transistor.[3] Since collector–emitter voltage is equal to the sum of its own base–emitter voltage and the collector-emitter voltage of the first transistor, both positive quantities in normal operation, it always exceeds the base-emitter voltage. (In symbols, always.) Thus the "saturation" voltage of a Darlington transistor is one VBE (about 0.65 V in silicon) higher than a single transistor saturation voltage, which is typically 0.1 - 0.2 V in silicon. For equal collector currents, this drawback translates to an increase in the dissipated power for the Darlington transistor over a single transistor. The increased low output level can cause troubles when TTL logic circuits are driven.

Another problem is a reduction in switching speed or response, because the first transistor cannot actively inhibit the base current of the second one, making the device slow to switch off. To alleviate this, the second transistor often has a resistor of a few hundred ohms connected between its base and emitter terminals.[1] This resistor provides a low-impedance discharge path for the charge accumulated on the base-emitter junction, allowing a faster transistor turn-off.

The Darlington pair has more phase shift at high frequencies than a single transistor and hence can more easily become unstable with negative feedback (i.e., systems that use this configuration can have poor phase margin due to the extra transistor delay).

Packaging

Integrated devices can take less space than two individual transistors because they can use a shared collector. Integrated Darlington pairs come packaged singly in transistor-like packages or as an array of devices (usually eight) in an integrated circuit.

Darlington pairs are available as integrated packages or can be made from two discrete transistors; Q1, the left-hand transistor in the diagram, can be a low power type, but normally Q2 (on the right) will need to be high power. The maximum collector current IC(max) of the pair is that of Q2. A typical integrated power device is the 2N6282, which includes a switch-off resistor and has a current gain of 2400 at IC=10A.

Applications

Safety

A Darlington pair can be sensitive enough to respond to the current passed by skin contact even at safe voltages. Thus it can form the input stage of a touch-sensitive switch.

Amplification

Darlington transistors can be used in high-current[clarification needed] circuits, such as those involving computer control of motors or relays. The current is amplified from the normal low level of the computer output line to the amount needed by the connected device.

See also



This article uses material from the Wikipedia article "Darlington transistor", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electronics & PCB

Cadence, Mentor Graphics, Eagle CAD, Altium Designer, AUTODESK EAGLE, Cadence Allegro, DesignSpark PCB , Mentor PADS, Mentor Xpedition, Novarm DipTrace, Pulsonix, TARGET 3001!, Xpedition xDX Designer, Zuken CADSTAR, Altium P-CAD, Agnisys, Altera Quartus, OrCAD, kiCAD, Solido Design Automation, ELectronics, PCB, Curcuit Board, 3D drawings, 3D library, 3D content, PCB Design, 2D symbols, 2D drawings, 2D icons, 2D schematics