Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article may be too long to read and navigate comfortably. Please consider splitting content into sub-articles, condensing it, or adding or removing subheadings. (October 2016) |
Uses | Application in educational demonstrations, novelty lighting, music |
---|---|
Inventor | Nikola Tesla |
Related items | Transformer, electromagnetic field, resonance |
The Tesla coil is an electrical resonant transformer circuit designed by inventor Nikola Tesla in 1891.[1][2] It is used to produce high-voltage, low-current, high frequency alternating-current electricity.[3][4][5][6][7][8][9] Tesla experimented with a number of different configurations consisting of two, or sometimes three, coupled resonant electric circuits.
Tesla used these circuits to conduct innovative experiments in electrical lighting, phosphorescence, X-ray generation, high frequency alternating current phenomena, electrotherapy, and the transmission of electrical energy without wires. Tesla coil circuits were used commercially in sparkgap radio transmitters for wireless telegraphy until the 1920s,[1][10][11][12][13][14] and in medical equipment such as electrotherapy and violet ray devices. Today their main use is for entertainment and educational displays, although small coils are still used today as leak detectors for high vacuum systems.[9]
A Tesla coil is a radio frequency oscillator that drives an air-core double-tuned resonant transformer to produce high voltages at low currents.[10][15][16][17][18][19] Tesla's original circuits as well as most modern coils use a simple spark gap to excite oscillations in the tuned transformer. More sophisticated designs use transistor or thyristor[15] switches or vacuum tube electronic oscillators to drive the resonant transformer.
Tesla coils can produce output voltages from 50 kilovolts to several million volts for large coils.[15][17][19] The alternating current output is in the low radio frequency range, usually between 50 kHz and 1 MHz.[17][19] Although some oscillator-driven coils generate a continuous alternating current, most Tesla coils have a pulsed output;[15] the high voltage consists of a rapid string of pulses of radio frequency alternating current.
The common spark-excited Tesla coil circuit, shown below, consists of these components:[16][20]
The specialized transformer used in the Tesla coil circuit, called a resonant transformer, oscillation transformer or radio-frequency (RF) transformer, functions differently from an ordinary transformer used in AC power circuits.[21][22][23] While an ordinary transformer is designed to transfer energy efficiently from primary to secondary winding, the resonant transformer is also designed to temporarily store electrical energy. Each winding has a capacitance across it and functions as an LC circuit (resonant circuit, tuned circuit), storing oscillating electrical energy, analogously to a tuning fork. The primary coil (L1) consisting of a relatively few turns of heavy copper wire or tubing, is connected to a capacitor (C1) through the spark gap (SG).[15][16] The secondary coil (L2) consists of many turns (hundreds to thousands) of fine wire on a hollow cylindrical form inside the primary. The secondary is not connected to an actual capacitor, but it also functions as an LC circuit, the inductance of (L2) resonates with stray capacitance (C2), the sum of the stray parasitic capacitance between the windings of the coil, and the capacitance of the toroidal metal electrode attached to the high voltage terminal. The primary and secondary circuits are tuned so they resonate at the same frequency, they have the same resonant frequency. This allows them to exchange energy, so the oscillating current alternates back and forth between the primary and secondary coils.
The peculiar design of the coil is dictated by the need to achieve low resistive energy losses (high Q factor) at high frequencies,[17] which results in the largest secondary voltages:
The output circuit can have two forms:
The circuit operates in a rapid, repeating cycle in which the supply transformer (T) charges the primary capacitor (C1) up, which then discharges in a spark through the spark gap, creating a brief pulse of oscillating current in the primary circuit which excites a high oscillating voltage across the secondary:[18][20][23][27]
This entire cycle takes place very rapidly, the oscillations dying out in a time of the order of a millisecond. Each spark across the spark gap produces a pulse of damped sinusoidal high voltage at the output terminal of the coil. Each pulse dies out before the next spark occurs, so the coil generates a string of damped waves, not a continuous sinusoidal voltage.[18] The high voltage from the supply transformer that charges the capacitor is a 50 or 60 Hz sine wave. Depending on how the spark gap is set, usually one or two sparks occur at the peak of each half-cycle of the mains current, so there are more than a hundred sparks per second. Thus the spark at the spark gap appears continuous, as do the high voltage streamers from the top of the coil.
The supply transformer (T) secondary winding is connected across the primary tuned circuit. It might seem that the transformer would be a leakage path for the RF current, damping the oscillations. However its large inductance gives it a very high impedance at the resonant frequency, so it acts as an open circuit to the oscillating current. If the supply transformer has inadequate leakage inductance, radio frequency chokes are placed in its secondary leads to block the RF current.
To produce the largest output voltage, the primary and secondary tuned circuits are adjusted to resonance with each other.[17][18][21][29] Since the secondary circuit is usually not adjustable, this is generally done by an adjustable tap on the primary coil. If the two coils were separate, the resonant frequencies of the primary and secondary circuits,
and
, would be determined by the inductance and capacitance in each circuit
However, because they are coupled together, the frequency at which the secondary resonates is affected by the primary circuit and the coupling coefficient , and occurs at its antiresonant frequency[30][31]
So resonance, and the highest voltages occur when
Thus the condition for resonance between primary and secondary is
However the Tesla transformer is very loosely coupled, and the coupling coefficient is small, in the range 0.05 to 0.2. So the factor
is close to unity, 0.98 to 0.999, so the two resonant frequencies differ by 2% at most. Therefore, most sources[17][18][21] state the transformer is resonant when the resonant frequencies of primary and secondary are equal.
The resonant frequency of Tesla coils is in the low radio frequency (RF) range, usually between 50 kHz and 1 MHz. However, because of the impulsive nature of the spark they produce broadband radio noise, and without shielding can be a significant source of RFI, interfering with nearby radio and television reception.
In a resonant transformer the high voltage is produced by resonance; the output voltage is not proportional to the turns ratio, as in an ordinary transformer.[23][32] It can be calculated approximately from conservation of energy. At the beginning of the cycle, when the spark starts, all of the energy in the primary circuit is stored in the primary capacitor
. If
is the voltage at which the spark gap breaks down, which is usually close to the peak output voltage of the supply transformer T, this energy is
During the "ring up" this energy is transferred to the secondary circuit. Although some is lost as heat in the spark and other resistances, in modern coils, over 85% of the energy ends up in the secondary.[18] At the peak () of the secondary sinusoidal voltage waveform, all the energy in the secondary
is stored in the capacitance
between the ends of the secondary coil
Assuming no energy losses, . Substituting into this equation and simplifying, the peak secondary voltage is[17][18][23]
|
The second formula above is derived from the first using the resonance condition .[23] Since the capacitance of the secondary coil is very small compared to the primary capacitor, the primary voltage is stepped up to a high value.[18]
It might seem that the output voltage could be increased indefinitely by reducing and
. However, as the output voltage increases, it reaches the point where the air next to the high voltage terminal ionizes and air discharges; coronas, brush discharges and streamer arcs, break out from the terminal. This happens when the electric field strength exceeds the dielectric strength of the air, about 30 kV per centimeter, and occurs first at sharp points and edges on the high voltage terminal. The resulting energy loss damps the oscillation, so the above lossless model is no longer accurate, and the voltage does not reach the theoretical maximum above.[18][23][25] The output voltage of open-air Tesla coils is limited to around several million volts by air breakdown, but higher voltages can be achieved by coils immersed in pressurized tanks of insulating oil.
Most Tesla coil designs have a smooth spherical or toroidal shaped metal electrode on the high voltage terminal. The electrode serves as one plate of a capacitor, with the Earth as the other plate, forming the tuned circuit with the secondary winding. Although the "toroid" increases the secondary capacitance, which tends to reduce the peak voltage, its main effect is that its large diameter curved surface reduces the potential gradient (electric field) at the high voltage terminal, increasing the voltage threshold at which corona and streamer arcs form.[33] Suppressing premature air breakdown and energy loss allows the voltage to build to higher values on the peaks of the waveform, creating longer, more spectacular streamers.[23]
If the top electrode is large and smooth enough, the electric field at its surface may never get high enough even at the peak voltage to cause air breakdown, and air discharges will not occur. Some entertainment coils have a sharp "spark point" projecting from the torus to start discharges.[33]
The term "Tesla coil" is applied to a number of high voltage resonant transformer circuits.
Tesla coil circuits can be classified by the type of "excitation" they use, what type of circuit is used to apply current to the primary winding of the resonant transformer:[34][35]
Tesla circuits can also be classified by how many coils (inductors) they contain:[36][37]
Nikola Tesla patented the Tesla coil circuit April 25, 1891.[44][2] and first publicly demonstrated it May 20, 1891 in his lecture "Experiments with Alternate Currents of Very High Frequency and Their Application to Methods of Artificial Illumination" before the American Institute of Electrical Engineers at Columbia College, New York.[45][46][47] Although Tesla patented many similar circuits during this period, this was the first that contained all the elements of the Tesla coil: high voltage primary transformer, capacitor, spark gap, and air core "oscillation transformer".
During the Industrial Revolution the electrical industry exploited direct current (DC) and low frequency alternating current (AC), but not much was known about frequencies above 20 kHz, what are now called radio frequencies. In 1887, four years previously, Heinrich Hertz had discovered Hertzian waves (radio waves), electromagnetic waves which oscillated at very high frequencies.[49][50][51] This attracted much attention, and a number of researchers began experimenting with high frequency currents.
Tesla's background was in the new field of alternating current power systems, so he understood transformers and resonance.[50][47] In 1888 he decided that high frequencies were the most promising field for research, and set up a laboratory at 33 South Fifth Avenue, New York for researching them, initially repeating Hertz's experiments.
He first developed alternators as sources of high frequency current, but by 1890 found they were limited to frequencies of about 20 kHz.[47] In search of higher frequencies he turned to spark-excited resonant circuits.[50] Tesla's innovation was in applying resonance to transformers.[52] Transformers functioned differently at high frequencies than at the low frequencies used in power systems; the iron core in low frequency transformers caused energy losses due to eddy currents and hysteresis.[50] Tesla[43] [52][47] and Elihu Thomson[42][53][54] independently developed a new type of transformer without an iron core, the "oscillation transformer", and the Tesla coil circuit to drive it to produce high voltages.
Tesla invented the Tesla coil during efforts to develop a "wireless" lighting system, with gas discharge light bulbs that would glow in an oscillating electric field from a high voltage, high frequency power source.[50][47] For a high frequency source Tesla powered a Ruhmkorff coil (induction coil) with his high frequency alternator. He found that the core losses due to the high frequency current overheated the iron core in the Ruhmkorff coil and melted the insulation between the primary and secondary windings. To fix this problem Tesla changed the design so that there was an air gap instead of insulating material between the windings, and made the iron core adjustable so it could be moved in or out of the coil[55] He eventually found the highest voltages could be produced when the iron core was omitted. Tesla also found he needed to put the capacitor normally used in the Ruhmkorff circuit between his alternator and the coil's primary winding to avoid burning out the coil. By adjusting the coil and capacitor Tesla found he could take advantage of the resonance set up between the two to achieve even higher frequencies.[56] He found that the highest voltages were generated when the "closed" primary circuit with the capacitor was in resonance with the "open" secondary winding.[52][47]
Tesla was not the first to invent this circuit.[60][54] Henry Rowland built a spark-excited resonant transformer circuit (above) in 1889[42] and Elihu Thomson had experimented with similar circuits in 1890, including one which could produce 64 inch (1.6 m) sparks,[48][61][62] [41] and other sources confirm Tesla was not the first.[53][63][54] However he was the first to see practical applications for it and patent it. Tesla did not perform detailed mathematical analyses of the circuit, relying instead on trial and error and his intuitive understanding of resonance.[47] He even realized that the secondary coil functioned as a quarter-wave resonator; he specified the length of the wire in the secondary coil must be a quarter wavelength at the resonant frequency.[64][47] The first mathematical analyses of the circuit were done by Anton Oberbeck (1895)[65][54] and Paul Drude (1904).[66][44]
A charismatic showman and self-promoter, in 1891-1893 Tesla used the Tesla coil in dramatic public lectures demonstrating the new science of high voltage, high frequency electricity.[67] The radio frequency AC electric currents produced by a Tesla coil did not behave like the DC or low frequency AC current scientists of the time were familiar with. In lectures at Columbia College May 20, 1891,[45] scientific societies in Britain and France during a 1892 European speaking tour,[69] the Franklin Institute, Philadelphia in February 1893, and the National Electric Light Association, St. Louis in March 1893,[70] he impressed audiences with spectacular brush discharges and streamers, heated iron by induction heating, showed RF current could pass through insulators and be conducted by a single wire without a return path, and powered light bulbs and motors without wires.[67] He demonstrated that high frequency currents often did not cause the sensation of electric shock, applying hundreds of thousands of volts to his own body,[71][67] causing his body to light up with a glowing corona discharge in the darkened room. These lectures introduced the "Tesla oscillator" to the scientific community, and made Tesla internationally famous.[72][51]
Tesla employed the Tesla coil in his efforts to achieve wireless power transmission,[75] his lifelong dream. In the period 1891 to 1900 he used it to perform some of the first experiments in wireless power,[76][77][78] transmitting radio frequency power across short distances by inductive coupling between coils of wire.[77][78][79] In his early 1890s demonstrations such as those before the American Institute of Electrical Engineers[79] and at the 1893 Columbian Exposition in Chicago he lit light bulbs from across a room.[78] He found he could increase the distance by using a receiving LC circuit tuned to resonance with the Tesla coil's LC circuit,[52] transferring energy by resonant inductive coupling.[78] At his Colorado Springs laboratory during 1899-1900, by using voltages of the order of 10 million volts generated by his enormous magnifying transmitter coil (described below), he was able to light three incandescent lamps at a distance of about 100 feet (30 m).[73][6][80] Today the resonant inductive coupling discovered by Tesla is a familiar concept in electronics, widely used in IF transformers and short range wireless power transmission systems[78][81] such as cellphone charging pads.
It is now understood that inductive and capacitive coupling are "near-field" effects,[78] so they cannot be used for long-distance transmission.[73][82][83][84] However, Tesla was obsessed with developing a long range wireless power transmission system which could transmit power from power plants directly into homes and factories without wires, described in a visionary June 1900 article in Century Magazine; "The Problem of Increasing Human Energy".[85] He claimed to be able to transmit power on a worldwide scale, using a method that involved conduction through the Earth and atmosphere.[74][86][87][75][88] Tesla believed that the entire Earth could act as an electrical resonator, and that by driving current pulses into the Earth at its resonant frequency from a grounded Tesla coil with an elevated capacitance, the potential of the Earth could be made to oscillate, creating global standing waves, and this alternating current could be received with a capacitive antenna tuned to resonance with it at any point on Earth.[89][90][91][86] Another of his ideas was that transmitting and receiving terminals could be suspended in the air by balloons at 30,000 feet (9,100 m) altitude, where the air pressure is lower.[90][57][74][75] At this altitude, he thought, a layer of electrically conductive rarefied air would allow electricity to be sent at high voltages (hundreds of millions of volts) over long distances. Tesla envisioned building a global network of wireless power stations, which he called his "World Wireless System", which would transmit both information and electric power to everyone on Earth.[92] There is no reliable evidence that he ever transmitted significant amounts of power beyond the short range demonstrations above.[73][93][77][94][50][95][96][97][98]
Tesla's wireless research required increasingly high voltages, and he had reached the limit of the voltages he could generate within the space of his New York lab. Between 1899-1900 he built a laboratory in Colorado Springs and performed experiments on wireless transmission there.[39] The Colorado Springs laboratory had one of the largest Tesla coils ever built, which Tesla called a "magnifying transmitter" as it was intended to transmit power to a distant receiver.[99] With an input power of 300 kilowatts it could produce potentials of the order of 10 million volts,[39][89] at frequencies of 50–150 kHz, creating huge "lightning bolts" reportedly up to 135 feet long.[17][94] During experiments, it caused an overload which set fire to the alternator of the Colorado Springs power company, destroying it, and Tesla had to rebuild the alternator.[17]
In the magnifying transmitter, Tesla used a modified design (see circuit) which he had been experimenting with since before 1898 and patented in 1902,[38][32] different from his previous double-tuned circuits. In addition to the primary (L1) and secondary (L2) coils, it had a third coil (L3) which he called the "extra" coil, not magnetically coupled to the others, attached to the top terminal of the secondary.[39] When driven by the secondary it produced additional high voltage by resonance, being adjusted to resonate with its own parasitic capacitance (C2)[39] The use of a series-fed resonator coil to generate high voltages was independently discovered by Paul Marie Oudin in 1893 and employed in his Oudin coil.[100]
The Colorado Springs apparatus consisted of a 51-foot (15.5 m) diameter Tesla transformer composed of a secondary winding (L2) of 50 turns of heavy wire wound on an 6-foot (2 m) high circular wooden "fence" around the periphery of the lab, and a single-turn primary (L1) either mounted on the fence or buried in the ground under it.[101][102] The primary was connected to a bank of oil capacitors (C1) to make a tuned circuit, with a rotary spark gap (SG), powered by 20 to 40 kilovolts from a powerful utility step-up transformer (T). The top of the secondary was connected to the 100-turn 8 ft (2.4 m) diameter "extra" or "resonator" coil (L3) in the center of the room. It's high voltage end was connected to a telescoping 143 foot (43.6 m) "antenna" rod with a 30-inch (1 m) metal ball on top which could project through the roof of the lab. By cranking the rod up or down he could adjust the capacitance in the circuit of the extra coil, tuning it to resonance with the rest of the circuit.[103]
In 1901, convinced his wireless theories were correct, Tesla with financing from banker J. P. Morgan began construction of a high-voltage wireless station, now called the Wardenclyffe Tower, at Shoreham, New York.[86][104] Although it was built as a transatlantic radiotelegraphy station, Tesla also intended it to transmit electric power without wires as a prototype transmitter for his proposed "World Wireless System".[99][92] Essentially an enormous Tesla coil, it consisted of a powerhouse with a 400-horsepower generator and a 187-foot (57 m) tower topped by a 68-foot (21 m) diameter metal dome capacitive electrode.[99][105] Underneath the surface was an elaborate ground system that Tesla said was needed to "grip the earth" to create the oscillating earth currents which he believed would transmit the power.
By 1904 his investors had pulled out[92] and the facility was never completed; it was torn down in 1916.[87][99] Although Tesla seems to have believed his wireless power ideas were proven,[94] he had a history of making claims that he had not confirmed by experiment,[106][107][108] and there seems to be no evidence that he ever transmitted significant power beyond the short-range demonstrations mentioned above.[73][93][77][94][50][95][97][98][96] The few reports of long-distance power transmission by Tesla are not from reliable sources. For example, a widely repeated myth is that in 1899 he wirelessly lit 200 light bulbs at a distance of 26 miles (42 km).[93][94] There is no independent confirmation of this supposed demonstration;[93][94] Tesla did not mention it,[94] and it does not appear in his laboratory notes.[89][109] It originated in 1944 from Tesla's first biographer, John J. O'Neill,[6] who said he pieced it together from "fragmentary material... in a number of publications".[110]
In the 100 years since, others such as Robert Golka[101][111][112] have built equipment similar to Tesla's, but long distance power transmission has not been demonstrated,[113][78][6][94] and the scientific consensus is his World Wireless system would not have worked.[114][76][77][87][94][95][107][96] Contemporary scientists point out that while Tesla's coils (with appropriate antennas) can function as radio transmitters, transmitting energy in the form of radio waves, the frequency he used, around 150 kHz, is far too low for practical long range power transmission.[77][94][97] At these wavelengths the radio waves spread out in all directions and cannot be focused on a distant receiver.[76][77][94][95][107] Tesla's world power transmission scheme remains today what it was in Tesla's time: a bold, fascinating dream.[87][95]
One of the largest applications of the Tesla coil circuit was in early radio transmitters called spark gap transmitters. The first radio wave generators, invented by Heinrich Hertz in 1887, were spark gaps connected directly to antennas, powered by induction coils.[118][119][51] Because they lacked a resonant circuit, these transmitters produced highly damped radio waves. As a result, their transmissions occupied an extremely wide bandwidth of frequencies. When multiple transmitters were operating in the same area their frequencies overlapped and they interfered with one another, causing garbled reception. There was no way for a receiver to select one signal over another.[119][118]
In 1892 William Crookes, a friend of Tesla, had given a lecture[120] on the uses of radio waves in which he suggested using resonance to reduce the bandwidth in transmitters and receivers. By using resonant circuits, different transmitters could be "tuned" to transmit on different frequencies. With narrower bandwidth, separate transmitter frequencies would no longer overlap, so a receiver could receive a particular transmission by "tuning" its resonant circuit to the same frequency as the transmitter.[118][51][116] This is the system used in all modern radio.
With an appropriate wire antenna, the Tesla coil circuit could function as such a narrow bandwidth radio transmitter.[10][53][17][1] In his March 1893 St. Louis lecture,[70] Tesla demonstrated a wireless system that was the first use of tuned circuits in radio, although he used it for wireless power transmission, not radio communication.[72][51][121][116][122][123] A grounded spark-excited capacitor-tuned Tesla transformer attached to an elevated wire antenna transmitted radio waves, which were received across the room by a wire antenna attached to a receiver consisting of a second grounded resonant transformer tuned to the transmitter's frequency, which lighted a Geissler tube.[124][118][116][123] This system, patented by Tesla September 2, 1897,[74] was the first use of the "four circuit" concept later claimed by Marconi.[125][123][72][122] However, Tesla was mainly interested in wireless power and never developed a practical radio communication system.[94][8][124][118] In fact, he never believed that radio waves could be used for practical communication, instead clinging to an erroneous theory that radio communication was due to currents in the Earth.[126]
Practical radiotelegraphy communication systems were developed by Guglielmo Marconi beginning in 1895. By 1897 the advantages of narrow-bandwidth (lightly damped) systems noted by Crookes were recognized, and resonant circuits, capacitors and inductors, were incorporated in transmitters and receivers.[121] The "closed primary, open secondary" resonant transformer circuit used by Tesla proved a superior transmitter,[122] because the loosely-coupled transformer partially isolated the oscillating primary circuit from the energy-radiating antenna circuit, reducing the damping, allowing it to produce long "ringing" waves which had a narrower bandwidth.[54][53][118][127] Versions of the circuit were patented by Marconi,[115][122] John Stone Stone[128] and Oliver Lodge,[129] and were widely used in radio for twenty years.[51][121][75][118][116] In 1906 Max Wien invented the quenched or "series" spark gap, which extinguished the spark after the energy had been transferred to the secondary, allowing the secondary to oscillate freely after that, reducing damping and bandwidth still more.
Although their damping had been reduced as much as possible, spark transmitters still produced damped waves which had a wide bandwidth, creating interference with other transmitters. Around 1920 they became obsolete, superseded by vacuum tube transmitters which generated continuous waves at a single frequency, which could also be modulated to carry sound. Tesla's resonant transformer continued to be used in vacuum tube transmitters and receivers, and is a key component in radio to this day.[14]
During the "spark era" the radio engineering profession gave credit to Tesla,[118] his circuit became known as the "Tesla coil" or "Tesla transformer".[51][53][12] However Tesla did not benefit financially, due to competing patent claims. Marconi had claimed rights to the "closed primary open secondary" transmitter circuit in his controversial 1900 "four circuit" wireless patent.[115][125][122][75][116] Tesla sued Marconi in 1915 for patent infringement, but didn't have the resources to pursue the action.[118][122][121][75] However, in 1943, in a separate suit brought by the Marconi Company against the US government for use of its patents in WW1, the US Supreme Court invalidated Marconi's 1900 patent claim to the "four circuit" concept.[130][51][75][116][13] The ruling cited the prior patents of Tesla, Lodge, and Stone,[118][51] but did not decide which of these parties had rights to the circuit.[75][122][116] Of course by this time the issue was moot; the patent had expired in 1915 and spark transmitters had long been obsolete.
Although there is some disagreement over the role Tesla himself played in the invention of radio,[131][51][75][13] sources agree on the importance of his circuit in early radio transmitters.[116][132][17][1][122][118][14] From a modern perspective, most spark transmitters could be regarded as Tesla coils.[17][10]
Tesla had observed as early as 1891 that high frequency currents above 10 kHz did not cause the sensation of electric shock, and in fact currents that would be lethal at lower frequencies could be passed through the body without apparent harm.[134][135][136] He experimented on himself, and claimed daily applications of high voltage relieved depression.[137] He was one of the first to observe the heating effect of high frequency currents on the body, the basis of diathermy.[138][139] During his highly publicized early 1890s demonstrations he passed hundreds of thousands of volts through his body.[71][67] With characteristic hyperbole he called electricity "the greatest of all doctors"[137] and suggested burying wires under classrooms so its stimulating effect would improve performance of "dull" schoolchildren.[139][140] Tesla wrote a pioneering paper in 1898 on the medical uses of high frequency currents[135][141][136] but did little further work on the subject.
A few other researchers were also experimentally applying high frequency currents to the body at this time.[142][143][144][42][145] Elihu Thomson, the co-inventor of the Tesla coil, was one, so in medicine the Tesla coil became known as the "Tesla-Thomson apparatus".[42] In France, from 1889 physician and pioneering biophysicist Jacques d'Arsonval had been documenting the physiological effects of high frequency current on the body, and had made the same discoveries as Tesla.[146][138][145] During his 1892 European trip Tesla met with D'Arsonval and was flattered to find they were using similar circuits. D'Arsonval's spark-excited resonant circuits (above) did not produce as high voltage as the Tesla transformer.[42] In 1893 French physician Paul Marie Oudin added a "resonator" coil to the D'Arsonval circuit to create the high voltage Oudin coil,[145][147] a circuit very similar to the Tesla coil, which was widely used for treating patients in Europe.[42]
During this period, people were fascinated by the new technology of electricity, and many believed it had miraculous curative or "vitalizing" powers.[148] Medical ethics were also looser, and doctors could experiment on their patients. By the turn of the century, application of high voltage, "high frequency" currents to the body had become part of a Victorian era medical field, part legitimate experimental medicine and part quack medicine,[136] called electrotherapy.[148][100][149] Manufacturers produced medical apparatus to generate "Tesla currents", "D'Arsonval currents", and "Oudin currents" for physicians. In electrotherapy, a pointed electrode attached to the high voltage terminal of the coil was held near the patient, and the luminous brush discharges from it (called "effluves") were applied to parts of the body to treat a wide variety of medical conditions. In order to apply the electrode directly to the skin, or tissues inside the mouth, anus or vagina, a "vacuum electrode" was used, consisting of a metal electrode sealed inside a partially evacuated glass tube, which produced a dramatic violet glow. The glass wall of the tube and the skin surface formed a capacitor which limited the current to the patient, preventing discomfort. These vacuum electrodes were later manufactured with handheld Tesla coils to make "violet ray" wands, sold to the public as a quack home medical device.[150][151]
The popularity of electrotherapy peaked after World War 1,[138][148] but by the 1920s authorities began to crack down on fraudulent medical treatments, and electrotherapy largely became obsolete. A part of the field that survived was diathermy, the application of high frequency current to heat body tissue, pioneered by German physician Karl Nagelschmidt in 1907 using Tesla coils.[138][145] By 1930 "long wave" (0.5~2 MHz) Tesla coil diathermy machines were being replaced by "short wave" (10~100 MHz) vacuum tube diathermy machines,[138][145] but Tesla coils continued to be used in both diathermy[138] and quack medical devices like violet ray[150] until World War 2.
During the 1920s and 30s all unipolar (single terminal) high voltage medical coils came to be called Oudin coils, so today's unipolar Tesla coils are sometimes referred to as "Oudin coils".[152]
The Tesla coil's spectacular displays of sparks, and the fact that its currents could pass through the human body without causing electric shock, led to its use in the entertainment business.
In the early 20th century it appeared in traveling carnivals, freak shows and circus and carnival sideshows, which often had an act in which a performer would pass high voltages through his body[71][155][153] [156][157] Performers such as "Dr. Resisto", "The Human Dynamo", "Electrice", "The Great Volta", and "Madamoiselle Electra" would have their body connected to the high voltage terminal of a hidden Tesla coil, causing sparks to shoot from their fingertips and other parts of their body, and Geissler tubes to light up when held in their hand or even brought near them.[154][158] They could also light candles or cigarettes with their fingers.[153] Although they didn't usually cause electric shocks, RF arc discharges from the bare skin could cause painful burns; to prevent them performers sometimes wore metal thimbles on their fingertips[153] (Rev. Moon, center image above, is using them). These acts were extremely dangerous and could kill the performer if the Tesla coil was misadjusted.[156] In carny lingo this was called an "electric chair act" because it often included a spark-laced "electrocution" of the performer in an electric chair,[156][157] exploiting public fascination with this exotic new method of capital punishment, which had become the United States' dominant method of execution around 1900. Today entertainers still perform high voltage acts with Tesla coils,[159][160] but modern bioelectromagnetics has brought a new awareness of the hazards of Tesla coil currents, and allowing them to pass through the body is today considered extremely dangerous.
Tesla coils were also used as dramatic props in early mystery and science fiction motion pictures, starting in the silent era.[71] The crackling, writhing sparks emanating from the electrode of a giant Tesla coil became Hollywood's iconic symbol of the "mad scientist's" lab, recognized throughout the world.[161] This was probably because the eccentric Nikola Tesla himself, with his famous high voltage demonstrations and his mysterious Colorado Springs laboratory, was one of the main prototypes from which the "mad scientist" stock character originated.[161][162] Some early films in which Tesla coils appeared were Wolves of Kultur (1918), The Power God (1926), Metropolis (1927), Frankenstein (1931) and its many sequels such as Son of Frankenstein (1939), The Mask of Fu Manchu (1932), Chandu the Magician (1932), The Lost City (1935), and The Clutching Hand (1936)[163][71] and many later films and television shows. By the 1980s, effects like high voltage sparks were being added to movies by CGI as visual effects in post-production, eliminating the need for dangerous high voltage Tesla coils on sets.
The Tesla coils for many of these movies were constructed by Kenneth Strickfaden (1896-1984) who, beginning with his spectacular effects in the 1931 Frankenstein, became Hollywood's preeminent electrical special effects expert.[71][164] His large "Meg Senior" Tesla coil seen in many of these movies consisted of a 6-foot 1000 turn conical secondary and a 10 turn primary, connected to a capacitor through a rotary spark gap, powered by a 20 kV transformer.[164] It could produce 6 foot sparks. Some of his last gigs were the reassembly of the original 1931 Frankenstein high voltage apparatus for the Mel Brooks satire Young Frankenstein (1974), and construction of a million volt Tesla coil which produced 12 foot sparks for a 1976 stage show by the rock band Kiss.[163]
Ever since Tesla's 1890s lectures, Tesla coils have been used as attractions in educational exhibits and science fairs. They have become a way to counter the stereotype that science is boring.[166] In the early 20th century, experts like Henry Transtrom and Earle Ovington gave high voltage demonstrations at "electric fairs".[154] High school classes built Tesla coils.
From 1933 into the 1980s, between movie jobs Hollywood special effects expert Ken Strickfaden would take his high voltage apparatus on the road in an exhibition called "Science on Parade" and later "The Kenstric Space Age Science Show" to high schools, colleges, World Fairs and expositions.[166] These spectacular shows, which reached 48 states, had a seminal influence on the birth of the modern "coiling" movement.[163] A number of present-day Tesla hobbyists such as William Wysock say they were inspired to build Tesla coils by seeing Strickfaden's show.[166]
One of the oldest and best-known coils still in operation is the "GPO-1" at Griffith Park Observatory in Los Angeles. It was originally one of a pair of coils built in 1910 by Earle L. Ovington, a friend of Tesla and manufacturer of high voltage electrotherapy apparatus.[167][168][71] For a number of years Ovington displayed them at the December electrical trade show at Madison Square Garden in New York City, using them for demonstrations of high voltage science, which Tesla himself sometimes attended.[71] Called the Million Volt Oscillator, the twin coils were installed on the balcony at the show. Every hour the lights were dimmed and the public was treated to a display of 10 foot arcs.[168] Ovington gave the coils to his friend Dr. Frederick Finch Strong, a leading figure in the alternative health field of electrotherapy. In 1937 Strong donated the coils to the Griffith Observatory. The museum didn't have room to display both, but one coil was restored by Kenneth Strickfaden and has been in daily operation ever since.[71] It consists of a 48 in. (1.2 m) high conical secondary coil topped by a 12 in. (30 cm) diameter copper ball electrode, with a 9-turn spiral primary of 2 in. copper strip, a glass plate capacitor (replacing the original Leyden jars), and rotary spark gap.[167] Its output has been estimated at 1.3 million volts.[168]
In addition to its use in spark-gap radio transmitters and electrotherapy described above, the Tesla coil circuit was also used in the early 20th century in x-ray machines, ozone generators for water purification, and induction heating equipment. However, in the 1920s vacuum tube oscillators replaced it in all these applications.[10] The triode vacuum tube was a much better radio frequency current generator than the noisy, hot, ozone-producing spark, and could produce continuous waves. After this, industrial use of the Tesla coil was mainly limited to a few specialized applications which were suited to its unique characteristics, such as high voltage insulation testing.
In 1926, pioneering accelerator physicists Merle Tuve and Gregory Breit built a 5 million volt Tesla coil as a linear particle accelerator.[169][170][171] The bipolar coil consisted of a pyrex tube a meter long wound with 8000 turns of fine wire, with round corona caps on each end, and a 5 turn spiral primary coil surrounding it at the center. It was operated in a tank of insulating oil pressurized to 500 psi which allowed it to reach a potential of 5.2 megavolts. Although it was used for a short period in 1929-30 it was not a success because the particles' acceleration had to be completed within the brief period of a half cycle of the RF voltage.
In 1970 Robert K. Golka built a replica of Tesla's huge Colorado Springs magnifying transmitter in a shed at Wendover Air Force Base, Utah, using data he found in Tesla's lab notes archived at the Nikola Tesla Museum in Beograd, Serbia.[101][111] [112][40] This was one of the first experiments with the magnifier circuit since Tesla's time. The coil generated 12 million volts. Golka used it to try to duplicate Tesla's reported synthesis of ball lightning.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (August 2015) (Learn how and when to remove this template message) |
Modern high-voltage enthusiasts usually build Tesla coils similar to some of Tesla's "later" 2-coil air-core designs. These typically consist of a primary tank circuit, a series LC (inductance-capacitance) circuit composed of a high-voltage capacitor, spark gap and primary coil, and the secondary LC circuit, a series-resonant circuit consisting of the secondary coil plus a terminal capacitance or "top load". In Tesla's more advanced (magnifier) design, a third coil is added. The secondary LC circuit is composed of a tightly coupled air-core transformer secondary coil driving the bottom of a separate third coil helical resonator. Modern 2-coil systems use a single secondary coil. The top of the secondary is then connected to a topload terminal, which forms one 'plate' of a capacitor, the other 'plate' being the earth (or "ground"). The primary LC circuit is tuned so that it resonates at the same frequency as the secondary LC circuit. The primary and secondary coils are magnetically coupled, creating a dual-tuned resonant air-core transformer. Earlier oil-insulated Tesla coils needed large and long insulators at their high-voltage terminals to prevent discharge in air. Later Tesla coils spread their electric fields over larger distances to prevent high electrical stresses in the first place, thereby allowing operation in free air. Most modern Tesla coils also use toroid-shaped output terminals. These are often fabricated from spun metal or flexible aluminum ducting. The toroidal shape helps to control the high electrical field near the top of the secondary by directing sparks outward and away from the primary and secondary windings.
A more complex version of a Tesla coil, termed a "magnifier" by Tesla, uses a more tightly coupled air-core resonance "driver" transformer (or "master oscillator") and a smaller, remotely located output coil (called the "extra coil" or simply the resonator) that has a large number of turns on a relatively small coil form. The bottom of the driver's secondary winding is connected to ground. The opposite end is connected to the bottom of the extra coil through an insulated conductor that is sometimes called the transmission line. Since the transmission line operates at relatively high RF voltages, it is typically made of 1" diameter metal tubing to reduce corona losses. Since the third coil is located some distance away from the driver, it is not magnetically coupled to it. RF energy is instead directly coupled from the output of the driver into the bottom of the third coil, causing it to "ring up" to very high voltages. The combination of the two-coil driver and third coil resonator adds another degree of freedom to the system, making tuning considerably more complex than that of a 2-coil system. The transient response for multiple resonance networks (of which the Tesla magnifier is a sub-set) has only recently been solved.[172] It is now known that a variety of useful tuning "modes" are available, and in most operating modes the extra coil will ring at a different frequency than the master oscillator.[173]
This section does not cite any sources. Please help improve this section by adding citations to reliable sources. Unsourced material may be challenged and removed. (August 2015) (Learn how and when to remove this template message) |
Modern transistor or vacuum tube Tesla coils do not use a primary spark gap. Instead, the transistor(s) or vacuum tube(s) provide the switching or amplifying function necessary to generate RF power for the primary circuit. Solid-state Tesla coils use the lowest primary operating voltage, typically between 155 and 800 volts, and drive the primary winding using either a single, half-bridge, or full-bridge arrangement of bipolar transistors, MOSFETs or IGBTs to switch the primary current. Vacuum tube coils typically operate with plate voltages between 1500 and 6000 volts, while most spark gap coils operate with primary voltages of 6,000 to 25,000 volts. The primary winding of a traditional transistor Tesla coil is wound around only the bottom portion of the secondary coil. This configuration illustrates operation of the secondary as a pumped resonator. The primary 'induces' alternating voltage into the bottom-most portion of the secondary, providing regular 'pushes' (similar to providing properly timed pushes to a playground swing). Additional energy is transferred from the primary to the secondary inductance and top-load capacitance during each "push", and secondary output voltage builds (called 'ring-up'). An electronic feedback circuit is usually used to adaptively synchronize the primary oscillator to the growing resonance in the secondary, and this is the only tuning consideration beyond the initial choice of a reasonable top-load.
In a dual resonant solid-state Tesla coil (DRSSTC), the electronic switching of the solid-state Tesla coil is combined with the resonant primary circuit of a spark-gap Tesla coil. The resonant primary circuit is formed by connecting a capacitor in series with the primary winding of the coil, so that the combination forms a series tank circuit with a resonant frequency near that of the secondary circuit. Because of the additional resonant circuit, one manual and one adaptive tuning adjustment are necessary. Also, an interrupter is usually used to reduce the duty cycle of the switching bridge, to improve peak power capabilities; similarly, IGBTs are more popular in this application than bipolar transistors or MOSFETs, due to their superior power handling characteristics. A current-limiting circuit is usually used to limit maximum primary tank current (which must be switched by the IGBT's) to a safe level. Performance of a DRSSTC can be comparable to a medium-power spark-gap Tesla coil, and efficiency (as measured by spark length versus input power) can be significantly greater than a spark-gap Tesla coil operating at the same input power.
This section does not cite any sources. Please help improve this section by adding citations to reliable sources. Unsourced material may be challenged and removed. (August 2015) (Learn how and when to remove this template message) |
A large Tesla coil of more modern design often operates at very high peak power levels, up to many megawatts (millions of watts[174]). It is therefore adjusted and operated carefully, not only for efficiency and economy, but also for safety. If, due to improper tuning, the maximum voltage point occurs below the terminal, along the secondary coil, a discharge (spark) may break out and damage or destroy the coil wire, supports, or nearby objects.
Tesla experimented with these, and many other, circuit configurations (see right). The Tesla coil primary winding, spark gap and tank capacitor are connected in series. In each circuit, the AC supply transformer charges the tank capacitor until its voltage is sufficient to break down the spark gap. The gap suddenly fires, allowing the charged tank capacitor to discharge into the primary winding. Once the gap fires, the electrical behavior of either circuit is identical. Experiments have shown that neither circuit offers any marked performance advantage over the other.
However, in the typical circuit, the spark gap's short circuiting action prevents high-frequency oscillations from 'backing up' into the supply transformer. In the alternate circuit, high amplitude high frequency oscillations that appear across the capacitor also are applied to the supply transformer's winding. This can induce corona discharges between turns that weaken and eventually destroy the transformer's insulation. Experienced Tesla coil builders almost exclusively use the top circuit, often augmenting it with low pass filters (resistor and capacitor (RC) networks) between the supply transformer and spark gap to help protect the supply transformer. This is especially important when using transformers with fragile high-voltage windings, such as neon sign transformers (NSTs). Regardless of which configuration is used, the HV transformer must be of a type that self-limits its secondary current by means of internal leakage inductance. A normal (low leakage inductance) high-voltage transformer must use an external limiter (sometimes called a ballast) to limit current. NSTs are designed to have high leakage inductance to limit their short circuit current to a safe level.
The primary coil's resonant frequency is tuned to that of the secondary, by using low-power oscillations, then increasing the power (and retuning if necessary) until the system operates properly at maximum power. While tuning, a small projection (called a "breakout bump") is often added to the top terminal in order to stimulate corona and spark discharges (sometimes called streamers) into the surrounding air. Tuning can then be adjusted so as to achieve the longest streamers at a given power level, corresponding to a frequency match between the primary and secondary coil. Capacitive 'loading' by the streamers tends to lower the resonant frequency of a Tesla coil operating under full power. A toroidal topload is often preferred to other shapes, such as a sphere. A toroid with a major diameter that is much larger than the secondary diameter provides improved shaping of the electrical field at the topload. This provides better protection of the secondary winding (from damaging streamer strikes) than a sphere of similar diameter. And, a toroid permits fairly independent control of topload capacitance versus spark breakout voltage. A toroid's capacitance is mainly a function of its major diameter, while the spark breakout voltage is mainly a function of its minor diameter.
While generating discharges, electrical energy from the secondary and toroid is transferred to the surrounding air as electrical charge, heat, light, and sound. The process is similar to charging or discharging a capacitor, except that a Tesla coil uses AC instead of DC. The current that arises from shifting charges within a capacitor is called a displacement current. Tesla coil discharges are formed as a result of displacement currents as pulses of electrical charge are rapidly transferred between the high-voltage toroid and nearby regions within the air (called space charge regions). Although the space charge regions around the toroid are invisible, they play a profound role in the appearance and location of Tesla coil discharges.
When the spark gap fires, the charged capacitor discharges into the primary winding, causing the primary circuit to oscillate. The oscillating primary current creates an oscillating magnetic field that couples to the secondary winding, transferring energy into the secondary side of the transformer and causing it to oscillate with the toroid capacitance to ground. Energy transfer occurs over a number of cycles, until most of the energy that was originally in the primary side is transferred to the secondary side. The greater the magnetic coupling between windings, the shorter the time required to complete the energy transfer. As energy builds within the oscillating secondary circuit, the amplitude of the toroid's RF voltage rapidly increases, and the air surrounding the toroid begins to undergo dielectric breakdown, forming a corona discharge.
As the secondary coil's energy (and output voltage) continue to increase, larger pulses of displacement current further ionize and heat the air at the point of initial breakdown. This forms a very electrically conductive "root" of hotter plasma, called a leader, that projects outward from the toroid. The plasma within the leader is considerably hotter than a corona discharge, and is considerably more conductive. In fact, its properties are similar to an electric arc. The leader tapers and branches into thousands of thinner, cooler, hair-like discharges (called streamers). The streamers look like a bluish 'haze' at the ends of the more luminous leaders. The streamers transfer charge between the leaders and toroid to nearby space charge regions. The displacement currents from countless streamers all feed into the leader, helping to keep it hot and electrically conductive.
The primary break rate of sparking Tesla coils is slow compared to the resonant frequency of the resonator-topload assembly. When the switch closes, energy is transferred from the primary LC circuit to the resonator where the voltage rings up over a short period of time up culminating in the electrical discharge. In a spark gap Tesla coil, the primary-to-secondary energy transfer process happens repetitively at typical pulsing rates of 50–500 times per second, depending on the frequency of the input line voltage. At these rates, previously-formed leader channels do not get a chance to fully cool down between pulses. So, on successive pulses, newer discharges can build upon the hot pathways left by their predecessors. This causes incremental growth of the leader from one pulse to the next, lengthening the entire discharge on each successive pulse. Repetitive pulsing causes the discharges to grow until the average energy available from the Tesla coil during each pulse balances the average energy being lost in the discharges (mostly as heat). At this point, dynamic equilibrium is reached, and the discharges have reached their maximum length for the Tesla coil's output power level. The unique combination of a rising high-voltage radio frequency envelope and repetitive pulsing seem to be ideally suited to creating long, branching discharges that are considerably longer than would be otherwise expected by output voltage considerations alone. High-voltage, low-energy discharges create filamentary multibranched discharges which are purplish-blue in colour. High-voltage, high-energy discharges create thicker discharges with fewer branches, are pale and luminous, almost white, and are much longer than low-energy discharges, because of increased ionisation. A strong smell of ozone and nitrogen oxides will occur in the area. The important factors for maximum discharge length appear to be voltage, energy, and still air of low to moderate humidity. There are comparatively few scientific studies about the initiation and growth of pulsed lower-frequency RF discharges, so some aspects of Tesla coil air discharges are not as well understood when compared to DC, power-frequency AC, HV impulse, and lightning discharges.
Tesla coil circuits were used commercially in sparkgap radio transmitters for wireless telegraphy until the 1920s,[1][10][11] and in electrotherapy and pseudomedical devices such as violet ray. Today, although small Tesla coils are used as leak detectors in scientific high vacuum systems[9] and igniters in arc welders,[175] their main use is entertainment and educational displays, Tesla coils are built by many high-voltage enthusiasts, research institutions, science museums, and independent experimenters. Although electronic circuit controllers have been developed, Tesla's original spark gap design is less expensive and has proven extremely reliable.
Tesla coils are very popular devices among certain electrical engineers and electronics enthusiasts. Builders of Tesla coils as a hobby are called "coilers". A very large Tesla coil, designed and built by Syd Klinge, is shown every year at the Coachella Valley Music and Arts Festival, in Coachella, Indio, California, USA. People attend "coiling" conventions where they display their home-made Tesla coils and other electrical devices of interest. Austin Richards, a physicist in California, created a metal Faraday Suit in 1997 that protects him from Tesla Coil discharges. In 1998, he named the character in the suit Doctor MegaVolt and has performed all over the world and at Burning Man 9 different years.
Low-power Tesla coils are also sometimes used as a high-voltage source for Kirlian photography.[176]
Tesla coils can also be used to generate sounds, including music, by modulating the system's effective "break rate" (i.e., the rate and duration of high power RF bursts) via MIDI data and a control unit. The actual MIDI data is interpreted by a microcontroller which converts the MIDI data into a PWM output which can be sent to the Tesla coil via a fiber optic interface.[177][178] The YouTube video Super Mario Brothers theme in stereo and harmony on two coils shows a performance on matching solid state coils operating at 41 kHz. The coils were built and operated by designer hobbyists Jeff Larson and Steve Ward. The device has been named the Zeusaphone, after Zeus, Greek god of lightning, and as a play on words referencing the Sousaphone. The idea of playing music on the singing Tesla coils flies around the world and a few followers[179] continue the work of initiators. An extensive outdoor musical concert has demonstrated using Tesla coils during the Engineering Open House (EOH) at the University of Illinois at Urbana-Champaign. The Icelandic artist Björk used a Tesla coil in her song "Thunderbolt" as the main instrument in the song. The musical group ArcAttack uses modulated Tesla coils and a man in a chain-link suit to play music.
The world's largest currently existing two-coil Tesla coil is a 130,000-watt unit, part of a 38-foot-tall (12 m) sculpture titled Electrum owned by Alan Gibbs and currently resides in a private sculpture park at Kakanui Point near Auckland, New Zealand.[180] The most powerful conical Tesla coil (1.5 million volts) was installed in 2002 at the Mid-America Science Museum in Hot Springs, Arkansas.[181] This is a replica of the Griffith Observatory conical coil installed in 1936.
Scientists working with high vacuum systems test for the presence of tiny pin holes in the apparatus (especially a newly blown piece of glassware) using high-voltage discharges produced by a small handheld Tesla coil. When the system is evacuated the high voltage electrode of the coil is played over the outside of the apparatus. The discharge travels through any pin hole immediately below it, producing a corona discharge inside the evacuated space which illuminates the hole, indicating points that need to be annealed or reblown before they can be used in an experiment.
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (August 2015) (Learn how and when to remove this template message) |
The dangers of contact with high-frequency electric current are sometimes perceived as being less than at lower frequencies, because the subject usually does not feel pain or a 'shock'. This is often erroneously attributed to skin effect, a phenomenon that tends to inhibit alternating current from flowing inside conducting media. It was thought that in the body, Tesla currents travelled close to the skin surface, making them safer than lower-frequency electric currents.
Although skin effect limits Tesla currents to the outer fraction of an inch in metal conductors, the 'skin depth' of human flesh is deeper than that of a metallic conductor due to higher resistivity and lower permittivity. Calculations of skin depth of body tissues at the frequency of Tesla coils show that it can be greater than the thickness of the body.[182][183][184] Thus there seems to be nothing to prevent high-frequency Tesla currents from passing through deeper portions of a subject's body, such as vital organs and blood vessels, which may be better conducting. The reason for the lack of pain is that a human being's nervous system does not sense the flow of potentially dangerous electric currents above 15–20 kHz; essentially, for nerves to be activated, a significant number of ions must cross their membranes before the current (and hence voltage) reverses. Since the body no longer provides a warning 'shock', novices may touch the output streamers of small Tesla coils without feeling painful shocks. However, anecdotal evidence among Tesla coil experimenters indicates temporary tissue damage may still occur and be observed as muscle pain, joint pain, or tingling for hours or even days afterwards. This is believed to be caused by the damaging effects of internal current flow, and is especially common with continuous wave, solid state or vacuum tube Tesla coils operating at relatively low frequencies (tens to hundreds of kHz). It is possible to generate very high frequency currents (tens to hundreds of MHz) that do have a smaller penetration depth in flesh. These are often used for medical and therapeutic purposes such as electrocauterization and diathermy. The designs of early diathermy machines were based on Tesla coils or Oudin coils.
Large Tesla coils and magnifiers can deliver dangerous levels of high-frequency current, and they can also develop significantly higher voltages (often 250,000–500,000 volts, or more). Because of the higher voltages, large systems can deliver higher energy, potentially lethal, repetitive high-voltage capacitor discharges from their top terminals. Doubling the output voltage quadruples the electrostatic energy stored in a given top terminal capacitance. Professionals usually use other means of protection such as a Faraday cage or a metallic mail suit to prevent dangerous currents from entering their bodies.
The most serious dangers associated with Tesla coil operation are associated with the primary circuit. It is capable of delivering a sufficient current at a significant voltage to stop the heart of a careless experimenter. Because these components are not the source of the trademark visual or auditory coil effects, they may easily be overlooked as the chief source of hazard. Should a high-frequency arc strike the exposed primary coil while, at the same time, another arc has also been allowed to strike to a person, the ionized gas of the two arcs forms a circuit that may conduct lethal, low-frequency current from the primary into the person.
Further, great care must be taken when working on the primary section of a coil even when it has been disconnected from its power source for some time. The tank capacitors can remain charged for days with enough energy to deliver a fatal shock. Proper designs always include 'bleeder resistors' to bleed off stored charge from the capacitors. In addition, a safety shorting operation is performed on each capacitor before any internal work is performed.[185]
This article uses material from the Wikipedia article "Tesla coil", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced