An O-ring, also known as a packing, or a toric joint, is a mechanical gasket in the shape of a torus; it is a loop of elastomer with a round cross-section, designed to be seated in a groove and compressed during assembly between two or more parts, creating a seal at the interface.
The O-ring may be used in static applications or in dynamic applications where there is relative motion between the parts and the O-ring. Dynamic examples include rotating pump shafts and hydraulic cylinder pistons.
O-rings are one of the most common seals used in machine design because they are inexpensive, easy to make, and reliable and have simple mounting requirements. They can seal tens of megapascals (thousands of psi) of pressure.
O-rings can be produced by extrusion, injection molding, pressure molding or transfer molding.[1]
The first patent for the O-ring, is dated May 12, 1896 as a Swedish patent. J. O. Lundberg, the inventor of the O-ring, received the patent.[2] The US patent[3] for the O-ring was filed in 1937 by a then 72-year-old Danish-born machinist, Niels Christensen.[4] Soon after migrating to the USA in 1891, he patented an air brake system for streetcars (trams). Despite his legal efforts, his intellectual property rights were passed from company to company until they ended up at Westinghouse.[4] During World War II, the US government commandeered the O-ring patent as a critical war-related item and gave the right to manufacture to other organizations. Christensen received a lump sum payment of US$75,000 for his efforts. Litigation resulted in a $100,000 payment to his heirs in 1971, 19 years after his death.[5]
O-rings are available in various metric and inch standard sizes. Sizes are specified by the inside diameter and the cross section diameter (thickness). In the US the most common standard inch sizes are per SAE AS568C specification (e.g. AS568-214). ISO 3601-1:2012 contains the most commonly used standard sizes, both inch and metric, worldwide. The UK also has standards sizes known as BS sizes, typically ranging from BS001 to BS932. Several other size specifications also exist.
Successful O-ring joint design requires a rigid mechanical mounting that applies a predictable deformation to the O-ring. This introduces a calculated mechanical stress at the O-ring contacting surfaces. As long as the pressure of the fluid being contained does not exceed the contact stress of the O-ring, leaking cannot occur. Fortunately, the pressure of the contained fluid transfers through the essentially incompressible O-ring material, and the contact stress rises with increasing pressure. For this reason, an O-ring can easily seal high pressure as long as it does not fail mechanically. The most common failure is extrusion through the mating parts.
The seal is designed to have a point contact between the O-ring and sealing faces. This allows a high local stress, able to contain high pressure, without exceeding the yield stress of the O-ring body. The flexible nature of O-ring materials accommodates imperfections in the mounting parts. But it is still important to maintain good surface finish of those mating parts, especially at low temperatures where the seal rubber reaches its glass transition temperature and becomes increasingly crystalline. Surface finish is also especially important in dynamic applications. A surface finish that is too rough will abrade the surface of the O-ring, and a surface that is too smooth will not allow the seal to be adequately lubricated by a fluid film.
In vacuum applications, the permeability of the material makes point contacts quite useless. Instead, higher mounting forces are used and the ring fills the whole groove. Also, round back-up rings are used to save the ring from excessive deformation [6][7][8] Because the ring feels the ambient pressure and the partial pressure of gases only at the seal, their gradients will be steep near the seal and shallow in the bulk (opposite to the gradient of the contact stress [9] See: Vacuum flange#KF.2FQF. High-vacuum systems below 10−9 Torr use copper or nickel O-rings. Also, vacuum systems that have to be immersed in liquid nitrogen use indium O-rings, because rubber becomes hard and brittle at low temperatures.
In some high-temperature applications, O-rings may need to be mounted in a tangentially compressed state, to compensate for the Gow-Joule effect.
O-rings come in a variety of sizes British Standard (BS) which are imperial sizes or metric sizes. Typical dimensions of an O-ring are internal dimension (id), outer dimension (od) and thickness / cross section (cs)
Metric O-rings are usually defined by the internal dimension x the cross section. Typical part number for a metric O-ring - ID x CS [material & shore hardness] 2x1N70 = defines this O-ring as 2mm id with 1mm cross section made from Nitrile rubber which is 70Sh
BS O-rings are defined by a standard reference.
O-ring selection is based on chemical compatibility, application temperature, sealing pressure, lubrication requirements, durometer, size and cost.[10]
Synthetic rubbers - Thermosets:
This section appears to contradict itself on scope of the term "O-ring". Please see the talk page for more information. (November 2014) |
For sealings, there are variations in cross-section design other than circular. The shape can have different profiles, an x-shaped profile, commonly called the X-ring, Q-ring, or by the trademarked name Quad Ring. When squeezed upon installation, they seal with 4 contact surfaces—2 small contact surfaces on the top and bottom. This contrasts with the standard O-ring's comparatively larger single contact surfaces top and bottom. X-rings are most commonly used in reciprocating applications, where they provide reduced running and breakout friction and reduced risk of spiraling when compared to O-rings.
There are also rings with a square profile, commonly called square-cuts, lathe cuts, or Square rings. When O-rings were selling at a premium because of the novelty, lack of efficient manufacturing processes and high labor content, Square rings were introduced as an economical substitution for O-rings. The square ring is typically manufactured by molding an elastomer sleeve which is then lathe-cut. This style of seal is sometimes less expensive to manufacture with certain materials and molding technologies (compression molding, transfer molding, injection molding), especially in low volumes. The physical sealing performance of square rings in static applications is superior to that of O-rings, however in dynamic applications it is inferior to that of O-rings. Square rings are usually only used in dynamic applications as energizers in cap seal assemblies. Square rings can also be more difficult to install than O-rings.
Similar devices with a non-round cross-sections are called seals, packings or gaskets. See also washers.[13]
Automotive cylinder heads are typically sealed by flat gaskets faced with copper.
Knife edges pressed into copper gaskets are used for high vacuum.
Elastomers or soft metals that solidify in place are used as seals.
O-ring materials may be subjected to high or low temperatures, chemical attack, vibration, abrasion, and movement. Elastomers are selected according to the situation.
There are O-ring materials which can tolerate temperatures as low as -200 C or as high as 250+ C. At the low end, nearly all engineering materials become rigid and fail to seal; at the high end, the materials often burn or decompose. Chemical attack can degrade the material, start brittle cracks or cause it to swell. For example, NBR seals can crack when exposed to ozone gas at very low concentrations, unless protected. Swelling by contact with a low viscosity fluid causes an increase in dimensions, and also lowers the tensile strength of the rubber. Other failures can be caused by using the wrong size of ring for a specific recess, which may cause extrusion of the rubber.
Elastomers are sensitive to ionizing radiation. In typical applications, O-rings are well protected from less penetrating radiation such as ultraviolet and soft X-rays, but more penetrating radiation such as neutrons may cause rapid deterioration. In such environments, soft metal seals are used.
There are a few common reasons for O-Ring Failure:
1. Installation Damage – This is caused by improper installation of the O-ring.
2. Spiral Failure – Found on long-stroke piston seals and – to a lesser degree – on rod seals. The seal gets “hung up” at one point on its diameter (against the cylinder wall) and slides and rolls at the same time. This twists the O-ring as the sealed device is cycled and finally causes a series of deep spiral cuts (typically at a 45 degree angle) on the surface of the seal.
3. Explosive Decompression - An O-ring embolism, also called gas expansion rupture, occurs when high pressure gas becomes trapped inside the elastomeric seal element. This expansion causes blisters and ruptures on the surface of the seal.
The failure of an O-ring seal was determined to be the cause of the Space Shuttle Challenger disaster on January 28, 1986. A crucial factor was cold weather prior to the launch. This was famously demonstrated on television by Caltech physics professor Richard Feynman, when he placed a small O-ring into ice-cold water, and subsequently showed its loss of pliability before an investigative committee.
The material of the failed O-ring was FKM, which was specified by the shuttle motor contractor, Morton-Thiokol. When an O-ring is cooled below its Tg (glass transition temperature), it loses its elasticity and becomes brittle. More importantly, when an O-ring is cooled near, but not beyond, its Tg, the cold O-ring, once compressed, will take longer than normal to return to its original shape. O-rings (and all other seals) work by creating positive pressure against a surface thereby preventing leaks. On the night before the launch, exceedingly low air temperatures were recorded. On account of this, NASA technicians performed an inspection. The ambient temperature was within launch parameters, and the launch sequence was allowed to proceed. However, the temperature of the rubber O-rings remained significantly lower than that of the surrounding air. During his investigation of the launch footage, Feynman observed a small out-gassing event from the Solid Rocket Booster (SRB) at the joint between two segments in the moments immediately preceding the disaster. This was blamed on a failed O-ring seal. The escaping high temperature gas impinged upon the external tank, and the entire vehicle was destroyed as a result.
The rubber industry has gone through its share of transformation after the accident. Many O-rings now come with batch and cure date coding, as in the medicine industry, to precisely track and control distribution. For aerospace and military/defense applications, O-rings are usually individually packaged and labeled with the material, cure date, and batch information. O-rings can, if needed, be recalled off the shelf.[14] Furthermore, O-rings and other seals are routinely batch-tested for quality control by the manufacturers, and often undergo Q/A several more times by the distributor and ultimate end users.
As for the SRBs themselves, NASA and Morton-Thiokol redesigned them with a new joint design, which now incorporated three O-rings instead of two, with the joints themselves having onboard heaters that can be turned on when temperatures drop below 50 °F (10 °C). No O-ring issues have occurred since Challenger, and they did not play a role in the Space Shuttle Columbia disaster of 2003.
An O-ring is one of the simplest, yet highly critical, precision mechanical components ever developed. But, there are new advances that may take some of the burden of critical sealing away from the O-ring. There are cottage industries of elastomer consultants assisting in designing O-ring-less pressure vessels. Nano-technology-rubber is one such new frontier. Presently, these advancements are increasing the importance of O-rings. Since O-rings encompass the areas of chemistry and material science, any advancement in nano-rubber will affect the O-ring industry.
Already, there are elastomers filled with nano-carbon and nano-PTFE and molded into O-rings used in high-performance applications. For example, carbon nanotubes are used in electrostatic dissipative applications and nano-PTFE is used in ultra pure semiconductor applications. The use of nano-PTFE in fluoroelastomers and perfluoroelastomers improves abrasion resistance, lowers friction, lowers permeation, and can act as clean filler.
Using conductive carbon black or other fillers can exhibit the useful properties of conductive rubber, namely preventing electrical arcing, static sparks, and the overall build-up of charge within rubber that may cause it to behave like a capacitor (electrostatic dissipative). By dissipating these charges, these materials, which include doped carbon-black and rubber with metal filling additives, reduce the risk of ignition, which can be useful for fuel lines.
This article uses material from the Wikipedia article "O-ring", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD