powered by CADENAS

Social Share

Angular rate sensor (2891 views - Mechanical Engineering)

Rate sensors are devices that directly measure angular rate, without integration in conditioning electronics. Gyroscopes also measure angular rate. Generally gyroscopes are able to measure a constant rotation rate, while rate sensors also include devices with a low cut off frequency that is other than zero.
Go to Article

Angular rate sensor

Angular rate sensor

Rate sensors are devices that directly measure angular rate, without integration in conditioning electronics. Gyroscopes also measure angular rate. Generally gyroscopes are able to measure a constant rotation rate, while rate sensors also include devices with a low cut off frequency that is other than zero.

Technologies

Main technologies for rate sensors:

There are two types of MET rate sensors that directly measure angular rate: one that is able to measure constant angular rate (DC sensitive) and one that is not.

A non–DC-sensitive angular rate sensor consists of a toroid filled with a special electrolyte that moves when the device is rotated about its measurement axis. When this happens the electrolyte flows through the sensing element, which is rigidly fixed inside the channel, and the motion is detected. The output signal is proportional to the angular rate due to internal integration that occurs inside of the sensing element. The cutoff frequency for measurements can be as low as 0.005 Hz.

A DC-sensitive angular rate sensor or gyroscope has a more complex design and uses measurement of Coriolis acceleration to determine angular rate.

Uses

Modern cars typically contain a Yaw-rate sensor.



This article uses material from the Wikipedia article "Angular rate sensor", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD