Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article has multiple issues. Please help improve it or discuss these issues on the talk page. (Learn how and when to remove these template messages)
(Learn how and when to remove this template message)
|
Private | |
Industry | Watch manufacturing |
Founded | 1884 (1884), in Saint-Imier, Switzerland |
Founder | Léon Breitling |
Headquarters | Grenchen, Switzerland |
Number of locations | Switzerland |
Products | Wristwatches |
Owner | CVC Capital Partners |
Website |
www |
Breitling SA (German pronunciation: [braɪtliŋ]) is a Swiss watchmaker based in Grenchen, Switzerland. Founded in 1884 by Léon Breitling in Saint-Imier. Breitling is known for precision-made chronometers useful to aviators.
Breitling SA was founded in Saint-Imier, Bernese Jura by Léon Breitling in 1884.[1]
Breitling watches are made in Switzerland using Swiss components. Breitling makes two movements: the calibre B01 and calibre B04, a B01 with an added GMT module.[2] ETA and Valjoux are the primary suppliers of ébauches used in certain Breitling watches. The ébauches are completed in the Breitling Chronometrie Workshops before undergoing COSC (Contrôle Officiel Suisse des Chronomètres) certification.
In 2009 Breitling developed the B01, a mechanical chronograph movement, used in the Breitling Chronomat 01, the first watch produced entirely by Breitling. The Chronomat has ever since used a Breitling movement with the latest addition (2012) to the range being the Chronomat GMT Limited, a limited edition watch; and the Breitling Chronomat 44 GMT, both with the B04 movement.[citation needed]
In April 2017 it was announced that Breitling had been sold to CVC Capital Partners for over $870m.
The company fits certified chronometers in all models.[3] Watches are usually marketed towards either diving (SuperOcean) or aviation (Navitimer). Aviation models such as the Navitimer offer aviation functions largely as complications, since their function in aviation has largely been replaced by modern electronic instruments. The styling of Breitling watches is characterized by polished cases, bracelets and large watch faces which are designed to improve readability. Many models have an automatic winding mechanism that is purely mechanical (i.e. using no electronic components) and frequently have complications.
In the 1940s, Breitling added a circular slide rule to the bezel of their chronograph models for use by aircraft pilots. This became the famous Navitimer model. During the 1950s and 1960s, a version of the Navitimer was offered by the Aircraft Owners and Pilots Association with the AOPA logo on the dial.
In 1961, Scott Carpenter, one of the original astronauts in the Mercury space program, approached Breitling with idea of incorporating a 24-hour dial instead of the normal 12-hour dial. This was needed because of the lack of day and night during space travel. Breitling complied, and produced the 24-hour Navitimer which Carpenter wore on his 1962 space flight. Breitling then proceeded to produce the 24-hour version as the so-called Cosmonaute Navitimer - under both Breitling and AOPA logos.[4] By the 1990s, the use of logos for military aviation customers had also expanded to include various unit logos on the Aerospace and Chronospace Auto models, primarily those of squadrons and usually part of a group purchase by the pilots and navigators/flight officers of that particular unit.[5]
The Breitling Emergency watch contains a radio transmitter for civil aviation use which broadcasts on the 121.5 MHz distress frequency and serves as a back-up for ELT-type airborne beacons.[6] For military users, the Emergency has a miniaturized transmitter operating on the 243.0 MHz military aviation emergency frequency. Under normal conditions—flat terrain or calm seas—the signal can be picked up at a range of up to 90 nautical miles (167 km) by search aircraft flying at 20,000 feet (6,000 m).[7] Since 1 February 2009, the Cospas-Sarsat Satellite System has not monitored the 121.5/243.0 MHz frequency; however, the signal transmitted by the Emergency was never strong enough to be picked up by satellite, and Breitling has announced that, as these frequencies will still be monitored by aviation, particularly during the localization phase of a rescue attempt, there are no plans to modify the signal's frequency.[citation needed]
Reuters reported that in January 2003 two British pilots, Squadron Leader Steve Brooks and Flight Lieutenant Hugh Quentin-Smith, crashed their helicopter in Antarctica and were rescued after activating their Breitling Emergency transmitter watches.[8]
The Emergency is available for customers who do not hold a pilot's licence, but they must sign an agreement stating that they will bear the full costs of a rescue intervention should they trigger the distress beacon.[citation needed]
The model was heavily advertised by the Breitling Orbiter 3—both Brian Jones and Bertrand Piccard were wearing the Emergency. Breitling sponsored the Orbiter 3 project, which in 1999 became the first balloon to completely orbit the Earth without landing. A commemorative Orbiter 3 version of the Emergency watch was subsequently produced, with a production run of 1,999.
In April 2013, Breitling announced a new version of the Emergency watch.[9] This upgrade transmits on the 121.5 MHz frequency, but adds the 406.04 MHz signal that is monitored by satellites. It has a separate, rechargeable battery for the transmitter.
As part of 10th anniversary of a Breitling–Bentley Motors partnership, the Bentley B04 GMT, B05 Unitime and B06 (based on COSC Certified Breitling Calibre B04, B05 and B06 respectively) were produced.[10]
Breitling was a sponsor of Team Bentley during their Le Mans 24 Hours campaign, running from 2001 to 2003. To commemorate this, it created the Breitling Bentley 24 Le Mans Watch.[citation needed]
In the 1965 James Bond movie Thunderball, Bond is given a Breitling Top Time by Q, who tells him it is also a geiger counter. The geiger counter in the watch enables Bond to track down two stolen nuclear warheads. After the movie was filmed the watch disappeared. In 2012 it resurfaced in a car boot sale in England where it was bought for GB£25. It later sold at auction at Christie's auction house for over GB£100,000.[11][12]
Wikimedia Commons has media related to Breitling. |
This article uses material from the Wikipedia article "Breitling SA", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,brand,good,trademark,company,copyright,good