powered by CADENAS

Social Share

Current sensor (4903 views - Electrical Engineering)

A current sensor is a device that detects electric current (AC or DC) in a wire, and generates a signal proportional to that current. The generated signal could be analog voltage or current or even a digital output. The generated signal can be then used to display the measured current in an ammeter, or can be stored for further analysis in a data acquisition system, or can be used for the purpose of control. The sensed current and the output signal can be: Alternating current input, analog output, which duplicates the wave shape of the sensed current. bipolar output, which duplicates the wave shape of the sensed current. unipolar output, which is proportional to the average or RMS value of the sensed current. Direct current input, unipolar, with a unipolar output, which duplicates the wave shape of the sensed current digital output, which switches when the sensed current exceeds a certain threshold
Go to Article

Current sensor

Current sensor

A current sensor is a device that detects electric current (AC or DC) in a wire, and generates a signal proportional to that current. The generated signal could be analog voltage or current or even a digital output. The generated signal can be then used to display the measured current in an ammeter, or can be stored for further analysis in a data acquisition system, or can be used for the purpose of control.

The sensed current and the output signal can be:

  • Alternating current input,
    • analog output, which duplicates the wave shape of the sensed current.
    • bipolar output, which duplicates the wave shape of the sensed current.
    • unipolar output, which is proportional to the average or RMS value of the sensed current.
  • Direct current input,
    • unipolar, with a unipolar output, which duplicates the wave shape of the sensed current
    • digital output, which switches when the sensed current exceeds a certain threshold

Technologies

The Hall Effect current sensor is a type of current sensor which is based on the Hall Effect phenomenon discovered by Edwin Hall in 1879.

Hall Effect current sensors can measure all types of current signals (i.e. AC, DC, or pulsating current).

These sensors are currently being used widely in many industries because of their vast applications and the type of output they provide, which can be manipulated and can be used for various application.

See also



This article uses material from the Wikipedia article "Current sensor", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced