powered by CADENAS

Social Share

Water sensor (2938 views - Plant Design)

The Water in Fuel Sensor or WiF sensor indicates the presence of water in the fuel. It is installed in the fuel filter and when the water level in the water separator reaches the warning level, the Wif sends an electrical signal to the ECU or to dashboard (lamp). The WiF is used especially in the Common Rail engines to avoid the Fuel injector damage. The WiF sensor uses the difference of electric conductivity through water and diesel fuel by 2 electrodes. First generation WiF sensors use a potting resin to isolate the electronic circuit, while the latest generation of Wif sensors (the WS3 sensor in Surface-mount technology) are made totally without leakage using an innovative co-moulding process. The latest generation of WiF sensors have a high resistance to vibrations and to thermal excursion cycles. The main automotive WiF designer and producer is SMP Poland.
Go to Article

Water sensor

Water sensor

The Water in Fuel Sensor or WiF sensor indicates the presence of water in the fuel. It is installed in the fuel filter and when the water level in the water separator reaches the warning level, the Wif sends an electrical signal to the ECU or to dashboard (lamp). The WiF is used especially in the Common Rail engines to avoid the Fuel injector damage.

The WiF sensor uses the difference of electric conductivity through water and diesel fuel by 2 electrodes.

First generation WiF sensors use a potting resin to isolate the electronic circuit, while the latest generation of Wif sensors (the WS3 sensor in Surface-mount technology) are made totally without leakage using an innovative co-moulding process.

The latest generation of WiF sensors have a high resistance to vibrations and to thermal excursion cycles.

The main automotive WiF designer and producer is SMP Poland.



This article uses material from the Wikipedia article "Water sensor", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Plant Design

Aveva Tribon, Aveva PDMS, Intergraph Smartplant, Intergraph Smartmarine, Offshore, Onshore, Marine, Shipyard, Plantdesign