This article contains content that is written like an advertisement. Please help improve it by removing promotional content and inappropriate external links, and by adding encyclopedic content written from a neutral point of view. (October 2014) (Learn how and when to remove this template message) |
Developer(s) | Spatial Corporation |
---|---|
Stable release |
Version 2017 1.0[1]
/ July 2016 |
Operating system | Windows 7 (and above), Mac OS X (Apple Computer) and Linux (Red Hat) |
Type | 3D modeler |
License | Proprietary software |
Website | www.spatial.com |
The 3D ACIS Modeler (ACIS) is a geometric modeling kernel developed by Spatial Corporation (formerly Spatial Technology), part of Dassault Systemes. ACIS is used by many software developers in industries such as computer-aided design (CAD), computer-aided manufacturing (CAM), computer-aided engineering (CAE), architecture, engineering and construction (AEC), coordinate-measuring machine (CMM), 3D animation, and shipbuilding. ACIS provides software developers and manufacturers the underlying 3D modeling functionality.
ACIS features an open,[citation needed] object-oriented C++ architecture that enables robust, 3D modelling capabilities. ACIS is used to construct applications with hybrid modeling features, since it integrates wireframe model, surface, and solid modeling functionality with both manifold and non-manifold topology, and a rich set of geometric operations.
As a geometric kernel, ACIS is a second generation system, coming after the first generation Romulus.[2]
There are several versions about what the word ACIS actually stands for, or whether it is an acronym at all. The most popular version is that ACIS stands for Alan, Charles, Ian's System (Alan Grayer, Charles Lang and Ian Braid as part of Three-Space Ltd.), or Alan, Charles, Ian and Spatial (as the system was later on sold to Spatial Technology, now Spatial Corp). However, when asked,[by whom?] the creators of ACIS would simply suggest that its name was derived from Greek mythology (See also Acis).[citation needed]
In 1985 Charles Lang and Ian Braid (creators of Romulus and Romulus-D) formed Three-Space Ltd. (Cambridge, England) which had been retained by Dick Sowar's Spatial Technology (which had been founded by Sowar in 1986) to develop the ACIS solid modeling kernel for Spatial Technology's Strata CAM software. The first version of ACIS was released in 1989 and was quickly licensed by HP for integration into its ME CAD software.
In late 2000, around the time when Spatial was acquired by Dassault Systemes, the ACIS file format changed slightly and was no longer openly published.
A software component is a functionally specialized unit of software—a collection of software items (functions, classes, etc.) grouped together to serve some distinct purpose. It serves as a constituent part of a whole software system or product. A product is one or more software components that are assembled together and sold as a package. Components can be arranged in different combinations to form different products.
The ACIS product line is designed using software component technology, which allows an application to use only the components it requires. In some cases, more than one component is available (either from Spatial or third party vendors) for a given purpose, so application developers can use the component that best meets their needs. For example, several rendering components are available from Spatial, and developers use the one that works best for their platform or application.
Platform | Operating System | Compiler | 32-bit | 64-bit |
---|---|---|---|---|
Microsoft | Windows 7 | Visual C++ 2010, Visual C++ 2013, Visual C++ 2013, Visual C++ 2015 | Yes | Yes |
Microsoft | Windows 8, Windows 8.1, Windows 10 | Visual C++ 2010, Visual C++ 2013, Visual C++ 2013, Visual C++ 2015 | No | Yes |
Red Hat | Enterprise Linux, Version 5.0, Enterprise Linux, Version 6.0, Enterprise Linux, Version 7.0 | GNU C++ gcc 4.1.2 | Yes | Yes |
Apple | OS X 10.7.5, OS X 10.10 | Clang version 4.1 compiler 64-bit | No | Yes |
ACIS core functionality[3] can be subclassified into three categories, namely:
ACIS saves modeling information to external files which have an open format allowing external applications, even those not based on ACIS, access to the ACIS geometric model. The basic information needed to understand the ACIS file format (focusing on the reading, or restore, operation), includes the structure of the save file format, how data is encapsulated, the types of data written, and subtypes and references.
ACIS supports two kinds of save files, Standard ACIS Text (SAT), and Standard ACIS Binary (SAB). The two formats store identical information, so the term SAT file is generally used to refer to either when no distinction is needed.
In the narrow sense, SAT files are ASCII text files that may be viewed with a simple text editor. A SAT file contains carriage returns, white space and other formatting that makes it readable to the human eye. A SAT file has a .sat file extension.
SAB files cannot be viewed with a simple text editor and are meant for compactness and not for human readability. A SAB file has a .sab file extension. A SAB file uses delimiters between elements and binary tags, without additional formatting.
A save file contains:
Beginning with ACIS Release 6.3, it is required that the product ID and units be populated for the file header before you can save a SAT file.
ACIS is currently being developed by Spatial. They maintain the concept of a current version (release) number in ACIS, as well as a save version number. The save version allows one to create a SAT save file that can be read by a previous version of ACIS.
Beginning with ACIS Release 4.0, the SAT save file format does not change with minor releases, only with major releases. This allows applications that are based upon the same major version of ACIS to exchange data without being concerned about the save version. To provide this interoperability in a simple implementation, ACIS save files have contained a symbol that accurately identified the major version number, but not the minor version. This meant that applications created using the same major version of ACIS would produce compatible save files, regardless of their minor versions. This was accomplished by simply not incrementing the internal minor version number between major versions.
Beginning with Release 7.0, ACIS started again providing accurate major, minor, and point version numbers. Beginning with Release 2016 1.0 in September, 2015, Spatial updated to Semantic Versioning, and now describes versions by the model year and major, minor and point releases within that model year.
To summarize how release numbers and SAT changes are related:
Release | Date |
---|---|
2017 1.0 | July 2016 |
2016 1.0 | September 2015 |
R25 | July 2014 |
R24 | June 2013 |
R23 | August 2012 |
R22 | July 2011 |
R21 | May 2010 |
R20 | May 2009 |
R19 | July 2008 |
R18 | November 2007 |
R17 | April 2007 |
R16 | January 2006 |
In 2013 the following software uses ACIS as its geometric kernel/engine: AutoCAD, BricsCAD, SpaceClaim[4] and Cimatron.
This article uses material from the Wikipedia article "ACIS", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,Models,Catalogs,Drawings,Library,Symbols,Objects,OEM