Developer | CNC Software inc. |
---|---|
Latest release | Mastercam 2018 |
Available in | multi-language |
License | proprietary |
Official website | Official web page |
Founded in MA in 1983,[1] CNC Software, Inc. is one of the oldest developers of PC-based computer-aided design / computer-aided manufacturing (CAD/CAM) software. They are one of the first to introduce CAD/CAM software designed for both machinists and engineers. Mastercam, CNC Software’s main product, started as a 2D CAM system with CAD tools that let machinists design virtual parts on a computer screen and also guided computer numerical controlled (CNC) machine tools in the manufacture of parts. Since then, Mastercam has grown into the most widely used CAD/CAM package in the world.[2] CNC Software, Inc. is now located in Tolland, Connecticut.
Mastercam’s comprehensive set of predefined toolpaths—including contour, drill, pocketing, face, peel mill, engraving, surface high speed, advanced multiaxis, and many more—enable machinists to cut parts efficiently and accurately. Mastercam users can create and cut parts using one of many supplied machine and control definitions, or they can use Mastercam’s advanced tools to create their own customized definitions.
Mastercam also offers a level of flexibility that allows the integration of 3rd party applications, called C-hooks, to address unique machine or process specific scenarios.
Mastercam's name is a double entendre: it implies mastery of CAM (computer-aided manufacturing), which involves today's latest machine tool control technology; and it simultaneously pays homage to yesterday's machine tool control technology by echoing the older term master cam, which referred to the main cam or model that a tracer followed in order to control the movements of a mechanically automated machine tool.
With the release of Mastercam 2017, Mastercam entered the 3rd interface in the product history moving to a familiar Windows Office tab format. Prior to Mastercam 2017 was Version X that was introduced in 2005. With Verison X the application became a true Windows-based application, as opposed to one ported over from DOS. It also represented a fundamental shift in the way the application was configured. Mastercam supports many types of machines, each with a choice of levels of functionality, as well as offers optional add-ins for 4-axis and 5-axis machining. The following list describes the Mastercam product levels that were updated with the release of Matercam 2017:
The Router products are targeted to the woodworking industries but are virtually identical to the Mill line with additional of support for router specific functions such as aggregate heads, drill blocks and saws.
CAM software | |
---|---|
Open source | |
Proprietary |
This article uses material from the Wikipedia article "Mastercam", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,Models,Catalogs,Drawings,Library,Symbols,Objects,OEM