powered by CADENAS

Social Share

Dive Xtras (141 views - Manufacturer & Supplier)

Dive Xtras is a manufacturer of diver propulsion vehicles (DPVs) or dive scooters in Mukilteo, Washington, United States.
Go to Article

Dive Xtras

Dive Xtras

Dive Xtras is a manufacturer of diver propulsion vehicles (DPVs) or dive scooters in Mukilteo, Washington, United States.

History

Established in 2003 by Ben McGeever and Andrew Georgitsis, Dive Xtras introduced their first DPV in 2005.[1] This DPV was innovative in that it was the first to utilize a brushless motor and electronic speed control. The combination of these features with NiMh battery technology drastically reduced the weight of DPVs at the time.[2][3][4]

Models

  • Sierra Std - The Sierra standard body X-Scooter is the lightest scooter in the Dive Xtras family.
  • CUDA 400 - NiMh version of the CUDA Fury 1150 (aka mini CUDA).
  • CUDA 550 - The first "CUDA". Slightly shorter than the 650. Used a 550 watt hour battery pack.
  • CUDA 650 - The CUDA 650 is the front runner of the CUDA models. At 53 lbs, it is a lightweight compared to more traditional lead acid scooters, yet packs the performance of a heavyweight.
  • Cuda 850 - Second production CUDA model. Longer than the 650.
  • CUDA Fury 1150 - This X-Scooter sets new standards for performance. Only 5 lbs/2 kg heavier than a Sierra, but with the performance of almost two CUDA 650s.
  • Piranha - Next generation of DPVs. Completely modular scooter giving the diver the ability to choose 1, 2, or 3 batteries and easily swap them out at a moment's notice. It has the best power to weight ratio on the DPV market at 25lb-2.5hrs (P1), 34lb-5hrs (P2), & 43lb-7.5hrs (P3).

Accessories

On December 15, 2011 Dive Xtras filed a patent for a "Device for Operating Touch Screen Devices in a Protective Housing." On March 20, 2012 Dive Xtras announced on their website a depth rated underwater housing for a Samsung Galaxy Tab 7 Plus. The housing gives the user full operation of the tablet underwater by using a mouse-like device to interact with a touch screen.

Military use

Dive Xtras DPVs are used by various military forces around the world to aid in various maritime interdiction tasks.[5] In addition to the units sold into Canada, various South East Asian navies currently use a modified version of the Dive Xtras CUDA. Military products are primarily distributed by Divex Asia Pacific in southeast Asia.

In the media

  • Featured in Mission: Impossible III. Ethan Hunt (Tom Cruise) is rescued by Luther (Ving Rhames) when he uses a Sierra X-Scooter to tow himself and gear scuba diving under the Vatican.
  • In the book Pulse, by Jeremy Robinson, a Dive Xtras DPV (Sierra CSI) is used.[6]
  • Photos of Dive Xtras DPVs often appear in diving publications, as they are frequently used during diving activities noteworthy enough to warrant publication.[7][8][9][10]

Claroworks and Google Streetview underwater

The product development arm of Dive Xtras, Claroworks, designed and built the camera systems used by the Catlin Seaview Survey[11] and Google to map the Galápagos Islands.[12][13] The camera system, Seaview SVII, shoots 360-degree images, and is mounted on a modified Cuda 650 vehicle. The Seaview SVII also uses Dive Xtras tablet housing for controls.

  1. ^ staff (2006). "X-Scooter by Dive Xtras". Advanced Diver Magazine (22): 65–67. Retrieved 2013-04-08.
  2. ^ X-Ray Magazine, Global, Issue 26, Girls On Speed
  3. ^ Diver Magazine DPV review 2005 Archived July 10, 2011, at the Wayback Machine
  4. ^ TahoeBenchmark2008 Page 21, Design Efficiency Results
  5. ^ Canadian Forces Lookout Magazine, Feb 1st 2010
  6. ^ Pulse, A book by Jeremy Robinson ISBN 0-312-54028-0
  7. ^ DYK Magazine, Scandinavia, Issue 11, Monkey Diving. Original
  8. ^ X-Ray Magazine, Global, Issue 31, Extreme Exploration Dives, Goto Page 16
  9. ^ UnderWater magazine, Volume 18
  10. ^ Deeper Blue News, Formula 3 Freediving
  11. ^ Technology, Catlin SeaView Survey
  12. ^ Googles launch Video
  13. ^ Behind the scenes


This article uses material from the Wikipedia article "Dive Xtras", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Manufacturer & Supplier

3D,supplier,distributor,manufacturer,B2B, purchase, procure, sourcing,e-procurement,buy,sell,products