powered by CADENAS

Social Share

Compressed air (14396 views - Mechanical Engineering)

Compressed air is air kept under a pressure that is greater than atmospheric pressure. Compressed air is an important medium for transfer of energy in industrial processes. Compressed air is used for power tools such as air hammers, drills, wrenches and others. Compressed air is used to atomize paint, to operate air cylinders for automation, and can also be used to propel vehicles.Brakes applied by compressed air made large railway trains safer and more efficient to operate. Compressed air brakes are also found on large highway vehicles. In Europe, 10 percent of all industrial electricity consumption is to produce compressed air—amounting to 80 terawatt hours consumption per year.
Go to Article

Compressed air

Compressed air

Compressed air is air kept under a pressure that is greater than atmospheric pressure. Compressed air is an important medium for transfer of energy in industrial processes. Compressed air is used for power tools such as air hammers, drills, wrenches and others. Compressed air is used to atomize paint, to operate air cylinders for automation, and can also be used to propel vehicles.Brakes applied by compressed air made large railway trains safer and more efficient to operate. Compressed air brakes are also found on large highway vehicles.

In Europe, 10 percent of all industrial electricity consumption is to produce compressed air—amounting to 80 terawatt hours consumption per year.[1][2]

History

Industrial use of piped compressed air for power transmission was developed in the mid 19th century; unlike steam, compressed air could be piped for long distances without losing pressure due to condensation. An early major application of compressed air was in the drilling of the Mont Cenis Tunnel in Switzerland in 1861, where a 600 kPa (87 psi) compressed air plant provided power to pneumatic drills, increasing productivity greatly over previous manual drilling methods. Compressed air drills were applied at mines in the United States in the 1870s. George Westinghouse invented air brakes for trains starting in 1869; these brakes considerably improved the safety of rail operations. [3]In the 19th century, Paris had a system of pipes installed for municipal distribution of compressed air to power machines and to operate generators for lighting. Early air compressors were steam-driven, but in certain locations a trompe could directly obtain compressed air from the force of falling water. [4]

Uses of compressed air

In industry, compressed air is so widely used that it is often regarded as the fourth utility, after electricity, natural gas and water. However, compressed air is more expensive than the other three utilities when evaluated on a per unit energy delivered basis.[5]

Compressed air is used for many purposes, including:

Design of systems

Compressor rooms must be designed with ventilation systems to remove waste heat produced by the compressors. [8]

When air at atmospheric pressure is compressed, it contains much more water vapor than the high-pressure air can hold. Relative humidity is governed by the properties of water and is not affected by air pressure. Management of the excessive moisture is a requirement of a compressed air distribution system. System designers must ensure that piping maintains a slope, to prevent accumulation of moisture in low parts of the piping system. Drain valves may be installed at multiple points of a large system to allow trapped water to be blown out. Taps from piping headers may be arranged at the tops of pipes, so that moisture is not carried over into piping branches feeding equipment. [9] Piping sizes are selected to avoid excessive energy loss in the piping system due to excess velocity in straight pipes at times of peak demand, [10]or due to turbulence at pipe fittings. [11]


See also



This article uses material from the Wikipedia article "Compressed air", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD