Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article does not cite any sources. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (November 2012) (Learn how and when to remove this template message) |
A cold start is an attempt to start a vehicle's engine when it is cold, relative to its normal operating temperature, often due to normal cold weather. A cold start situation is commonplace, as weather conditions in most climates will naturally be at a lower temperature than the typical operating temperature of an engine. Occasionally, the term also refers to starting the engine of a vehicle that has been inactive or abandoned for a significant amount of time such as months, years or even decades.
Cold starts are more difficult than starting a vehicle that has been run recently (typically between 90 minutes and 2 hours). More effort is needed to turn over a cold engine for multiple reasons:
The problem of cold starting has been greatly reduced since the introduction of engine starters, which are now commonplace on all modern vehicles. The higher revs that can be achieved using electric starter motors improves the chance of successful ignition.
Starting fluid, a volatile liquid, is sometimes sprayed into the combustion chamber of an engine to assist the starting procedure.
Diesel engines make use of glow plugs to heat the combustion chamber prior to ignition, improving the conditions inside the engine, while certain manufacturers have incorporated a block heater, which heats the engine block prior to ignition to reduce the problem of cold starting.
This automobile-related article is a stub. You can help Wikipedia by expanding it. |
This article uses material from the Wikipedia article "Cold start (automotive)", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD