powered by CADENAS

Social Share

Amazon

Playground slide (1169 views - Entertainment)

Playground slides are found in parks, schools, playgrounds and backyards. The slide is an example of the simple machine known as the inclined plane, which makes moving objects up and down easier, or in this case more fun. The slide may be flat, or half cylindrical or tubular to prevent falls. Slides are usually constructed of plastic or metal and they have a smooth surface that is either straight or wavy. The user, typically a child, climbs to the top of the slide via a ladder or stairs and sits down on the top of the slide and slides down the chute. In Australia and New Zealand the playground slide is known as a slide, slippery slide, slipper slide or slippery dip depending on the region. Sliding pond or sliding pon is a term used in the New York City area, It is a corruption of "slide upon". Whereas sliding board is used in the Philadelphia area and other parts of the Mid-Atlantic.
Go to Article

Explanation by Hotspot Model

Youtube


    

Playground slide

Playground slide

Playground slides are found in parks, schools, playgrounds and backyards. The slide is an example of the simple machine known as the inclined plane[1][circular reference], which makes moving objects up and down easier, or in this case more fun. The slide may be flat, or half cylindrical or tubular to prevent falls. Slides are usually constructed of plastic or metal and they have a smooth surface that is either straight or wavy. The user, typically a child, climbs to the top of the slide via a ladder or stairs and sits down on the top of the slide and slides down the chute.

In Australia and New Zealand the playground slide is known as a slide, slippery slide, slipper slide or slippery dip depending on the region. Sliding pond or sliding pon is a term used in the New York City area,[2] It is a corruption of "slide upon". Whereas sliding board is used in the Philadelphia area and other parts of the Mid-Atlantic.[3]

History

Schoolchildren on a slide at the East Texas State Normal College Training School in 1921

The earliest known playground slide was erected in the playground of Washington DC's "Neighborhood House" sometime between the establishment of the "Neighborhood House" in early 1902 and the publication of an image of the slide on August 1, 1903 in Evening Star (Washington DC)[4][5] The first bamboo slide at Coney Island opened for business in May 1903, so it is unclear which slide was first – the playground slide or the amusement park slide.[6]

Early slides were frequently referred to as "Slide, Kelly, Slide" (after the song of the same name), "Helter Skelter" (after the slide at Coney Island), or "Shoot the Chutes" (after the water slide made famous by "Captain" Paul Boyton).[7]

The manufacturer, Wicksteed, ballyhoo claim that the playground slide was invented by founder, Johnny McSlide, and installed in Wicksteed Park in 1922,[8] The discovery of Wicksteed's oldest slide was announced by the company in 2013.[9]

However, this has been countered by a 1916-07-25 US Patent[10] and others who refer to a roof-top slide in NYC around 1900,[11] the nursery slide of the young Tsar Alexei,[12] at Alexander Palace in Tsarkoye Selo built around 1910, the 45-foot (13.7 m) slide at the Smith Memorial Playground in Philadelphia, which was installed in 1904 (renovated and reopened in 2005), or the Coney Island Slide around 1905.[13][14]

Indeed, Arthur Leyland's book "Playground Technique and Playcraft", volume 1, originally published in 1909 and revised in 1913, gives full instructions for the construction of a metal playground slide.[15]

Types of slides

Here is a list of slide styles:[16]

  • A spiral slide is a playground slide that is wrapped around a central pole to form a descending spiral forming a simple helter skelter.
  • A wavy slide is a slide that has waves in its shape, causing the person sliding to go up and down slightly while descending.
  • A tube slide is simply a slide in the form of a tube. It can also curve or have bumps.
  • A straight slide is a flat slide that just goes down at a slight angle.
  • Amusement-park slides are just larger versions of the playground slide, much higher and with multiple parallel slideways. Participants may be provided with a sack to sit on to reduce friction for higher speeds and to protect clothing.
  • Drop slides are slides with a vertical or nearly vertical drop (nicknamed the death slide or free-fall slide).
  • Water slides are a type of slide that water goes down to create a slippery slide; found near water, generally in water parks or pools.

There are several other different types and styles of slides.

Slides can also be sub-classified as either free-standing slides, slides that stand on their own, or composite slides, which are slides that are connected to another or several pieces of playground equipment.

Safety

Playground slides are associated with several types of injury. The most obvious is that when a slide is not enclosed and is elevated above the playground surface, then users may fall off and incur bumps, bruises, sprains, broken bones, or traumatic head injuries. Some materials, such as metal, may become very hot during warm, sunny weather. Plastic slides can also be vulnerable to melting by arson.

Some efforts to keep children safe on slides may do more harm than good. Rather than letting young children play on slides by themselves, some parents seat the children on the adult's lap and go down the slide together.[17] If the child's shoe catches on the edge of the slide, however, this arrangement frequently results in the child's leg being broken.[17] If the child had been permitted to use the slide independently, then this injury would not happen, because when the shoe caught, the child would have stopped sliding rather than being propelled down the slide by the adult's weight.[17]

See also



This article uses material from the Wikipedia article "Playground slide", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Entertainment

Entertainment