powered by CADENAS

Social Share

Amazon

Programming tool (10216 views - Computer)

A programming tool or software development tool is a computer program that software developers use to create, debug, maintain, or otherwise support other programs and applications. The term usually refers to relatively simple programs, that can be combined together to accomplish a task, much as one might use multiple hand tools to fix a physical object. The most basic tools are a source code editor and a compiler or interpreter, which are used ubiquitously and continuously. Other tools are used more or less depending on the language, development methodology, and individual engineer, and are often used for a discrete task, like a debugger or profiler. Tools may be discrete programs, executed separately – often from the command line – or may be parts of a single large program, called an integrated development environment (IDE). In many cases, particularly for simpler use, simple ad hoc techniques are used instead of a tool, such as print debugging instead of using a debugger, manual timing (of overall program or section of code) instead of a profiler, or tracking bugs in a text file or spreadsheet instead of a bug tracking system. The distinction between tools and applications is murky. For example, developers use simple databases (such as a file containing a list of important values) all the time as tools. However a full-blown database is usually thought of as an application or software in its own right. For many years, computer-assisted software engineering (CASE) tools were sought after. Successful tools have proven elusive. In one sense, CASE tools emphasized design and architecture support, such as for UML. But the most successful of these tools are IDEs.
Go to Article

Youtube


    

Programming tool

Programming tool

Software development
Core activities
Paradigms and models
Methodologies and frameworks
Supporting disciplines
Practices
Tools
Standards and Bodies of Knowledge
Glossaries

A programming tool or software development tool is a computer program that software developers use to create, debug, maintain, or otherwise support other programs and applications. The term usually refers to relatively simple programs, that can be combined together to accomplish a task, much as one might use multiple hand tools to fix a physical object. The most basic tools are a source code editor and a compiler or interpreter, which are used ubiquitously and continuously. Other tools are used more or less depending on the language, development methodology, and individual engineer, and are often used for a discrete task, like a debugger or profiler. Tools may be discrete programs, executed separately – often from the command line – or may be parts of a single large program, called an integrated development environment (IDE). In many cases, particularly for simpler use, simple ad hoc techniques are used instead of a tool, such as print debugging instead of using a debugger, manual timing (of overall program or section of code) instead of a profiler, or tracking bugs in a text file or spreadsheet instead of a bug tracking system.

The distinction between tools and applications is murky. For example, developers use simple databases (such as a file containing a list of important values) all the time as tools.[dubious ] However a full-blown database is usually thought of as an application or software in its own right. For many years, computer-assisted software engineering (CASE) tools were sought after. Successful tools have proven elusive. In one sense, CASE tools emphasized design and architecture support, such as for UML. But the most successful of these tools are IDEs.

Uses of programming tools

Translating from human to computer language

Modern computers are very complex and in order to productively program them, various abstractions are needed. For example, rather than writing down a program's binary representation a programmer will write a program in a programming language like C, Java or Python. Programming tools like assemblers, compilers and linkers translate a program from a human write-able and readable source language into the bits and bytes that can be executed by a computer. Interpreters interpret the program on the fly to produce the desired behavior.

These programs perform many well defined and repetitive tasks that would nonetheless be time consuming and error-prone when performed by a human, like laying out parts of a program in memory and fixing up the references between parts of a program as a linker does. Optimizing compilers on the other hand can perform complex transformations on the source code in order to improve the execution speed or other characteristics of a program. This allows a programmer to focus more on higher level, conceptual aspects of a program without worrying about the details of the machine it is running on.

Making program information available for humans

Because of the high complexity of software, it is not possible to understand most programs at a single glance even for the most experienced software developer. The abstractions provided by high-level programming languages also make it harder to understand the connection between the source code written by a programmer and the actual program's behaviour. In order to find bugs in programs and to prevent creating new bugs when extending a program, a software developer uses some programming tools to visualize all kinds of information about programs.

For example, a debugger allows a programmer to extract information about a running program in terms of the source language used to program it. The debugger can compute the value of a variable in the source program from the state of the concrete machine by using information stored by the compiler. Memory debuggers can directly point out questionable or outright wrong memory accesses of running programs which may otherwise remain undetected and are a common source of program failures.

List of tools

Software tools come in many forms:

IDEs

Integrated development environments combine the features of many tools into one package. They for example make it easier to do specific tasks, such as searching for content only in files in a particular project. IDEs may for example be used for development of enterprise-level applications.

Different aspects of IDEs for specific programming languages can be found in this comparison of integrated development environments.

See also



This article uses material from the Wikipedia article "Programming tool", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Computer

Computer, Hardware, Software