powered by CADENAS

Social Share

Amazon

Golf club (3030 views - Sports List)

A golf club is a club used to hit a golf ball in a game of golf. Each club is composed of a shaft with a grip and a club head. Woods are mainly used for long-distance fairway or tee shots; irons, the most versatile class, are used for a variety of shots; hybrids that combine design elements of woods and irons are becoming increasingly popular; putters are used mainly on the green to roll the ball into the hole. A standard set consists of 14 golf clubs, and while there are traditional combinations sold at retail as matched sets, players are free to use any combination of 14 or fewer legal clubs. An important variation in different clubs is loft, or the angle between the club's face and the vertical plane. It is loft that is the primary determinant of the ascending trajectory of the golf ball, with the tangential angle of the club head's swing arc at impact being a secondary and relatively minor consideration (though these small changes in swing angle can nevertheless have a significant influence on launch angle when using low-lofted clubs). The impact of the club compresses the ball, while grooves on the club face give the ball backspin. Together, the compression and backspin create lift. The majority of woods and irons are labeled with a number; higher numbers indicate shorter shafts and higher lofts, which give the ball a higher and shorter trajectory.
Go to Article

Explanation by Hotspot Model

Youtube


    

Golf club

Golf club

Golf club

Licensed under Creative Commons Attribution 2.0 (post406).

A golf club is a club used to hit a golf ball in a game of golf. Each club is composed of a shaft with a grip and a club head. Woods are mainly used for long-distance fairway or tee shots; irons, the most versatile class, are used for a variety of shots; hybrids that combine design elements of woods and irons are becoming increasingly popular; putters are used mainly on the green to roll the ball into the hole. A standard set consists of 14 golf clubs, and while there are traditional combinations sold at retail as matched sets, players are free to use any combination of 14 or fewer legal clubs.

An important variation in different clubs is loft, or the angle between the club's face and the vertical plane. It is loft that is the primary determinant of the ascending trajectory of the golf ball, with the tangential angle of the club head's swing arc at impact being a secondary and relatively minor consideration (though these small changes in swing angle can nevertheless have a significant influence on launch angle when using low-lofted clubs). The impact of the club compresses the ball, while grooves on the club face give the ball backspin. Together, the compression and backspin create lift. The majority of woods and irons are labeled with a number; higher numbers indicate shorter shafts and higher lofts, which give the ball a higher and shorter trajectory.

Materials

The shafts of the woods were made of different types of wood before being replaced by hickory in the middle of the 19th century. The varieties of woods included ash, purpleheart, orangewood, and blue-mahoo. Despite the strength of hickory, the long-nose club of the mid nineteenth century was still prone to breaking at the top of the back swing. The club heads were often made from woods including apple, pear, dogwood, and beech in the early times until persimmon became the main material. Golf clubs have been improved and the shafts are now made of steel, titanium, other types of metals or carbon fiber. The shaft is a tapered steel tube or a series of stepped steel tubes in telescopic fashion. This has improved the accuracy of golfers. The grips of the clubs are made from leather or rubber.

Club types

Wood

Woods are long-distance clubs, meant to drive the ball a great distance down the fairway towards the hole. They generally have a large head and a long shaft for maximum club speed. Historically woods were made from persimmon wood although some manufacturers—notably Ping—developed laminated woods. In 1979, TaylorMade Golf introduced the first metal wood made of steel. Even more recently manufacturers have started using materials such as carbon fiber, titanium, or scandium. Even though most ‘woods’ are made from different metals, they are still called ‘woods’ to denote the general shape and their intended use on the golf course. Most woods made today have a graphite shaft and a mostly-hollow titanium, composite, or steel head, of relatively light weight allowing faster club-head speeds. Woods are the longest clubs and the most powerful of all the golf clubs. There are typically three to four woods in a set which are used from the tee box and, if on a long hole, possibly for the second or even third shot. The biggest wood, known as the driver or one wood, is often made of hollowed out titanium with feather-light shafts. The length of the woods has been increasing in recent decades, and a typical driver with a graphite shaft is now 45.5 inches (1,160 mm) long. The woods may also have very large heads, up to 460 cm3 (28 cu in) in volume (the maximum allowed by the USGA in sanctioned events; drivers with even larger club-head volumes are available for long-drive competitions and informal games). The shafts range from senior to extra-stiff depending upon each player’s preference.

Iron

Irons are clubs with a solid, all-metal head featuring a flat angled face, and a shorter shaft and more upright lie angle than a wood, for ease of access. Irons are designed for a variety of shots from all over the course, from the tee box on short or dog-legged holes, to the fairway or rough on approach to the green, to tricky situations like punching through or lobbing over trees, getting out of hazards, or hitting from tight lies requiring a compact swing. Most of the irons have a number from 1 to 9 (the numbers in most common use are from 3 to 9), corresponding to their relative loft angle within a matched set. Irons are typically grouped according to their intended distance (which also roughly corresponds to their shaft length and thus their difficulty to hit the ball); in the numbered irons, there are long irons (2–4), medium irons (5–7), and short irons (8–9), with progressively higher loft angles, shorter shafts, and heavier club heads.

As with woods, ’irons’ get their name because they were originally made from forged iron. Modern irons are investment-cast out of steel alloys, which allows for better-engineered ‘cavity-back’ designs that have lower centers of mass and higher moments of inertia, making the club easier to hit and giving better distance than older forged ’muscle-back’ designs. Forged irons with less perimeter weighting are still seen, especially in sets targeting low-handicap and scratch golfers, because this less forgiving design allows a skilled golfer to intentionally hit a curved shot (a ’fade’ or ’draw’), to follow the contour of the fairway or ’bend’ a shot around an obstacle.

Wedge

Wedges are a subclass of irons with greater loft than the numbered irons (generally starting at 47°–48° of loft, above the 9-iron's 44°–45°), and other features such as high-mass club heads and wide soles that allow for easier use in tricky lies. Wedges are used for a variety of short-distance, high-altitude, high-accuracy ’utility’ shots, such as hitting the ball onto the green (’approach’ shots), placing the ball accurately on the fairway for a better shot at the green (’lay-up’ shots), or hitting the ball out of hazards or rough onto the green (chipping). There are five types of wedges, with lofts ranging from 45° to 64°: pitching wedge (PW, 48–50°), gap wedge (GW, also ‘approach’, ’attack’, ’utility’, or ’dual’ wedge, typically 52–54°), sand wedge (SW, 55–56°), lob wedge (LW, 58°–60°), and ultra lob wedge (sometimes called the ’flop wedge’ or FW, 64°–68°).

Hybrid

Hybrids are a cross between a wood and an iron, giving these clubs the wood's long distance and higher launch, with the iron's familiar swing. The club head of a hybrid has a wood-inspired, slightly convex face, and is typically hollow like modern metal woods to allow for high impulse on impact and faster swing speeds. The head is usually smaller than true woods, however, not extending as far back from the face, and the lie and shaft length are similar to an iron giving similar swing mechanics. These clubs generally replace low-numbered irons in a men's set (between 2 and 5, most commonly 3–4), which are typically the hardest clubs in a player's bag to hit well. By doing so they also generally make higher-lofted woods redundant as well. However, some manufacturers produce ’iron replacement’ sets that use hybrid designs to replace an entire set of traditional irons, from 3 to pitching wedge. Ladies' and seniors' sets commonly feature a combination of high-lofted woods (up to 7-wood) and hybrids to replace the 5, 6 and 7-irons, allowing these players to get greater carry distances with slower swings.

Putter

Putters are a special class of clubs with a loft not exceeding ten degrees, designed primarily to roll the ball along the grass, generally from a point on the putting green toward the hole. Contrary to popular belief, putters do have a loft (often 5° from truly perpendicular at impact) that helps to lift the ball from any indentation it has made. Newer putters also include grooves on the face to promote roll rather than a skid off the impact. This increases rolling distance and reduces bouncing over the turf. Putters are the only class of club allowed to have certain features, such as two striking faces, non-circular grip cross-sections, bent shafts or hosels, and appendages designed primarily to aid players' aim.

Chipper

Present in some golfers' bags is the chipper, a club designed to feel like a putter but with a more lofted face, used with a putting motion to lift the ball out of the higher grass of the rough and fringe and drop it on the green, where it will then roll like a putt. This club replaces the use of a high-lofted iron to make the same shot, and allows the player to make the shot from a stance and with a motion nearly identical to a putt, which is more difficult with a lofted iron due to a difference in lie angle.

Most chippers have a loft greater than 10 degrees, which is the maximum loft permitted by the Rules of Golf for a club to be classed as a putter, so these clubs are actually classed as irons. To be legal for sanctioned play, a chipper cannot have any feature that is defined in the rules as allowable only on putters, e.g. two striking faces or a flat-topped ’putter grip’. This disqualifies many chipper designs, but there are some USGA-conforming chippers, and non-conforming designs can still be used in non-sanctioned ’informal’ play.

Construction

Shaft

The shaft is a tapered tube made of metal (usually steel) or carbon fiber composite (referred to as graphite). The shaft is roughly 0.5 inches (13 mm) in diameter near the grip and from 34 to 48 inches (86 to 122 cm) in length. Shafts weigh from 45 to 150 grams (1.6 to 5.3 oz), depending on the material and length.[1]

Shafts are quantified in a number of different ways. The most common is the shaft flex. Simply, the shaft flex is the amount that the shaft will bend when placed under a load. A stiffer shaft will not flex as much, which requires more power to flex and "whip" through the ball properly (which results in higher club speed at impact for more distance), while a more flexible shaft will whip with less power required for better distance on slower swings, but may torque and over-flex if swung with too much power causing the head not to be square at impact, resulting in lower accuracy. Most shaft makers offer a variety of flexes. The most common are: L/W (Lady/Women's), A/I (Soft Regular, Intermediate or Senior), R (Regular), S (Stiff), and X (Tour Stiff, Extra Stiff or Strong). A regular flex shaft is generally appropriate for those with an average head speed (80–94 mph (129–151 km/h)), while an A-Flex (or senior shaft) is for players with a slower swing speed (70–79 mph (113–127 km/h)), and the stiffer shafts, such as S-Flex and X-Flex (Stiff and Extra-Stiff shafts) are reserved only for those players with an above average swinging speed, usually above 100 mph (160 km/h). Some companies also offer a "stiff-regular" or "firm" flex for players whose club speed falls in the upper range of a Regular shaft (90–100 mph (140–160 km/h)), allowing golfers and club makers to fine-tune the flex for a stronger amateur-level player.[2]

At impact, the club head can twist as a result of torque applied to the shaft, reducing accuracy as the face of the club is not square to the player's stance. The ability of a shaft to twist along its length due to this torque is fundamentally a function of the flex of the shaft itself; a stiffer shaft will also torque less. To counter torque in more flexible shafts, club makers design the shafts with varying degrees of torque through their length, particularly along the thinnest part of the shaft where it joins with the club head. This results in a point at which the shaft is most flexible, called the "kick point"; above that point the increasing diameter of the shaft makes it more rigid, while below that point the shaft is reinforced internally to reduce torquing of the club head. Shafts have typically been classified as having a low, medium or high kick; a low kick means the shaft will store energy closer to the club head, which means the club head can twist more but also allows for higher club head speeds. A high kick shaft will store energy closer to the grip; such a shaft will feel firmer when swinging it and will give better control over direction, but the same strength swing will flex the shaft less, which will reduce club-head speed.

Widely overlooked as a part of the club, the shaft is considered by many to be the engine of the modern club head. Shafts range in price from a mere US$4 to over US$1200. Current graphite shafts weigh considerably less than their steel counterparts (sometimes weighing less than 50 grams (1.8 oz) for a driver shaft), allowing for lighter clubs that can be swung at greater speed. Beginning in the late 1990s, custom shafts have been integrated into the club-making process. These shafts will, within a given flex rating, address specific criteria, such as to launch the ball higher or lower or to adjust for the timing of a player's swing to load and unload the shaft at the correct moments of the swing for maximum power. Whereas in the past each club could come with only one shaft, today's club heads can be fitted with dozens of different shafts, each with slight variation in behavior, creating the potential for a much better fit for the average golfer.[3]

Grip

The grip of the club is attached to the opposite end of the shaft from the club head, and is the part of the club the player holds on to while swinging. Originally, the grip was composed of one or more leather strips wrapped around the shaft. The leather outer wrap on a grip is still seen on some clubs, most commonly putters, but most modern grips are a one-piece "sleeve" made of rubber, synthetic or composite material that is slid over the shaft and secured with an adhesive. These sleeve grips allow club makers and golfers to customize the grip's diameter, consistency (softness/firmness) and texturing pattern to best fit the player. Clubs with an outer "wrap" of leather or leather-like synthetic still typically have a "sleeve" form underneath to add diameter to the grip and give it its basic profile.

Grip rules

According to the rules of golf, all club grips must have the same cross-section shape along their entire length (the diameter can vary), and with the exception of the putter, must have a circular cross-section. The putter may have any cross section that is symmetrical along the length of the grip through at least one plane; "shield" profiles with a flat top and curved underside are common. Grips may taper from thick to thin along their length (and virtually all do), but they are not allowed to have any waisting (a thinner section of the grip surrounded by thicker sections above and below it) or bulges (thicker sections of the grip surrounded by thinner sections). Minor variations in surface texture (such as the natural variation of a "wrap"-style grip) are not counted unless significant.[citation needed]

Re-gripping

Advances in materials have resulted in more durable, longer-lasting soft grips, but nevertheless grips do eventually dry out, harden, or are otherwise damaged and must be replaced. Replacement grips sold as do-it-yourself kits are generally inexpensive and of high quality, although custom grips that are larger, softer, or textured differently from the everyday "wrap"-style grip are generally bought and installed by a clubsmith.[citation needed]

Re-gripping used to require toxic, flammable solvents to soften and activate the adhesive, and a vise to hold the club steady while the grip was forced on. The newest replacement kits, however, use double-sided tape with a water-activated adhesive that is slippery when first activated, allowing easier installation. Once the adhesive cures, it creates a very strong bond between grip and shaft and the grip is usually impossible to remove without cutting it off.

Hosel

The hosel is the portion of the club head to which the shaft attaches. Though largely ignored by players, hosel design is integral to the balance, feel and power of a club. Modern hosels are designed to place as little mass as possible over the top of the striking face of the club, which lowers the center of gravity of the club for better distance.

Club head

Each head has one face which contacts the ball during the stroke. Putters may have two striking faces, as long as they are identical and symmetrical. Some chippers (a club similar in appearance to a double-sided putter but having a loft of 35–45 degrees) have two faces, but are not legal. Page 135 of the 2009 USGA rules of golf states:[4]

The club head must have only one striking face, except that a putter may have two such faces if their characteristics are the same, and they are opposite each other.[4]

Page 127 of the USGA rules of golf states:[5]

A putter is a club with a loft not exceeding ten degrees designed primarily for use on the putting green.[5]

Therefore, any double sided club with a loft greater than 10 degrees is not legal.[4][5]

Ferrule

The trim ring, usually black (It may have additional trim colors), that is found directly on top of the hosel on many woods and irons. The ferrule is mostly decorative, creating a continuous line between the shaft and the wider hosel, but in some cases it can form part of the securing mechanism between hosel and shaft. Ferrules of differing weights can fine-tune the center of mass of the overall club head, but for these minute adjustments, screw-in weighted inserts at specific points on the club head are usually used instead.

Club sets

The rules of golf limit each player to a maximum of 14 clubs in their bag. Strict rules prohibit sharing of clubs between players that each have their own set (if two players share clubs, they may not have more than 14 clubs combined), and while occasional lending of a club to a player is generally overlooked, habitual borrowing of other players' clubs or the sharing of a single bag of clubs slows play considerably when both players need the same club.

The most common set of men's clubs is:

  • A driver, usually numbered a 1-wood regardless of actual loft, which varies from 8° up to 13°
  • A fairway wood, typically numbered a 3-wood and lofted about 15° (though 2- and 4-woods are sometimes seen)
  • A matched set of 7 numbered irons from 3 through 9, plus a pitching wedge or "10-iron"
  • A sand wedge
  • A putter

The above set is only 12 clubs; these (or equivalent hybrid substitutes) are found in virtually every golf bag. To this, players typically add two of the following:

  • Another fairway wood, often a 5-wood lofted around 18°, to allow other options besides long irons in the 180–250 yard range,
  • A hybrid, typically lofted for similar distance as a 3- or 4-iron and usually replacing instead of supplementing those clubs in the bag, and/or
  • An additional wedge, usually either:
    • A gap wedge lofted near 52° to fit between the modern pitching and sand wedges in loft, or
    • A lob wedge, typically lofted around 60°, used for tight approach shots from the rough or sand.
  • A chipper.

Women's club sets are similar in overall makeup, but typically have higher lofts and shorter, more flexible shafts in retail sets to accommodate the average female player's height and swing speed.

Variations on this basic set abound; several club options usually exist for almost any shot depending on the player's skill level and playing style, and the only club universally considered to be indispensable is the putter. Some consider the modern deep-faced driver to be equally irreplaceable; this is cause for some debate, as professional players including Tiger Woods have played and won tournaments without using a driver, instead using a 3-wood for tee shots and making up the difference on the approach using a lower-lofted iron.

The most common omissions are the "long irons", numbered from 2 to 5, which are notoriously difficult to hit well. The player can supplement the gaps in distance with either higher-numbered woods such as the 5 and even the 7-wood, or may replace the long irons with equivalently-numbered hybrid clubs. If hybrids are used, higher-lofted woods are often omitted as redundant, but ladies' and seniors' sets commonly feature both hybrids and high-lofted woods, omitting the long irons entirely in favor of the lofted woods, and replacing the mid-irons (5–7) with hybrids. The combination allows for higher launch angles on the long-distance clubs, which gives better distance with slower swing speeds. Where a club is omitted and not replaced with a club of similar function, players may add additional clubs of a different function such as additional wedges.

While 14 clubs is a maximum, it is not a minimum; players are free to use any lesser number of clubs they think will be useful, so substitutions for the common omissions above are not always made; a player may simply choose to play without a 5-wood or 2–4 irons, instead using a 4-wood and moving directly to their 5-iron as desired distance decreases (a 4-wood in a skilled golfer's hands averages 200 yards; a 5-iron in the same player's hands would be about 160, which is a large gap but not unplayable). Other clubs may be omitted as well. On courses where bags must be carried by the player, the player may take only the odd-numbered irons; without the 4, 6 or 8 irons (the 3 is sometimes removed instead of the 4) the bag's weight is considerably reduced. Carrying only a driver, 3-wood, 4-hybrid, 5-7-9 irons, pitching and sand wedges, and a putter reduces the number of clubs in the bag to 9; this is a common load-out for a "Sunday bag" taken to the driving range or to an informal game. A skilled player can usually overcome the lesser selection of club lofts by reducing their swing speed on a lower-loft iron and/or placing the ball further forward in their stance to get the same carry distance and/or launch angle as the next higher loft number.

Regulations

The ruling authorities of golf, The R&A (an offshoot of The Royal and Ancient Golf Club of St Andrews) and the United States Golf Association (USGA), reserve the right to define what shapes and physical characteristics of clubs are permissible in tournament play. The current rules for club design, including the results of various rulings on clubs introduced for play, are defined in Appendix II of the Rules of Golf.

The overarching principle of club design used by both authorities is defined in Appendix II-1a, which states: "The club must not be substantially different from the traditional and customary form and make. The club must be composed of a shaft and a head and it may also have material added to the shaft to enable the player to obtain a firm hold (see 3 below). All parts of the club must be fixed so that the club is one unit, and it must have no external attachments." In addition, Appendix II-4a states, regarding club heads, that "the club head must be generally plain in shape. All parts must be rigid, structural in nature and functional. The club head or its parts must not be designed to resemble any other object. It is not practicable to define 'plain in shape' precisely and comprehensively."

These two rules are used as the basis for most of the more specific rules of Appendix II, including that no club may have a concave face (1931) and various rules defining what is "traditional" about the shapes of specific clubs, while allowing for the progression of technology. The "traditional and customary" rule was originally used to ban the introduction of steel club shafts (patented in 1910), as that material was not traditional for shafts; that specific ban was rescinded in 1924 by the USGA (the R&A would continue to ban steel shafts until 1929),[6] and steel would become universal until the development of graphite shafts whose introduction was less controversial. The "plain in shape" rule was more recently bent to allow for non-traditional driver club head shapes, such as squares, as a compromise to club-makers after imposing and enforcing a 460cc volume limit on these same club heads.

Many recently developed woods have a marked "trampoline effect" (a large deformation of the face upon impact followed by a quick restoration to original dimensions, acting like a slingshot), resulting in very high ball speeds and great lengths of tee shots. As of 1 January 2008, the USGA and R&A have settled on a regulation that limits the acceptable "trampoline effect" to a coefficient of restitution (COR)—a measurement of the efficiency of the transfer of energy from the club head to the ball—of .830.[7]

Other large scale USGA rulings involve a 1990 lawsuit, and subsequent settlement, against Karsten Manufacturing, makers of the PING brand, for their use of square, or U-grooves in their immensely popular Ping Eye2 irons. The USGA argued that players who used the Eye2 had an unfair advantage in imparting spin on the ball, which helps to stop the ball on the putting greens. The USGA utilized John L. Saksun, founder of Canadian golf company Accuform Golf, as a consultant to set up methods of measuring the unique grooves and determining PING's compliance with the rulings.[8] Saksun, by proposing a cost-effective solution to help PING change the design of subsequent Eye2s, saved PING hundreds of millions. PING subsequently withdrew their US$100 million lawsuit against the USGA. Ping’s older clubs were "grandfathered in" and allowed to remain in play as part of the settlement.[9] However, the USGA has begun phasing in a ban on square grooves in golf. Manufacturers were required to discontinue noncompliant clubs by January 1, 2011.[10] According to the USGA, as January 1, 2010, professional golfers on one of the top tours, or those attempting to qualify for one of the three Open Championships (since then four) will need to use new conforming wedges (those without square grooves).[11][12] Moreover, those who plan to qualify for any other USGA championship (Amateur championships -- under 18, Amateur, over 25, and over 50 in both sexes, and four-ball, along with international team championships), will need new conforming wedges by 2014. In addition, this regulation includes IGF and USGA-sanctioned regional amateur events as well, as a "condition of competition". [11] Wedges that conform to the new standard are often marketed as "CC" or "Condition of Competition" wedges; this moniker is likely to fall into disuse as players upgrade clubs and the use of non-conforming irons diminishes.

See also



This article uses material from the Wikipedia article "Golf club", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Sports List

Air sports
• Aerobatics
• Air racing
• Cluster ballooning
• Hopper ballooning

Wingsuit flying
• Gliding
• Hang gliding
• Powered hang glider
• Human powered aircraft
• Model aircraft
• Parachuting
• Banzai skydiving
• BASE jumping
• Skydiving
• Skysurfing
• Wingsuit flying
• Paragliding
• Powered paragliding
• Paramotoring
• Ultralight aviation

Archery
• Field archery
• Flight archery
• Gungdo
• Indoor archery
• Kyūdō
• Popinjay
• Target archery

Ball-over-net games
• Badminton
• Ball badminton
• Biribol
• Bossaball
• Fistball
• Footbag net
• Football tennis
• Footvolley
• Hooverball
• Jianzi
• Padel
• Peteca
• Pickleball
• Platform tennis
• Sepak takraw
• Sipa
• Throwball
• Volleyball
• Beach volleyball
• Water volleyball
• Paralympic volleyball
• Wallyball
• Ringo


Basketball family
• Basketball
• Beach basketball
• Deaf basketball
• Streetball
• Water basketball
• Wheelchair basketball
• Cestoball
• Korfball
• Netball
• Fastnet
• Indoor netball
• Ringball
• Slamball

Bat-and-ball (safe haven)
• Baseball
• Softball
• Slow pitch
• Fast-pitch softball
• 16-inch softball
• Bat and trap
• British baseball – four posts
• Brännboll – four bases
• Corkball – four bases (no base-running)
• Cricket – two creases
• Indoor cricket
• Limited overs cricket
• One Day International
• Test cricket
• Twenty20
• Danish longball
• Kickball
• Kilikiti
• Lapta – two salos (bases)
• The Massachusetts Game – four bases
• Matball
• Oina
• Old cat – variable
• Over-the-line – qv
• Palant
• Pesäpallo – four bases
• Punchball
• Rounders – four bases or posts
• Scrub baseball – four bases (not a team game per se)
• Stickball – variable
• Stool ball – two stools
• Tee-ball
• Town ball – variable
• Vigoro – two wickets
• Wireball
• Wiffleball

Baton twirling
• Baton twirling

Acro sports
• Ballet
• Dancing
• Cheerleading
• Gymnastics

Performance sports
• Drum corps
• Marching band

Board sports

• Skateboarding
• Scootering
• Casterboarding
• Freeboard (skateboard)
• Longboarding
• Streetboarding
• Skysurfing
• Streetluge
• Snowboarding
• Mountainboarding
• Sandboarding
• Snowkiting
• Surfing
• Wakesurfing
• Bodyboarding
• Riverboarding
• Skimboarding
• Windsurfing
• Wakeboarding
• Kneeboarding
• Paddleboarding

Catch games
• Dodgeball
• Ga-ga
• Keep away
• Kin-Ball
• Newcomb ball
• Quidditch
• Rundown (a.k.a. Pickle)
• Yukigassen

Climbing

• Abseiling
• Aid climbing
• Ice climbing
• Mixed climbing
• Mountaineering
• Rock climbing
• Bouldering
• Deep-water soloing
• Sport climbing
• Traditional climbing
• Other
• Canyoning (Canyoneering)
• Coasteering
• Hiking
• Rope climbing
• Pole climbing

Cycling

• Artistic cycling
• BMX
• Cyclo-cross
• Cross-country mountain biking
• Cycle polo
• Cycle speedway
• Downhill mountain biking
• Dirt jumping
• Enduro mountain biking
• Freestyle BMX
• Hardcourt Bike Polo
• Road bicycle racing
• Track cycling
• Underwater cycling

Skibob
• Skibobbing

Unicycle

• Mountain unicycling
• Unicycling
• Unicycle basketball
• Unicycle hockey
• Unicycle trials
Combat sports: wrestling and martial arts
• Aiki-jūjutsu
• Aikido
• Jujutsu
• Judo
• Brazilian jiu-jitsu
• Sambo (martial art)
• Sumo
• Wrestling
• Amateur wrestling
• Greco-Roman wrestling
• Freestyle wrestling
• Folk wrestling
• Boli Khela
• Collar-and-elbow
• Cornish wrestling
• Dumog
• Glima
• Gouren
• Kurash
• Lancashire wrestling
• Catch wrestling
• Malla-yuddha
• Mongolian wrestling
• Pehlwani
• Professional wrestling
• Schwingen
• Shuai jiao
• Ssireum
• Varzesh-e Pahlavani
• Yağlı Güreş
• Greek wrestling

Striking

• Choi Kwang-Do
• Cockfighting
• Boxing
• Bokator
• Capoeira
• Fujian White Crane
• Karate
• Kenpō
• Kickboxing
• Lethwei
• Muay Thai
• Pradal serey
• Sanshou
• Savate
• Shaolin Kung Fu
• Sikaran
• Silat
• Subak
• Taekkyeon
• Taekwondo
• Taidō
• Tang Soo Do
• Wing Chun
• Zui quan

Mixed or hybrid
• Baguazhang
• Bando
• Bartitsu
• Bujinkan
• Hapkido
• Hwa Rang Do
• Jeet Kune Do
• Kajukenbo
• Kalaripayattu
• Krav Maga
• Kuk Sool Won
• Marine Corps Martial Arts Program
• Mixed martial arts
• Northern Praying Mantis
• Ninjutsu
• Pankration
• Pencak Silat
• Sanshou
• Shidōkan Karate
• Shōrin-ryū Shidōkan
• Shoot boxing
• Shootfighting
• Shorinji Kempo
• Systema
• T'ai chi ch'uan
• Vajra-mushti
• Vale tudo
• Vovinam
• Xing Yi Quan
• Zen Bu Kan Kempo

Weapons
• Axe throwing
• Battōjutsu
• Boffer fighting
• Eskrima
• Egyptian stick fencing
• Fencing
• Gatka
• Hojōjutsu
• Iaidō
• Iaijutsu
• Jōdō
• Jogo do pau
• Jūkendō
• Jittejutsu
• Kendo
• Kenjutsu
• Krabi–krabong
• Kung fu
• Kyūdō
• Kyūjutsu
• Modern Arnis
• Naginatajutsu
• Nguni stick-fighting
• Okinawan kobudō
• Shurikenjutsu
• Silambam
• Sōjutsu
• Sword fighting
• Wushu
• Kumdo
• Wing Chun


Skirmish
• Airsoft
• Laser tag
• Paintball


Cue sports
• Carom billiards
• Three-cushion
• Five-pins
• Balkline and straight rail
• Cushion caroms
• Four-ball (yotsudama)
• Artistic billiards
• Novuss (and cued forms of carrom)
• Pocket billiards (pool)
• Eight-ball
• Blackball (a.k.a. British eight-ball pool)
• Nine-ball
• Straight pool (14.1 continuous)
• One-pocket
• Three-ball
• Seven-ball
• Ten-ball
• Rotation
• Baseball pocket billiards
• Cribbage (pool)
• Bank pool
• Artistic pool
• Trick shot competition
• Speed pool
• Bowlliards
• Chicago
• Kelly pool
• Cutthroat
• Killer
• Russian pyramid
• Snooker
• Sinuca brasileira
• Six-red snooker
• Snooker plus
• Hybrid carom–pocket games
• English billiards
• Bottle pool
• Cowboy
• Obstacle variations
• Bagatelle
• Bar billiards
• Bumper pool
• Table Sports
• Foosball


Equine sports
• Buzkashi
• Barrel racing
• Campdrafting
• Cirit
• Charreada
• Chilean rodeo
• Cross country
• Cutting
• Dressage
• Endurance riding
• English pleasure
• Equitation
• Eventing
• Equestrian vaulting
• Gymkhana
• Harness racing
• Horse racing
• Horseball
• Hunter
• Hunter-jumpers
• Jousting
• Pato
• Reining
• Rodeo
• Show jumping
• Steeplechase
• Team penning
• Tent pegging
• Western pleasure


Fishing
• Angling
• Big-game fishing
• Casting
• Noodling
• Spearfishing
• Sport fishing
• Surf fishing
• Rock fishing
• Fly fishing
• Ice fishing

Flying disc sports

• Beach ultimate
• Disc dog
• Disc golf
• Disc golf (urban)
• Dodge disc
• Double disc court
• Flutterguts
• Freestyle
• Freestyle competition
• Goaltimate
• Guts
• Hot box
• Ultimate

Football

• Ancient games
• Chinlone
• Cuju
• Episkyros
• Harpastum
• Kemari
• Ki-o-rahi
• Marn Grook
• Woggabaliri
• Yubi lakpi
• Medieval football
• Ba game
• Caid
• Calcio Fiorentino
• Camping (game)
• Chester-le-Street
• Cnapan
• Cornish hurling
• Haxey Hood
• Knattleikr
• La soule
• Lelo burti
• Mob football
• Royal Shrovetide Football
• Uppies and Downies
• Association football
• Jorkyball
• Paralympic football
• Powerchair Football
• Reduced variants
• Five-a-side football
• Beach soccer
• Futebol de Salão
• Futsal
• Papi fut
• Indoor soccer
• Masters Football
• Street football
• Freestyle football
• Keepie uppie
• Swamp football
• Three sided football
• Australian football
• Nine-a-side footy
• Rec footy
• Metro footy
• English school games
• Eton College
• Field game
• Wall game
• Harrow football
• Gaelic football
• Ladies' Gaelic football
• Gridiron football
• American football
• Eight-man football
• Flag football
• Indoor football
• Arena football
• Nine-man football
• Six-man football
• Sprint football
• Touch football
• Canadian football
• Street football (American)
• Rugby football
• Beach rugby
• Rugby league
• Masters Rugby League
• Mod league
• Rugby league nines
• Rugby league sevens
• Tag rugby
• Touch football
• Wheelchair rugby league
• Rugby union
• American flag rugby
• Mini rugby
• Rugby sevens
• Tag rugby
• Touch rugby
• Rugby tens
• Snow rugby
• Hybrid codes
• Austus
• Eton wall game
• International rules football
• Samoa rules
• Speedball
• Universal football
• Volata


Golf

• Miniature golf
• Match play
• Skins game
• Speed golf
• Stroke play
• Team play
• Shotgun start

Gymnastics

• Acrobatic gymnastics
• Aerobic gymnastics
• Artistic gymnastics
• Balance beam
• Floor
• High bar
• Parallel bars
• Pommel horse
• Still rings
• Uneven bars
• Vault
• Juggling
• Rhythmic gymnastics
• Ball
• Club
• Hoop
• Ribbon
• Rope
• Rope jumping
• Slacklining
• Trampolining
• Trapeze
• Flying trapeze
• Static trapeze
• Tumbling

Handball family
• Goalball
• Hitbal
• Tchoukball
• Team handball
• Beach handball
• Czech handball
• Field handball
• Torball
• Water polo

Hunting

• Beagling
• Big game hunting
• Deer hunting
• Fox hunting
• Hare coursing
• Wolf hunting

Ice sports
• Bandy
• Rink bandy
• Broomball
• Curling
• Ice hockey
• Ringette
• Ice yachting
• Figure skating


Kite sports
• Kite buggy
• Kite fighting
• Kite landboarding
• Kitesurfing
• Parasailing
• Snow kiting
• Sport kite (Stunt kite)

Mixed discipline
• Adventure racing
• Biathlon
• Duathlon
• Decathlon
• Heptathlon
• Icosathlon
• Modern pentathlon
• Pentathlon
• Tetrathlon
• Triathlon

Orienteering family
• Geocaching
• Orienteering
• Rogaining
• Letterboxing
• Waymarking

Pilota family
• American handball
• Australian handball
• Basque pelota
• Jai alai
• Fives
• Eton Fives
• Rugby Fives
• Frisian handball
• Four square
• Gaelic handball
• Jeu de paume
• Palla
• Patball
• Valencian pilota

Racquet (or racket) sports
• Badminton
• Ball badminton
• Basque pelota
• Frontenis
• Xare
• Beach tennis
• Fives
• Matkot
• Padel
• Paleta Frontón
• Pelota mixteca
• Pickleball
• Platform tennis
• Qianball
• Racketlon
• Racquetball
• Racquets
• Real tennis
• Soft tennis
• Speed-ball
• Speedminton
• Squash
• Hardball squash
• Squash tennis
• Stické
• Table tennis
• Tennis
Remote control
• Model aerobatics
• RC racing
• Robot combat
• Slot car racing

Rodeo-originated
• Bullriding
• Barrel Racing
• Bronc Riding
• Saddle Bronc Riding
• Roping
• Calf Roping
• Team Roping
• Steer Wrestling
• Goat Tying

Running
• Endurance
• 5K run
• 10K run
• Cross-country running
• Half marathon
• Marathon
• Road running
• Tower running
• Ultramarathon
• Sprint
• Hurdles

Sailing / Windsurfing
• Ice yachting
• Land sailing
• Land windsurfing
• Sailing
• Windsurfing
• Kiteboarding
• Dinghy sailing

Snow sports
• Alpine skiing
• Freestyle skiing
• Nordic combined
• Nordic skiing
• Cross-country skiing
• Telemark skiing
• Ski jumping
• Ski touring
• Skijoring
• Speed skiing

Sled sports

• Bobsleigh
• Luge
• Skibobbing
• Skeleton
• Toboggan

Shooting sports
• Clay pigeon shooting
• Skeet shooting
• Trap shooting
• Sporting clays
• Target shooting
• Field target
• Fullbore target rifle
• High power rifle
• Benchrest shooting
• Metallic silhouette
• Practical shooting
• Cowboy action shooting
• Metallic silhouette shooting
Stacking
• Card stacking
• Dice stacking
• Sport stacking

Stick and ball games
• Hornussen

Hockey
• Hockey
• Ball hockey
• Bando
• Bandy
• Rink bandy
• Broomball
• Moscow broomball
• Field hockey
• Indoor field hockey
• Floorball
• Ice hockey

Ice hockey 
 • Pond hockey
• Power hockey
• Ringette
• Sledge hockey
• Underwater ice hockey
• Roller hockey
• Inline hockey
• Roller hockey (Quad)
• Skater hockey
• Rossall Hockey
• Spongee
• Street hockey
• Underwater hockey
• Unicycle hockey

Hurling and shinty
• Cammag
• Hurling
• Camogie
• Shinty
• Composite rules shinty-hurling

Lacrosse
• Lacrosse
• Box lacrosse
• Field lacrosse
• Women's lacrosse
• Intercrosse


Polo
• Polo
 • Bicycle polo
• Canoe polo
• Cowboy polo
• Elephant polo
• Horse polo
• Segway polo
• Yak polo

Street sports
• Free running
• Freestyle footbag
• Freestyle football
• Powerbocking
• Parkour
• Scootering
• Street workout

Tag games

• British bulldogs (American Eagle)
• Capture the flag
• Hana Ichi Monme
• Hide and seek
• Jugger
• Kabaddi
• Kho kho
• Kick the can
• Oztag
• Red rover
• Tag

Walking
• Hiking
• Backpacking (wilderness)
• Racewalking
• Bushwhacking
• Walking

Wall-and-ball
• American handball
• Australian handball
• Basque pelota
• Butts Up
• Chinese handball
• Fives
• Gaelic handball
• International fronton
• Jorkyball
• Racquetball
• Squash
• Squash tennis
• Suicide (game)
• Valencian frontó
• Wallball
• Wallyball

Aquatic & paddle sports
• Creeking
• Flyak
• Freeboating
• Sea kayaking
• Squirt boating
• Surf kayaking
• Whitewater kayaking

Rafting
• Rafting
• White water rafting

Rowing
• Rowing (sport)
• Gig racing
• Coastal and ocean rowing
• Surfboat
• Single scull
Other paddling sports
• Dragon boat racing
• Stand up paddle boarding
• Water polo
• Canoe polo
• Waboba

Underwater
• Underwater football
• Underwater rugby
• Underwater hockey

Competitive swimming
• Backstroke
• Breaststroke
• Butterfly stroke
• Freestyle swimming
• Individual medley
• Synchronized swimming
• Medley relay

Kindred activities
• Bifins (finswimming)
• Surface finswimming

Subsurface and recreational
• Apnoea finswimming
• Aquathlon (underwater wrestling)
• Freediving
• Immersion finswimming
• Scuba diving
• Spearfishing
• Snorkelling
• Sport diving (sport)
• Underwater hockey
• Underwater orienteering
• Underwater photography (sport)
• Underwater target shooting
Diving
• Cliff diving
• Diving

Weightlifting
• Basque traditional weightlifting
• Bodybuilding
• Highland games
• Olympic weightlifting
• Powerlifting
• Strength athletics (strongman)
• Steinstossen

Motorized sports
• Autocross (a.k.a. Slalom)
• Autograss
• Banger racing
• Board track racing
• Demolition derby
• Desert racing
• Dirt track racing
• Drag racing
• Drifting
• Folkrace
• Formula racing
• Formula Libre
• Formula Student
• Hillclimbing
• Ice racing
• Kart racing
• Land speed records
• Legends car racing
• Midget car racing
• Monster truck
• Mud bogging
• Off-road racing
• Pickup truck racing
• Production car racing
• Race of Champions
• Rally raid
• Rallycross
• Rallying
• Regularity rally
• Road racing
• Short track motor racing
• Snowmobile racing
• Sports car racing
• Sprint car racing
• Street racing
• Stock car racing
• Time attack
• Tractor pulling
• Touring car racing
• Truck racing
• Vintage racing
• Wheelstand competition

Motorboat racing
• Drag boat racing
• F1 powerboat racing
• Hydroplane racing
• Jet sprint boat racing
• Offshore powerboat racing
• Personal water craft

Motorcycle racing
• Auto Race
• Board track racing
• Cross-country rally
• Endurance racing
• Enduro
• Freestyle motocross
• Grand Prix motorcycle racing
• Grasstrack
• Hillclimbing
• Ice racing
• Ice speedway
• Indoor enduro
• Motocross
• Motorcycle drag racing
• Motorcycle speedway
• Off-roading
• Rally raid
• Road racing
• Superbike racing
• Supercross
• Supermoto
• Supersport racing
• Superside
• Track racing
• Trial
• TT racing
• Free-style moto

Marker sports
• Airsoft
• Archery
• Paintball
• Darts

Musical sports
• Color guard
• Drum corps
• Indoor percussion
• Marching band

Fantasy sports
• Quidditch
• Hunger Games(Gladiating)
• Pod Racing
• Mortal Kombat(MMA)

Other
• Stihl Timbersports Series
• Woodsman

Overlapping sports
• Tennis
• Polocrosse
• Badminton
• Polo

Skating sports
• Aggressive inline skating
• Artistic roller skating
• Figure skating
• Freestyle slalom skating
• Ice dancing
• Ice skating
• Inline speed skating
• Rinkball
• Rink hockey
• Roller derby
• Roller skating
• Short track speed skating
• Skater hockey
• Speed skating
• Synchronized skating

Freestyle skiing
• Snowboarding
• Ski flying
• Skibob
• Snowshoeing
• Skiboarding