Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Swimming is the self-propulsion of a person through water, usually for recreation, sport, exercise, or survival. Locomotion is achieved through coordinated movement of the limbs, the body, or both. Humans can hold their breath underwater and undertake rudimentary locomotive swimming within weeks of birth, as a survival response.[1]
Swimming is consistently among the top public recreational activities,[2][3][4][5] and in some countries, swimming lessons are a compulsory part of the educational curriculum.[6] As a formalized sport, swimming features in a range of local, national, and international competitions, including every modern Summer Olympics.
Swimming relies on the nearly neutral buoyancy of the human body. On average, the body has a relative density of 0.98 compared to water, which causes the body to float. However, buoyancy varies on the basis of body composition, lung inflation, and the salinity of the water. Higher levels of body fat and saltier water both lower the relative density of the body and increase its buoyancy.
Since the human body is only slightly less dense than water, water supports the weight of the body during swimming. As a result, swimming is “low-impact” compared to land activities such as running. The density and viscosity of water also create resistance for objects moving through the water. Swimming strokes use this resistance to create propulsion, but this same resistance also generates drag on the body.
Hydrodynamics is important to stroke technique for swimming faster, and swimmers who want to swim faster or exhaust less try to reduce the drag of the body's motion through the water. To be more hydrodynamic, swimmers can either increase the power of their strokes or reduce water resistance, though power must increase by a factor of three to achieve the same effect as reducing resistance.[7] Efficient swimming by reducing water resistance involves a horizontal water position, rolling the body to reduce the breadth of the body in the water, and extending the arms as far as possible to reduce wave resistance.[7]
Just before plunging into the pool, swimmers may perform exercises such as squatting. Squatting helps in enhancing a swimmer’s start by warming up the thigh muscles.[8]
Human babies demonstrate an innate swimming or diving reflex from newborn until the age of approximately 6 months.[9] Other mammals also demonstrate this phenomenon (see mammalian diving reflex). The diving response involves apnea, reflex bradycardia, and peripheral vasoconstriction; in other words, babies immersed in water spontaneously hold their breath, slow their heart rate, and reduce blood circulation to the extremities (fingers and toes).[9] Because infants are innately able to swim, classes for babies of about 6 months old are offered in many locations. This helps build muscle memory and makes strong swimmers from a young age.
Swimming can be undertaken using a wide range of styles, known as 'strokes,' and these strokes are used for different purposes, or to distinguish between classes in competitive swimming. It is not necessary to use a defined stroke for propulsion through the water, and untrained swimmers may use a 'doggy paddle' of arm and leg movements, similar to the way four-legged animals swim.
There are four main strokes used in competition and recreation swimming: the front crawl, also known as freestyle, the breaststroke, the backstroke and the butterfly. Competitive swimming in Europe started around 1800, mostly using the breaststroke. In 1873, John Arthur Trudgen introduced the trudgen to Western swimming competitions.[10] The butterfly stroke developed in the 1930s, and was considered a variant of the breaststroke until accepted as a separate style in 1953.[11] Butterfly is considered the hardest stroke by many people, but it is the most effective for all-around toning and the building of muscles.[12] It also burns the most calories.[12]
Other strokes exist for specific purposes, such as training or rescue, and it is also possible to adapt strokes to avoid using parts of the body, either to isolate certain body parts, such as swimming with arms only or legs only to train them harder, or for use by amputees or those affected by paralysis.
Swimming has been recorded since prehistoric times, and the earliest records of swimming date back to Stone Age paintings from around 7,000 years ago. Written references date from 2000 BC. Some of the earliest references include the Epic of Gilgamesh, the Iliad, the Odyssey, the Bible (Ezekiel 47:5, Acts 27:42, Isaiah 25:11), Beowulf, and other sagas.
The coastal tribes living in the volatile Low Countries were known as excellent swimmers by the Romans. Men and horses of the Batavi tribe could cross the Rhine without losing formation, according to Tacitus. Dio Cassius describes one surprise tactic employed by Aulus Plautius against the Celts at the Battle of the Medway:[13]
The [British Celts] thought that Romans would not be able to cross it without a bridge, and consequently bivouacked in rather careless fashion on the opposite bank; but he sent across a detachment of [Batavii], who were accustomed to swim easily in full armour across the most turbulent streams. . . . Thence the Britons retired to the river Thames at a point near where it empties into the ocean and at flood-tide forms a lake. This they easily crossed because they knew where the firm ground and the easy passages in this region were to be found, but the Romans in attempting to follow them were not so successful. However, the [Batavii] swam across again and some others got over by a bridge a little way up-stream, after which they assailed the barbarians from several sides at once and cut down many of them."
In 1538, Nikolaus Wynmann, a Swiss–German professor of languages, wrote the earliest known complete book about swimming, Colymbetes, sive de arte natandi dialogus et festivus et iucundus lectu (The Swimmer, or A Dialogue on the Art of Swimming and Joyful and Pleasant to Read).[14]
There are many reasons why people swim, from swimming as a recreational pursuit to swimming as a necessary part of a job or other activity. Swimming may also be used to rehabilitate injuries, especially various cardiovascular and muscle injuries.
Many swimmers swim for recreation, with swimming consistently ranking as one of the physical activities people are most likely to take part in. Recreational swimming can also be used for exercise, relaxation or rehabilitation.[15] The support of the water, and the reduction in impact, make swimming accessible for people who are unable to undertake activities such as running.
Swimming is primarily a cardiovascular/aerobic exercise[16] due to the long exercise time, requiring a constant oxygen supply to the muscles, except for short sprints where the muscles work anaerobically. Furthermore, swimming can help tone and strengthen muscles.[17] As with most aerobic exercise, swimming reduces the harmful effects of stress. Swimming is also effective in improving health for people with cardiovascular problems and chronic illnesses. It is proven to positively impact the mental health of pregnant women and mothers. Swimming can even improve mood.[18]
As of 2013, the Americans with Disabilities Act requires that swimming pools in the United States be accessible to disabled swimmers.[19]
"Water-based exercise can benefit older adults by improving quality of life and decreasing disability. It also improves or maintains the bone health of post-menopausal women."[20]
Swimming as a sport predominantly involves participants competing to be the fastest over a given distance in a certain period of time. Competitors swim different distances in different levels of competition. For example, swimming has been an Olympic sport since 1896, and the current program includes events from 50 m to 1500 m in length, across all four main strokes and medley.
The sport is governed internationally by the Fédération Internationale de Natation (FINA), and competition pools for FINA events are 25 or 50 meters in length. In the United States, a pool 25 yards in length is commonly used for competition.
Other swimming and water-related sporting disciplines include open water swimming, diving, synchronized swimming, water polo, triathlon, and the modern pentathlon.
Some occupations require workers to swim, such as abalone and pearl diving, and spearfishing.
Swimming is used to rescue people in the water who are in distress, including exhausted swimmers, non-swimmers who have accidentally entered the water, and others who have come to harm on the water. Lifeguards or volunteer lifesavers are deployed at many pools and beaches worldwide to fulfill this purpose, and they, as well as rescue swimmers, may use specific swimming styles for rescue purposes.
Swimming is also used in marine biology to observe plants and animals in their natural habitat. Other sciences use swimming; for example, Konrad Lorenz swam with geese as part of his studies of animal behavior.
Swimming also has military purposes. Military swimming is usually done by special operation forces, such as Navy SEALs and US Army Special Forces. Swimming is used to approach a location, gather intelligence, engage in sabotage or combat, and subsequently depart. This may also include airborne insertion into water or exiting a submarine while it is submerged. Due to regular exposure to large bodies of water, all recruits in the United States Navy, Marine Corps, and Coast Guard are required to complete basic swimming or water survival training.
Swimming is also a professional sport. Companies sponsor swimmers who have the skills to compete at the international level. Many swimmers compete competitively to represent their home countries in the Olympics. Professional swimmers may also earn a living as entertainers, performing in water ballets.
Locomotion by swimming over brief distances is frequent when alternatives are precluded. There have been cases of political refugees swimming in the Baltic Sea[21] and of people jumping in the water and swimming ashore from vessels not intended to reach land where they planned to go.[22]
There are many risks associated with voluntary or involuntary human presence in water, which may result in death directly or through drowning asphyxiation. Swimming is both the goal of much voluntary presence and the prime means of regaining land in accidental situations.
Most recorded water deaths fall into these categories:
Adverse effects of swimming can include:
Around any pool area, safety equipment is often important,[24] and is a zoning requirement for most residential pools in the United States.[25] Supervision by personnel trained in rescue techniques is required at most competitive swimming meets and public pools.
Traditionally, children were considered not able to swim independently until 4 years of age,[26] although now infant swimming lessons are recommended to prevent drowning.[27]
In Sweden, Denmark, Norway, Estonia and Finland, the curriculum for the fifth grade (fourth grade in Estonia) states that all children should learn how to swim as well as how to handle emergencies near water. Most commonly, children are expected to be able to swim 200 metres (660 ft)—of which at least 50 metres (160 ft) on their back – after first falling into deep water and getting their head under water. Even though about 95 percent of Swedish school children know how to swim, drowning remains the third most common cause of death among children.[citation needed]
In both the Netherlands and Belgium swimming lessons under school time (schoolzwemmen, school swimming) are supported by the government. Most schools provide swimming lessons. There is a long tradition of swimming lessons in the Netherlands and Belgium, the Dutch translation for the breaststroke swimming style is even schoolslag (schoolstroke). In France, swimming is a compulsory part of the curriculum for primary schools. Children usually spend one semester per year learning swimming during CP/CE1/CE2/CM1 (1st, 2nd, 3rd and 4th grade).
In many places, swimming lessons are provided by local swimming pools, both those run by the local authority and by private leisure companies. Many schools also include swimming lessons into their Physical Education curricula, provided either in the schools' own pool or in the nearest public pool.
In the UK, the "Top-ups scheme" calls for school children who cannot swim by the age of 11 to receive intensive daily lessons. Children who have not reached Great Britain's National Curriculum standard of swimming 25 meters by the time they leave primary school receive a half-hour lesson every day for two weeks during term-time.[28]
In Canada and Mexico there has been a call to include swimming in public school curriculum.[29]
In the United States there is the Infant Swimming Resource (ISR)[30] initiative that provides lessons for infant children, to cope with an emergency where they have fallen into the water. They are taught how to roll-back-to-float (hold their breath underwater, to roll onto their back, to float unassisted, rest and breathe until help arrives).
In Switzerland, swimming lessons for babies are popular, to help them getting used to be in another element. At the competition level, unlike in other countries - such as the Commonwealth countries, swimming teams are not related to educational institutions (high-schools and universities), but rather to cities or regions.
Standard everyday clothing is usually impractical for swimming and is unsafe under some circumstances. Most cultures today expect swimmers to wear swimsuits.
Men's swimsuits commonly resemble shorts, or briefs. Casual men's swimsuits (for example, boardshorts) are rarely skintight, unlike competitive swimwear, like jammers or diveskins. In most cases, boys and men swim with their upper body exposed, except in countries where custom or law prohibits it in a public setting, or for practical reasons such as sun protection.
Modern women's swimsuits are generally skintight, covering the pubic region and the breasts (See bikini). Women's swimwear may also cover the midriff as well. Women's swimwear is often a fashion statement, and whether it is modest or not is a subject of debate by many groups, religious and secular.
Competitive swimwear is built so that the wearer can swim faster and more efficiently. Modern competitive swimwear is skintight and lightweight. There are many kinds of competitive swimwear for each gender. It is used in aquatic competitions, such as water polo, swim racing, diving, and rowing.
Wetsuits provide both thermal insulation and flotation. Many swimmers lack buoyancy in the leg. The wetsuit reduces density and therefore improves buoyancy while swimming. It provides insulation by absorbing some of the surrounding water, which then heats up when in direct contact with skin. The wetsuit is the usual choice for those who swim in cold water for long periods of time, as it reduces susceptibility to hypothermia.
Some people also choose to wear no clothing while swimming; this is known as skinny dipping. It was common for males to swim naked in a public setting up to the early 20th century. Today, skinny dipping can be a rebellious activity or merely a casual one.
This article uses material from the Wikipedia article "Swimming", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Air sports
• Aerobatics
• Air racing
• Cluster ballooning
• Hopper ballooning
Wingsuit flying
• Gliding
• Hang gliding
• Powered hang glider
• Human powered aircraft
• Model aircraft
• Parachuting
• Banzai skydiving
• BASE jumping
• Skydiving
• Skysurfing
• Wingsuit flying
• Paragliding
• Powered paragliding
• Paramotoring
• Ultralight aviation
Archery
• Field archery
• Flight archery
• Gungdo
• Indoor archery
• Kyūdō
• Popinjay
• Target archery
Ball-over-net games
• Badminton
• Ball badminton
• Biribol
• Bossaball
• Fistball
• Footbag net
• Football tennis
• Footvolley
• Hooverball
• Jianzi
• Padel
• Peteca
• Pickleball
• Platform tennis
• Sepak takraw
• Sipa
• Throwball
• Volleyball
• Beach volleyball
• Water volleyball
• Paralympic volleyball
• Wallyball
• Ringo
Basketball family
• Basketball
• Beach basketball
• Deaf basketball
• Streetball
• Water basketball
• Wheelchair basketball
• Cestoball
• Korfball
• Netball
• Fastnet
• Indoor netball
• Ringball
• Slamball
Bat-and-ball (safe haven)
• Baseball
• Softball
• Slow pitch
• Fast-pitch softball
• 16-inch softball
• Bat and trap
• British baseball – four posts
• Brännboll – four bases
• Corkball – four bases (no base-running)
• Cricket – two creases
• Indoor cricket
• Limited overs cricket
• One Day International
• Test cricket
• Twenty20
• Danish longball
• Kickball
• Kilikiti
• Lapta – two salos (bases)
• The Massachusetts Game – four bases
• Matball
• Oina
• Old cat – variable
• Over-the-line – qv
• Palant
• Pesäpallo – four bases
• Punchball
• Rounders – four bases or posts
• Scrub baseball – four bases (not a team game per se)
• Stickball – variable
• Stool ball – two stools
• Tee-ball
• Town ball – variable
• Vigoro – two wickets
• Wireball
• Wiffleball
Baton twirling
• Baton twirling
Acro sports
• Ballet
• Dancing
• Cheerleading
• Gymnastics
Performance sports
• Drum corps
• Marching band
Board sports
• Skateboarding
• Scootering
• Casterboarding
• Freeboard (skateboard)
• Longboarding
• Streetboarding
• Skysurfing
• Streetluge
• Snowboarding
• Mountainboarding
• Sandboarding
• Snowkiting
• Surfing
• Wakesurfing
• Bodyboarding
• Riverboarding
• Skimboarding
• Windsurfing
• Wakeboarding
• Kneeboarding
• Paddleboarding
Catch games
• Dodgeball
• Ga-ga
• Keep away
• Kin-Ball
• Newcomb ball
• Quidditch
• Rundown (a.k.a. Pickle)
• Yukigassen
Climbing
• Abseiling
• Aid climbing
• Ice climbing
• Mixed climbing
• Mountaineering
• Rock climbing
• Bouldering
• Deep-water soloing
• Sport climbing
• Traditional climbing
• Other
• Canyoning (Canyoneering)
• Coasteering
• Hiking
• Rope climbing
• Pole climbing
Cycling
• Artistic cycling
• BMX
• Cyclo-cross
• Cross-country mountain biking
• Cycle polo
• Cycle speedway
• Downhill mountain biking
• Dirt jumping
• Enduro mountain biking
• Freestyle BMX
• Hardcourt Bike Polo
• Road bicycle racing
• Track cycling
• Underwater cycling
Skibob
• Skibobbing
Unicycle
• Mountain unicycling
• Unicycling
• Unicycle basketball
• Unicycle hockey
• Unicycle trials
Combat sports: wrestling and martial arts
• Aiki-jūjutsu
• Aikido
• Jujutsu
• Judo
• Brazilian jiu-jitsu
• Sambo (martial art)
• Sumo
• Wrestling
• Amateur wrestling
• Greco-Roman wrestling
• Freestyle wrestling
• Folk wrestling
• Boli Khela
• Collar-and-elbow
• Cornish wrestling
• Dumog
• Glima
• Gouren
• Kurash
• Lancashire wrestling
• Catch wrestling
• Malla-yuddha
• Mongolian wrestling
• Pehlwani
• Professional wrestling
• Schwingen
• Shuai jiao
• Ssireum
• Varzesh-e Pahlavani
• Yağlı Güreş
• Greek wrestling
Striking
• Choi Kwang-Do
• Cockfighting
• Boxing
• Bokator
• Capoeira
• Fujian White Crane
• Karate
• Kenpō
• Kickboxing
• Lethwei
• Muay Thai
• Pradal serey
• Sanshou
• Savate
• Shaolin Kung Fu
• Sikaran
• Silat
• Subak
• Taekkyeon
• Taekwondo
• Taidō
• Tang Soo Do
• Wing Chun
• Zui quan
Mixed or hybrid
• Baguazhang
• Bando
• Bartitsu
• Bujinkan
• Hapkido
• Hwa Rang Do
• Jeet Kune Do
• Kajukenbo
• Kalaripayattu
• Krav Maga
• Kuk Sool Won
• Marine Corps Martial Arts Program
• Mixed martial arts
• Northern Praying Mantis
• Ninjutsu
• Pankration
• Pencak Silat
• Sanshou
• Shidōkan Karate
• Shōrin-ryū Shidōkan
• Shoot boxing
• Shootfighting
• Shorinji Kempo
• Systema
• T'ai chi ch'uan
• Vajra-mushti
• Vale tudo
• Vovinam
• Xing Yi Quan
• Zen Bu Kan Kempo
Weapons
• Axe throwing
• Battōjutsu
• Boffer fighting
• Eskrima
• Egyptian stick fencing
• Fencing
• Gatka
• Hojōjutsu
• Iaidō
• Iaijutsu
• Jōdō
• Jogo do pau
• Jūkendō
• Jittejutsu
• Kendo
• Kenjutsu
• Krabi–krabong
• Kung fu
• Kyūdō
• Kyūjutsu
• Modern Arnis
• Naginatajutsu
• Nguni stick-fighting
• Okinawan kobudō
• Shurikenjutsu
• Silambam
• Sōjutsu
• Sword fighting
• Wushu
• Kumdo
• Wing Chun
Skirmish
• Airsoft
• Laser tag
• Paintball
Cue sports
• Carom billiards
• Three-cushion
• Five-pins
• Balkline and straight rail
• Cushion caroms
• Four-ball (yotsudama)
• Artistic billiards
• Novuss (and cued forms of carrom)
• Pocket billiards (pool)
• Eight-ball
• Blackball (a.k.a. British eight-ball pool)
• Nine-ball
• Straight pool (14.1 continuous)
• One-pocket
• Three-ball
• Seven-ball
• Ten-ball
• Rotation
• Baseball pocket billiards
• Cribbage (pool)
• Bank pool
• Artistic pool
• Trick shot competition
• Speed pool
• Bowlliards
• Chicago
• Kelly pool
• Cutthroat
• Killer
• Russian pyramid
• Snooker
• Sinuca brasileira
• Six-red snooker
• Snooker plus
• Hybrid carom–pocket games
• English billiards
• Bottle pool
• Cowboy
• Obstacle variations
• Bagatelle
• Bar billiards
• Bumper pool
• Table Sports
• Foosball
Equine sports
• Buzkashi
• Barrel racing
• Campdrafting
• Cirit
• Charreada
• Chilean rodeo
• Cross country
• Cutting
• Dressage
• Endurance riding
• English pleasure
• Equitation
• Eventing
• Equestrian vaulting
• Gymkhana
• Harness racing
• Horse racing
• Horseball
• Hunter
• Hunter-jumpers
• Jousting
• Pato
• Reining
• Rodeo
• Show jumping
• Steeplechase
• Team penning
• Tent pegging
• Western pleasure
Fishing
• Angling
• Big-game fishing
• Casting
• Noodling
• Spearfishing
• Sport fishing
• Surf fishing
• Rock fishing
• Fly fishing
• Ice fishing
Flying disc sports
• Beach ultimate
• Disc dog
• Disc golf
• Disc golf (urban)
• Dodge disc
• Double disc court
• Flutterguts
• Freestyle
• Freestyle competition
• Goaltimate
• Guts
• Hot box
• Ultimate
Football
• Ancient games
• Chinlone
• Cuju
• Episkyros
• Harpastum
• Kemari
• Ki-o-rahi
• Marn Grook
• Woggabaliri
• Yubi lakpi
• Medieval football
• Ba game
• Caid
• Calcio Fiorentino
• Camping (game)
• Chester-le-Street
• Cnapan
• Cornish hurling
• Haxey Hood
• Knattleikr
• La soule
• Lelo burti
• Mob football
• Royal Shrovetide Football
• Uppies and Downies
• Association football
• Jorkyball
• Paralympic football
• Powerchair Football
• Reduced variants
• Five-a-side football
• Beach soccer
• Futebol de Salão
• Futsal
• Papi fut
• Indoor soccer
• Masters Football
• Street football
• Freestyle football
• Keepie uppie
• Swamp football
• Three sided football
• Australian football
• Nine-a-side footy
• Rec footy
• Metro footy
• English school games
• Eton College
• Field game
• Wall game
• Harrow football
• Gaelic football
• Ladies' Gaelic football
• Gridiron football
• American football
• Eight-man football
• Flag football
• Indoor football
• Arena football
• Nine-man football
• Six-man football
• Sprint football
• Touch football
• Canadian football
• Street football (American)
• Rugby football
• Beach rugby
• Rugby league
• Masters Rugby League
• Mod league
• Rugby league nines
• Rugby league sevens
• Tag rugby
• Touch football
• Wheelchair rugby league
• Rugby union
• American flag rugby
• Mini rugby
• Rugby sevens
• Tag rugby
• Touch rugby
• Rugby tens
• Snow rugby
• Hybrid codes
• Austus
• Eton wall game
• International rules football
• Samoa rules
• Speedball
• Universal football
• Volata
Golf
• Miniature golf
• Match play
• Skins game
• Speed golf
• Stroke play
• Team play
• Shotgun start
Gymnastics
• Acrobatic gymnastics
• Aerobic gymnastics
• Artistic gymnastics
• Balance beam
• Floor
• High bar
• Parallel bars
• Pommel horse
• Still rings
• Uneven bars
• Vault
• Juggling
• Rhythmic gymnastics
• Ball
• Club
• Hoop
• Ribbon
• Rope
• Rope jumping
• Slacklining
• Trampolining
• Trapeze
• Flying trapeze
• Static trapeze
• Tumbling
Handball family
• Goalball
• Hitbal
• Tchoukball
• Team handball
• Beach handball
• Czech handball
• Field handball
• Torball
• Water polo
Hunting
• Beagling
• Big game hunting
• Deer hunting
• Fox hunting
• Hare coursing
• Wolf hunting
Ice sports
• Bandy
• Rink bandy
• Broomball
• Curling
• Ice hockey
• Ringette
• Ice yachting
• Figure skating
Kite sports
• Kite buggy
• Kite fighting
• Kite landboarding
• Kitesurfing
• Parasailing
• Snow kiting
• Sport kite (Stunt kite)
Mixed discipline
• Adventure racing
• Biathlon
• Duathlon
• Decathlon
• Heptathlon
• Icosathlon
• Modern pentathlon
• Pentathlon
• Tetrathlon
• Triathlon
Orienteering family
• Geocaching
• Orienteering
• Rogaining
• Letterboxing
• Waymarking
Pilota family
• American handball
• Australian handball
• Basque pelota
• Jai alai
• Fives
• Eton Fives
• Rugby Fives
• Frisian handball
• Four square
• Gaelic handball
• Jeu de paume
• Palla
• Patball
• Valencian pilota
Racquet (or racket) sports
• Badminton
• Ball badminton
• Basque pelota
• Frontenis
• Xare
• Beach tennis
• Fives
• Matkot
• Padel
• Paleta Frontón
• Pelota mixteca
• Pickleball
• Platform tennis
• Qianball
• Racketlon
• Racquetball
• Racquets
• Real tennis
• Soft tennis
• Speed-ball
• Speedminton
• Squash
• Hardball squash
• Squash tennis
• Stické
• Table tennis
• Tennis
Remote control
• Model aerobatics
• RC racing
• Robot combat
• Slot car racing
Rodeo-originated
• Bullriding
• Barrel Racing
• Bronc Riding
• Saddle Bronc Riding
• Roping
• Calf Roping
• Team Roping
• Steer Wrestling
• Goat Tying
Running
• Endurance
• 5K run
• 10K run
• Cross-country running
• Half marathon
• Marathon
• Road running
• Tower running
• Ultramarathon
• Sprint
• Hurdles
Sailing / Windsurfing
• Ice yachting
• Land sailing
• Land windsurfing
• Sailing
• Windsurfing
• Kiteboarding
• Dinghy sailing
Snow sports
• Alpine skiing
• Freestyle skiing
• Nordic combined
• Nordic skiing
• Cross-country skiing
• Telemark skiing
• Ski jumping
• Ski touring
• Skijoring
• Speed skiing
Sled sports
• Bobsleigh
• Luge
• Skibobbing
• Skeleton
• Toboggan
Shooting sports
• Clay pigeon shooting
• Skeet shooting
• Trap shooting
• Sporting clays
• Target shooting
• Field target
• Fullbore target rifle
• High power rifle
• Benchrest shooting
• Metallic silhouette
• Practical shooting
• Cowboy action shooting
• Metallic silhouette shooting
Stacking
• Card stacking
• Dice stacking
• Sport stacking
Stick and ball games
• Hornussen
Hockey
• Hockey
• Ball hockey
• Bando
• Bandy
• Rink bandy
• Broomball
• Moscow broomball
• Field hockey
• Indoor field hockey
• Floorball
• Ice hockey
Ice hockey
• Pond hockey
• Power hockey
• Ringette
• Sledge hockey
• Underwater ice hockey
• Roller hockey
• Inline hockey
• Roller hockey (Quad)
• Skater hockey
• Rossall Hockey
• Spongee
• Street hockey
• Underwater hockey
• Unicycle hockey
Hurling and shinty
• Cammag
• Hurling
• Camogie
• Shinty
• Composite rules shinty-hurling
Lacrosse
• Lacrosse
• Box lacrosse
• Field lacrosse
• Women's lacrosse
• Intercrosse
Polo
• Polo
• Bicycle polo
• Canoe polo
• Cowboy polo
• Elephant polo
• Horse polo
• Segway polo
• Yak polo
Street sports
• Free running
• Freestyle footbag
• Freestyle football
• Powerbocking
• Parkour
• Scootering
• Street workout
Tag games
• British bulldogs (American Eagle)
• Capture the flag
• Hana Ichi Monme
• Hide and seek
• Jugger
• Kabaddi
• Kho kho
• Kick the can
• Oztag
• Red rover
• Tag
Walking
• Hiking
• Backpacking (wilderness)
• Racewalking
• Bushwhacking
• Walking
Wall-and-ball
• American handball
• Australian handball
• Basque pelota
• Butts Up
• Chinese handball
• Fives
• Gaelic handball
• International fronton
• Jorkyball
• Racquetball
• Squash
• Squash tennis
• Suicide (game)
• Valencian frontó
• Wallball
• Wallyball
Aquatic & paddle sports
• Creeking
• Flyak
• Freeboating
• Sea kayaking
• Squirt boating
• Surf kayaking
• Whitewater kayaking
Rafting
• Rafting
• White water rafting
Rowing
• Rowing (sport)
• Gig racing
• Coastal and ocean rowing
• Surfboat
• Single scull
Other paddling sports
• Dragon boat racing
• Stand up paddle boarding
• Water polo
• Canoe polo
• Waboba
Underwater
• Underwater football
• Underwater rugby
• Underwater hockey
Competitive swimming
• Backstroke
• Breaststroke
• Butterfly stroke
• Freestyle swimming
• Individual medley
• Synchronized swimming
• Medley relay
Kindred activities
• Bifins (finswimming)
• Surface finswimming
Subsurface and recreational
• Apnoea finswimming
• Aquathlon (underwater wrestling)
• Freediving
• Immersion finswimming
• Scuba diving
• Spearfishing
• Snorkelling
• Sport diving (sport)
• Underwater hockey
• Underwater orienteering
• Underwater photography (sport)
• Underwater target shooting
Diving
• Cliff diving
• Diving
Weightlifting
• Basque traditional weightlifting
• Bodybuilding
• Highland games
• Olympic weightlifting
• Powerlifting
• Strength athletics (strongman)
• Steinstossen
Motorized sports
• Autocross (a.k.a. Slalom)
• Autograss
• Banger racing
• Board track racing
• Demolition derby
• Desert racing
• Dirt track racing
• Drag racing
• Drifting
• Folkrace
• Formula racing
• Formula Libre
• Formula Student
• Hillclimbing
• Ice racing
• Kart racing
• Land speed records
• Legends car racing
• Midget car racing
• Monster truck
• Mud bogging
• Off-road racing
• Pickup truck racing
• Production car racing
• Race of Champions
• Rally raid
• Rallycross
• Rallying
• Regularity rally
• Road racing
• Short track motor racing
• Snowmobile racing
• Sports car racing
• Sprint car racing
• Street racing
• Stock car racing
• Time attack
• Tractor pulling
• Touring car racing
• Truck racing
• Vintage racing
• Wheelstand competition
Motorboat racing
• Drag boat racing
• F1 powerboat racing
• Hydroplane racing
• Jet sprint boat racing
• Offshore powerboat racing
• Personal water craft
Motorcycle racing
• Auto Race
• Board track racing
• Cross-country rally
• Endurance racing
• Enduro
• Freestyle motocross
• Grand Prix motorcycle racing
• Grasstrack
• Hillclimbing
• Ice racing
• Ice speedway
• Indoor enduro
• Motocross
• Motorcycle drag racing
• Motorcycle speedway
• Off-roading
• Rally raid
• Road racing
• Superbike racing
• Supercross
• Supermoto
• Supersport racing
• Superside
• Track racing
• Trial
• TT racing
• Free-style moto
Marker sports
• Airsoft
• Archery
• Paintball
• Darts
Musical sports
• Color guard
• Drum corps
• Indoor percussion
• Marching band
Fantasy sports
• Quidditch
• Hunger Games(Gladiating)
• Pod Racing
• Mortal Kombat(MMA)
Other
• Stihl Timbersports Series
• Woodsman
Overlapping sports
• Tennis
• Polocrosse
• Badminton
• Polo
Skating sports
• Aggressive inline skating
• Artistic roller skating
• Figure skating
• Freestyle slalom skating
• Ice dancing
• Ice skating
• Inline speed skating
• Rinkball
• Rink hockey
• Roller derby
• Roller skating
• Short track speed skating
• Skater hockey
• Speed skating
• Synchronized skating
Freestyle skiing
• Snowboarding
• Ski flying
• Skibob
• Snowshoeing
• Skiboarding