The three typical components of triathlon: swimming, cycling, and running. | |
Highest governing body | International Triathlon Union |
---|---|
First played | 1920s |
Characteristics | |
Contact | No |
Mixed gender | Yes, separate competitions & mixed relays |
Type | Endurance sport |
Presence | |
Country or region | Worldwide |
Olympic | Yes, since 2000 |
Paralympic | Yes, Paratriathlon since 2016 |
World Games | 1989 (invitational) – 1993 |
A triathlon is a multisport race with three continuous and sequential endurance races.[1] The word is of Greek origin, from τρεῖς or treis (three) and ἆθλος or athlos (competition).[2]
While variations of the sport exist, the most common form includes swimming, cycling, and running over various distances. Triathletes compete for fastest overall course completion, including timed transitions between the three races.[1]
A transition area is set up where the athletes change gear for different segments of the race. This is where the switches from swimming to cycling and cycling to running occur. These areas are used to store bicycles, performance apparel, and any other accessories needed for the next stage of the race. The transition from swim to bike is referred to as T1 and that between the bike and run is referred to as T2. The athlete's overall time for the race includes time spent in T1 and T2.[3] Transition areas vary in size depending on the number of participants expected. In addition, these areas provide a social headquarters before the race.[4]
The nature of the sport focuses on persistent and often periodized training in each of the three disciplines, as well as combination workouts and general strength conditioning.[5]
The evolution of triathlon as a distinct event is difficult to trace with precision. Many, including triathlon historian and author Scott Tinley, consider events in early twentieth century France to be the beginnings of triathlon, with many three element multisport events of differing composition appearing all called by different names.[6][7] The earliest record for an event was from 1901 in Joinville-le-Pont, Val-de-Marne it called itself "Les trois sports" (The three sports) it was advertised as an event for "The sportsmen of the time" and consisted of a run bicycle and canoe segment.[8] By 19 June 1921 the event in Joinville-le-Pont had become more like a standard triathlon with the canoe element being replaced with a swim, newspaper L’Auto stating the race consisted of a 3km run, a 12km bike ride and the crossing of the river Marne, all staged consecutively and without a break.[8][9][10] Throughout the 1920s other bike, run, and swim events had appeared in different cities such as the "Course des Trois Sports” in Marseilles.[11] And "La Course des Débrouillards" in Poissy.[8] [10] These multisport events would continue to slowly spread and grow in popularity such by 1934 "Les Trois Sports" was being hosted in the city of La Rochelle though it consisted three distinct events, swimming a channel crossing (200m),a bike competition around the harbour of La Rochelle and the parc Laleu(10km), and a run in the stadium André-Barbeau(1.2km).[12] Throughout this growth with new events appearing no unified rules ever existed and as a whole would remain a minority event on the world stage.
The first modern swim/bike/run event was held at Mission Bay, San Diego, California on September 25, 1974.[13] The race was conceived and directed by two members of the San Diego Track Club, Jack Johnstone and Don Shanahan.[14] Johnstone recalls that he was a part of the 70s jogging craze in America and that after entering a few races he was not regaining his "mediocre fitness" despite having being a member of the 1957 Collegiate and AAU All-American swim teams.[15] Then in 1973, Johnstone learned of the Dave Pain Birthday Biathlon[note 1], a 4.5 mile run followed by what was billed as a quarter-mile swim (the actual distance was between 200 and 300 yards). The following year after competing in the event for the second time and placing in the top ten Johnstone desired more of this style of race and with equal emphasis on the swim, so he petitioned the chairman of the San Diego Track Club who told him he would add a race to the club calendar but the rest of the race was up to Johnstone to organise and at the same time to contact Don Shanahan so there wouldn't be too many "weird" races on the club schedule. Shanahan told Johnstone that he wanted to include a biking leg to the race, whilst hesitant Johnstone agreed to the addition. When naming the event the pair used the unofficially agreed naming system for multisport event (already used for pentathlon, heptathlon, and decathlon), of using the prefix Greek number for the number of events trias (three) and suffix of athlos the Greek for a competition, hence named the event the Mission Bay Triathlon.[16] It is worthy of note that neither founder had heard of the French events, both believing their race a unique idea.[17]
On Wednesday, September 25, 1974 the race started, it began with a run of a three-mile loop, then biking twice around Fiesta Island for a total of five miles entrants would then get off the bikes, take their shoes off and run into the water swimming to the mainland, then ran in bare feet before swimming again along the bay, then did one last swim up to the entrance of Fiesta Island before crawling up a steep dirt bank to finish.[18] Most participants were not skilled swimmers, so Johnstone recruited his 13-year-old son to float on his surfboard and act as lifeguard.[15][18]Also some participants took longer than expected, and it began to get dark as they finished their swims. Shanahan recalls they pulled up a few cars and turned on the headlights so the athletes could see.[19]The large number of entrants 46 surprised Johnstone and Shanahan with entrants mainly from local running clubs, two notable entrants Judy and John Collins, would four years later found the event which brought international attention to the new sport Ironman Hawaii.[15]
This section is empty. You can help by adding to it. (February 2019) |
With the sport's popularity growing in the US its spread outside the country seemed inevitable, by 1980 triathlon had made its way across the Atlantic to northern Europe with the first European triathlon held on 30th August, 1980 in Pilsen, Czechoslovakia. The Netherlands, Belgium and West Germany follow after, all hosting an event in 1981, but the media coverage of these events is almost non-existent. [20]
Then in 1982, the event organiser IMG, worked in partnership with the American channel CBS (direct competitor of ABC who held the exclusive rights to Hawaii), to create a new event that would take place in Europe. The initial aim was to establish a new premier competition, the European Triathlon, with the goal of being of the same size and prestige to directly compete with that of Hawaii.[21] Originally the event was to be hosted in Monaco, but with the death of Princess Grace in September of 1982 the previous agreements fell through; however, IMG refused to cancel the event so it was reorganised to be hosted in Nice, France. The first Nice Triathlon was held on 20 November 1982 where fifty seven competitors took the start, for an ill-defined competition that consisted of 1,500 meters of swimming, 100 kilometres of cycling and a marathon.[22] In December of that year the national television station France 2 broadcast a program, Voyage au bout de la souffrance (Journey to the End of Suffering) which detailed the events of the Nice Triathlon. This program shocked many that watched and was the introduction of the sport to the general public.[21] Some fans of traditional sports strongly criticised this new practice as seven of the entrants were hospitalised due to the swim, as the temperature of the Mediterranean was only 14°C.[21] Despite this criticism IMG's plan succeeded and throughout the 1980s. The Nice triathlon was, alongside Hawaii, one of the two important Long Distance races each year for both prize money and media attention.[citation needed]
The year 1985 saw the creation of the first international triathlon structure, the European Triathlon Union (ETU) with the objectives to federate the triathlon structures in each European country and to act as a counterbalance to American triathlon in the creation of a future worldwide federation.[23] The following year, the eleven nations that composed the ETU met in Brussels to standardise the national structures of each European country. During this time France dominated discussions, as it was the only federation recognised by its own National Olympic Committee. With the legitimacy from CONADET, forerunner of the French Triathlon Federation (FFTri), which has been organising triathlon in France since 1984 the French system became standard all over Europe.[23]
The first attempt to create a global triathlon entity was the Triathlon Federation International (TFI), it had only 22 members most of which were national European federations. But immediately fights of influences broke out between the European and UK-American federations over many issues, particularly in view of a favourable vote system for the ETU, this causes immediate fracturing and the TFI never fully establish itself.[23]
Around the same time, Canadian Les McDonald held talks with Juan Antonio Samaranch, then President of the International Olympic Committee. Samaranch had already declared his intention to add triathlon to the Olympic games as fast as possible, and assured that triathlon could appear as a demonstration sport at the 1992 Olympic Games in Barcelona but only under the auspices of the International Union of Modern Pentathlon and Biathlon (UIPMB).[24] [25] Many within the triathlon community were unhappy with the arrangement wishing for their own federation not to be held as part of UIPMB. Unable to accept the offer, Samaranch established an Olympic working committee for triathlon in an effort to form a consensus on an Olympic route for the sport. McDonald was selected as President of the committee, while Sweden's Sture Jonasson was elected as Secretary.[25]
Then in February 1989, an informal meeting was held in Vancouver, Canada where members of the working committee worked nonstop for a week on the statutes and regulations of the future International Triathlon Union (ITU). Then on 1 April 1989, 30 National Federations attended the first ITU Congress in Avignon, France. After further discussions on the way forward to reach the Olympics, including the refusal to follow the path of the UIPMB and how triathlon should develop both economically and as a sport, the Congress endorses the creation of the International Triathlon Union and elects its first executive committee. McDonald was elected President. The city of Avignon is also give the honour of hosting the first World Championship.[26]
In 1991, the IOC recognized the ITU as the sole governing body for the sport of triathlon at its 97th session in Birmingham, UK.[27] In 1993 the Pan American Games approved triathlon for competition at the 1995 Pan Am Games in Mar del Plata, Argentina. Then in September of 1994, triathlon was added to the Olympic program as a medal earning sport at the 2000 Olympic Games in Sydney, Australia.[27]
The International Triathlon Union (ITU) was founded in 1989 as the international governing body of the sport, with the chief goal, at that time, of putting triathlon on the Olympic program.[28] The ITU sanctions and organises the World Triathlon Series and World Cup races each year, with annual world champions crowned each year for elite pro-triathletes, junior pro-triathletes, and age-group athletes. ITU races are conducted in a draft legal format for the bike leg, whereas drafting is not permitted at the amateur level. In addition, the ITU has a Long Distance Triathlon series.
The World Triathlon Corporation (WTC) is a private company that sanctions and organises the Ironman and Ironman 70.3 races each year. These races serve as qualifying events for their own annual World Championships. The Ironman World Championship is held annually in Kailua-Kona, Hawaii in October while the Ironman 70.3 World Championship is held in September and changes location each year. The "Ironman" and "Iron" brands are property of the WTC. Therefore, long-distance multi-sport events organized by groups other than the WTC may not officially be called "Ironman" or "Iron" races.[29] For its part, the ITU does not sanction WTC races;[30] however, USAT uses a combination of ITU and WTC rules to sanction WTC's branded events.[31]
Many other organisations exist from local clubs hosting one 100 entrant race a year up to companies like the Challenge Family brand produces long-distance events around the world, and includes events like Challenge Roth.[32] International Ultra-Triathlon Association (IUTA) is the official governing body of Ultratriathlon, which involves triathlon in distances longer than an iron-distance race.[33]
Two major rule making bodies, the ITU and WTC, had an overlap of rules and authority, an issue which began to create conflict in the 2000s.[34] This culminated in 2005 when the ITU and USAT asked all national triathlon federations to refuse to continue sanctioning any WTC events.[35] The reasons for this stemmed from WTC not recognising the ITU as the sport's governing body as WTC was attempting to set up their own federation. Furthermore, ITU and USAT argued against supporting WTC because they were a profit driven organisation, that it was directly conflicting with ITU titles, such as the long and standard distance world championship, and that the WTC was not following World Anti-Doping Agency (WADA) rules. If ITU member nations did not not comply with International Olympic Committee (IOC) Charter rules they risked being excluded from the Olympic program.[36] However, in 2006, the ITU backed down on its stance allowing national federations to once again sanction WTC events. This was due to an out of court settlement days before a lawsuit at the court for the arbitration of sports.[37] This settlement had a large effect on WTC races including WADA membership for the WTC and out of competition testing for elite athletes.
Since 2008, coinciding with leadership changes at both the ITU and WTC, the two organisations have been slowly working together. Efforts in 2012[38] and 2014[39] resulted in the announcement that Ironman would standardise the rule set for its 2015 races, and would start the unification toward ITU rules on long distance racing with specific interest on the drafting and penalty rules.[40][41]
In 2017 the ITU and WTC signed a memorandum of understanding in which the two organisations stated they will:[42]
Name | Swim | Bicycle | Run | Notes |
---|---|---|---|---|
Kids of Steel | 100–750 m (110–820 yd) |
5–15 km (3.1–9.3 mi) |
1–5 km (0.62–3.11 mi) |
Distances vary with age of athlete. See: Ironkids |
Novice (Australia) | 300 m (330 yd) |
8 km (5.0 mi) |
2 km (1.2 mi) |
Standard novice distance course in Australia (often called enticer triathlons). |
3–9–3 (New Zealand) | 300 m (330 yd) |
9 km (5.6 mi) |
3 km (1.9 mi) |
Standard novice distance course in New Zealand. |
Super Sprint | 400 m (0.25 mi) |
10 km (6.2 mi) |
2.5 km (1.6 mi) |
Standard Super Sprint course. |
Novice (Europe) | 400 m (0.25 mi) |
20 km (12 mi) |
5 km (3.1 mi) |
Standard novice/fitness distance course in Europe. |
Sprint | 750 m (0.47 mi) |
20 km (12 mi) |
5 km (3.1 mi) |
Half the Olympic distance. For pool-based races, a 400 or 500 m (1,300 or 1,600 ft) swim is common. |
Olympic | 1.5 km (0.93 mi) |
40 km (25 mi) |
10 km (6.2 mi) |
Also known as "international distance", "standard course", or "short course". |
Triathlon 70.3 | 1.9 km (1.2 mi) |
90 km (56 mi) |
21.1 km (13.1 mi) |
Also known as "middle distance", "70.3" (total miles traveled), or "half-ironman". |
ITU-Long Distance (O2) | 3.0 km (1.9 mi) |
80 km (50 mi) |
20 km (12 mi) |
Double Olympic Distance[43] distance of the ITU Long Distance Triathlon World Championships 2007 and 2009. |
Triathlon 140.6 | 3.9 km (2.4 mi) |
181 km (112 mi) |
42.2 km (26.2 mi) |
Also known as "long distance", "full distance", "140.6" (total miles traveled), or "Ironman Triathlon".[44] |
ITU-Long Distance (O3) | 4.0 km (2.5 mi) |
120 km (75 mi) |
30 km (19 mi) |
So-called triple Olympic Distance,[43] distance of the ITU Long Distance Triathlon World Championships most years including 2011. |
Source:[45][46] |
Triathlons longer than full distance are classed as Ultra-triathlons.
Triathlons are not necessarily restricted to these prescribed distances. Distances can be any combination of distance set by race organizers to meet various distance constraints or to attract a certain type of athlete.
The standard Olympic distance of 1.5/40/10 km (0.93/24.8/6.2 miles) was created by longtime triathlon race director Jim Curl in the mid-1980s, after he and partner Carl Thomas produced the U.S. Triathlon Series (USTS) between 1982 and 1997.[47]
In addition to the above distances, two new long distance events have appeared, the 111 and 222 events. The 111 distance is 1 km (0.62 mi) swimming, 100 km (62 mi) bicycling and 10 km (6.2 mi) running, totalling 111 km (69 mi). The 222 distance is double that.[48]
Most triathlons are individual events. Another format is relay triathlons, where a team of competitors take turns to compete at a race; each competitor must do a segment of swimming, cycling and running. The ITU Team Triathlon World Championships began with two separate classifications for men and women. In 2009, it adopted a 4x4 mixed relay format, where each team has two men and two women. The Youth Olympic Games also has a 4x mixed relay triathlon event.
The ITU accepts a 5% margin of error in the cycle and run course distances.[49] Though there can be some variation in race distances, particularly among short triathlons, most triathlons conform to one of those above standards.
In general, participation in a triathlon requires an athlete to register and sign up in advance of the actual race. After registration, racers are often provided a race number, colored swim cap, and, if the event is being electronically timed, a timing band. Athletes will either be provided or briefed on details of the course, rules, and any problems to look out for (road conditions, closures, traffic lights, aid stations).[50] At a major event, such as an Ironman or a long course championship, triathletes may be required to set up and check-in their bike in the transition area a day or two before the race start, leaving it overnight and under guard.[51]
On the day of the race, before the start of competition, athletes will generally be provided with a bike rack to hold their bicycle and a small section of ground space for shoes, clothing, etc. in the transition area. In some triathlons, there are two transition areas, one for the swim/bike change, then one for the bike/run change at a different location.[52]
Racers are generally categorized into separate professional and amateur categories. Amateurs, who make up the large majority of triathletes, are often referred to as "age groupers" since they are typically further classified by sex and age; which offers the opportunity to compete against others of one's own gender and age group. The age groups are defined in five- or ten-year intervals.[52] There is typically a lower age limit; which can vary from race to race. In some triathlons, heavier amateur athletes may have the option to compete against others closer to their own weight since weight is often considered an impediment to speed. As an example, under USA Triathlon rules, "Clydesdale" athletes are those men over 220 lb (100 kg), while "Athena" athletes are women over 165 lb (75 kg).[53] Other races and organizations can choose whether or not to offer Clydesdale- and Athena-type divisions and set their own weight standards.
Depending on the type and size of the race, there may be any of the following methods implemented to start the race. In a mass start, all athletes enter the water and begin the competition following a single start signal. In wave start events, smaller groups of athletes begin the race every few minutes. An athlete's wave is usually determined either by age group or by predicted swim time. Wave starts are more common in shorter races where a large number of amateur athletes are competing.[54] Another option is individual time trial starts, where athletes enter the water one at a time, a few seconds apart.[55]
The swim leg usually proceeds around a series of marked buoys before athletes exit the water near the transition area. Racers exit out of the water, enter the transition area, and change from their swim gear and into their cycling gear. Competition and pressure for faster times have led to the development of specialized triathlon clothing that is adequate for both swimming and cycling, allowing many racers to have a transition that consists of only removing their wetsuit, cap, and goggles and pulling on a helmet and cycling shoes. In some cases, racers leave their cycling shoes attached to their bicycle pedals and slip their feet into them while riding. Some triathletes don't wear socks, decreasing their time spent in transition even more.
The cycling stage proceeds around a marked course, typically on public roads. In many cases, especially smaller triathlons, roads are not closed to automobiles; however, traffic coordinators are often present to help control traffic. Typically, the cycling stage finishes back at the same transition area. Racers enter the transition area, rack their bicycles, and quickly change into running shoes before heading out for the final stage. The running stage usually ends at a separate finish line near the transition area.
In most races, "aid stations" located on the bike and run courses provide water and energy drinks to the athletes as they pass by. Aid stations at longer events may often provide various types of food as well, including such items as energy bars, energy gels, fruit, cookies, soup, and ice.
Once the triathletes have completed the event, there is typically another aid station for them to get water, fruit, and other post-race refreshments. Occasionally, at the end of larger or longer events, the provided amenities and post-race celebrations may be more elaborate.
While specific rules for triathlon can vary depending on the governing body (e.g. USA Triathlon, ITU), as well as for an individual race venue, there are some basic universal rules. Traditionally, triathlon is an individual sport and each athlete is competing against the course and the clock for the best time. As such, athletes are not allowed to receive assistance from anyone else outside the race, with the exception of race-sanctioned aid volunteers who distribute food and water on the course.[56][57]
Triathlons are timed in five sequential sections:
Results are usually posted on official websites and will show for each triathlete his/her swim time; cycle time (with transitions included); run time; and total time. Some races also post transition times separately.
Other rules of triathlon vary from race to race and generally involve descriptions of allowable equipment (for example, wetsuits are allowed in USAT events in the swimming stage of some races when the water temperature is below 78.1 °F [25.6 °C]),[53] and prohibitions against interference between athletes.[57] Additionally, the use of flippers or other swim propulsion and flotation aids are illegal in triathlon and can result in disqualification.[53]
One rule involving the cycle leg is that the competitor's helmet must be donned before the competitor mounts (or even takes possession of, in certain jurisdictions[58]) the bike and must remain on until the competitor has dismounted; the competitor is not required to wear the helmet when not on the bicycle (e.g. while repairing a mechanical problem). Failure to comply with this rule will result in disqualification.[53][57] Additionally, while on the bike course, all bicycles shall be propelled only by human force and human power. Other than pushing a bicycle, any propulsive action brought on by use of the hands is prohibited. Should a competitor's bike malfunction they can proceed with the race as long as they are doing so with their bicycle in tow.[53] There are also strict rules regarding the 'bike mount' line. Competitors may not begin riding their bicycle out of transition until they are over a clearly marked line. Mounting the bike prior to this may incur a penalty (example: a 15-second time penalty at the London 2012 Olympics was awarded to Jonathan Brownlee, a competitor from Great Britain, for mounting his bike too early.)[57][59]
Other time penalties can be incurred during the race for, among other things, drafting on the bike in a non-drafting race, improper passing, littering on course, and unsportsmanlike conduct.[53][60]
Participants in triathlon often use the sport to improve or maintain their physical fitness.[61][62] With each sport being an endurance event, training for a triathlon provides cardiovascular exercise benefits.[63] Additionally, triathletes encounter fewer injuries than those who only use running as part of their exercise routine due to the incorporation of low impact swim and bike training.[64]
Triathletes spend many hours training for competitions, like other endurance event participants.[65] There are three components that have been researched to improve endurance sports performance; aerobic capacity, lactate threshold, and economy.[66] Injuries that are incurred from long hours of a single activity are not as common in triathlon as they are in single sport events. The cross-training effect that athletes achieve from training for one sport by doing a second activity applies to triathlon training.[64] Additional activities that triathletes perform for cross-training benefits are yoga, pilates, and weight training.[67]
Triathletes will often use their legs less vigorously and more carefully than other swimmers, conserving their leg muscles for the cycle and run to follow. Many triathletes use altered swim strokes to compensate for turbulent, aerated water and to conserve energy for a long swim. In addition, the majority of triathlons involve open-water (outdoor) swim stages, rather than pools with lane markers. As a result, triathletes in the swim stage must jockey for position, and can gain some advantage by drafting, following a competitor closely to swim in their slipstream. Triathletes will often use "dolphin kicking" and diving to make headway against waves, and body surfing to use a wave's energy for a bit of speed at the end of the swim stage. Also, open-water swims necessitate "sighting": raising the head to look for landmarks or buoys that mark the course. A modified stroke allows the triathlete to lift the head above water to sight without interrupting the swim or wasting energy.
Because open water swim areas are often cold and because wearing a wetsuit provides a competitive advantage, specialized triathlon wetsuits have been developed in a variety of styles to match the conditions of the water. For example, wetsuits that are sleeveless and cut above the knee are designed for warmer waters, while still providing buoyancy. Wetsuits are legal in sanctioned events at which the surface water temperature is 78 °F (26 °C) or less.[53] In non-sanctioned events or in "age group" classes where most racers are simply participating for the enjoyment of the sport instead of vying for official triathlon placing, wetsuits can often be used at other temperatures. Race directors will sometimes discourage or ban wetsuits if the water temperature is above 84 °F (29 °C) due to overheating that can occur while wearing a wetsuit.[68] Other rules have been implemented by race organizers regarding both wetsuit thickness as well as the use of "swim skins;" which need to be considered by those participating in future triathlons. Some triathlon sanctioning bodies have placed limits on the thickness of the wetsuit material. Under ITU and some national governing bodies' rules no wetsuit may have a thickness of more than 5 mm (0.20 in).[69]
Triathlon cycling can differ from most professional bicycle racing depending on whether drafting is allowed during competition. In some competitions, like those governed by USA Triathlon and the World Triathlon Corporation, drafting is not allowed,[53] and thus the cycling portion more closely resembles individual time trial racing. In other races, such as those in World Cup and Championship racing, drafting and the formation of pelotons are legal.[1][57] This places an emphasis on running performance as several athletes will enter the bike to run transition at the same time due to drafting.[70]
Triathlon bicycles are generally optimized for aerodynamics, having special handlebars called aero-bars or tri-bars, aerodynamic wheels, and other components. Triathlon bikes use a specialized geometry, including a steep seat-tube angle both to improve aerodynamics and to spare muscle groups needed for running (see also triathlon equipment). At the end of the bike segment, triathletes also often cycle with a higher cadence (revolutions per minute), which serves in part to keep the muscles loose and flexible for running.
The primary distinguishing feature of running in a triathlon is that it occurs after the athlete has already been exercising in two other disciplines for an extended period of time, so many muscles are already tired. The effect of switching from cycling to running can be profound; first-time triathletes are often astonished at their muscle weakness, which may be caused by lactate accumulation and the bizarre, sometimes painful sensation in their thighs a few hundred yards into the run, and discover that they run at a much slower pace than they are accustomed to in training. Triathletes train for this phenomenon through transition workouts known as "bricks": back-to-back workouts involving two disciplines, most commonly cycling and running.
The change over from sport to sport takes place in a designated transition area. The transition provides a staging area where bicycles, running shoes, hydration and other gear is set up ready to be used during the course of the event. The first transition, known as T1, is between the swim-to-bike segments of the race. The second transition, T2, is between the bike-to-run segments. Most events have one common transition area for both T1 and T2, while some point to point events have two separate transition areas. The time spent in transition is a timed segment and contributes towards the overall finishing time of the event.
The sport made its debut on the Olympic program at the Sydney Games in 2000 over the Olympic Distance (swim: 1,500 m [1,650 yd] – bike: 40 km [24.9 mi] – run: 10 km [6.2 mi]).
Paratriathlon at the Summer Paralympics debuted at the 2016 Summer Paralympics held in Rio de Janeiro, Brazil.[71][72]. Paratriathlon is a variant of the triathlon for athletes with a physical disability. The Paralympic event originally scheduled a sprint race with athletes competing in six categories according to the nature of their physical impairments.[73][74]
Thousands of individual triathlons are held around the world each year. A few of these races are well known because they have a long history or because they have particularly grueling courses and race conditions.
This article uses material from the Wikipedia article "Triathlon", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Air sports
• Aerobatics
• Air racing
• Cluster ballooning
• Hopper ballooning
Wingsuit flying
• Gliding
• Hang gliding
• Powered hang glider
• Human powered aircraft
• Model aircraft
• Parachuting
• Banzai skydiving
• BASE jumping
• Skydiving
• Skysurfing
• Wingsuit flying
• Paragliding
• Powered paragliding
• Paramotoring
• Ultralight aviation
Archery
• Field archery
• Flight archery
• Gungdo
• Indoor archery
• Kyūdō
• Popinjay
• Target archery
Ball-over-net games
• Badminton
• Ball badminton
• Biribol
• Bossaball
• Fistball
• Footbag net
• Football tennis
• Footvolley
• Hooverball
• Jianzi
• Padel
• Peteca
• Pickleball
• Platform tennis
• Sepak takraw
• Sipa
• Throwball
• Volleyball
• Beach volleyball
• Water volleyball
• Paralympic volleyball
• Wallyball
• Ringo
Basketball family
• Basketball
• Beach basketball
• Deaf basketball
• Streetball
• Water basketball
• Wheelchair basketball
• Cestoball
• Korfball
• Netball
• Fastnet
• Indoor netball
• Ringball
• Slamball
Bat-and-ball (safe haven)
• Baseball
• Softball
• Slow pitch
• Fast-pitch softball
• 16-inch softball
• Bat and trap
• British baseball – four posts
• Brännboll – four bases
• Corkball – four bases (no base-running)
• Cricket – two creases
• Indoor cricket
• Limited overs cricket
• One Day International
• Test cricket
• Twenty20
• Danish longball
• Kickball
• Kilikiti
• Lapta – two salos (bases)
• The Massachusetts Game – four bases
• Matball
• Oina
• Old cat – variable
• Over-the-line – qv
• Palant
• Pesäpallo – four bases
• Punchball
• Rounders – four bases or posts
• Scrub baseball – four bases (not a team game per se)
• Stickball – variable
• Stool ball – two stools
• Tee-ball
• Town ball – variable
• Vigoro – two wickets
• Wireball
• Wiffleball
Baton twirling
• Baton twirling
Acro sports
• Ballet
• Dancing
• Cheerleading
• Gymnastics
Performance sports
• Drum corps
• Marching band
Board sports
• Skateboarding
• Scootering
• Casterboarding
• Freeboard (skateboard)
• Longboarding
• Streetboarding
• Skysurfing
• Streetluge
• Snowboarding
• Mountainboarding
• Sandboarding
• Snowkiting
• Surfing
• Wakesurfing
• Bodyboarding
• Riverboarding
• Skimboarding
• Windsurfing
• Wakeboarding
• Kneeboarding
• Paddleboarding
Catch games
• Dodgeball
• Ga-ga
• Keep away
• Kin-Ball
• Newcomb ball
• Quidditch
• Rundown (a.k.a. Pickle)
• Yukigassen
Climbing
• Abseiling
• Aid climbing
• Ice climbing
• Mixed climbing
• Mountaineering
• Rock climbing
• Bouldering
• Deep-water soloing
• Sport climbing
• Traditional climbing
• Other
• Canyoning (Canyoneering)
• Coasteering
• Hiking
• Rope climbing
• Pole climbing
Cycling
• Artistic cycling
• BMX
• Cyclo-cross
• Cross-country mountain biking
• Cycle polo
• Cycle speedway
• Downhill mountain biking
• Dirt jumping
• Enduro mountain biking
• Freestyle BMX
• Hardcourt Bike Polo
• Road bicycle racing
• Track cycling
• Underwater cycling
Skibob
• Skibobbing
Unicycle
• Mountain unicycling
• Unicycling
• Unicycle basketball
• Unicycle hockey
• Unicycle trials
Combat sports: wrestling and martial arts
• Aiki-jūjutsu
• Aikido
• Jujutsu
• Judo
• Brazilian jiu-jitsu
• Sambo (martial art)
• Sumo
• Wrestling
• Amateur wrestling
• Greco-Roman wrestling
• Freestyle wrestling
• Folk wrestling
• Boli Khela
• Collar-and-elbow
• Cornish wrestling
• Dumog
• Glima
• Gouren
• Kurash
• Lancashire wrestling
• Catch wrestling
• Malla-yuddha
• Mongolian wrestling
• Pehlwani
• Professional wrestling
• Schwingen
• Shuai jiao
• Ssireum
• Varzesh-e Pahlavani
• Yağlı Güreş
• Greek wrestling
Striking
• Choi Kwang-Do
• Cockfighting
• Boxing
• Bokator
• Capoeira
• Fujian White Crane
• Karate
• Kenpō
• Kickboxing
• Lethwei
• Muay Thai
• Pradal serey
• Sanshou
• Savate
• Shaolin Kung Fu
• Sikaran
• Silat
• Subak
• Taekkyeon
• Taekwondo
• Taidō
• Tang Soo Do
• Wing Chun
• Zui quan
Mixed or hybrid
• Baguazhang
• Bando
• Bartitsu
• Bujinkan
• Hapkido
• Hwa Rang Do
• Jeet Kune Do
• Kajukenbo
• Kalaripayattu
• Krav Maga
• Kuk Sool Won
• Marine Corps Martial Arts Program
• Mixed martial arts
• Northern Praying Mantis
• Ninjutsu
• Pankration
• Pencak Silat
• Sanshou
• Shidōkan Karate
• Shōrin-ryū Shidōkan
• Shoot boxing
• Shootfighting
• Shorinji Kempo
• Systema
• T'ai chi ch'uan
• Vajra-mushti
• Vale tudo
• Vovinam
• Xing Yi Quan
• Zen Bu Kan Kempo
Weapons
• Axe throwing
• Battōjutsu
• Boffer fighting
• Eskrima
• Egyptian stick fencing
• Fencing
• Gatka
• Hojōjutsu
• Iaidō
• Iaijutsu
• Jōdō
• Jogo do pau
• Jūkendō
• Jittejutsu
• Kendo
• Kenjutsu
• Krabi–krabong
• Kung fu
• Kyūdō
• Kyūjutsu
• Modern Arnis
• Naginatajutsu
• Nguni stick-fighting
• Okinawan kobudō
• Shurikenjutsu
• Silambam
• Sōjutsu
• Sword fighting
• Wushu
• Kumdo
• Wing Chun
Skirmish
• Airsoft
• Laser tag
• Paintball
Cue sports
• Carom billiards
• Three-cushion
• Five-pins
• Balkline and straight rail
• Cushion caroms
• Four-ball (yotsudama)
• Artistic billiards
• Novuss (and cued forms of carrom)
• Pocket billiards (pool)
• Eight-ball
• Blackball (a.k.a. British eight-ball pool)
• Nine-ball
• Straight pool (14.1 continuous)
• One-pocket
• Three-ball
• Seven-ball
• Ten-ball
• Rotation
• Baseball pocket billiards
• Cribbage (pool)
• Bank pool
• Artistic pool
• Trick shot competition
• Speed pool
• Bowlliards
• Chicago
• Kelly pool
• Cutthroat
• Killer
• Russian pyramid
• Snooker
• Sinuca brasileira
• Six-red snooker
• Snooker plus
• Hybrid carom–pocket games
• English billiards
• Bottle pool
• Cowboy
• Obstacle variations
• Bagatelle
• Bar billiards
• Bumper pool
• Table Sports
• Foosball
Equine sports
• Buzkashi
• Barrel racing
• Campdrafting
• Cirit
• Charreada
• Chilean rodeo
• Cross country
• Cutting
• Dressage
• Endurance riding
• English pleasure
• Equitation
• Eventing
• Equestrian vaulting
• Gymkhana
• Harness racing
• Horse racing
• Horseball
• Hunter
• Hunter-jumpers
• Jousting
• Pato
• Reining
• Rodeo
• Show jumping
• Steeplechase
• Team penning
• Tent pegging
• Western pleasure
Fishing
• Angling
• Big-game fishing
• Casting
• Noodling
• Spearfishing
• Sport fishing
• Surf fishing
• Rock fishing
• Fly fishing
• Ice fishing
Flying disc sports
• Beach ultimate
• Disc dog
• Disc golf
• Disc golf (urban)
• Dodge disc
• Double disc court
• Flutterguts
• Freestyle
• Freestyle competition
• Goaltimate
• Guts
• Hot box
• Ultimate
Football
• Ancient games
• Chinlone
• Cuju
• Episkyros
• Harpastum
• Kemari
• Ki-o-rahi
• Marn Grook
• Woggabaliri
• Yubi lakpi
• Medieval football
• Ba game
• Caid
• Calcio Fiorentino
• Camping (game)
• Chester-le-Street
• Cnapan
• Cornish hurling
• Haxey Hood
• Knattleikr
• La soule
• Lelo burti
• Mob football
• Royal Shrovetide Football
• Uppies and Downies
• Association football
• Jorkyball
• Paralympic football
• Powerchair Football
• Reduced variants
• Five-a-side football
• Beach soccer
• Futebol de Salão
• Futsal
• Papi fut
• Indoor soccer
• Masters Football
• Street football
• Freestyle football
• Keepie uppie
• Swamp football
• Three sided football
• Australian football
• Nine-a-side footy
• Rec footy
• Metro footy
• English school games
• Eton College
• Field game
• Wall game
• Harrow football
• Gaelic football
• Ladies' Gaelic football
• Gridiron football
• American football
• Eight-man football
• Flag football
• Indoor football
• Arena football
• Nine-man football
• Six-man football
• Sprint football
• Touch football
• Canadian football
• Street football (American)
• Rugby football
• Beach rugby
• Rugby league
• Masters Rugby League
• Mod league
• Rugby league nines
• Rugby league sevens
• Tag rugby
• Touch football
• Wheelchair rugby league
• Rugby union
• American flag rugby
• Mini rugby
• Rugby sevens
• Tag rugby
• Touch rugby
• Rugby tens
• Snow rugby
• Hybrid codes
• Austus
• Eton wall game
• International rules football
• Samoa rules
• Speedball
• Universal football
• Volata
Golf
• Miniature golf
• Match play
• Skins game
• Speed golf
• Stroke play
• Team play
• Shotgun start
Gymnastics
• Acrobatic gymnastics
• Aerobic gymnastics
• Artistic gymnastics
• Balance beam
• Floor
• High bar
• Parallel bars
• Pommel horse
• Still rings
• Uneven bars
• Vault
• Juggling
• Rhythmic gymnastics
• Ball
• Club
• Hoop
• Ribbon
• Rope
• Rope jumping
• Slacklining
• Trampolining
• Trapeze
• Flying trapeze
• Static trapeze
• Tumbling
Handball family
• Goalball
• Hitbal
• Tchoukball
• Team handball
• Beach handball
• Czech handball
• Field handball
• Torball
• Water polo
Hunting
• Beagling
• Big game hunting
• Deer hunting
• Fox hunting
• Hare coursing
• Wolf hunting
Ice sports
• Bandy
• Rink bandy
• Broomball
• Curling
• Ice hockey
• Ringette
• Ice yachting
• Figure skating
Kite sports
• Kite buggy
• Kite fighting
• Kite landboarding
• Kitesurfing
• Parasailing
• Snow kiting
• Sport kite (Stunt kite)
Mixed discipline
• Adventure racing
• Biathlon
• Duathlon
• Decathlon
• Heptathlon
• Icosathlon
• Modern pentathlon
• Pentathlon
• Tetrathlon
• Triathlon
Orienteering family
• Geocaching
• Orienteering
• Rogaining
• Letterboxing
• Waymarking
Pilota family
• American handball
• Australian handball
• Basque pelota
• Jai alai
• Fives
• Eton Fives
• Rugby Fives
• Frisian handball
• Four square
• Gaelic handball
• Jeu de paume
• Palla
• Patball
• Valencian pilota
Racquet (or racket) sports
• Badminton
• Ball badminton
• Basque pelota
• Frontenis
• Xare
• Beach tennis
• Fives
• Matkot
• Padel
• Paleta Frontón
• Pelota mixteca
• Pickleball
• Platform tennis
• Qianball
• Racketlon
• Racquetball
• Racquets
• Real tennis
• Soft tennis
• Speed-ball
• Speedminton
• Squash
• Hardball squash
• Squash tennis
• Stické
• Table tennis
• Tennis
Remote control
• Model aerobatics
• RC racing
• Robot combat
• Slot car racing
Rodeo-originated
• Bullriding
• Barrel Racing
• Bronc Riding
• Saddle Bronc Riding
• Roping
• Calf Roping
• Team Roping
• Steer Wrestling
• Goat Tying
Running
• Endurance
• 5K run
• 10K run
• Cross-country running
• Half marathon
• Marathon
• Road running
• Tower running
• Ultramarathon
• Sprint
• Hurdles
Sailing / Windsurfing
• Ice yachting
• Land sailing
• Land windsurfing
• Sailing
• Windsurfing
• Kiteboarding
• Dinghy sailing
Snow sports
• Alpine skiing
• Freestyle skiing
• Nordic combined
• Nordic skiing
• Cross-country skiing
• Telemark skiing
• Ski jumping
• Ski touring
• Skijoring
• Speed skiing
Sled sports
• Bobsleigh
• Luge
• Skibobbing
• Skeleton
• Toboggan
Shooting sports
• Clay pigeon shooting
• Skeet shooting
• Trap shooting
• Sporting clays
• Target shooting
• Field target
• Fullbore target rifle
• High power rifle
• Benchrest shooting
• Metallic silhouette
• Practical shooting
• Cowboy action shooting
• Metallic silhouette shooting
Stacking
• Card stacking
• Dice stacking
• Sport stacking
Stick and ball games
• Hornussen
Hockey
• Hockey
• Ball hockey
• Bando
• Bandy
• Rink bandy
• Broomball
• Moscow broomball
• Field hockey
• Indoor field hockey
• Floorball
• Ice hockey
Ice hockey
• Pond hockey
• Power hockey
• Ringette
• Sledge hockey
• Underwater ice hockey
• Roller hockey
• Inline hockey
• Roller hockey (Quad)
• Skater hockey
• Rossall Hockey
• Spongee
• Street hockey
• Underwater hockey
• Unicycle hockey
Hurling and shinty
• Cammag
• Hurling
• Camogie
• Shinty
• Composite rules shinty-hurling
Lacrosse
• Lacrosse
• Box lacrosse
• Field lacrosse
• Women's lacrosse
• Intercrosse
Polo
• Polo
• Bicycle polo
• Canoe polo
• Cowboy polo
• Elephant polo
• Horse polo
• Segway polo
• Yak polo
Street sports
• Free running
• Freestyle footbag
• Freestyle football
• Powerbocking
• Parkour
• Scootering
• Street workout
Tag games
• British bulldogs (American Eagle)
• Capture the flag
• Hana Ichi Monme
• Hide and seek
• Jugger
• Kabaddi
• Kho kho
• Kick the can
• Oztag
• Red rover
• Tag
Walking
• Hiking
• Backpacking (wilderness)
• Racewalking
• Bushwhacking
• Walking
Wall-and-ball
• American handball
• Australian handball
• Basque pelota
• Butts Up
• Chinese handball
• Fives
• Gaelic handball
• International fronton
• Jorkyball
• Racquetball
• Squash
• Squash tennis
• Suicide (game)
• Valencian frontó
• Wallball
• Wallyball
Aquatic & paddle sports
• Creeking
• Flyak
• Freeboating
• Sea kayaking
• Squirt boating
• Surf kayaking
• Whitewater kayaking
Rafting
• Rafting
• White water rafting
Rowing
• Rowing (sport)
• Gig racing
• Coastal and ocean rowing
• Surfboat
• Single scull
Other paddling sports
• Dragon boat racing
• Stand up paddle boarding
• Water polo
• Canoe polo
• Waboba
Underwater
• Underwater football
• Underwater rugby
• Underwater hockey
Competitive swimming
• Backstroke
• Breaststroke
• Butterfly stroke
• Freestyle swimming
• Individual medley
• Synchronized swimming
• Medley relay
Kindred activities
• Bifins (finswimming)
• Surface finswimming
Subsurface and recreational
• Apnoea finswimming
• Aquathlon (underwater wrestling)
• Freediving
• Immersion finswimming
• Scuba diving
• Spearfishing
• Snorkelling
• Sport diving (sport)
• Underwater hockey
• Underwater orienteering
• Underwater photography (sport)
• Underwater target shooting
Diving
• Cliff diving
• Diving
Weightlifting
• Basque traditional weightlifting
• Bodybuilding
• Highland games
• Olympic weightlifting
• Powerlifting
• Strength athletics (strongman)
• Steinstossen
Motorized sports
• Autocross (a.k.a. Slalom)
• Autograss
• Banger racing
• Board track racing
• Demolition derby
• Desert racing
• Dirt track racing
• Drag racing
• Drifting
• Folkrace
• Formula racing
• Formula Libre
• Formula Student
• Hillclimbing
• Ice racing
• Kart racing
• Land speed records
• Legends car racing
• Midget car racing
• Monster truck
• Mud bogging
• Off-road racing
• Pickup truck racing
• Production car racing
• Race of Champions
• Rally raid
• Rallycross
• Rallying
• Regularity rally
• Road racing
• Short track motor racing
• Snowmobile racing
• Sports car racing
• Sprint car racing
• Street racing
• Stock car racing
• Time attack
• Tractor pulling
• Touring car racing
• Truck racing
• Vintage racing
• Wheelstand competition
Motorboat racing
• Drag boat racing
• F1 powerboat racing
• Hydroplane racing
• Jet sprint boat racing
• Offshore powerboat racing
• Personal water craft
Motorcycle racing
• Auto Race
• Board track racing
• Cross-country rally
• Endurance racing
• Enduro
• Freestyle motocross
• Grand Prix motorcycle racing
• Grasstrack
• Hillclimbing
• Ice racing
• Ice speedway
• Indoor enduro
• Motocross
• Motorcycle drag racing
• Motorcycle speedway
• Off-roading
• Rally raid
• Road racing
• Superbike racing
• Supercross
• Supermoto
• Supersport racing
• Superside
• Track racing
• Trial
• TT racing
• Free-style moto
Marker sports
• Airsoft
• Archery
• Paintball
• Darts
Musical sports
• Color guard
• Drum corps
• Indoor percussion
• Marching band
Fantasy sports
• Quidditch
• Hunger Games(Gladiating)
• Pod Racing
• Mortal Kombat(MMA)
Other
• Stihl Timbersports Series
• Woodsman
Overlapping sports
• Tennis
• Polocrosse
• Badminton
• Polo
Skating sports
• Aggressive inline skating
• Artistic roller skating
• Figure skating
• Freestyle slalom skating
• Ice dancing
• Ice skating
• Inline speed skating
• Rinkball
• Rink hockey
• Roller derby
• Roller skating
• Short track speed skating
• Skater hockey
• Speed skating
• Synchronized skating
Freestyle skiing
• Snowboarding
• Ski flying
• Skibob
• Snowshoeing
• Skiboarding