Licensed under Creative Commons Attribution-Share Alike 3.0 (Lidingo).
Look up stable in Wiktionary, the free dictionary. |
A stable is a building in which livestock, especially horses, are kept. It most commonly means a building that is divided into separate stalls for individual animals. There are many different types of stables in use today; the American-style barn, for instance, is a large barn with a door at each end and individual stalls inside or free-standing stables with top and bottom-opening doors. The term "stable" is also used to describe a group of animals kept by one owner, regardless of housing or location.
The exterior design of a stable can vary widely, based on climate, building materials, historical period and cultural styles of architecture. A wide range of building materials can be used, including masonry (bricks or stone), wood and steel. Stables also range widely in size, from a small building housing one or two animals to facilities at agricultural shows or race tracks that can house hundreds of animals.
The stable is typically historically the second-oldest building type on the farm. The world’s oldest horse stables were discovered in the ancient city of Pi-Ramesses in Qantir, in Ancient Egypt, and were established by Ramesses II (c.1304-1237 BC). These stables covered approximately 182,986 square feet, had floors sloped for drainage, and could contain about 480 horses.[1] Free-standing stables began to be built from the 16th century. They were well built and placed near the house because these animals were highly valued and carefully maintained. They were once vital to the economy and an indicator of their owners' position in the community. Relatively few examples survive of complete interiors (i.e. with stalls, mangers and feed racks) from the mid-19th century or earlier.[2][3]
Traditionally, stables in Great Britain had a hayloft on their first (i.e. upper) floor and a pitching door at the front. Doors and windows were symmetrically arranged. Their interiors were divided into stalls and usually included a large stall for a foaling mare or sick horse. The floors were cobbled (or, later, bricked) and featured drainage channels. Outside steps to the first floor were common for farm hands to live in the building.[4][clarification needed]
For horses, stables are often part of a larger complex which includes trainers, vets and farriers.
"Stable" is used metaphorically to refer to a group of people – often (but not exclusively) sportspeople – trained, coached, supervised or managed by the same person or organisation. For example, art galleries typically refer to the artists they represent as their stable of artists.
Historically, the headquarters of a unit of cavalry, not simply their horses' accommodation, would be known as "a stable".
A shed row-style stable at a riding club in Panama.
Stables of the Einsiedeln Abbey, Switzerland.
A horse stable, over 100 years old, still in use at Stanford University.
A row-style stable in Žabnik at Sveti Martin na Muri, Croatia.
Media related to stables at Wikimedia Commons.
This article uses material from the Wikipedia article "Stable", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library