powered by CADENAS

Social Share

Amazon

Bearing surface (3705 views - Mechanical Engineering)

A bearing surface in mechanical engineering is the area of contact between two objects. It usually is used in reference to bolted joints and bearings, but can be applied to a wide variety of engineering applications. On a screw the bearing area loosely refers to the underside of the head. Strictly speaking, the bearing area refers to the area of the screw head that directly bears on the part being fastened.For a cylindrical bearing it is the projected area perpendicular to the applied force.On a spring the bearing area refers to the amount of area on the top or bottom surface of the spring in contact with the constraining part.The ways of machine tools, such as dovetail slides, box ways, prismatic ways, and other types of machine slides are also bearing surfaces.
Go to Article

Explanation by Hotspot Model

Youtube


    

Bearing surface

Bearing surface

A bearing surface in mechanical engineering is the area of contact between two objects. It usually is used in reference to bolted joints and bearings, but can be applied to a wide variety of engineering applications.

On a screw the bearing area loosely refers to the underside of the head.[1] Strictly speaking, the bearing area refers to the area of the screw head that directly bears on the part being fastened.[2]

For a cylindrical bearing it is the projected area perpendicular to the applied force.[3]

On a spring the bearing area refers to the amount of area on the top or bottom surface of the spring in contact with the constraining part.[4]

The ways of machine tools, such as dovetail slides, box ways, prismatic ways, and other types of machine slides are also bearing surfaces.

See also



This article uses material from the Wikipedia article "Bearing surface", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD