powered by CADENAS

Social Share

Amazon

Tongue-and-groove pliers (3021 views - Tooling)

Tongue-and-groove pliers are a type of slip-joint pliers. They are also known as water pump pliers, adjustable pliers, groove-joint pliers, arc-joint pliers, Multi-Grips, tap or pipe spanners, gland pliers and Channellocks (i.e., Channellock brand pliers).
Go to Article

Explanation by Hotspot Model

Youtube


    

Tongue-and-groove pliers

Tongue-and-groove pliers

Tongue-and-groove pliers are a type of slip-joint pliers. They are also known as water pump pliers, adjustable pliers, groove-joint pliers, arc-joint pliers, Multi-Grips, tap or pipe spanners, gland pliers and Channellocks (i.e., Channellock brand pliers).

Design

They have serrated jaws generally set 45 to 60 degrees from the handles. The lower jaw can be moved to a number of positions by sliding along a tracking section under the upper jaw. An advantage of this design is that the pliers can adjust to a number of sizes without the distance in the handle growing wider. These pliers often have long handles—commonly 9.5 to 12 inches long—for increased leverage.[1][2][3]

Uses

Tongue-and-groove pliers are commonly used for turning and holding nuts and bolts, gripping irregularly shaped objects, and clamping materials.

History

This design of pliers was invented and popularized by the Champion–DeArment Tool Company in 1934 under the brand name Channellock (after which the company was later renamed)[4] but are also now produced by a number of other manufacturers.

Gallery

  1. ^ US 2592927 
  2. ^ US 4890519 
  3. ^ "Common Maintenance Tools and Their Use: Water-Pump Pliers and Groove-Joint Pliers". Aviation Boatswains Mate E - Aviation theories and other practices. Retrieved 2010-03-29.
  4. ^ US 1950362 


This article uses material from the Wikipedia article "Tongue-and-groove pliers", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing