Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Joe Mabel).
The monkey wrench is a type of adjustable wrench, a later American development of eighteenth-century English coach wrenches. It was widely used in the nineteenth and early twentieth centuries but is now seldom used in the mechanical trades, having been mostly replaced by the newer style of shifting (adjustable) spanner/wrench. It is still of interest as an antique among tool collectors and is still occasionally used in maintenance and repair when it happens to be convenient. The term monkey wrench is also sometimes used loosely, usually by non-tradespeople, to refer to the pipe wrench (owing to their broadly similar shapes), but tradespeople (plumbers, pipefitters) usually speak more precisely than that. A wrench with smooth jaws (no teeth) is not used for turning threaded pipe.
These are also known as a Ford wrench owing to this type of wrench being included in the tool kit supplied with every Ford Model A. They are still used by aircraft technicians, mainly when large but low torque fasteners are involved.
The World English Dictionary gives a nautical definition for monkey, as a modifier "denoting a small light structure or piece of equipment contrived to suit an immediate purpose: a monkey foresail ; a monkey bridge."[1]
Adjustable coach wrenches for the odd-sized nuts of wagon wheels were manufactured in England and exported to North America in the late eighteenth and early nineteenth centuries. They were set either by sliding a wedge, or later by twisting the handle, which turned a screw, narrowing or widening the jaws. In 1840, Worcester, Massachusetts knife manufacturer Loring Coes invented a screw-based coach wrench design in which the jaw width was set with a spinning ring fixed under the sliding lower jaw, above the handle. This was patented in 1841 and the tools were advertised and sold in the United States as monkey wrenches, a term which was already in use for the English handle-set coach wrenches.[2] For the next eighty-seven years a very wide and popular range of monkey wrenches was manufactured by Coes family partnerships, licensees and companies, which filed further wrench patents throughout the nineteenth century. Some Coes wrenches could be bought with wooden knife handles, harking back to the company's early knife making business. In 1909 the Coes Wrench Company advertised a six-foot-long "key" wrench, shaped like a monkey wrench, for use on railroads.[3][4] The Coes wrench designs were acquired by longtime toolmaker Bemis & Call of Springfield, Massachusetts in 1928. After 1939 its successor companies manufactured monkey wrenches from Coes designs until the mid-1960s, yielding a production run of over 120 years.[2][5][6]
Monkey wrenches are still manufactured and are used for some heavy tasks, but they have otherwise been mostly replaced by the shifting adjustable wrench/spanner, which is much lighter and has a smaller head, allowing it to fit more easily into tight spaces.
The following story can be found in sundry publications from the late nineteenth and early twentieth centuries:
That handy tool, the "monkey-wrench", is not so named because it is a handy thing to monkey with, or for any kindred reason. "Monkey" is not its name at all, Charles Moncky, the inventor of it, sold his patent for $5000, and invested the money in a house in Williamsburg, Kings County, where he now lives.[7][8]
Although this story was refuted by historical and patent research in the late nineteenth century,[2] it appears to have been inspired by a real person. Charles Monk (not Moncky) lived in the Williamsburg section of Brooklyn in the 1880s where he made and sold moulder's tools, not mechanics' tools like a monkey wrench.[9] He could not have invented or named the "monkey wrench" because he was born after the term, "monkey wrench", first appeared in print.[9]
Wikimedia Commons has media related to Monkey wrenches. |
This article uses material from the Wikipedia article "Monkey wrench", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
tooling,tool,drill,cam,manufacturing