powered by CADENAS

Social Share

Amazon

Caffeine (12940 views - Medicine & Health)

Caffeine is a central nervous system (CNS) stimulant of the methylxanthine class. It is the world's most widely consumed psychoactive drug. Unlike many other psychoactive substances, it is legal and unregulated in nearly all parts of the world. There are several known mechanisms of action to explain the effects of caffeine. The most prominent is that it reversibly blocks the action of adenosine on its receptor and consequently prevents the onset of drowsiness induced by adenosine. Caffeine also stimulates certain portions of the autonomic nervous system. Caffeine is a bitter, white crystalline purine, a methylxanthine alkaloid, and is chemically related to the adenine and guanine bases of deoxyribonucleic acid (DNA) and ribonucleic acid (RNA). It is found in the seeds, nuts, or leaves of a number of plants native to Africa, East Asia and South America, and helps to protect them against predator insects and to prevent germination of nearby seeds. The most well-known source of caffeine is the coffee bean, a misnomer for the seed of Coffea plants. Beverages containing caffeine are ingested to relieve or prevent drowsiness and to improve performance. To make these drinks, caffeine is extracted by steeping the plant product in water, a process called infusion. Caffeine-containing drinks, such as coffee, tea, and cola, are very popular; as of 2014, 85% of American adults consumed some form of caffeine daily, consuming 164 mg on average.Caffeine can have both positive and negative health effects. It can treat and prevent the premature infant breathing disorders bronchopulmonary dysplasia of prematurity and apnea of prematurity. Caffeine citrate is on the WHO Model List of Essential Medicines. It may confer a modest protective effect against some diseases, including Parkinson's disease. Some people experience sleep disruption or anxiety if they consume caffeine, but others show little disturbance. Evidence of a risk during pregnancy is equivocal; some authorities recommend that pregnant women limit consumption to the equivalent of two cups of coffee per day or less. Caffeine can produce a mild form of drug dependence – associated with withdrawal symptoms such as sleepiness, headache, and irritability – when an individual stops using caffeine after repeated daily intake. Tolerance to the autonomic effects of increased blood pressure and heart rate, and increased urine output, develops with chronic use (i.e., these symptoms become less pronounced or do not occur following consistent use).Caffeine is classified by the US Food and Drug Administration as generally recognized as safe (GRAS). Toxic doses, over 10 grams per day for an adult, are much higher than the typical dose of under 500 milligrams per day. A cup of coffee contains 80–175 mg of caffeine, depending on what "bean" (seed) is used and how it is prepared (e.g., drip, percolation, or espresso). Thus it requires roughly 50–100 ordinary cups of coffee to reach the toxic dose. However, pure powdered caffeine, which is available as a dietary supplement, can be lethal in tablespoon-sized amounts.
Go to Article

Explanation by Hotspot Model

Youtube


    

Caffeine

Caffeine

Caffeine

Caffeine
Clinical data
Pronunciation/kæˈfn, ˈkæfn/
SynonymsGuaranine
Methyltheobromine
1,3,7-Trimethylxanthine
Theine
AHFS/Drugs.comMonograph
Pregnancy
category
  • AU: A
  • US: C (Risk not ruled out)
Dependence
liability
Physical: low–moderate[1][2][3][4] Psychological: low[5]
Addiction
liability
Low[4] / none[1][2][3]
Routes of
administration
By mouth, insufflation, enema, rectal, intravenous
Drug classStimulant
ATC code
Legal status
Legal status
  • In general: unscheduled
Pharmacokinetic data
Bioavailability99%[7]
Protein binding25–36%[6]
MetabolismPrimary: CYP1A2[6]
Minor: CYP2E1,[6] CYP3A4,[6] CYP2C8,[6] CYP2C9[6]
MetabolitesParaxanthine (84%)
Theobromine (12%)
Theophylline (4%)
Onset of action~1 hour[7]
Elimination half-lifeAdults: 3–7 hours[6]
Infants: 65–130 hours[6]
Duration of action3–4 hours[7]
ExcretionUrine (100%)
Identifiers
CAS Number
PubChem CID
IUPHAR/BPS
DrugBank
ChemSpider
UNII
KEGG
ChEBI
ChEMBL
PDB ligand
CompTox Dashboard (EPA)
ECHA InfoCard100.000.329
Chemical and physical data
FormulaC8H10N4O2
Molar mass194.19 g/mol g·mol−1
3D model (JSmol)
Density1.23 g/cm3
Melting point235 to 238 °C (455 to 460 °F) (anhydrous)[8][9]
See also: data page

Caffeine is a central nervous system (CNS) stimulant of the methylxanthine class.[10] It is the world's most widely consumed psychoactive drug.[11] Unlike many other psychoactive substances, it is legal and unregulated in nearly all parts of the world. There are several known mechanisms of action to explain the effects of caffeine. The most prominent is that it reversibly blocks the action of adenosine on its receptor and consequently prevents the onset of drowsiness induced by adenosine. Caffeine also stimulates certain portions of the autonomic nervous system.

Caffeine is a bitter, white crystalline purine, a methylxanthine alkaloid, and is chemically related to the adenine and guanine bases of deoxyribonucleic acid (DNA) and ribonucleic acid (RNA). It is found in the seeds, nuts, or leaves of a number of plants native to Africa, East Asia and South America,[12] and helps to protect them against predator insects and to prevent germination of nearby seeds.[13] The most well-known source of caffeine is the coffee bean, a misnomer for the seed of Coffea plants. Beverages containing caffeine are ingested to relieve or prevent drowsiness and to improve performance. To make these drinks, caffeine is extracted by steeping the plant product in water, a process called infusion. Caffeine-containing drinks, such as coffee, tea, and cola, are very popular; as of 2014, 85% of American adults consumed some form of caffeine daily, consuming 164 mg on average.[14]

Caffeine can have both positive and negative health effects. It can treat and prevent the premature infant breathing disorders bronchopulmonary dysplasia of prematurity and apnea of prematurity. Caffeine citrate is on the WHO Model List of Essential Medicines.[15] It may confer a modest protective effect against some diseases,[16] including Parkinson's disease.[17] Some people experience sleep disruption or anxiety if they consume caffeine, but others show little disturbance. Evidence of a risk during pregnancy is equivocal; some authorities recommend that pregnant women limit consumption to the equivalent of two cups of coffee per day or less.[18][19] Caffeine can produce a mild form of drug dependence – associated with withdrawal symptoms such as sleepiness, headache, and irritability – when an individual stops using caffeine after repeated daily intake.[1][3][5] Tolerance to the autonomic effects of increased blood pressure and heart rate, and increased urine output, develops with chronic use (i.e., these symptoms become less pronounced or do not occur following consistent use).[20]

Caffeine is classified by the US Food and Drug Administration as generally recognized as safe (GRAS). Toxic doses, over 10 grams per day for an adult, are much higher than the typical dose of under 500 milligrams per day.[21] A cup of coffee contains 80–175 mg of caffeine, depending on what "bean" (seed) is used and how it is prepared (e.g., drip, percolation, or espresso). Thus it requires roughly 50–100 ordinary cups of coffee to reach the toxic dose. However, pure powdered caffeine, which is available as a dietary supplement, can be lethal in tablespoon-sized amounts.

Use

Medical

Caffeine is used in:

Enhancing performance

Cognitive

Caffeine is a central nervous system stimulant that reduces fatigue and drowsiness.[10] At normal doses, caffeine has variable effects on learning and memory, but it generally improves reaction time, wakefulness, concentration, and motor coordination.[35][36] The amount of caffeine needed to produce these effects varies from person to person, depending on body size and degree of tolerance.[35] The desired effects arise approximately one hour after consumption, and the desired effects of a moderate dose usually subside after about three or four hours.[7]

Caffeine can delay or prevent sleep and improves task performance during sleep deprivation.[37] Shift workers who use caffeine make fewer mistakes due to drowsiness.[38]

A systematic review and meta-analysis from 2014 found that concurrent caffeine and L-theanine use has synergistic psychoactive effects that promote alertness, attention, and task switching;[39] these effects are most pronounced during the first hour post-dose.[39]

Physical

Caffeine is a proven ergogenic aid in humans.[40] Caffeine improves athletic performance in aerobic (especially endurance sports) and anaerobic conditions.[40] Moderate doses of caffeine (around 5 mg/kg[40]) can improve sprint performance,[41] cycling and running time trial performance,[40] endurance (i.e., it delays the onset of muscle fatigue and central fatigue),[40][42][43] and cycling power output.[40] Caffeine increases basal metabolic rate in adults.[44][45][46]

Caffeine improves muscular strength and power,[47] and may enhance muscular endurance.[48] Caffeine also enhances performance on anaerobic tests.[49] Caffeine consumption before constant load exercise is associated with reduced perceived exertion. While this effect is not present during exercise-to-exhaustion exercise, performance is significantly enhanced. This is congruent with caffeine reducing perceived exertion, because exercise-to-exhaustion should end at the same point of fatigue.[50] Caffeine also improves power output and reduces time to completion in aerobic time trials,[51] an effect positively (but not exclusively) associated with longer duration exercise.[52]

Specific populations

Adults

For the general population of healthy adults, Health Canada advises a daily intake of no more than 400 mg.[53]

Children

In healthy children, caffeine intake produces effects that are "modest and typically innocuous".[54] There is no evidence that coffee stunts a child's growth.[55] For children age 12 and under, Health Canada recommends a maximum daily caffeine intake of no more than 2.5 milligrams per kilogram of body weight. Based on average body weights of children, this translates to the following age-based intake limits:[53]

Age range Maximum recommended daily caffeine intake
4–6 45 mg (slightly more than in 12 oz of a typical caffeinated soft drink)
7–9 62.5 mg
10–12 85 mg (about ½ cup of coffee)

Adolescents

Health Canada has not developed advice for adolescents because of insufficient data. However, they suggest that daily caffeine intake for this age group be no more than 2.5 mg/kg body weight. This is because the maximum adult caffeine dose may not be appropriate for light-weight adolescents or for younger adolescents who are still growing. The daily dose of 2.5 mg/kg body weight would not cause adverse health effects in the majority of adolescent caffeine consumers. This is a conservative suggestion since older and heavier weight adolescents may be able to consume adult doses of caffeine without suffering adverse effects.[53]

Pregnancy and breastfeeding

The UK Food Standards Agency has recommended that pregnant women should limit their caffeine intake, out of prudence, to less than 200 mg of caffeine a day – the equivalent of two cups of instant coffee, or one and a half to two cups of fresh coffee.[56] The American Congress of Obstetricians and Gynecologists (ACOG) concluded in 2010 that caffeine consumption is safe up to 200 mg per day in pregnant women.[19] For women who breastfeed, are pregnant, or may become pregnant, Health Canada recommends a maximum daily caffeine intake of no more than 300 mg, or a little over two 8 oz (237 mL) cups of coffee.[53]

There are conflicting reports in the scientific literature about caffeine use during pregnancy.[57] A 2011 review found that caffeine during pregnancy does not appear to increase the risk of congenital malformations, miscarriage or growth retardation even when consumed in moderate to high amounts.[58] Other reviews, however, concluded that there is some evidence that higher caffeine intake by pregnant women may be associated with a higher risk of giving birth to a low birth weight baby,[59] and may be associated with a higher risk of pregnancy loss.[60] A systematic review, analyzing the results of observational studies, suggests that women who consume large amounts of caffeine (greater than 300 mg/day) prior to becoming pregnant may have a higher risk of experiencing pregnancy loss.[61]

Adverse effects

Physical

Caffeine can increase blood pressure and cause vasoconstriction.[62][63][64] Coffee and caffeine can affect gastrointestinal motility and gastric acid secretion.[65][66][67] Caffeine in low doses may cause weak bronchodilation for up to four hours in asthmatics.[68] In postmenopausal women, high caffeine consumption can accelerate bone loss.[69][70]

Doses of caffeine equivalent to the amount normally found in standard servings of tea, coffee and carbonated soft drinks appear to have no diuretic action.[71] However, acute ingestion of caffeine in large doses (at least 250–300 mg, equivalent to the amount found in 2–3 cups of coffee or 5–8 cups of tea) results in a short-term stimulation of urine output in individuals who have been deprived of caffeine for a period of days or weeks.[71] This increase is due to both a diuresis (increase in water excretion) and a natriuresis (increase in saline excretion); it is mediated via proximal tubular adenosine receptor blockade.[72] The acute increase in urinary output may increase the risk of dehydration. However, chronic users of caffeine develop a tolerance to this effect and experience no increase in urinary output.[73][74]

Psychological

Minor undesired symptoms from caffeine ingestion not sufficiently severe to warrant a psychiatric diagnosis are common and include mild anxiety, jitteriness, insomnia, increased sleep latency, and reduced coordination.[35][75] Caffeine can have negative effects on anxiety disorders.[76] According to a 2011 literature review, caffeine use is positively associated with anxiety and panic disorders.[77] At high doses, typically greater than 300 mg, caffeine can both cause and worsen anxiety.[78] For some people, discontinuing caffeine use can significantly reduce anxiety.[79] In moderate doses, caffeine has been associated with reduced symptoms of depression and lower suicide risk.[80]

Increased consumption of coffee and caffeine is associated with a decreased risk of depression.[81][82]

Some textbooks state that caffeine is a mild euphoriant,[83][84][85] others state that it is not a euphoriant,[86][87] and one states that it is and is not a euphoriant.[88]

Caffeine-induced anxiety disorder is a subclass of the DSM-5 diagnosis of substance/medication-induced anxiety disorder.[89]

Reinforcement disorders

Addiction

Whether caffeine can result in an addictive disorder depends on how addiction is defined. Compulsive caffeine consumption under any circumstances has not been observed, and caffeine is therefore not generally considered addictive.[90] However, some diagnostic models, such as the ICDM-9 and ICD-10, include a classification of caffeine addiction under a broader diagnostic model.[91] Some state that certain users can become addicted and therefore unable to decrease use even though they know there are negative health effects.[92][93]

Caffeine does not appear to be a reinforcing stimulus, and some degree of aversion may actually occur, with people preferring placebo over caffeine in a study on drug abuse liability published in an NIDA research monograph.[94] Some state that research does not provide support for an underlying biochemical mechanism for caffeine addiction.[1][95][96][97] Other research states it can affect the reward system.[98]

"Caffeine addiction" was added to the ICDM-9 and ICD-10. However, its addition was contested with claims that this diagnostic model of caffeine addiction is not supported by evidence.[1][2][99] The American Psychiatric Association's DSM-5 does not include the diagnosis of a caffeine addiction but proposes criteria for the disorder for more study.[89][100]

Dependence and withdrawal

Withdrawal can cause mild to clinically significant distress or impairment in daily functioning. The frequency at which this occurs is self reported at 11%, but in lab tests only half of the people who report withdrawal actually experience it, casting doubt on many claims of dependence.[101] Mild physical dependence and withdrawal symptoms may occur upon abstinence, with greater than 100 mg caffeine per day, although these symptoms last no longer than a day.[1] Some symptoms associated with psychological dependence may also occur during withdrawal.[5] Caffeine dependence can involve withdrawal symptoms such as fatigue, headache, irritability, depressed mood, reduced contentedness, inability to concentrate, sleepiness or drowsiness, stomach pain, and joint pain.[1][5]

The ICD-10 includes a diagnostic model for caffeine dependence, but the DSM-5 does not.[3][99] The APA, which published the DSM-5, acknowledged that there was sufficient evidence in order to create a diagnostic model of caffeine dependence for the DSM-5, but they noted that the clinical significance of this disorder is unclear.[3] The DSM-5 instead lists "caffeine use disorder" in the emerging models section of the manual.[3]

Tolerance to the effects of caffeine occurs for caffeine induced elevations in blood pressure and the subjective feelings of nervousness. Sensitization, the process whereby effects become more prominent with use, occurs for positive effects such as feelings of alertness and well being.[101] Tolerance varies for daily, regular caffeine users and high caffeine users. High doses of caffeine (750 to 1200 mg/day spread throughout the day) have been shown to produce complete tolerance to some, but not all of the effects of caffeine. Doses as low as 100 mg/day, such as a 6 oz cup of coffee or two to three 12 oz servings of caffeinated soft-drink, may continue to cause sleep disruption, among other intolerances. Non-regular caffeine users have the least caffeine tolerance for sleep disruption.[102] Some coffee drinkers develop tolerance to its undesired sleep-disrupting effects, but others apparently do not.[103]

Risk of other diseases

A protective effect of caffeine against Alzheimer's disease and dementia is possible but the evidence is inconclusive.[104][105][106] It may protect people from liver cirrhosis.[107] Caffeine may lessen the severity of acute mountain sickness if taken a few hours prior to attaining a high altitude.[108] One meta analysis has found that caffeine consumption is associated with a reduced risk of type 2 diabetes.[109] Two meta analyses have reported that caffeine consumption is associated with a linear reduction in risk for Parkinson's disease.[110][17] Caffeine consumption may be associated with reduced risk of depression,[81] although conflicting results have been reported.[82]

Caffeine increases intraocular pressure in those with glaucoma but does not appear to affect normal individuals.[111]

Overdose

Consumption of 1–1.5 grams (1,000–1,500 mg) per day is associated with a condition known as caffeinism.[113] Caffeinism usually combines caffeine dependency with a wide range of unpleasant symptoms including nervousness, irritability, restlessness, insomnia, headaches, and palpitations after caffeine use.[114]

Caffeine overdose can result in a state of central nervous system over-stimulation called caffeine intoxication (DSM-IV 305.90).[115] This syndrome typically occurs only after ingestion of large amounts of caffeine, well over the amounts found in typical caffeinated beverages and caffeine tablets (e.g., more than 400–500 mg at a time). The symptoms of caffeine intoxication are comparable to the symptoms of overdoses of other stimulants: they may include restlessness, fidgeting, anxiety, excitement, insomnia, flushing of the face, increased urination, gastrointestinal disturbance, muscle twitching, a rambling flow of thought and speech, irritability, irregular or rapid heart beat, and psychomotor agitation.[112] In cases of much larger overdoses, mania, depression, lapses in judgment, disorientation, disinhibition, delusions, hallucinations, or psychosis may occur, and rhabdomyolysis (breakdown of skeletal muscle tissue) can be provoked.[116][117]

Massive overdose can result in death.[118][119] The LD50 of caffeine in humans is dependent on individual sensitivity, but is estimated to be 150–200 milligrams per kilogram of body mass (75–100 cups of coffee for a 70 kilogram adult).[120][failed verification] A number of fatalities have been caused by overdoses of readily available powdered caffeine supplements, for which the estimated lethal amount is less than a tablespoon.[121] The lethal dose is lower in individuals whose ability to metabolize caffeine is impaired due to genetics or chronic liver disease.[122] A death was reported in a man with liver cirrhosis who overdosed on caffeinated mints.[123][124][125]

Treatment of mild caffeine intoxication is directed toward symptom relief; severe intoxication may require peritoneal dialysis, hemodialysis, or hemofiltration.[112]

Interactions

Caffeine is a substrate for CYP1A2, and interacts with many substances through this and other mechanisms.[126]

Alcohol

According to DSST, alcohol provides a reduction in performance and caffeine has a significant improvement in performance.[127] When alcohol and caffeine are consumed jointly, the effects produced by caffeine are affected, but the alcohol effects remain the same.[128] For example, when additional caffeine is added, the drug effect produced by alcohol is not reduced.[128] However, the jitteriness and alertness given by caffeine is decreased when additional alcohol is consumed.[128] Alcohol consumption alone reduces both inhibitory and activational aspects of behavioral control. Caffeine antagonizes the activational aspect of behavioral control, but has no effect on the inhibitory behavioral control.[129] The Dietary Guidelines for Americans recommend avoidance of concomitant consumption of alcohol and caffeine, as this may lead to increased alcohol consumption, with a higher risk of alcohol-associated injury.

Tobacco

Smoking tobacco increases caffeine clearance by 56%.[130]

Birth control

Birth control pills can extend the half-life of caffeine, requiring greater attention to caffeine consumption.[131]

Medications

Caffeine sometimes increases the effectiveness of some medications, such as those for headaches.[132] Caffeine was determined to increase the potency of some over-the-counter analgesic medications by 40%.[133]

The pharmacological effects of adenosine may be blunted in individuals taking large quantities of methylxanthines like caffeine.[134]

Pharmacology

Pharmacodynamics

Structure of a typical chemical synapse

In the absence of caffeine and when a person is awake and alert, little adenosine is present in (CNS) neurons. With a continued wakeful state, over time adenosine accumulates in the neuronal synapse, in turn binding to and activating adenosine receptors found on certain CNS neurons; when activated, these receptors produce a cellular response that ultimately increases drowsiness. When caffeine is consumed, it antagonizes adenosine receptors; in other words, caffeine prevents adenosine from activating the receptor by blocking the location on the receptor where adenosine binds to it. As a result, caffeine temporarily prevents or relieves drowsiness, and thus maintains or restores alertness.[6]

Receptor and ion channel targets

Caffeine is an antagonist at all four adenosine receptor subtypes (A1, A2A, A2B, and A3), although with varying potencies.[6][135] The affinity (KD) values of caffeine for the human adenosine receptors are 12 μM at A1, 2.4 μM at A2A, 13 μM at A2B, and 80 μM at A3.[135] Knockout mouse studies have specifically implicated antagonism of the A2A receptor as responsible for the wakefulness-promoting effects of caffeine.[135] Antagonism of adenosine receptors by caffeine stimulates the medullary vagal, vasomotor, and respiratory centers, which increases respiratory rate, reduces heart rate, and constricts blood vessels.[6] Adenosine receptor antagonism also promotes neurotransmitter release (e.g., monoamines and acetylcholine), which endows caffeine with its stimulant effects;[6][136] adenosine acts as an inhibitory neurotransmitter that suppresses activity in the central nervous system. Heart palpitations are caused by blockade of the A1 receptor.[6]

Because caffeine is both water- and lipid-soluble, it readily crosses the blood–brain barrier that separates the bloodstream from the interior of the brain. Once in the brain, the principal mode of action is as a nonselective antagonist of adenosine receptors (in other words, an agent that reduces the effects of adenosine). The caffeine molecule is structurally similar to adenosine, and is capable of binding to adenosine receptors on the surface of cells without activating them, thereby acting as a competitive antagonist.[137]

In addition to its activity at adenosine receptors, caffeine is an inositol trisphosphate receptor 1 antagonist and a voltage-independent activator of the ryanodine receptors (RYR1, RYR2, and RYR3).[138] It is also a competitive antagonist of the ionotropic glycine receptor.[139]

Effects on striatal dopamine

While caffeine does not directly bind to any dopamine receptors, it influences the binding activity of dopamine at its receptors in the striatum by binding to adenosine receptors that have formed GPCR heteromers with dopamine receptors, specifically the A1D1 receptor heterodimer (this is a receptor complex with 1 adenosine A1 receptor and 1 dopamine D1 receptor) and the A2AD2 receptor heterotetramer (this is a receptor complex with 2 adenosine A2A receptors and 2 dopamine D2 receptors).[140][141][142][143] The A2A–D2 receptor heterotetramer has been identified as a primary pharmacological target of caffeine, primarily because it mediates some of its psychostimulant effects and its pharmacodynamic interactions with dopaminergic psychostimulants.[141][142][143]

Caffeine also causes the release of dopamine in the dorsal striatum and nucleus accumbens core (a substructure within the ventral striatum), but not the nucleus accumbens shell, by antagonizing A1 receptors in the axon terminal of dopamine neurons and A1A2A heterodimers (a receptor complex composed of 1 adenosine A1 receptor and 1 adenosine A2A receptor) in the axon terminal of glutamate neurons.[140][144] During chronic caffeine use, caffeine-induced dopamine release within the nucleus accumbens core is markedly reduced due to drug tolerance.[140][144]

Enzyme targets

Caffeine, like other xanthines, also acts as a phosphodiesterase inhibitor.[145] As a competitive nonselective phosphodiesterase inhibitor,[146] caffeine raises intracellular cAMP, activates protein kinase A, inhibits TNF-alpha[147][148] and leukotriene[149] synthesis, and reduces inflammation and innate immunity.[149] Caffeine also affects the cholinergic system where it inhibits the enzyme acetylcholinesterase.

Off-target effects

Caffeine antagonizes adenosine A2A receptors in the ventrolateral preoptic area (VLPO), thereby reducing inhibitory GABA neurotransmission to the tuberomammillary nucleus, a histaminergic projection nucleus that activation-dependently promotes arousal.[144] Disinhibition of the tuberomammillary nucleus is the chief mechanism by which caffeine produces wakefulness-promoting effects.[144]

Pharmacokinetics

Caffeine from coffee or other beverages is absorbed by the small intestine within 45 minutes of ingestion and distributed throughout all bodily tissues.[151] Peak blood concentration is reached within 1–2 hours.[152] It is eliminated by first-order kinetics.[153] Caffeine can also be absorbed rectally, evidenced by suppositories of ergotamine tartrate and caffeine (for the relief of migraine)[154] and chlorobutanol and caffeine (for the treatment of hyperemesis).[155] However, rectal absorption is less efficient than oral: the maximum concentration (Cmax) and total amount absorbed (AUC) are both about 30% (i.e., 1/3.5) of the oral amounts.[156]

Caffeine's biological half-life – the time required for the body to eliminate one-half of a dose – varies widely among individuals according to factors such as pregnancy, other drugs, liver enzyme function level (needed for caffeine metabolism) and age. In healthy adults, caffeine's half-life is between 3 and 7 hours.[6] Smoking decreases the half-life by 30–50%,[103] while oral contraceptives can double it[103] and pregnancy can raise it to as much as 15 hours during the third trimester.[103] In newborns the half-life can be 80 hours or more, dropping very rapidly with age, possibly to less than the adult value by age 6 months.[103] The antidepressant fluvoxamine (Luvox) reduces the clearance of caffeine by more than 90%, and increases its elimination half-life more than tenfold; from 4.9 hours to 56 hours.[157]

Caffeine is metabolized in the liver by the cytochrome P450 oxidase enzyme system, in particular, by the CYP1A2 isozyme, into three dimethylxanthines,[158] each of which has its own effects on the body:

1,3,7-Trimethyluric acid is a minor caffeine metabolite.[6] Each of these metabolites is further metabolized and then excreted in the urine. Caffeine can accumulate in individuals with severe liver disease, increasing its half-life.[159]

A 2011 review found that increased caffeine intake was associated with a variation in two genes that increase the rate of caffeine catabolism. Subjects who had this mutation on both chromosomes consumed 40 mg more caffeine per day than others.[160] This is presumably due to the need for a higher intake to achieve a comparable desired effect, not that the gene led to a disposition for greater incentive of habituation.

Chemistry

Pure anhydrous caffeine is a bitter-tasting, white, odorless powder with a melting point of 235–238 °C.[8][9] Caffeine is moderately soluble in water at room temperature (2 g/100 mL), but very soluble in boiling water (66 g/100 mL).[161] It is also moderately soluble in ethanol (1.5 g/100 mL).[161] It is weakly basic (pKa of conjugate acid = ~0.6) requiring strong acid to protonate it.[162] Caffeine does not contain any stereogenic centers[163] and hence is classified as an achiral molecule.[164]

The xanthine core of caffeine contains two fused rings, a pyrimidinedione and imidazole. The pyrimidinedione in turn contains two amide functional groups that exist predominantly in a zwitterionic resonance the location from which the nitrogen atoms are double bonded to their adjacent amide carbons atoms. Hence all six of the atoms within the pyrimidinedione ring system are sp2 hybridized and planar. Therefore, the fused 5,6 ring core of caffeine contains a total of ten pi electrons and hence according to Hückel's rule is aromatic.[165]

Synthesis

The biosynthesis of caffeine is an example of convergent evolution among different species.[170][171][172]

Caffeine may be synthesized in the lab starting with dimethylurea and malonic acid.[clarification needed][168][169][173]

Commercial supplies of caffeine are not usually manufactured synthetically because the chemical is readily available as a byproduct of decaffeination.[174]

Decaffeination

Extraction of caffeine from coffee, to produce caffeine and decaffeinated coffee, can be performed using a number of solvents. Benzene, chloroform, trichloroethylene, and dichloromethane have all been used over the years but for reasons of safety, environmental impact, cost, and flavor, they have been superseded by the following main methods:

  • Water extraction: Coffee beans are soaked in water. The water, which contains many other compounds in addition to caffeine and contributes to the flavor of coffee, is then passed through activated charcoal, which removes the caffeine. The water can then be put back with the beans and evaporated dry, leaving decaffeinated coffee with its original flavor. Coffee manufacturers recover the caffeine and resell it for use in soft drinks and over-the-counter caffeine tablets.[175]
  • Supercritical carbon dioxide extraction: Supercritical carbon dioxide is an excellent nonpolar solvent for caffeine, and is safer than the organic solvents that are otherwise used. The extraction process is simple: CO
    2
    is forced through the green coffee beans at temperatures above 31.1 °C and pressures above 73 atm. Under these conditions, CO
    2
    is in a "supercritical" state: It has gaslike properties that allow it to penetrate deep into the beans but also liquid-like properties that dissolve 97–99% of the caffeine. The caffeine-laden CO
    2
    is then sprayed with high-pressure water to remove the caffeine. The caffeine can then be isolated by charcoal adsorption (as above) or by distillation, recrystallization, or reverse osmosis.[175]
  • Extraction by organic solvents: Certain organic solvents such as ethyl acetate present much less health and environmental hazard than chlorinated and aromatic organic solvents used formerly. Another method is to use triglyceride oils obtained from spent coffee grounds.[175]

"Decaffeinated" coffees do in fact contain caffeine in many cases – some commercially available decaffeinated coffee products contain considerable levels. One study found that decaffeinated coffee contained 10 mg of caffeine per cup, compared to approximately 85 mg of caffeine per cup for regular coffee.[176]

Detection in body fluids

Caffeine can be quantified in blood, plasma, or serum to monitor therapy in neonates, confirm a diagnosis of poisoning, or facilitate a medicolegal death investigation. Plasma caffeine levels are usually in the range of 2–10 mg/L in coffee drinkers, 12–36 mg/L in neonates receiving treatment for apnea, and 40–400 mg/L in victims of acute overdosage. Urinary caffeine concentration is frequently measured in competitive sports programs, for which a level in excess of 15 mg/L is usually considered to represent abuse.[177]

Analogs

Some analog substances have been created which mimic caffeine's properties with either function or structure or both. Of the latter group are the xanthines DMPX[178] and 8-chlorotheophylline, which is an ingredient in dramamine. Members of a class of nitrogen substituted xanthines are often proposed as potential alternatives to caffeine.[179][unreliable source?] Many other xanthine analogues constituting the adenosine receptor antagonist class have also been elucidated.[180]

Some other caffeine analogs:

Precipitation of tannins

Caffeine, as do other alkaloids such as cinchonine, quinine or strychnine, precipitates polyphenols and tannins. This property can be used in a quantitation method.[181]

Natural occurrence

Around sixty plant species are known to contain caffeine.[182] Common sources are the "beans" (seeds) of the two cultivated coffee plants, Coffea arabica and Coffea canephora (the quantity varies, but 1.3% is a typical value); in the leaves of the tea plant; and in kola nuts. Other sources include yaupon holly leaves, South American holly yerba mate leaves, seeds from Amazonian maple guarana berries, and Amazonian holly guayusa leaves. Temperate climates around the world have produced unrelated caffeine-containing plants.

Caffeine in plants acts as a natural pesticide: it can paralyze and kill predator insects feeding on the plant.[183] High caffeine levels are found in coffee seedlings when they are developing foliage and lack mechanical protection.[184] In addition, high caffeine levels are found in the surrounding soil of coffee seedlings, which inhibits seed germination of nearby coffee seedlings, thus giving seedlings with the highest caffeine levels fewer competitors for existing resources for survival.[185] Caffeine is stored in tea leaves in two places. Firstly, in the cell vacuoles where it is complexed with polyphenols. This caffeine probably is released into the mouth parts of insects, to discourage herbivory. Secondly, around the vascular bundles, where it probably inhibits pathogenic fungi from entering and colonizing the vascular bundles.[186] Caffeine in nectar may improve the reproductive success of the pollen producing plants by enhancing the reward memory of pollinators such as honey bees.[187]

The differing perceptions in the effects of ingesting beverages made from various plants containing caffeine could be explained by the fact that these beverages also contain varying mixtures of other methylxanthine alkaloids, including the cardiac stimulants theophylline and theobromine, and polyphenols that can form insoluble complexes with caffeine.[188]

Products

Caffeine content in select food and drugs[189][190][191][192][193]
Product Serving size Caffeine per serving (mg) Caffeine (mg/L)
Caffeine tablet (regular-strength) 1 tablet 100
Caffeine tablet (extra-strength) 1 tablet 200
Excedrin tablet 1 tablet 65
Hershey's Special Dark (45% cacao content) 1 bar (43 g or 1.5 oz) 31
Hershey's Milk Chocolate (11% cacao content) 1 bar (43 g or 1.5 oz) 10
Percolated coffee 207 mL (7.0 US fl oz) 80–135 386–652
Drip coffee 207 mL (7.0 US fl oz) 115–175 555–845
Coffee, decaffeinated 207 mL (7.0 US fl oz) 5–15 24–72
Coffee, espresso 44–60 mL (1.5–2.0 US fl oz) 100 1,691–2,254
Tea – black, green, and other types, – steeped for 3 min. 177 millilitres (6.0 US fl oz) 22–74[192][193] 124–418
Guayakí yerba mate (loose leaf) 6 g (0.21 oz) 85[194] approx. 358
Coca-Cola 355 mL (12.0 US fl oz) 34 96
Mountain Dew 355 mL (12.0 US fl oz) 54 154
Pepsi Zero Sugar 355 mL (12.0 US fl oz) 69 194
Guaraná Antarctica 350 mL (12 US fl oz) 30 100
Jolt Cola 695 mL (23.5 US fl oz) 280 403
Red Bull 250 mL (8.5 US fl oz) 80 320

Products containing caffeine are coffee, tea, soft drinks ("colas"), energy drinks, other beverages, chocolate,[195] caffeine tablets, other oral products, and inhalation products.

Beverages

Coffee

The world's primary source of caffeine is the coffee "bean" (the seed of the coffee plant), from which coffee is brewed. Caffeine content in coffee varies widely depending on the type of coffee bean and the method of preparation used;[196] even beans within a given bush can show variations in concentration. In general, one serving of coffee ranges from 80 to 100 milligrams, for a single shot (30 milliliters) of arabica-variety espresso, to approximately 100–125 milligrams for a cup (120 milliliters) of drip coffee.[197][198] Arabica coffee typically contains half the caffeine of the robusta variety.[196] In general, dark-roast coffee has very slightly less caffeine than lighter roasts because the roasting process reduces caffeine content of the bean by a small amount.[197][198]

Tea

Tea contains more caffeine than coffee by dry weight. A typical serving, however, contains much less, since less of the product is used as compared to an equivalent serving of coffee. Also contributing to caffeine content are growing conditions, processing techniques, and other variables. Thus, teas contain varying amounts of caffeine.[199]

Tea contains small amounts of theobromine and slightly higher levels of theophylline than coffee. Preparation and many other factors have a significant impact on tea, and color is a very poor indicator of caffeine content. Teas like the pale Japanese green tea, gyokuro, for example, contain far more caffeine than much darker teas like lapsang souchong, which has very little.[199]

Soft drinks and energy drinks

Caffeine is also a common ingredient of soft drinks, such as cola, originally prepared from kola nuts. Soft drinks typically contain 0 to 55 milligrams of caffeine per 12 ounce serving.[200] By contrast, energy drinks, such as Red Bull, can start at 80 milligrams of caffeine per serving. The caffeine in these drinks either originates from the ingredients used or is an additive derived from the product of decaffeination or from chemical synthesis. Guarana, a prime ingredient of energy drinks, contains large amounts of caffeine with small amounts of theobromine and theophylline in a naturally occurring slow-release excipient.[201]

Other beverages

  • Mate is a drink popular in many parts of South America. Its preparation consists of filling a gourd with the leaves of the South American holly yerba mate, pouring hot but not boiling water over the leaves, and drinking with a straw, the bombilla, which acts as a filter so as to draw only the liquid and not the yerba leaves.[202]
  • Guaraná is a soft drink originating in Brazil made from the seeds of the Guaraná fruit.
  • The leaves of Ilex guayusa, the Ecuadorian holly tree, are placed in boiling water to make a guayusa tea.[203]

Chocolate

Chocolate derived from cocoa beans contains a small amount of caffeine. The weak stimulant effect of chocolate may be due to a combination of theobromine and theophylline, as well as caffeine.[204] A typical 28-gram serving of a milk chocolate bar has about as much caffeine as a cup of decaffeinated coffee. By weight, dark chocolate has one to two times the amount of caffeine as coffee: 80–160 mg per 100 g. Higher percentages of cocoa such as 90% amount to 200 mg per 100 g approximately and thus, a 100-gram 85% cocoa chocolate bar contains about 195 mg caffeine.[190]

Tablets

Tablets offer several advantages over coffee, tea, and other caffeinated beverages, including convenience, known dosage, and avoidance of concomitant intake of sugar, acids, and fluids. Manufacturers of caffeine tablets claim that using caffeine of pharmaceutical quality improves mental alertness.[citation needed] These tablets are commonly used by students studying for their exams and by people who work or drive for long hours.[205]

Other oral products

One U.S. company is marketing oral dissolvable caffeine strips.[206] Another intake route is SpazzStick, a caffeinated lip balm.[207] Alert Energy Caffeine Gum was introduced in the United States in 2013, but was voluntarily withdrawn after an announcement of an investigation by the FDA of the health effects of added caffeine in foods.[208]

Inhalants

There are several products being marketed that offer inhalers that deliver proprietary blends of supplements, with caffeine being a key ingredient.[209] In 2012, the FDA sent a warning letter to one of the companies marketing these inhalers, expressing concerns for the lack of safety information available about inhaled caffeine.[210]

Combinations with other drugs

History

Discovery and spread of use

According to Chinese legend, the Chinese emperor Shennong, reputed to have reigned in about 3000 BCE, inadvertently discovered tea when he noted that when certain leaves fell into boiling water, a fragrant and restorative drink resulted.[212] Shennong is also mentioned in Lu Yu's Cha Jing, a famous early work on the subject of tea.[213]

The earliest credible evidence of either coffee drinking or knowledge of the coffee plant appears in the middle of the fifteenth century, in the Sufi monasteries of the Yemen in southern Arabia.[214] From Mocha, coffee spread to Egypt and North Africa, and by the 16th century, it had reached the rest of the Middle East, Persia and Turkey. From the Middle East, coffee drinking spread to Italy, then to the rest of Europe, and coffee plants were transported by the Dutch to the East Indies and to the Americas.[215]

Kola nut use appears to have ancient origins. It is chewed in many West African cultures, in both private and social settings, to restore vitality and ease hunger pangs.

The earliest evidence of cocoa bean use comes from residue found in an ancient Mayan pot dated to 600 BCE. Also, chocolate was consumed in a bitter and spicy drink called xocolatl, often seasoned with vanilla, chile pepper, and achiote. Xocolatl was believed to fight fatigue, a belief probably attributable to the theobromine and caffeine content. Chocolate was an important luxury good throughout pre-Columbian Mesoamerica, and cocoa beans were often used as currency.[citation needed]

Xocolatl was introduced to Europe by the Spaniards, and became a popular beverage by 1700. The Spaniards also introduced the cacao tree into the West Indies and the Philippines. It was used in alchemical processes, where it was known as "black bean".[citation needed]

The leaves and stems of the yaupon holly (Ilex vomitoria) were used by Native Americans to brew a tea called asi or the "black drink".[216] Archaeologists have found evidence of this use far into antiquity,[217] possibly dating to Late Archaic times.[216]

Chemical identification, isolation, and synthesis

In 1819, the German chemist Friedlieb Ferdinand Runge isolated relatively pure caffeine for the first time; he called it "Kaffebase" (i.e., a base that exists in coffee).[218] According to Runge, he did this at the behest of Johann Wolfgang von Goethe.[a][220] In 1821, caffeine was isolated both by the French chemist Pierre Jean Robiquet and by another pair of French chemists, Pierre-Joseph Pelletier and Joseph Bienaimé Caventou, according to Swedish chemist Jöns Jacob Berzelius in his yearly journal. Furthermore, Berzelius stated that the French chemists had made their discoveries independently of any knowledge of Runge's or each other's work.[221] However, Berzelius later acknowledged Runge's priority in the extraction of caffeine, stating:[222] "However, at this point, it should not remain unmentioned that Runge (in his Phytochemical Discoveries, 1820, pages 146–147) specified the same method and described caffeine under the name Caffeebase a year earlier than Robiquet, to whom the discovery of this substance is usually attributed, having made the first oral announcement about it at a meeting of the Pharmacy Society in Paris."

Pelletier's article on caffeine was the first to use the term in print (in the French form Caféine from the French word for coffee: café).[223] It corroborates Berzelius's account:

Caffeine, noun (feminine). Crystallizable substance discovered in coffee in 1821 by Mr. Robiquet. During the same period – while they were searching for quinine in coffee because coffee is considered by several doctors to be a medicine that reduces fevers and because coffee belongs to the same family as the cinchona [quinine] tree – on their part, Messrs. Pelletier and Caventou obtained caffeine; but because their research had a different goal and because their research had not been finished, they left priority on this subject to Mr. Robiquet. We do not know why Mr. Robiquet has not published the analysis of coffee which he read to the Pharmacy Society. Its publication would have allowed us to make caffeine better known and give us accurate ideas of coffee's composition ...

Robiquet was one of the first to isolate and describe the properties of pure caffeine,[224] whereas Pelletier was the first to perform an elemental analysis.[225]

In 1827, M. Oudry isolated "théine" from tea,[226] but in 1838 it was proved by Mulder[227] and by Carl Jobst[228] that theine was actually the same as caffeine.

In 1895, German chemist Hermann Emil Fischer (1852–1919) first synthesized caffeine from its chemical components (i.e. a "total synthesis"), and two years later, he also derived the structural formula of the compound.[229] This was part of the work for which Fischer was awarded the Nobel Prize in 1902.[230]

Historic regulations

Because it was recognized that coffee contained some compound that acted as a stimulant, first coffee and later also caffeine has sometimes been subject to regulation. For example, in the 16th century Islamists in Mecca and in the Ottoman Empire made coffee illegal for some classes.[231][232][233] Charles II of England tried to ban it in 1676,[234][235] Frederick II of Prussia banned it in 1777,[236][237] and coffee was banned in Sweden at various times between 1756 and 1823.

In 1911, caffeine became the focus of one of the earliest documented health scares, when the US government seized 40 barrels and 20 kegs of Coca-Cola syrup in Chattanooga, Tennessee, alleging the caffeine in its drink was "injurious to health".[238] Although the judge ruled in favor of Coca-Cola, two bills were introduced to the U.S. House of Representatives in 1912 to amend the Pure Food and Drug Act, adding caffeine to the list of "habit-forming" and "deleterious" substances, which must be listed on a product's label.[239]

Society and culture

Regulations

The Food and Drug Administration (FDA) in the United States currently allows only beverages containing less than 0.02% caffeine;[240] but caffeine powder, which is sold as a dietary supplement, is unregulated.[241] It is a regulatory requirement that the label of most prepackaged foods must declare a list of ingredients, including food additives such as caffeine, in descending order of proportion. However, there is no regulatory provision for mandatory quantitative labeling of caffeine, (e.g., milligrams caffeine per stated serving size). There are a number of food ingredients that naturally contain caffeine. These ingredients must appear in food ingredient lists. However, as is the case for "food additive caffeine", there is no requirement to identify the quantitative amount of caffeine in composite foods containing ingredients that are natural sources of caffeine. While coffee or chocolate are broadly recognized as caffeine sources, some ingredients (e.g., guarana, yerba maté) are likely less recognized as caffeine sources. For these natural sources of caffeine, there is no regulatory provision requiring that a food label identify the presence of caffeine nor state the amount of caffeine present in the food.[242]

Consumption

Global consumption of caffeine has been estimated at 120,000 tonnes per year, making it the world's most popular psychoactive substance.[11] This amounts to one serving of a caffeinated beverage for every person every day.[11]

Religions

Some Church of God (Restoration) adherents, and Christian Scientists do not consume caffeine.[citation needed] Until recently, the Seventh-day Adventist Church asked for its members to "abstain from caffeinated drinks", but has removed this from baptismal vows (while still recommending abstention as policy).[243] Some from these religions believe that one is not supposed to consume a non-medical, psychoactive substance, or believe that one is not supposed to consume a substance that is addictive. The Church of Jesus Christ of Latter-day Saints has said the following with regard to caffeinated beverages: " . . . the Church revelation spelling out health practices (Doctrine and Covenants 89) does not mention the use of caffeine. The Church's health guidelines prohibit alcoholic drinks, smoking or chewing of tobacco, and 'hot drinks' – taught by Church leaders to refer specifically to tea and coffee."[244]

Gaudiya Vaishnavas generally also abstain from caffeine, because they believe it clouds the mind and over-stimulates the senses.[245] To be initiated under a guru, one must have had no caffeine, alcohol, nicotine or other drugs, for at least a year.[246]

Caffeinated beverages are widely consumed by Muslims today. In the 16th century, some Muslim authorities made unsuccessful attempts to ban them as forbidden "intoxicating beverages" under Islamic dietary laws.[247][248]

Other organisms

Recently discovered bacteria Pseudomonas putida CBB5 can live on pure caffeine and can cleave caffeine into carbon dioxide and ammonia.[249]

Caffeine is toxic to birds[250] and to dogs and cats,[251] and has a pronounced adverse effect on mollusks, various insects, and spiders.[252] This is at least partly due to a poor ability to metabolize the compound, causing higher levels for a given dose per unit weight.[150] Caffeine has also been found to enhance the reward memory of honey bees.[187]

Research

Caffeine has been used to double chromosomes in haploid wheat.[253]

See also



This article uses material from the Wikipedia article "Caffeine", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Medicine & Health

3D,virus,bacteria,medicine, molecule,atom,chemistry,labor