Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution 2.0 (Jonut).
A journalist is a person who collects, writes, or distributes news or other current information to the public. A journalist's work is called journalism. A journalist can work with general issues or specialize in certain issues. However, most journalists tend to specialize, and by cooperating with other journalists, produce journals that span many topics.[1] For example, a sports journalist covers news within the world of sports, but this journalist may be a part of a newspaper that covers many different topics.
A reporter is a type of journalist who researches, writes, and reports on information in order to present in sources, conduct interviews, engage in research, and make reports. The information-gathering part of a journalist's job is sometimes called reporting, in contrast to the production part of the job such as writing articles. Reporters may split their time between working in a newsroom and going out to witness events or interviewing people. Reporters may be assigned a specific beat or area of coverage.
Depending on the context, the term journalist may include various types of editors, editorial writers, columnists, and visual journalists, such as photojournalists (journalists who use the medium of photography).
Journalism has developed a variety of ethics and standards. While objectivity and a lack of bias are of primary concern and importance, more liberal types of journalism, such as advocacy journalism and activism, intentionally adopt a non-objective viewpoint. This has become more prevalent with the advent of social media and blogs, as well as other platforms that are used to manipulate or sway social and political opinions and policies. These platforms often project extreme bias, as "sources" are not always held accountable or considered necessary in order to produce a written, televised, or otherwise "published" end product.
Matthew C. Nisbet, who has written on science communication,[2] has defined a "knowledge journalist" as a public intellectual who, like Walter Lippmann, David Brooks, Fareed Zakaria, Naomi Klein, Michael Pollan, Thomas Friedman, and Andrew Revkin, sees their role as researching complicated issues of fact or science which most laymen would not have the time or access to information to research themselves, then communicating an accurate and understandable version to the public as a teacher and policy advisor.
In his best-known books, Public Opinion (1922) and The Phantom Public (1925), Lippmann argued that most individuals lacked the capacity, time, and motivation to follow and analyze news of the many complex policy questions that troubled society. Nor did they often directly experience most social problems, or have direct access to expert insights. These limitations were made worse by a news media that tended to over-simplify issues and to reinforce stereotypes, partisan viewpoints, and prejudices. As a consequence, Lippmann believed that the public needed journalists like himself who could serve as expert analysts, guiding “citizens to a deeper understanding of what was really important.”[3]
In 2018, the United States Department of Labor's Occupational Outlook Handbook reported that employment for the category, "reporters, correspondents and broadcast news analysts," will decline 9 percent between 2016 and 2026.[4]
Journalists sometimes expose themselves to danger, particularly when reporting in areas of armed conflict or in states that do not respect the freedom of the press. Organizations such as the Committee to Protect Journalists and Reporters Without Borders publish reports on press freedom and advocate for journalistic freedom. As of November 2011, the Committee to Protect Journalists reports that 887 journalists have been killed worldwide since 1992 by murder (71%), crossfire or combat (17%), or on dangerous assignment (11%). The "ten deadliest countries" for journalists since 1992 have been Iraq (230 deaths), Philippines (109), Russia (77), Colombia (76), Mexico (69), Algeria (61), Pakistan (59), India (49), Somalia (45), Brazil (31) and Sri Lanka (30).[5]
The Committee to Protect Journalists also reports that as of December 1, 2010, 145 journalists were jailed worldwide for journalistic activities. Current numbers are even higher. The ten countries with the largest number of currently-imprisoned journalists are Turkey (95),[6] China (34), Iran (34), Eritrea (17), Burma (13), Uzbekistan (6), Vietnam (5), Cuba (4), Ethiopia (4), and Sudan (3).[7]
Apart from the physical harm, journalists are harmed psychologically. This applies especially to war reporters, but their editorial offices at home often do not know how to deal appropriately with the reporters they expose to danger. Hence, a systematic and sustainable way of psychological support for traumatized journalists is strongly needed. However, only little and fragmented support programs exist so far.[8]
The Newseum in Washington, D.C. is home to the Journalists Memorial, which lists the names of over 2,100 journalists from around the world who were killed in the line of duty.
The relationship between a professional journalist and a source can be rather complex, and a source can sometimes impact the direction of the article written by the journalist. The article 'A Compromised Fourth Estate' uses Herbert Gans' metaphor to capture their relationship. He uses a dance metaphor 'The Tango' to illustrate the co-operative nature of their interactions "It takes two to tango". Herbert suggests that the source often leads but journalists commonly object to this notion for two reasons:
This dance metaphor helps showcase consensus within the relationship but the article fully describe the common relation between the two "A relationship with sources that is too cozy is potentially compromising of journalists’ integrity and risks becoming collusive. Journalists have typically favored a more robust, conflict model, based on a crucial assumption that if the media are to function as watchdogs of powerful economic and political interests, journalists must establish their independence of sources or risk the fourth estate being driven by the fifth estate of public relations".[9]
According to Reporters Without Borders' annual report, the year 2018 was the worst year on record for deadly violence and abuse toward journalists; there was a 15 per cent increase in such killings since 2017.[10][11] Ruben Pat was gunned down outside a Mexican beach bar. Yaser Murtaja was shot by an Israeli army sniper. Bulgarian Viktoria Marinova was beaten, raped and strangled. A car bomb killed Malta's Daphne Caruana Galizia. Jamal Khashoggi was killed inside Saudi Arabia's consulate in Istanbul on Oct 2.[12]
a reporter for Radio Azadi interviews a citizen in Helmand Province, Afghanistan, 2009.
Journalist interviews a cosplayer, 2012.
A reporter interviewing Boris Johnson when he was Mayor of London, 2014
Official tastes the water of a new well in front of journalists in Mogadishu, Somalia, 2014.
This article uses material from the Wikipedia article "Journalist", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
eclass, ecl@ss, cobie,cibse, unspsc, ominclass, uniclass, taric number